''' Validation : AFE79xx Library Version v1.67, v1.74 Case RX TX FB CLK Notes ---- ----------------- ----------------- ----------------- ----------- ------------ 1 245.76Msps, 24410 491.52Msps, 44210 491.52Msps, 22210 FADC=2949.12M DAC in interleaved mode SerDes=9830.4Mbps SerDes=9830.4Mbps SerDes=9830.4Mbps FDAC=8847.36M PLL0, NCO=3500M PLL0, NCO=3500M NCO=3500M REF=491.52M 2 245.76Msps, 24410 491.52Msps, 44210 491.52Msps, 22210 FADC=2949.12M DAC in straight mode SerDes=9830.4Mbps SerDes=9830.4Mbps SerDes=9830.4Mbps FDAC=8847.36M PLL0, NCO=3500M PLL0, NCO=3500M NCO=3500M REF=491.52M ''' setupParams.skipFpga = 1 sysParams = AFE.systemParams setupParams.fpgaRefClk = 122.880 #"clock the FPGA desired, transceiver clock //should be a multiple of 30.72 AFE.systemStatus.loadTrims = 1 sysParams.fbEnable = [False]*2 sysParams.FRef = 491.52 #defaultvalue 491.52 ##clock that goes into AFE. Change to 122.88 MHz for direct clock? sysParams.FadcRx = 1966.08 #default:2949.12 sysParams.FadcFb = 1966.08 #default:2949.12 sysParams.Fdac = 1966.08*2 #default:2949.12*3 #decimation: 16 #interpolation: 64 sysParams.externalClockRx=False #default:false sysParams.externalClockTx=False #default:false sysParams.enableDacInterleavedMode = False #DAC interleave mode to save power consumption. Fs/2 - Fin spur occurs sysParams.modeTdd = 0 # 0- Single TDD Pin for all Channels # 1- Separate Control for 2T/2R/1F # 2- Separate Control for 1T/1R/1F sysParams.topLevelSystemMode = 'StaticTDDMode' sysParams.RRFMode = 6 #0: 4T4R2F FDD mode #1: 4T4R1F FDD Mode #2: 4T2R2F FDD Mode Quad Band #5: 4T4R2F TDD Non-Shared #6: 4T4R1F TDD Non-Shared #7: 4T4R2F TDD Shared #8: 4T4R1F TDD Shared #10: 2T2R1F TDD AB / 2T2R1F FDD CD #11: 2T2R1F FDD AB / 2T2R1F TDD CD ##### RX ##### sysParams.rxEnable = [False,False,False,False] sysParams.ddcFactorRx = [16,16,16,16] # DDC decimation factor for RX A, B, C and D sysParams.numBandsRx = [0,0,0,0] sysParams.rxNco0 = [[2340,2340], #Band0, Band1 for RxA for NCO0 [2340,2340], #Band0, Band1 for RxB for NCO0 [2340,2340], #Band0, Band1 for RxC for NCO0 [2340,2340]] #Band0, Band1 for RxD for NCO0 ##### FB ##### sysParams.ddcFactorFb = [16,16] # DDC decimation factor for RX A, B, C and D sysParams.fbNco0 = [2340,2340] #Band0, Band1 for FbA for NCO0 sysParams.fbNco1 = [2340,2340] #Band0, Band1 for FbB for NCO1 ##### TX ##### sysParams.ducFactorTx = [32,32,32,32] # DDC decimation factor for RX A, B, C and D sysParams.numBandsTx = [0,0,0,0] sysParams.txNco0 = [[2340,2340], #Band0, Band1 for TxA for NCO0 [2340,2340], #Band0, Band1 for TxB for NCO0 [2340,2340], #Band0, Band1 for TxC for NCO0 [2340,2340]] #Band0, Band1 for TxD for NCO0 #sysParams.rxEnable = [True,False,True,False] #sysParams.fbEnable = [False,False] #sysParams.txEnable = [True,False,True,False] ################JESD PARAMS################ sysParams.jesdSystemMode = [3,3] #SystemMode 0: 2R1F-FDD ; rx1-rx2-fb-fb #SystemMode 1: 1R1F-FDD ; rx1-rx1-fb-fb #SystemMode 2: 2R-FDD ; rx1-rx1-rx2-rx2 #SystemMode 3: 1R ; rx1-rx1-rx1-rx1 #SystemMode 4: 1F ; fb-fb-fb-fb #SystemMode 5: 1R1F-TDD ; rx1/fb-rx1/fb-rx1/fb-rx1/fb #SystemMode 8: 1R1F-TDD 1R-FDD (FB-2Lanes)(RX1 RX2 interchanged) ; rx2/fb-rx2/fb-rx1-rx1 sysParams.jesdLoopbackEn = 0 #Make it 1 to Enable the JESDTX to JESDRX internal loopback sysParams.LMFSHdRx = ['22210', '22210', '22210', '22210'] #4 channels, 4 converters, 2 bytes per frame, 1 sample, 0 bits after ctrl bit # The 2nd and 4th are valid only for jesdSystemMode values in (2,6,7,8). For other modes, select 4 converter modes for 1st and 3rd. #44210 sysParams.LMFSHdFb = ["22210","22210"] #to be defined - leave as is sysParams.LMFSHdTx = ["22210","22210","22210","22210"] #2 channels aggregate, 4 converters, 2 bytes per frame, 1 sample, 0 bits after ctrl bit #44210 sysParams.jesdTxProtocol = [0,0] #204b sysParams.jesdRxProtocol = [0,0] #204b sysParams.rxJesdTxSyncMux = [0,0,0,0] #0000 because single link, for cmos sync bring ADC_SYNC0 to required pin sysParams.fbJesdTxSyncMux = [3,3] #1,1 for cmos sync, 3,3 for lvds sync sysParams.JesdRxSyncMux = [0,0,0,0] #0000 because single link, for cmos sync bring DAC_SYNC0 to required pin sysParams.serdesFirmware = True # If you want to lead any firmware, please speify the path here. Otherwise it will not write any firmware sysParams.jesdTxLaneMux = [0,1,2,3,4,5,6,7] # Enter which lanes you want in each location. # Note that across 2T Mux is not possible in 0.5. # For example, if you want to exchange the first two lines of each 2T, this should be [[1,0,2,3],[5,4,6,7]] sysParams.jesdRxLaneMux = [7,6,5,4,3,2,1,0] #[0,1,2,3,4,5,6,7] # Enter which lanes you want in each location. # Note that across 2R Mux is not possible in 0.5. # For example, if you want to exchange the first two lines of each 2R, this should be [[1,0,2,3],[5,4,6,7]] sysParams.jesdRxRbd = [4, 4] sysParams.rxJesdTxK = [16,16,16,16] sysParams.fbJesdTxK = [16,16] sysParams.jesdRxK = [16,16,16,16] # scrambler is enabled sysParams.rxJesdTxScr = [True]*4 sysParams.fbJesdTxScr = [True]*2 sysParams.jesdRxScr = [True]*4 AFE.systemStatus.loadTrims =1 ## The following parameters sets up the LMK04828 clocking schemes lmkParams.pllEn = True ##Jitter cleaner on lmkParams.inputClk = 122.88 #1474.56#737.28 lmkParams.lmkFrefClk = True #//Use the 122.88 clock as input reference for the PLL ## The following parameters sets up the register and macro dumps logDumpInst.setFileName(ASTERIX_DIR+DEVICES_DIR+r"\Afe79xxPg1.txt") logDumpInst.logFormat = 0x00 logDumpInst.rewriteFile = 1 logDumpInst.rewriteFileFormat4 = 1 device.optimizeWrites = 0 device.rawWriteLogEn = 1 ## The following parameters sets up the SYNCIN and SYNCOUT to interface with the TSW14J57 #sysParams.jesdABLvdsSync = 1 #sysParams.jesdCDLvdsSync = 1 #sysParams.rxJesdTxSyncMux = [0,0,0,0] #sysParams.fbJesdTxSyncMux = [0,0] #sysParams.jesdRxSyncMux = [0,0,0,0] #[0,0,1,1] #sysParams.syncLoopBack = True # ## The following parameters sets up the AGC # sysParams.agcParams[0].agcMode = 1 ##internal AGC # sysParams.agcParams[0].gpioRstEnable = 0 ##disable GPIO based reset to AGC detector # sysParams.agcParams[0].atken = [0, 1, 0] ##enable big and small step attack # sysParams.agcParams[0].decayen = [0,1,0] ##enable big and small step decay # sysParams.agcParams[0].atksize = [2,1,0] ## bigs step = 2dB, small step = 1dB # sysParams.agcParams[0].decaysize = [2,1,0] ##big step = 2dB, small step = 1dB # sysParams.agcParams[0].atkthreshold = [-1, -2, -14] ##attack threshold # sysParams.agcParams[0].decaythreshold = [-14, -6, -20] ##decay threshold # sysParams.agcParams[0].atkwinlength = [170, 170] ## detector time constant expressed inn absolute time in ns. # sysParams.agcParams[0].decaywinlength = 87380 ##detector time constant expressed in absolute time in ns. All detectors use the same value for decay time constant # sysParams.agcParams[0].atkNumHitsAbs = [8,8] ##absolute number of times signal crosses threshold. These crossing are with respect to the FADC/8 clock # sysParams.agcParams[0].decayNumHitsAbs = [100,100] ##absolute number of times signal crosses threshold. These crossing are with respect to the FADC/8 clock # sysParams.agcParams[0].minDsaAttn = 0 ##minimum DSA attenuation used by AGC # sysParams.agcParams[0].maxDsaAttn = 22 ##maximum DSA attenuation used by AGC # sysParams.agcParams[0].totalGainRange = 22 ##total gain range used by ALC for gain compensation # sysParams.agcParams[0].minAttnAlc = 0 ##minimum attenuation used by ALC for compensation when useMinAttnAgc = 0 # sysParams.agcParams[0].useMinAttnAgc = 1 ##enable ALC to use minimum attenuation from AGC for which compensation is required. # sysParams.agcParams[0].alcEn = 1 # sysParams.agcParams[0].alcMode = 0 ##floating point DGC # sysParams.agcParams[0].fltPtMode = 0 ##if exponent > 0, dont send MSB # sysParams.agcParams[0].fltPtFmt = 1 ##3 bit exponent ## The following parameters sets up the GPIOs sysParams.gpioMapping={ 'H8': 'ADC_SYNC0', 'H7': 'ADC_SYNC1', 'N8': 'ADC_SYNC2', 'N7': 'ADC_SYNC3', 'H9': 'DAC_SYNC0', 'G9': 'DAC_SYNC1', 'N9': 'DAC_SYNC2', 'P9': 'DAC_SYNC3', 'P14': 'GLOBAL_PDN', 'K14': 'FBABTDD', 'R6': 'FBCDTDD', 'H15': ['TXATDD','TXBTDD'], 'V5': ['TXCTDD','TXDTDD'], 'E7': ['RXATDD','RXBTDD'], 'R15': ['RXCTDD','RXDTDD']} #AFE.systemParams.papParams[0]['enable'] = True #AFE.systemParams.papParams[1]['enable'] = True #AFE.systemParams.papParams[2]['enable'] = True #AFE.systemParams.papParams[3]['enable'] = True ## Initiates LMK04828 and AFE79xx Bring-up setupParams.skipLmk = False AFE.initializeConfig() lmkParams.sysrefFreq = AFE.systemStatus.sysrefFreq AFE.LMK.lmkConfig() #-------------------------------------------------------------------------------------------------# #AFE.deviceBringup() #AFE.TOP.overrideTdd(15,0,15) # bit-wise; 4R,2F,4T