AFE79xxLibraryPG1p0 True spi - USB Instrument created. resetDevice Kintex RegProgrammer - USB Instrument created. Kintex RegProgrammer - USB Instrument created. Power Card - USB Instrument created. Version : 0x104204b Connected to Capture Card Loaded Libraries #================ ERRORS:0, WARNINGS:0 ================# #================ ERRORS:0, WARNINGS:0 ================# Version : 0x104204b Connected to Capture Card For bandwidth greater than 600MHz, Feedback Channels cannot be supported Switching to 204B JESD Mode Lane rate exceeded the max supported value in 204B mode for J58 FPGA board or Maximum Lane Rate (Mbps) parameter set incorrectly. Calculated lane rate: 30000.0Msps Switching to 204C JESD Mode For bandwidth greater than 600MHz, Feedback Channels cannot be supported Switching to 204B JESD Mode Lane rate exceeded the max supported value in 204B mode for J58 FPGA board or Maximum Lane Rate (Mbps) parameter set incorrectly. Calculated lane rate: 30000.0Msps Switching to 204C JESD Mode ################################################################### For bandwidth greater than 600MHz, Feedback Channels cannot be supported For these rates, 1KHz raster mode is not supported. Changing to 32-bit NCO mode. The External Sysref Frequency should be an integer factor of: 3.90625MHz 2T2R1F Number: 0 Valid Configuration: True laneRateRx: 24750.0 laneRateFb: 24750.0 laneRateTx: 24750.0 2T2R1F Number: 1 Valid Configuration: True laneRateRx: 24750.0 laneRateFb: 24750.0 laneRateTx: 24750.0 Matched for 204C mode:477 Connect 1500.0MHz reference clock at LMK_CLK_IN (J14) connector Generated system parameters successfully Refreshed GUI ################################################################### The External Sysref Frequency should be an integer factor of: 3.90625MHz 2T2R1F Number: 0 Valid Configuration: True laneRateRx: 24750.0 laneRateFb: 24750.0 laneRateTx: 24750.0 2T2R1F Number: 1 Valid Configuration: True laneRateRx: 24750.0 laneRateFb: 24750.0 laneRateTx: 24750.0 LMK Clock Divider - Device registers reset. LMK Clock Divider - Device registers reset. FPGA Reset device not found Resetting FPGA. Version : 0x104204b Connected to Capture Card Mismatch in the FPGA bit file version. AFE JESD Protocol is 204C but the FPGA bit file is 0x204b LMK and FPGA Configured. DONOT_OPEN_Atharv_FULL - Device registers reset. chipType: 0xa chipId: 0x78 chipVersion: 0x11 AFE Reset Done Fuse farm load autoload done successful No autload error Fuse farm load autoload done successful No autload error AFE MCU Wake up done and patch loaded. PLL Locked AFE PLL Configured. AFE SerDes Configured. AFE Digital Chains configured. AFE TX Analog configured. AFE RX Analog configured. AFE FB Analog configured. AFE JESD configured. AFE AGC configured. AFE GPIO configured. Sysref Read as expected Setting RBD to: 15 Setting RBD to: 15 ###########Device DAC JESD-RX 0 Link Status########### Serdes-FIFO error for lane 0: 1 LOS Indicator for (Serdes Loss of signal) lane 1: 1 Serdes-FIFO error for lane 1: 1 LOS Indicator for (Serdes Loss of signal) lane 2: 1 Serdes-FIFO error for lane 2: 1 LOS Indicator for (Serdes Loss of signal) lane 3: 1 Serdes-FIFO error for lane 3: 1 Comma Align Lock Lane2: False; Please check if the transmitter is sending data and eye is good. CS State TX0: 0b00000000 . It is expected to be 0b10101010 BUF State TX0: 0b01010101 . It is expected to be 0b11111111 Couldn't get the link up for device RX: 0; Alarms: 0xfe00 ################################### ###########Device DAC JESD-RX 1 Link Status########### LOS Indicator for (Serdes Loss of signal) lane 0: 1 Serdes-FIFO error for lane 0: 1 Serdes-FIFO error for lane 1: 1 LOS Indicator for (Serdes Loss of signal) lane 2: 1 Serdes-FIFO error for lane 2: 1 LOS Indicator for (Serdes Loss of signal) lane 3: 1 Comma Align Lock Lane2: False; Please check if the transmitter is sending data and eye is good. Comma Align Lock Lane3: False; Please check if the transmitter is sending data and eye is good. CS State TX0: 0b00000000 . It is expected to be 0b10101010 BUF State TX0: 0b01010101 . It is expected to be 0b11111111 Couldn't get the link up for device RX: 1; Alarms: 0x7d00 ################################### AFE Configuration Complete Function Execution Failed: setGoodRbd Function Execution Failed: setGoodRbd ###########Device DAC JESD-RX 0 Link Status########### Serdes-FIFO error for lane 0: 1 LOS Indicator for (Serdes Loss of signal) lane 1: 1 Serdes-FIFO error for lane 1: 1 LOS Indicator for (Serdes Loss of signal) lane 2: 1 Serdes-FIFO error for lane 2: 1 LOS Indicator for (Serdes Loss of signal) lane 3: 1 Serdes-FIFO error for lane 3: 1 Comma Align Lock Lane2: False; Please check if the transmitter is sending data and eye is good. CS State TX0: 0b00000000 . It is expected to be 0b10101010 BUF State TX0: 0b01010101 . It is expected to be 0b11111111 Couldn't get the link up for device RX: 0; Alarms: 0xfe00 ################################### ###########Device DAC JESD-RX 1 Link Status########### LOS Indicator for (Serdes Loss of signal) lane 0: 1 Serdes-FIFO error for lane 0: 1 Serdes-FIFO error for lane 1: 1 LOS Indicator for (Serdes Loss of signal) lane 2: 1 Serdes-FIFO error for lane 2: 1 LOS Indicator for (Serdes Loss of signal) lane 3: 1 Serdes-FIFO error for lane 3: 1 Comma Align Lock Lane2: False; Please check if the transmitter is sending data and eye is good. Comma Align Lock Lane3: False; Please check if the transmitter is sending data and eye is good. CS State TX0: 0b00000000 . It is expected to be 0b10101010 BUF State TX0: 0b01010101 . It is expected to be 0b11111111 Couldn't get the link up for device RX: 1; Alarms: 0xfd00 ###################################