**********************************************************
*************  Important Instructions Follow  ************
**********************************************************

All files exported to: Z:\\13\\05\\1305199\\24\Eagle\2014-12-15_07-53-03\2014-12-15_07-53-03.xml


To import your new library into Eagle:
1. Start Eagle.
2. Select File -> New -> Library from the menu.
3. In the blank library window, select File -> Execute Script from the menu.
5. Browse to your newly exported Eagle Script file (".scr" file extension)
6. After opening the file, the script will populate the new library.
7. Use File -> Save (or Save As..) to save the library to the desired location in Eagle native format.

For additional information, please visit this site:
http://www.accelerated-designs.com/help/Eagle_import.html

You may also find this video helpful:
http://youtu.be/5jGuWY-Yy3Q


Symbol "BSC042NE7NS3 G" renamed to "BSC042NE7NS3_G"
Component "GRM216R71H103KA01D" renamed to "GRM216R71H103KA01D"
Component "CC0805KRX7R9BB682" renamed to "CC0805KRX7R9BB682"
Component "CC0805KRX7R9BB561" renamed to "CC0805KRX7R9BB561"
Component "WB_CURRENT_LOAD" renamed to "WB_CURRENT_LOAD"
Component "C0805C104K5RACTU" renamed to "C0805C104K5RACTU"
Component "16SVPF1000M" renamed to "16SVPF1000M"
Component "GRM216R71E182KA01D" renamed to "GRM216R71E182KA01D"
Component "EMK212B7105KG-T" renamed to "EMK212B7105KG-T"
Component "MBR0540T1G" renamed to "MBR0540T1G"
Component "WB_GND" renamed to "WB_GND"
Component "SER2918H-153KL" renamed to "SER2918H-153KL"
Component "FDMS8460" renamed to "FDMS8460"
Component "BSC042NE7NS3 G" renamed to "BSC042NE7NS3_G"
Component "ERJ-6ENF2102V" renamed to "ERJ-6ENF2102V"
Component "ERJ-6ENF1004V" renamed to "ERJ-6ENF1004V"
Component "ERJ-6ENF1101V" renamed to "ERJ-6ENF1101V"
Component "ERJ-6ENF9761V" renamed to "ERJ-6ENF9761V"
Component "ERJ-6ENF4753V" renamed to "ERJ-6ENF4753V"
Component "CSNL1206FT3L00" renamed to "CSNL1206FT3L00"
Component "ERJ-6ENF4222V" renamed to "ERJ-6ENF4222V"
Component "ERJ-6ENF2101V" renamed to "ERJ-6ENF2101V"
Component "ERJ-6ENF2802V" renamed to "ERJ-6ENF2802V"
Component "LM5116MHX/NOPB" renamed to "LM5116MHX/NOPB"
Component "WB_BATTERY" renamed to "WB_BATTERY"
Component "35SVPF120M" renamed to "35SVPF120M"
The Symbol WB_CONTINUATION was missing a RefDes attribute, a refdes was created for the symbol.
The Symbol WB_CONTINUATION was missing a Type attribute, a type was created for the symbol.
The Symbol WB_CONTINUATION was missing a Value attribute, a value was created for the symbol.
The Symbol WB_N_MOSFET was missing a RefDes attribute, a refdes was created for the symbol.
The Symbol WB_N_MOSFET was missing a Type attribute, a type was created for the symbol.
The Symbol WB_N_MOSFET was missing a Value attribute, a value was created for the symbol.
The Symbol WB_BLOCK_IO was missing a RefDes attribute, a refdes was created for the symbol.
The Symbol WB_BLOCK_IO was missing a Type attribute, a type was created for the symbol.
The Symbol WB_BLOCK_IO was missing a Value attribute, a value was created for the symbol.
The Symbol WB_LM5116 was missing a RefDes attribute, a refdes was created for the symbol.
The Symbol WB_LM5116 was missing a Type attribute, a type was created for the symbol.
The Symbol WB_LM5116 was missing a Value attribute, a value was created for the symbol.
The Symbol WB_PRIM_AC_VOLTAGE_SOURCE was missing a RefDes attribute, a refdes was created for the symbol.
The Symbol WB_PRIM_AC_VOLTAGE_SOURCE was missing a Type attribute, a type was created for the symbol.
The Symbol WB_PRIM_AC_VOLTAGE_SOURCE was missing a Value attribute, a value was created for the symbol.
The Symbol WB_SYNC_CAPACITOR was missing a RefDes attribute, a refdes was created for the symbol.
The Symbol WB_SYNC_CAPACITOR was missing a Type attribute, a type was created for the symbol.
The Symbol WB_SYNC_CAPACITOR was missing a Value attribute, a value was created for the symbol.
The Symbol WB_PRIMITIVE_INDUCTOR was missing a RefDes attribute, a refdes was created for the symbol.
The Symbol WB_PRIMITIVE_INDUCTOR was missing a Type attribute, a type was created for the symbol.
The Symbol WB_PRIMITIVE_INDUCTOR was missing a Value attribute, a value was created for the symbol.
The Symbol WB_VOLTAGE_PROBE was missing a RefDes attribute, a refdes was created for the symbol.
The Symbol WB_VOLTAGE_PROBE was missing a Type attribute, a type was created for the symbol.
The Symbol WB_VOLTAGE_PROBE was missing a Value attribute, a value was created for the symbol.
The Symbol WB_PWL_VOLTAGE_SOURCE was missing a RefDes attribute, a refdes was created for the symbol.
The Symbol WB_PWL_VOLTAGE_SOURCE was missing a Type attribute, a type was created for the symbol.
The Symbol WB_PWL_VOLTAGE_SOURCE was missing a Value attribute, a value was created for the symbol.
The Symbol WB_SOURCE_RESISTOR was missing a RefDes attribute, a refdes was created for the symbol.
The Symbol WB_SOURCE_RESISTOR was missing a Type attribute, a type was created for the symbol.
The Symbol WB_SOURCE_RESISTOR was missing a Value attribute, a value was created for the symbol.
The Symbol WB_PRIM_PWL_VOLTAGE_SOURCE was missing a RefDes attribute, a refdes was created for the symbol.
The Symbol WB_PRIM_PWL_VOLTAGE_SOURCE was missing a Type attribute, a type was created for the symbol.
The Symbol WB_PRIM_PWL_VOLTAGE_SOURCE was missing a Value attribute, a value was created for the symbol.
The Symbol WB_PRIM_STARTUP_VOLTAGE_SOURCE was missing a RefDes attribute, a refdes was created for the symbol.
The Symbol WB_PRIM_STARTUP_VOLTAGE_SOURCE was missing a Type attribute, a type was created for the symbol.
The Symbol WB_PRIM_STARTUP_VOLTAGE_SOURCE was missing a Value attribute, a value was created for the symbol.
The Symbol WB_STARTUP_VOLTAGE_SOURCE was missing a RefDes attribute, a refdes was created for the symbol.
The Symbol WB_STARTUP_VOLTAGE_SOURCE was missing a Type attribute, a type was created for the symbol.
The Symbol WB_STARTUP_VOLTAGE_SOURCE was missing a Value attribute, a value was created for the symbol.
The Symbol WB_CURRENT_PROBE was missing a RefDes attribute, a refdes was created for the symbol.
The Symbol WB_CURRENT_PROBE was missing a Type attribute, a type was created for the symbol.
The Symbol WB_CURRENT_PROBE was missing a Value attribute, a value was created for the symbol.
The Symbol WB_PRIMITIVE_BATTERY was missing a RefDes attribute, a refdes was created for the symbol.
The Symbol WB_PRIMITIVE_BATTERY was missing a Type attribute, a type was created for the symbol.
The Symbol WB_PRIMITIVE_BATTERY was missing a Value attribute, a value was created for the symbol.
The Symbol WB_PWL_CURRENT_LOAD was missing a RefDes attribute, a refdes was created for the symbol.
The Symbol WB_PWL_CURRENT_LOAD was missing a Type attribute, a type was created for the symbol.
The Symbol WB_PWL_CURRENT_LOAD was missing a Value attribute, a value was created for the symbol.
The Symbol WB_LOAD_RESISTOR was missing a RefDes attribute, a refdes was created for the symbol.
The Symbol WB_LOAD_RESISTOR was missing a Type attribute, a type was created for the symbol.
The Symbol WB_LOAD_RESISTOR was missing a Value attribute, a value was created for the symbol.


Ultra Librarian Gold 6.4.107 Process Report


Message - Padstack "RX44Y57D0T" Shape(4) is a CIRCLE with no diameter.
Message - Padstack "RX152Y43D0T" Shape(4) is a CIRCLE with no diameter.
Message - Padstack "RX48Y30D0T" Shape(4) is a CIRCLE with no diameter.
Message - Padstack "RX210Y220D0T" Shape(4) is a CIRCLE with no diameter.
Message - Padstack "RX250Y208D0T" Shape(4) is a CIRCLE with no diameter.
Message - Padstack "RX62Y24p02D0T" Shape(4) is a CIRCLE with no diameter.
Message - Padstack "RXp965Yp533D0T" Shape(4) is a CIRCLE with no diameter.
Message - Padstack "RX4p805Y4p36D0T" Shape(4) is a CIRCLE with no diameter.
Message - Padstack "RX44Y71D0T" Shape(4) is a CIRCLE with no diameter.
Message - Padstack "RX56Y14D0T" Shape(4) is a CIRCLE with no diameter.
Message - Padstack "RX124Y171D0T" Shape(4) is a CIRCLE with no diameter.
Message - Component "GRM216R71H103KA01D" attribute "Cap" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "GRM216R71H103KA01D" attribute "ESR" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "GRM216R71H103KA01D" attribute "IRMS" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "GRM216R71H103KA01D" attribute "VDC" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "CC0805KRX7R9BB682" attribute "Cap" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "CC0805KRX7R9BB682" attribute "ESR" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "CC0805KRX7R9BB682" attribute "IRMS" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "CC0805KRX7R9BB682" attribute "VDC" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "CC0805KRX7R9BB561" attribute "Cap" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "CC0805KRX7R9BB561" attribute "ESR" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "CC0805KRX7R9BB561" attribute "IRMS" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "CC0805KRX7R9BB561" attribute "VDC" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "C0805C104K5RACTU" attribute "Cap" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "C0805C104K5RACTU" attribute "ESR" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "C0805C104K5RACTU" attribute "IRMS" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "C0805C104K5RACTU" attribute "VDC" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "16SVPF1000M" attribute "Datasheet URL" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "16SVPF1000M" attribute "Cap" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "16SVPF1000M" attribute "ESR" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "16SVPF1000M" attribute "IRMS" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "16SVPF1000M" attribute "VDC" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "GRM216R71E182KA01D" attribute "Cap" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "GRM216R71E182KA01D" attribute "ESR" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "GRM216R71E182KA01D" attribute "IRMS" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "GRM216R71E182KA01D" attribute "VDC" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "EMK212B7105KG-T" attribute "Cap" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "EMK212B7105KG-T" attribute "ESR" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "EMK212B7105KG-T" attribute "IRMS" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "EMK212B7105KG-T" attribute "VDC" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "MBR0540T1G" attribute "Datasheet URL" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "MBR0540T1G" attribute "Io" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "MBR0540T1G" attribute "VRRM" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "MBR0540T1G" attribute "VFatIo" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "SER2918H-153KL" attribute "Datasheet URL" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "SER2918H-153KL" attribute "L" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "SER2918H-153KL" attribute "DCR" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "SER2918H-153KL" attribute "IDC" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "FDMS8460" attribute "Datasheet URL" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "FDMS8460" attribute "VdsMax" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "FDMS8460" attribute "IdsMax" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "FDMS8460" attribute "Rdson45" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "FDMS8460" attribute "QgTyp" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "FDMS8460" attribute "Quantity" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "BSC042NE7NS3_G" attribute "Datasheet URL" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "BSC042NE7NS3_G" attribute "VdsMax" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "BSC042NE7NS3_G" attribute "IdsMax" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "BSC042NE7NS3_G" attribute "Rdson45" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "BSC042NE7NS3_G" attribute "QgTyp" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "BSC042NE7NS3_G" attribute "Quantity" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "ERJ-6ENF2102V" attribute "Resistance" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "ERJ-6ENF2102V" attribute "Power" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "ERJ-6ENF2102V" attribute "Tolerance" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "ERJ-6ENF1004V" attribute "Resistance" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "ERJ-6ENF1004V" attribute "Power" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "ERJ-6ENF1004V" attribute "Tolerance" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "ERJ-6ENF1101V" attribute "Resistance" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "ERJ-6ENF1101V" attribute "Power" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "ERJ-6ENF1101V" attribute "Tolerance" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "ERJ-6ENF9761V" attribute "Resistance" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "ERJ-6ENF9761V" attribute "Power" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "ERJ-6ENF9761V" attribute "Tolerance" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "ERJ-6ENF4753V" attribute "Resistance" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "ERJ-6ENF4753V" attribute "Power" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "ERJ-6ENF4753V" attribute "Tolerance" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "CSNL1206FT3L00" attribute "Resistance" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "CSNL1206FT3L00" attribute "Power" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "CSNL1206FT3L00" attribute "Tolerance" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "ERJ-6ENF4222V" attribute "Resistance" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "ERJ-6ENF4222V" attribute "Power" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "ERJ-6ENF4222V" attribute "Tolerance" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "ERJ-6ENF2101V" attribute "Resistance" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "ERJ-6ENF2101V" attribute "Power" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "ERJ-6ENF2101V" attribute "Tolerance" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "ERJ-6ENF2802V" attribute "Resistance" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "ERJ-6ENF2802V" attribute "Power" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "ERJ-6ENF2802V" attribute "Tolerance" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "LM5116MHX/NOPB" attribute "Datasheet URL" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "LM5116MHX/NOPB" attribute "Frequency" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "LM5116MHX/NOPB" attribute "Imax" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "LM5116MHX/NOPB" attribute "Package" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "LM5116MHX/NOPB" attribute "Mktg_Package" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "LM5116MHX/NOPB" attribute "NSID" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "35SVPF120M" attribute "Datasheet URL" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "35SVPF120M" attribute "Cap" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "35SVPF120M" attribute "ESR" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "35SVPF120M" attribute "IRMS" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.
Message - Component "35SVPF120M" attribute "VDC" references text style "" that is not in the database.
The default pattern text style "H50s3" was substituted.

TextStyle count:  24
Padstack count:   11
Pattern count:    8
Symbol count:     28
Component count:  25

Export


Footprint "WB_CURRENT_LOAD" has no layer data mapped and will be skipped.
Component "WB_CURRENT_LOAD" requires footprint "WB_CURRENT_LOAD" and will be skipped.
Footprint "WB_GND" has no layer data mapped and will be skipped.
Component "WB_GND" requires footprint "WB_GND" and will be skipped.
Footprint "WB_BATTERY" has no layer data mapped and will be skipped.
Component "WB_BATTERY" requires footprint "WB_BATTERY" and will be skipped.