Maximum Blind/Buried Via Stagger

Checks the maximum center-to-center distance between the connect point of one pin or blind/buried via (the x, y location of the pin or via) and the connect point of another pin. The two pins or vias must be on the same net with a single connect line joining them.



DRC Code: %2