Minimum Blind/Buried Via Stagger

Checks the minimum center-to-center distance between the connect points of two pins or vias (the x,y location of the pin or via), where the two pins or vias are on the same net and have a single connect line joining them.



DRC Code: %2