SimpleLink™ CC2745R10-Q1 LaunchPad™ Settings & Resources
The SimpleLink™ CC2745R10-Q1 LaunchPad™ contains a CC2745R10E0WRHARQ1 device.
Jumper Settings
- To enable the ITM, connect the
SWOpin to pin 11 on the XDS110 debugger interface, on the outside of the TXD pin (see device schematic, the pin itself may be unlabeled).
TI BoosterPacks™
The following BoosterPacks are used with some driver examples.
BP-BASSENSORSMKII BoosterPack
The TMP116’s power pin is not compatible with this LaunchPad. Use the following modification to enable the TMP116’s usage with the i2ctmp and portable examples.
- Use a jumper wire to connect BoosterPack pin header BP.28 (
T_V+) to BP.1 (3V3).
The OPT3001’s power and interrupt pins are not compatible with this LaunchPad. Use the following modification to enable the OPT3001’s usage with the i2copt3001_cpp example.
- Use a jumper wire to connect BoosterPack pin header BP.27 (
O_V+) to BP.18 (unlabeled). - Use a jumper wire to connect BoosterPack pin header BP.25 (
O_INT) to BP.7 (P05).
BOOSTXL-SHARP128 LCD & SD Card BoosterPack
- BoosterPack pin header BP.8 (
SD_CS) must be jumpered to BP.9 when using the SD card.
CC3200 Audio BoosterPack
The BoostPack’s DIN, BCLK and FSYNC/WCLK signal pins are not compatible with this LaunchPad. Use the following modifications to enable the CC3200 Audio BoosterPack’s usage with the i2secho example.
Attach the CC3200 Audio BoosterPack to the LP_EM_CC2745R10_Q1 and run jumper wires between the following pins on the CC3200 Audio BoosterPack:
- DIN:
P4.3andP3.9 - BCLK:
P4.9andP3.8 - FSYNC/WCLK:
P4.10andP3.7
See Audio BP User Guide (Figure 2-1), or the diagram below, for information on where these pins are located.