Low Power Vector Table #Set BT BR (GFSK) LP Vectors Values (note the need to multiply the output power in dBm by '2' Send_HCI_VS_DRPb_Set_Power_Vector 0xFD82, 0x00, -22.5 *2, -18 *2, -13.5 *2, -9 *2, - 4.5 *2, 0 *2, 5 *2, 10 *2, 0x3F, 0x00FF ./SS1Tool cmd 0x3F 0x182 0x00 0xD3 0xDC 0xE5 0xEE 0xF7 0x00 0x0A 0x14 0x3F 0xFF 0x00 #Set BT LE (BLE) LP Vectors Values (note the need to multiply the output power in dBm by '2' Send_HCI_VS_DRPb_Set_Power_Vector 0xFD82, 0x03, -22.5 *2, -18 *2, -13.5 *2, -9 *2, - 4.5 *2, 0 *2, 5 *2, 10 *2, 0x3F, 0x00FF ./SS1Tool cmd 0x3F 0x182 0x03 0xD3 0xDC 0xE5 0xEE 0xF7 0x00 0x0A 0x14 0x3F 0xFF 0x00 #Set ANT LP Vectors Values (note the need to multiply the output power in dBm by '2' Send_HCI_VS_DRPb_Set_Power_Vector 0xFD82, 0x04, -22.5 *2, -18 *2, -13.5 *2, -9 *2, - 4.5 *2, 0 *2, 5 *2, 10 *2, 0x3F, 0x00FF ./SS1Tool cmd 0x3F 0x182 0x04 0xD3 0xDC 0xE5 0xEE 0xF7 0x00 0x0A 0x14 0x3F 0xFF 0x00 #Set BT BR EDR 2MB LP Vectors Values (note the need to multiply the output power in dBm by '2' Send_HCI_VS_DRPb_Set_Power_Vector 0xFD82, 0x01, -25 *2, -20.5 *2, -16 *2, -11.5 *2, -7 *2, - 2 *2, 3 *2, 8 *2, 0x3F, 0x00FF ./SS1Tool cmd 0x3F 0x182 0x01 0xD3 0xDC 0xE5 0xEE 0xF7 0x00 0x0A 0x14 0x3F 0xFF 0x00 #Set BT BR EDR 3MB LP Vectors Values (note the need to multiply the output power in dBm by '2' Send_HCI_VS_DRPb_Set_Power_Vector 0xFD82, 0x02, -25 *2, -20.5 *2, -16 *2, -11.5 *2, -7 *2, - 2 *2, 3 *2, 8 *2, 0x3F, 0x00FF ./SS1Tool cmd 0x3F 0x182 0x02 0xD3 0xDC 0xE5 0xEE 0xF7 0x00 0x0A 0x14 0x3F 0xFF 0x00 High Power Vector Table Send_HCI_VS_DRPb_Set_Power_Vector 0xFD82, 8, -19.5 *2, -14.5 *2, -9.5 *2, - 4.5 *2, 0.5 *2, 5.5 *2, 10.5 *2, 15.5 *2, 0x3F, 0x00FF ./SS1Tool cmd 0x3F 0x182 0x08 0xD9 0xE3 0xED 0xF7 0x01 0x0B 0x15 0x1F 0x3F 0xFF 0x00 #Set BT LE (BLE) HP Vectors Values (note the need to multiply the output power in dBm by '2' Send_HCI_VS_DRPb_Set_Power_Vector 0xFD82, 9, -19.5 *2, -14.5 *2, -9.5 *2, - 4.5 *2, 0.5 *2, 5.5 *2, 10.5 *2, 15.5 *2, 0x3F, 0x00FF ./SS1Tool cmd 0x3F 0x182 0x09 0xD9 0xE3 0xED 0xF7 0x01 0x0B 0x15 0x1F 0x3F 0xFF 0x00 #Set ANT HP Vectors Values (note the need to multiply the output power in dBm by '2' Send_HCI_VS_DRPb_Set_Power_Vector 0xFD82, 10, -19.5 *2, -14.5 *2, -9.5 *2, - 4.5 *2, 0.5 *2, 5.5 *2, 10.5 *2, 15.5 *2, 0x3F, 0x00FF ./SS1Tool cmd 0x3F 0x182 0x0A 0xD9 0xE3 0xED 0xF7 0x01 0x0B 0x15 0x1F 0x3F 0xFF 0x00 #Set BT BR EDR 2MB HP Vectors Values (note the need to multiply the output power in dBm by '2' Send_HCI_VS_DRPb_Set_Power_Vector 0xFD82, 11, -22.5 *2, -18 *2, -13.5 *2, -9 *2, - 4.5 *2, 0 *2, 5 *2, 10 *2, 0x3F, 0x00FF ./SS1Tool cmd 0x3F 0x182 0x0B 0xD9 0xE3 0xED 0xF7 0x01 0x0B 0x15 0x1F 0x3F 0xFF 0x00 #Set BT BR EDR 3MB HP Vectors Values (note the need to multiply the output power in dBm by '2' Send_HCI_VS_DRPb_Set_Power_Vector 0xFD82, 12, -22.5 *2, -18 *2, -13.5 *2, -9 *2, - 4.5 *2, 0 *2, 5 *2, 10 *2, 0x3F, 0x00FF ./SS1Tool cmd 0x3F 0x182 0x0C 0xD9 0xE3 0xED 0xF7 0x01 0x0B 0x15 0x1F 0x3F 0xFF 0x00 Class 2 Power ROM Data Send_HCI_VS_DRPb_Set_Class2_Single_Power 0xFD87, 6, 6, 6, 6, 6, 6, 6, 6, 6, 6 ./SS1Tool cmd 0x3F 0x187 0x06 0x06 0x06 0x06 0x06 0x06 0x06 0x06 0x06 0x06 Run TPC Calibration # Run TPC calibration to update the ACW (Amplitude Control Word) to the PA Send_HCI_VS_DRPb_Enable_RF_Calibration_Enhanced 0xFDFB, 0x00, 0x00000800, 0x01 ./SS1Tool cmd 0x3F 0x1FB 0x00 0x00 0x08 0x00 0x00 0x01