sdraw
Example Summary
Sample application to read and write data onto an SD Card (SD interface).
Running this application will cause any filesystem on the SD card to become corrupted!
Peripherals Exercised
Board_GPIO_LED0- Indicates that the board was initialized withinmainThread()Board_SD0- Connection to the SD card
Resources & Jumper Settings
If you’re using an IDE (such as CCS or IAR), please refer to Board.html in your project directory for resources used and board-specific jumper settings. Otherwise, you can find Board.html in the directory <SDK_INSTALL_DIR>/source/ti/boards/<BOARD>.
This example requires an external SD Card BoosterPack.
Example Usage
Example output is generated through use of Display driver APIs. Refer to the Display driver documentation found in the SimpleLink MCU SDK User’s Guide.
- Open a serial session (e.g.
PuTTY, etc.) to the appropriate COM port.- The COM port can be determined via Device Manager in Windows or via
ls /dev/tty*in Linux.
- The COM port can be determined via Device Manager in Windows or via
The connection should have the following settings
Baud-rate: 115200
Data bits: 8
Stop bits: 1
Parity: None
Flow Control: None
Edit the sdraw.c file and set WRITEENABLE to 1, and build the example. This will allow data to be written to the SD card. WARNING: Any file system present on the SD card will be overwritten and corrupted by this action!
Run the example.
Board_GPIO_LED0turns ON to indicate driver initialization is complete.The example proceeds to write a buffer of data to the SD card, overwriting any filesystem currently present on the card.
The raw data that was written to the file is then read and compared with the original data. If the data read does not match what was written, an error message will be displayed.
Set WRITEENABLE back to 0, build, and run the example. The example will only read the contents of the file in this case.
Application Design Details
- This application demonstrates how to use the SD Card driver without a filesystem to perform disk I/O operations on an SD Card using simple write/read calls.
This application uses one thread:
The mainThread performs the following actions:
Create and initialize the SD driver object.
Calculate the total card capacity from the sector size and number of sectors on the SD card.
Write the default message in
textarrayto the file and print its contents to the console.Read back the message from the SD card into a temporary buffer,
cpy_buffand print its contents to the console.The SD driver is closed and the example is terminated.
TI-RTOS:
- When building in Code Composer Studio, the kernel configuration project will be imported along with the example. The kernel configuration project is referenced by the example, so it will be built first. The “release” kernel configuration is the default project used. It has many debug features disabled. These feature include assert checking, logging and runtime stack checks. For a detailed difference between the “release” and “debug” kernel configurations and how to switch between them, please refer to the SimpleLink MCU SDK User’s Guide. The “release” and “debug” kernel configuration projects can be found under <SDK_INSTALL_DIR>/kernel/tirtos/builds/<BOARD>/(release|debug)/(ccs|gcc).
FreeRTOS:
- Please view the
FreeRTOSConfig.hheader file for example configuration information.