#include #include #include #include #include #include #include #include #include /* Driver Header files */ #include #include #include #include /* Driver configuration */ #include "ti_drivers_config.h" /* Buffer size used for the file copy process */ #ifndef CPY_BUFF_SIZE #define CPY_BUFF_SIZE 2048 #endif /* String conversion macro */ #define STR_(n) #n #define STR(n) STR_(n) /* Drive number used for FatFs */ #define DRIVE_NUM 0 const char inputfile[] = "fat:"STR(DRIVE_NUM)":input.txt"; const char outputfile[] = "fat:"STR(DRIVE_NUM)":output.txt"; const char textarray[] = \ "***********************************************************************\n" "0 1 2 3 4 5 6 7\n" "Hello from System Integration Lab Ncflexe\n"; static Display_Handle display; /* File name prefix for this filesystem for use with TI C RTS */ char fatfsPrefix[] = "fat"; unsigned char cpy_buff[CPY_BUFF_SIZE + 1]; void *mainThread(void *arg0) { char input; const char echoPrompt[] = "Echoing characters:\r\n"; UART_Handle uart; UART_Params uartParams; SDFatFS_Handle sdfatfsHandle; /* Variables for the CIO functions */ FILE *src, *dst; /* Variables to keep track of the file copy progress */ unsigned int bytesRead = 0; unsigned int bytesWritten = 0; unsigned int filesize; unsigned int totalBytesCopied = 0; /* Call driver init functions */ GPIO_init(); UART_init(); Display_init(); SDFatFS_init(); /* Configure the LED pin */ GPIO_setConfig(CONFIG_GPIO_LED_0, GPIO_CFG_OUT_STD | GPIO_CFG_OUT_LOW); /* add_device() should be called once and is used for all media types */ add_device(fatfsPrefix, _MSA, ffcio_open, ffcio_close, ffcio_read, ffcio_write, ffcio_lseek, ffcio_unlink, ffcio_rename); /* Open the display for output */ display = Display_open(Display_Type_UART, NULL); if (display == NULL) { /* Failed to open display driver */ while (1); } /* Turn on user LED */ GPIO_write(CONFIG_GPIO_LED_0, CONFIG_GPIO_LED_ON); Display_printf(display, 0, 0, "Starting the fatsd example\n"); Display_printf(display, 0, 0, "This example requires a FAT filesystem on the SD card.\n"); Display_printf(display, 0, 0, "You will get errors if your SD card is not formatted with a filesystem.\n"); /* Mount and register the SD Card */ sdfatfsHandle = SDFatFS_open(CONFIG_SDFatFS_0, DRIVE_NUM); if (sdfatfsHandle == NULL) { Display_printf(display, 0, 0, "Error starting the SD card\n"); while (1); } else { Display_printf(display, 0, 0, "Drive %u is mounted\n", DRIVE_NUM); } /* Create a UART with data processing off. */ UART_Params_init(&uartParams); uartParams.writeDataMode = UART_DATA_BINARY; uartParams.readDataMode = UART_DATA_BINARY; uartParams.readReturnMode = UART_RETURN_FULL; uartParams.baudRate = 115200; uart = UART_open(CONFIG_UART_0, &uartParams); if (uart == NULL) { /* UART_open() failed */ while (1); } //UART_write(uart, echoPrompt, sizeof(echoPrompt)); /* Loop forever echoing */ /*while (1) { UART_read(uart, &input, 1); UART_write(uart, &input, 1); }*/ /* Try to open the source file */ src = fopen(inputfile, "r"); if (!src) { Display_printf(display, 0, 0, "Creating a new file \"%s\"...", inputfile); /* Open file for both reading and writing */ src = fopen(inputfile, "w+"); if (!src) { Display_printf(display, 0, 0, "Error: \"%s\" could not be created.\nPlease check the " "Board.html if additional jumpers are necessary.\n", inputfile); Display_printf(display, 0, 0, "Aborting...\n"); while (1); } while (1) { UART_read(uart, &input1, 1); UART_write(uart, &input1, 1); fwrite(textarray, 1, strlen(textarray), src); fwrite(input1,1,strlen(input1),src); fflush(src); } /* Reset the internal file pointer */ rewind(src); Display_printf(display, 0, 0, "done\n"); } else { Display_printf(display, 0, 0, "Using existing copy of \"%s\"\n", inputfile); } /* Create a new file object for the file copy */ dst = fopen(outputfile, "w"); if (!dst) { Display_printf(display, 0, 0, "Error opening \"%s\"\n", outputfile); Display_printf(display, 0, 0, "Aborting...\n"); while (1); } else { Display_printf(display, 0, 0, "Starting file copy\n"); } /* Copy the contents from the src to the dst */ while (true) { /* Read from source file */ bytesRead = fread(cpy_buff, 1, CPY_BUFF_SIZE, src); if (bytesRead == 0) { break; /* Error or EOF */ } /* Write to dst file */ bytesWritten = fwrite(cpy_buff, 1, bytesRead, dst); if (bytesWritten < bytesRead) { Display_printf(display, 0, 0, "Disk Full\n"); break; /* Error or Disk Full */ } /* Update the total number of bytes copied */ totalBytesCopied += bytesWritten; } fflush(dst); /* Get the filesize of the source file */ fseek(src, 0, SEEK_END); filesize = ftell(src); rewind(src); /* Close both inputfile[] and outputfile[] */ fclose(src); fclose(dst); Display_printf(display, 0, 0, "File \"%s\" (%u B) copied to \"%s\" (Wrote %u B)\n", inputfile, filesize, outputfile, totalBytesCopied); /* Now output the outputfile[] contents onto the console */ dst = fopen(outputfile, "r"); if (!dst) { Display_printf(display, 0, 0, "Error opening \"%s\"\n", outputfile); Display_printf(display, 0, 0, "Aborting...\n"); while (1); } /* Print file contents */ while (true) { /* Read from output file */ bytesRead = fread(cpy_buff, 1, CPY_BUFF_SIZE, dst); if (bytesRead == 0) { break; /* Error or EOF */ } cpy_buff[bytesRead] = '\0'; /* Write output */ Display_printf(display, 0, 0, "%s", cpy_buff); } /* Close the file */ fclose(dst); /* Stopping the SDCard */ SDFatFS_close(sdfatfsHandle); Display_printf(display, 0, 0, "Drive %u unmounted\n", DRIVE_NUM); return (NULL); } /* * ======== fatfs_getFatTime ======== */ int32_t fatfs_getFatTime(void) { /* * FatFs uses this API to get the current time in FatTime format. User's * must implement this function based on their system's timekeeping * mechanism. See FatFs documentation for details on FatTime format. */ /* Jan 1 2017 00:00:00 */ return (0x4A210000); }