/**************************************************************************************************
  Filename:       simpleGATTprofile.h
  Revised:        $Date: 2010-08-06 08:56:11 -0700 (Fri, 06 Aug 2010) $
  Revision:       $Revision: 23333 $

  Description:    This file contains the Simple GATT profile definitions and
                  prototypes.

  Copyright 2010 - 2013 Texas Instruments Incorporated. All rights reserved.

  IMPORTANT: Your use of this Software is limited to those specific rights
  granted under the terms of a software license agreement between the user
  who downloaded the software, his/her employer (which must be your employer)
  and Texas Instruments Incorporated (the "License").  You may not use this
  Software unless you agree to abide by the terms of the License. The License
  limits your use, and you acknowledge, that the Software may not be modified,
  copied or distributed unless embedded on a Texas Instruments microcontroller
  or used solely and exclusively in conjunction with a Texas Instruments radio
  frequency transceiver, which is integrated into your product.  Other than for
  the foregoing purpose, you may not use, reproduce, copy, prepare derivative
  works of, modify, distribute, perform, display or sell this Software and/or
  its documentation for any purpose.

  YOU FURTHER ACKNOWLEDGE AND AGREE THAT THE SOFTWARE AND DOCUMENTATION ARE
  PROVIDED “AS IS” WITHOUT WARRANTY OF ANY KIND, EITHER EXPRESS OR IMPLIED, 
  INCLUDING WITHOUT LIMITATION, ANY WARRANTY OF MERCHANTABILITY, TITLE, 
  NON-INFRINGEMENT AND FITNESS FOR A PARTICULAR PURPOSE. IN NO EVENT SHALL
  TEXAS INSTRUMENTS OR ITS LICENSORS BE LIABLE OR OBLIGATED UNDER CONTRACT,
  NEGLIGENCE, STRICT LIABILITY, CONTRIBUTION, BREACH OF WARRANTY, OR OTHER
  LEGAL EQUITABLE THEORY ANY DIRECT OR INDIRECT DAMAGES OR EXPENSES
  INCLUDING BUT NOT LIMITED TO ANY INCIDENTAL, SPECIAL, INDIRECT, PUNITIVE
  OR CONSEQUENTIAL DAMAGES, LOST PROFITS OR LOST DATA, COST OF PROCUREMENT
  OF SUBSTITUTE GOODS, TECHNOLOGY, SERVICES, OR ANY CLAIMS BY THIRD PARTIES
  (INCLUDING BUT NOT LIMITED TO ANY DEFENSE THEREOF), OR OTHER SIMILAR COSTS.

  Should you have any questions regarding your right to use this Software,
  contact Texas Instruments Incorporated at www.TI.com. 
**************************************************************************************************/

#ifndef SIMPLEGATTPROFILE_H
#define SIMPLEGATTPROFILE_H

#ifdef __cplusplus
extern "C"
{
#endif

/*********************************************************************
 * INCLUDES
 */

/*********************************************************************
 * CONSTANTS
 */

// Profile Parameters
#define SIMPLEPROFILE_CHAR1                   0  // RW uint8 - Profile Characteristic 1 value 
#define SIMPLEPROFILE_CHAR2                   1  // RW uint8 - Profile Characteristic 2 value
#define SIMPLEPROFILE_CHAR3                   2  // RW uint8 - Profile Characteristic 3 value
#define SIMPLEPROFILE_CHAR4                   3  // RW uint8 - Profile Characteristic 4 value
#define SIMPLEPROFILE_CHAR5                   4  // RW uint8 - Profile Characteristic 5 value
#define SIMPLEPROFILE_CHAR6                   5  // RW uint8 - Profile Characteristic 6 value
#define SIMPLEPROFILE_CHAR7                   6  // RW uint8 - Profile Characteristic 7 value
#define SIMPLEPROFILE_CHAR8                   7  // RW uint8 - Profile Characteristic 8 value
#define SIMPLEPROFILE_CHAR9                   8  // RW uint8 - Profile Characteristic 9 value
#define SIMPLEPROFILE_CHAR10                   9  // RW uint8 - Profile Characteristic 10 value

// Simple Profile Service UUID
#define SIMPLEPROFILE_SERV_UUID               0x1523
    
// Key Pressed UUID
#define SIMPLEPROFILE_CHAR1_UUID            0x1524
#define SIMPLEPROFILE_CHAR2_UUID            0xFFF2
#define SIMPLEPROFILE_CHAR3_UUID            0x0002
#define SIMPLEPROFILE_CHAR4_UUID            0xFFF4
#define SIMPLEPROFILE_CHAR5_UUID            0xFFF5
#define SIMPLEPROFILE_CHAR6_UUID            0x1526
#define SIMPLEPROFILE_CHAR7_UUID            0x152A
#define SIMPLEPROFILE_CHAR8_UUID            0x152C
#define SIMPLEPROFILE_CHAR9_UUID            0x152D
#define SIMPLEPROFILE_CHAR10_UUID           0x0003
  
// Simple Keys Profile Services bit fields
#define SIMPLEPROFILE_SERVICE               0x00000001

// Length of Characteristic 5 in bytes
#define SIMPLEPROFILE_CHAR5_LEN           5
#define SIMPLEPROFILE_CHAR1_LEN           16
#define SIMPLEPROFILE_CHAR2_LEN           2
#define SIMPLEPROFILE_CHAR3_LEN           2
#define SIMPLEPROFILE_CHAR4_LEN           20
#define SIMPLEPROFILE_CHAR6_LEN           8
#define SIMPLEPROFILE_CHAR7_LEN           4 
#define SIMPLEPROFILE_CHAR8_LEN           7
#define SIMPLEPROFILE_CHAR9_LEN           2
#define SIMPLEPROFILE_CHAR10_LEN          20

#define IBEACONPROFILE_CALIBRATEDRSSI_MEM_ID    0x80
#define IBEACONPROFILE_TXPOWER_MEM_ID           0x81
#define IBEACONPROFILE_MAJOR_MEM_ID             0x82
#define IBEACONPROFILE_MINOR_MEM_ID             0x83
#define id5										0x84
#define id6										0x85
#define id7										0x86
#define id8										0x87
#define id9										0x88
#define id10									0x89
#define id11									0x8A
#define id12									0x8B
#define id13									0x8C
#define id14									0x8D
#define id15									0x8E
#define id16									0x8F
// taken from Application unique IDs space (0x80 - 0x8F)



/*********************************************************************
 * TYPEDEFS
 */

  
/*********************************************************************
 * MACROS
 */

/*********************************************************************
 * Profile Callbacks
 */

// Callback when a characteristic value has changed
typedef void (*simpleProfileChange_t)( uint8 paramID );

typedef struct
{
  simpleProfileChange_t        pfnSimpleProfileChange;  // Called when characteristic value changes
} simpleProfileCBs_t;

    

/*********************************************************************
 * API FUNCTIONS 
 */


/*
 * SimpleProfile_AddService- Initializes the Simple GATT Profile service by registering
 *          GATT attributes with the GATT server.
 *
 * @param   services - services to add. This is a bit map and can
 *                     contain more than one service.
 */

extern bStatus_t SimpleProfile_AddService( uint32 services );

/*
 * SimpleProfile_RegisterAppCBs - Registers the application callback function.
 *                    Only call this function once.
 *
 *    appCallbacks - pointer to application callbacks.
 */
extern bStatus_t SimpleProfile_RegisterAppCBs( simpleProfileCBs_t *appCallbacks );

/*
 * SimpleProfile_SetParameter - Set a Simple GATT Profile parameter.
 *
 *    param - Profile parameter ID
 *    len - length of data to right
 *    value - pointer to data to write.  This is dependent on
 *          the parameter ID and WILL be cast to the appropriate 
 *          data type (example: data type of uint16 will be cast to 
 *          uint16 pointer).
 */
extern bStatus_t SimpleProfile_SetParameter( uint8 param, uint8 len, void *value );
  
/*
 * SimpleProfile_GetParameter - Get a Simple GATT Profile parameter.
 *
 *    param - Profile parameter ID
 *    value - pointer to data to write.  This is dependent on
 *          the parameter ID and WILL be cast to the appropriate 
 *          data type (example: data type of uint16 will be cast to 
 *          uint16 pointer).
 */
extern bStatus_t SimpleProfile_GetParameter( uint8 param, void *value );


/*********************************************************************
*********************************************************************/

#ifdef __cplusplus
}
#endif

#endif /* SIMPLEGATTPROFILE_H */