SimpleLink™ CC2745R10-Q1 LaunchPad™ Settings & Resources
The SimpleLink™ CC2745R10-Q1 LaunchPad™ contains a CC2745R10E0WRHARQ1 device.
Jumper Settings
- Close the
LEDsjumpers to enable the on-board LEDs.
TI BoosterPacks™
The following BoosterPacks are used with some driver examples.
BP-BASSENSORSMKII BoosterPack
The TMP116’s power pin is not compatible with this LaunchPad. Use the following modification to enable the TMP116’s usage with the i2ctmp and portable examples.
- Use a jumper wire to connect BoosterPack pin header BP.28 (
T_V+) to BP.1 (3V3).
The OPT3001’s power and interrupt pins are not compatible with this LaunchPad. Use the following modification to enable the OPT3001’s usage with the i2copt3001_cpp example.
- Use a jumper wire to connect BoosterPack pin header BP.27 (
O_V+) to BP.18 (unlabeled). - Use a jumper wire to connect BoosterPack pin header BP.25 (
O_INT) to BP.7 (P05).
BOOSTXL-SHARP128 LCD & SD Card BoosterPack
- BoosterPack pin header BP.8 (
SD_CS) must be jumpered to BP.9 when using the SD card.
CC3200 Audio BoosterPack
The BoosterPack’s DIN, BCLK and FSYNC/WCLK signal pins are not compatible with this LaunchPad. Use one of the following modifications to enable the CC3200 Audio BoosterPack’s usage with the i2secho example.
Option 1: Jumper Wires
Attach the CC3200 Audio BoosterPack to the LP_EM_CC2745R10_Q1 and run jumper wires between the following pins on the CC3200 Audio BoosterPack:
- DIN:
P4.3andP3.9 - BCLK:
P4.9andP3.8 - FSYNC/WCLK:
P4.10andP3.7
See Audio BP User Guide (Figure 2-1), or the diagram below, for information on where these pins are located.
Option 2: Soldering
Alternatively, move 0-ohm resistors on LP_EM_CC2745R10_Q1 to make it compatible with the CC3200 Audio BoosterPack:
- DIN: Remove
R77and mountR76 - BCLK: Remove
R72and mountR75 - FSYNC/WCLK: Remove
R74and mountR74
BP-EM-CS BoosterPack
When using a CC27XX board, connect the P1 and P2 jumpers, and disconnect the P3 and P4 jumpers on the BoosterPack. Add only the VC pins labelled CC27XX in SysConfig and make sure they are configured as output.
The VC pins are used to select the antenna on the BoosterPack:
| RF1 (J2) | RF2 (A1) | RF3 (A2) | RF4 (J3) | |
|---|---|---|---|---|
| VC1 | 0 | 0 | 1 | 1 |
| VC2 | 0 | 1 | 0 | 1 |