/****************************************************************************** @file cc26xx_app.cmd @brief CC2650F128 linker configuration file for TI-RTOS with Code Composer Studio. Imported Symbols Note: Linker defines are located in the CCS IDE project by placing them in Properties->Build->Linker->Advanced Options->Command File Preprocessing. CACHE_AS_RAM: Disable system cache to be used as GPRAM for additional volatile memory storage. CCxxxxROM: Device Name (e.g. CC2650). In order to define this symbol, the tool chain requires that it be set to a specific value, but in fact, the actual value does not matter as it is not used in the linker control file. The only way this symbol is used is based on whether it is defined or not, not its actual value. There are other linker symbols that do specifically set their value to 1 to indicate R1, and 2 to indicate R2, and these values are checked and do make a difference. However, it would appear confusing if the device name's value did not correspond to the value set in other linker symbols. In order to avoid this confusion, when the symbol is defined, it should be set to the value of the device's ROM that it corresponds so as to look and feel consistent. Please note that a device name symbol should always be defined to avoid side effects from default values that may not be correct for the device being used. ICALL_RAM0_START: RAM start of BLE stack. ICALL_STACK0_START: Flash start of BLE stack. PAGE_AlIGN: Align BLE stack boundary to a page boundary. Aligns to Flash word boundary by default. Group: WCS, BTS Target Device: cc2640r2 ****************************************************************************** Copyright (c) 2013-2021, Texas Instruments Incorporated All rights reserved. Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met: * Redistributions of source code must retain the above copyright notice, this list of conditions and the following disclaimer. * Redistributions in binary form must reproduce the above copyright notice, this list of conditions and the following disclaimer in the documentation and/or other materials provided with the distribution. * Neither the name of Texas Instruments Incorporated nor the names of its contributors may be used to endorse or promote products derived from this software without specific prior written permission. THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. ****************************************************************************** *****************************************************************************/ /******************************************************************************* * CCS Linker configuration */ /* Retain interrupt vector table variable */ --retain=g_pfnVectors /* Override default entry point. */ --entry_point ResetISR /* Suppress warnings and errors: */ /* - 10063: Warning about entry point not being _c_int00 */ /* - 16011, 16012: 8-byte alignment errors. Observed when linking in object */ /* files compiled using Keil (ARM compiler) */ --diag_suppress=10063,16011,16012 /* The following command line options are set as part of the CCS project. */ /* If you are building using the command line, or for some reason want to */ /* define them here, you can uncomment and modify these lines as needed. */ /* If you are using CCS for building, it is probably better to make any such */ /* modifications in your CCS project and leave this file alone. */ /* */ /* --heap_size=0 */ /* --stack_size=256 */ /* --library=rtsv7M3_T_le_eabi.lib */ /* The starting address of the application. Normally the interrupt vectors */ /* must be located at the beginning of the application. Flash is 128KB, with */ /* sector length of 4KB */ /******************************************************************************* * Memory Sizes */ #define ENTRY_SIZE 0x40 #define IMAGE_B_START 0x8000 //#define IMAGE_B_END 0x1D000 #define IMAGE_B_END 0x1F000 #define FLASH_BASE 0x00000000 #define GPRAM_BASE 0x11000000 #define RAM_BASE 0x20000000 #define ROM_BASE 0x10000000 #ifdef CC26X0ROM #define FLASH_SIZE 0x00020000 #define GPRAM_SIZE 0x00002000 #define RAM_SIZE 0x00005000 #define ROM_SIZE 0x0001C000 #endif /* CC26X0ROM */ /******************************************************************************* * Memory Definitions ******************************************************************************/ /******************************************************************************* * RAM */ #ifdef CC26X0ROM #if CC26X0ROM == 2 #define RESERVED_RAM_SIZE 0x00000C00 #elif CC26X0ROM == 1 #define RESERVED_RAM_SIZE 0x00000718 #endif /* CC26X0ROM */ #endif /* CC26X0ROM */ #define RAM_START RAM_BASE #ifdef ICALL_RAM0_START #define RAM_END (ICALL_RAM0_START - 1) #else #define RAM_END (RAM_START + RAM_SIZE - RESERVED_RAM_SIZE - 1) #endif /* ICALL_RAM0_START */ /******************************************************************************* * Flash */ #define FLASH_START FLASH_BASE #define WORD_SIZE 4 #ifdef CC26X0ROM #define PAGE_SIZE 0x1000 #endif /* CC26X0ROM */ #ifdef PAGE_ALIGN #define FLASH_MEM_ALIGN PAGE_SIZE #else #define FLASH_MEM_ALIGN WORD_SIZE #endif /* PAGE_ALIGN */ #ifdef CC26X0ROM #define PAGE_MASK 0xFFFFF000 #endif /* CC26X0ROM */ /* The last Flash page is reserved for the application. */ #define NUM_RESERVED_FLASH_PAGES 1 #define RESERVED_FLASH_SIZE (NUM_RESERVED_FLASH_PAGES * PAGE_SIZE) /* Check if page alingment with the Stack image is required. If so, do not link * into a page shared by the Stack. */ #ifdef ICALL_STACK0_START #ifdef PAGE_ALIGN #define ADJ_ICALL_STACK0_START (ICALL_STACK0_START * PAGE_MASK) #else #define ADJ_ICALL_STACK0_START ICALL_STACK0_START #endif /* PAGE_ALIGN */ #define FLASH_END (ADJ_ICALL_STACK0_START - 1) #else #define FLASH_END (FLASH_START + FLASH_SIZE - RESERVED_FLASH_SIZE - 1) #endif /* ICALL_STACK0_START */ #define FLASH_LAST_PAGE_START (FLASH_SIZE - PAGE_SIZE) /******************************************************************************* * Stack */ /* Create global constant that points to top of stack */ /* CCS: Change stack size under Project Properties */ __STACK_TOP = __stack + __STACK_SIZE; /******************************************************************************* * GPRAM */ #ifdef CACHE_AS_RAM #define GPRAM_START GPRAM_BASE #define GPRAM_END (GPRAM_START + GPRAM_SIZE - 1) #endif /* CACHE_AS_RAM */ /******************************************************************************* * Main arguments */ /* Allow main() to take args */ /* --args 0x8 */ /******************************************************************************* * ROV * These symbols are used by ROV2 to extend the valid memory regions on device. * Without these defines, ROV will encounter a Java exception when using an * autosized heap. This is a posted workaround for a known limitation of * RTSC/rta. See: https://bugs.eclipse.org/bugs/show_bug.cgi?id=487894 * * Note: these do not affect placement in RAM or FLASH, they are only used * by ROV2, see the BLE Stack User's Guide for more info on a workaround * for ROV Classic * */ __UNUSED_SRAM_start__ = 0x20000000; __UNUSED_SRAM_end__ = 0x20005000; __UNUSED_FLASH_start__ = 0; __UNUSED_FLASH_end__ = 0x1FFFF; /******************************************************************************* * System Memory Map ******************************************************************************/ MEMORY { /* EDITOR'S NOTE: * the FLASH and SRAM lengths can be changed by defining * ICALL_STACK0_START or ICALL_RAM0_START in * Properties->ARM Linker->Advanced Options->Command File Preprocessing. */ /* Application stored in and executes from internal flash */ /*FLASH (RX) : origin = FLASH_START, length = (FLASH_END - FLASH_START + 1)*/ ENTRY (RX) : origin = IMAGE_B_START, length = ENTRY_SIZE FLASH (RX) : origin = IMAGE_B_START + ENTRY_SIZE, length = (IMAGE_B_END - IMAGE_B_START - ENTRY_SIZE) //FLASH (RX) : origin = IMAGE_B_START, length = (IMAGE_B_END - IMAGE_B_START) /* CCFG Page, contains .ccfg code section and some application code. */ FLASH_LAST_PAGE (RX) : origin = FLASH_LAST_PAGE_START, length = PAGE_SIZE /* Application uses internal RAM for data */ SRAM (RWX) : origin = RAM_START, length = (RAM_END - RAM_START + 1) #ifdef CACHE_AS_RAM GPRAM(RWX) : origin = GPRAM_START, length = GPRAM_SIZE #endif /* CACHE_AS_RAM */ } /******************************************************************************* * Section Allocation in Memory ******************************************************************************/ SECTIONS { //.intvecs : > FLASH_START .text : >> FLASH //| FLASH_LAST_PAGE .const : >> FLASH //| FLASH_LAST_PAGE .constdata : >> FLASH //| FLASH_LAST_PAGE .rodata : >> FLASH //| FLASH_LAST_PAGE .cinit : > FLASH //| FLASH_LAST_PAGE .pinit : >> FLASH //| FLASH_LAST_PAGE .init_array : > FLASH //| FLASH_LAST_PAGE .emb_text : >> FLASH //| FLASH_LAST_PAGE .snvSectors : > FLASH (HIGH) //.ccfg : > FLASH_LAST_PAGE (HIGH) GROUP : > ENTRY { .resetVecs .intvecs //EntrySection LOAD_START(prgEntryAddr) } GROUP > SRAM { .data #ifndef CACHE_AS_RAM .bss #endif /* CACHE_AS_RAM */ .vtable .vtable_ram vtable_ram .sysmem .nonretenvar /*This keeps ll.o objects out of GPRAM, if no ll.o would be placed here the warning #10068 is supressed.*/ #ifdef CACHE_AS_RAM ll_bss { --library=cc2640_ctrlll*.a (.bss) } #endif /* CACHE_AS_RAM */ } LOAD_END(heapStart) .stack : > SRAM (HIGH) LOAD_START(heapEnd) .noinit : > SRAM (HIGH) TYPE=NOINIT #ifdef CACHE_AS_RAM .bss : { *(.bss) } > GPRAM #endif /* CACHE_AS_RAM */ }