/*************DAC REGISTER VALUES*********/ (0x30,0,0); (0x30,1,1); (0x30,0x04,0x00); (0x30,0x0b,0x81); (0x30,0x0c,0x82); (0x30,0x0d,0x00); (0x30,0x0e,0x80); (0x30,0x1b,0x00); (0x30,0x1c,0x00); (0x30,0x3c,0x08); (0x30,0,0); (0x30,0x1f,0x00); (0x30,0x20,0x00); (0x30,0x21,0x00); (0x30,0x25,0xCC); (0x30,0x26,0x00); (0x30,0x3B,0x0A); (0x30,0x0f,0x02); (0x30,0x10,0x00); (0x30,0x11,0x08); (0x30,0x15,0x01); (0x30,0x16,0x00); (0x30,0x3E,0x00); (0x30,0,1); (0x30,1,8); (0x30,2,0); (0x30,0x7b,1); (0x30,14,0x18); (0x30,10,0x4B); (0x30,3,0); (0x30,4,0); (0x30,0x09,0x08) (0x30,0x0E,18); (0x30,0x12,0); (0x30,18,0x1B); (0x30,0,0); (0x30,0x3f,0xD6); (0x30,0x40,0x00); (0x30,0x41,10); (0x30,0x42,10); /*********ADC REGISTER VALUES**********/ (0x30,0,0); (0x30,1,1); (0x30,0x15,0x01); (0x30,0x16,0x00); (0x30,0x0f,0x02); (0x30,0x10,0x00); (0x30,0x12,0x81); (0x30,0x13,0x82); (0x30,0x14,0x80); (0x30,0x0f,0x02); (0x30,0x10,0x00); (0x30,0x11,0x08); (0x30,0x15,0x01); (0x30,0x16,0x00); (0x30,0x3E,0x00); (0x30,0x24,0xee); (0x30,0,1); (0x30,0x3D,0xff); (0x30,0x47,0x32); (0x30,0x7B,0x01); (0x30,52,0x30); (0x30,54,0x03); (0x30,55,0x03); (0x30,57,0x03); (0x30,0,0); (0x30,0x51,0xC0); (0x30,0x52,0x00); (0x30,0x1d,0x11);