---------------------------------------------------------------------------------- -- Company: -- Engineer: -- -- Create Date: 20:04:18 08/19/2017 -- Design Name: -- Module Name: DAC8775_SPI - Behavioral -- Project Name: -- Target Devices: -- Tool versions: -- Description: -- -- Dependencies: -- -- Revision: -- Revision 0.01 - File Created -- Additional Comments: -- ---------------------------------------------------------------------------------- ---------------------------------------------------------------------------------- -- Company: -- Engineer: -- -- Create Date: 15:03:30 02/06/2014 -- Design Name: -- Module Name: AD9361_SPI - Behavioral -- Project Name: -- Target Devices: -- Tool versions: -- Description: -- -- Dependencies: -- -- Revision: -- Revision 0.01 - File Created -- Additional Comments: -- ---------------------------------------------------------------------------------- library IEEE; use IEEE.STD_LOGIC_1164.ALL; use IEEE.STD_LOGIC_ARITH.ALL; use IEEE.STD_LOGIC_UNSIGNED.ALL; -- Uncomment the following library declaration if using -- arithmetic functions with Signed or Unsigned values --use IEEE.NUMERIC_STD.ALL; -- Uncomment the following library declaration if instantiating -- any Xilinx primitives in this code. --library UNISIM; --use UNISIM.VComponents.all; entity DAC8775_SPI is Port( clk,rst,en : in std_logic; -- System Clock spi_din : in std_logic; spi_clk : out std_logic; -- SPI Clock spi_en : out std_logic; ldac : out std_logic; --LDAC signal spi_dout : out std_logic; spi_addr : in std_logic_vector (7 downto 0); spi_data : in std_logic_vector (15 downto 0); spi_rd_data : out std_logic_vector (15 downto 0); data_rdy : out std_logic ); end DAC8775_SPI; architecture Behavioral of DAC8775_SPI is type states is (idle, start_spi,write_high, write_low, read_high, read_low, rd_data_high, rd_data_low,write_low_end,write_high_end,rd_data_low_end); signal c_s,n_s : states; signal count : integer range 0 to 24; signal rd_count : integer range 0 to 24; signal addr_temp : std_logic_vector (7 downto 0); signal rd_data_temp : std_logic_vector (15 downto 0); signal wr_data_temp : std_logic_vector (15 downto 0); signal send_temp : std_logic_vector (23 downto 0); --attribute KEEP : string; --attribute KEEP of spi_addr : signal is "TRUE"; begin process(clk,rst) begin If rising_edge (clk) then if (rst='0') then spi_clk <='0'; spi_en <='1'; ldac <='0'; spi_dout <='0'; spi_rd_data <= (others=>'0'); data_rdy <= '0'; count <= 23; rd_count <= 0; rd_data_temp <= (others=>'0'); addr_temp <= spi_addr; send_temp <= addr_temp & wr_data_temp; wr_data_temp <= spi_data; data_rdy <='0'; else c_s <= n_s; case n_s is when idle => spi_clk <='0'; spi_en <='1'; ldac <='0'; spi_dout <='0'; addr_temp <= spi_addr; wr_data_temp <= spi_data; spi_rd_data <= rd_data_temp; send_temp <= addr_temp & wr_data_temp; count <= 23; rd_count <= 15; data_rdy <= '1'; when start_spi => send_temp <= addr_temp & wr_data_temp; count <= 23; rd_count <= 15; spi_en <='0'; ldac <='1'; when write_high => spi_clk <='1'; spi_dout <= send_temp(count); when write_low => spi_clk <='0'; count <= count -1; when write_high_end => spi_clk <= '1'; spi_dout <= send_temp(count); when write_low_end => spi_clk <='0'; when read_high => spi_clk <='1'; spi_dout <= send_temp(count); data_rdy <='0'; when read_low => spi_clk <='0'; spi_dout <= send_temp(count); count <= count - 1; data_rdy <='0'; when rd_data_high=> spi_clk <='1'; spi_dout <= '0'; rd_data_temp(rd_count)<= spi_din; data_rdy <='0'; when rd_data_low => spi_clk <='0'; rd_count <= rd_count-1; data_rdy <='0'; when rd_data_low_end => spi_clk <='0'; data_rdy <='0'; when others => spi_clk <='0'; spi_en <='1'; ldac <='0'; spi_dout <='0'; spi_rd_data <= (others=>'0'); data_rdy <= '0'; count <= 23; rd_count <= 0; rd_data_temp <= (others=>'0'); addr_temp <= (others =>'0'); wr_data_temp <= (others =>'0'); send_temp <= (others =>'0'); data_rdy <='0'; end case; end if; End If; end process; -----------STATE MACHINE OPERATION----------- process (c_s,en,addr_temp,count,rd_count ) begin n_s <= c_s; case c_s is when idle => if (en='1') then n_s <= start_spi; else n_S <= idle; end if; when start_spi => if (addr_temp(7)='0') then n_s <= write_high; else n_s <= read_high; end if; when write_high => n_s <= write_low; when write_low => if (count =0) then n_s <= write_high_end; else n_s <= write_high; end if; when write_high_end => n_s <=write_low_end; when write_low_end => n_s <= idle; when read_high => n_s <= read_low; when read_low => if (count <= 15) then n_s <= rd_data_high; else n_s <= read_high; end if; when rd_data_high => if (rd_count <= 0) then n_s <= rd_data_low_end; else n_S <= rd_data_low; end if; when rd_data_low => n_s <= rd_data_high; when rd_data_low_end => n_s <= idle; when others => n_s <= idle; end case; end process; end Behavioral;