[Start: Texas Instruments XDS2xx USB Debug Probe_0] Execute the command: %ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -S integrity [Result] -----[Print the board config pathname(s)]------------------------------------ C:\Users\Servo\AppData\Local\TEXASI~1\CCS\ ti\2\0\BrdDat\testBoard.dat -----[Print the reset-command software log-file]----------------------------- This utility has selected a 560/2xx-class product. This utility will load the program 'xds2xxu.out'. The library build date was 'May 30 2018'. The library build time was '22:31:29'. The library package version is '8.0.27.9'. The library component version is '35.35.0.0'. The controller does not use a programmable FPGA. The controller has a version number of '13' (0x0000000d). The controller has an insertion length of '0' (0x00000000). This utility will attempt to reset the controller to enter SWD mode. -----[Print the reset-command hardware log-file]----------------------------- This emulator does not create a reset log-file. -----[Perform the SWD Mode Integrity test]----------------------------------- This test will read the IDCODE register 1 time. The IDCODE register value is 0x0bb11477. The SWD Mode Integrity test has succeeded. [End: Texas Instruments XDS2xx USB Debug Probe_0]