U-Boot SPL 2024.04-ti-gd1e3aedf631f (Jan 12 2025 - 17:12:54 +0000) SYSFW ABI: 4.0 (firmware rev 0x000a '10.0.8--v10.00.08 (Fiery Fox)') EEPROM not available at 0x50, trying to read at 0x51 Reading on-board EEPROM at 0x51 failed -121 SPL initial stack usage: 13456 bytes Trying to boot from MMC2 Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Loading Environment from nowhere... OK Starting ATF on ARM64 core... NOTICE: BL31: v2.10.0(release):v2.10.0-367-g00f1ec6b87-dirty NOTICE: BL31: Built : 16:09:05, Feb 9 2024 ERROR: Timeout waiting for thread SP_RESPONSE to fill ERROR: Thread SP_RESPONSE verification failed (-60) ERROR: Message receive failed (-60) ERROR: Failed to get response (-60) ERROR: Transfer send failed (-60) ERROR: Timeout waiting for thread SP_RESPONSE to fill ERROR: Thread SP_RESPONSE verification failed (-60) ERROR: Message receive failed (-60) ERROR: Failed to get response (-60) ERROR: Transfer send failed (-60) ERROR: Unable to query firmware capabilities (-60) I/TC: I/TC: OP-TEE version: 4.2.0-dev (gcc version 13.3.0 (GCC)) #1 Fri Apr 12 09:51:21 UTC 2024 aarch64 I/TC: WARNING: This OP-TEE configuration might be insecure! I/TC: WARNING: Please check https://optee.readthedocs.io/en/latest/architecture/porting_guidelines.html I/TC: Primary CPU initializing I/TC: GIC redistributor base address not provided I/TC: Assuming default GIC group status and modifier E/TC:0 0 k3_sec_proxy_verify_thread:108 Queue is busy E/TC:0 0 k3_sec_proxy_recv:196 Thread SEC_PROXY_RESPONSE_THREAD verification failed. ret = -65523 E/TC:0 0 ti_sci_get_response:101 Message receive failed (-65523) E/TC:0 0 ti_sci_do_xfer:150 Failed to get response (-65523) E/TC:0 0 ti_sci_init:486 Unable to communicate with control firmware (-65523) E/TC:0 0 call_initcalls:43 Initcall __text_start + 0x00070af8 failed E/TC:0 0 k3_sec_proxy_verify_thread:108 Queue is busy E/TC:0 0 k3_sec_proxy_recv:196 Thread SEC_PROXY_RESPONSE_THREAD verification failed. ret = -65523 E/TC:0 0 ti_sci_get_response:101 Message receive failed (-65523) E/TC:0 0 ti_sci_do_xfer:150 Failed to get response (-65523) E/TC:0 0 k3_sec_proxy_verify_thread:108 Queue is busy E/TC:0 0 k3_sec_proxy_recv:196 Thread SEC_PROXY_RESPONSE_THREAD verification failed. ret = -65523 E/TC:0 0 ti_sci_get_response:101 Message receive failed (-65523) E/TC:0 0 ti_sci_do_xfer:150 Failed to get response (-65523) E/TC:0 0 k3_sec_proxy_verify_thread:108 Queue is busy E/TC:0 0 k3_sec_proxy_recv:196 Thread SEC_PROXY_RESPONSE_THREAD verification failed. ret = -65523 E/TC:0 0 ti_sci_get_response:101 Message receive failed (-65523) E/TC:0 0 ti_sci_do_xfer:150 Failed to get response (-65523) E/TC:0 0 tee_otp_get_hw_unique_key:97 Could not get HUK E/TC:0 0 call_initcalls:43 Initcall __text_start + 0x00070b20 failed I/TC: Activated SA2UL device E/TC:0 0 k3_sec_proxy_verify_thread:108 Queue is busy E/TC:0 0 k3_sec_proxy_recv:196 Thread SEC_PROXY_RESPONSE_THREAD verification failed. ret = -65523 E/TC:0 0 ti_sci_get_response:101 Message receive failed (-65523) E/TC:0 0 ti_sci_do_xfer:150 Failed to get response (-65523) E/TC:0 0 k3_sec_proxy_verify_thread:108 Queue is busy E/TC:0 0 k3_sec_proxy_recv:196 Thread SEC_PROXY_RESPONSE_THREAD verification failed. ret = -65523 E/TC:0 0 ti_sci_get_response:101 Message receive failed (-65523) E/TC:0 0 ti_sci_do_xfer:150 Failed to get response (-65523) E/TC:0 0 sa2ul_init:106 Could not change TRNG firewall owner E/TC:0 0 call_initcalls:43 Initcall __text_start + 0x00070b28 failed E/TC:0 0 E/TC:0 0 Core data-abort at address 0x14 (translation fault) E/TC:0 0 esr 0x96000005 ttbr0 0x9e8a2000 ttbr1 0x00000000 cidr 0x0 E/TC:0 0 cpu #0 cpsr 0x600003c4 E/TC:0 0 x0 000000009e875000 x1 0000000000000000 E/TC:0 0 x2 0000000000000000 x3 0000000000000000 E/TC:0 0 x4 0000000000000050 x5 000000009e892d70 E/TC:0 0 x6 ffffffffffffffb0 x7 0000000000010cb0 E/TC:0 0 x8 0000000000010cb0 x9 000000009e892f80 E/TC:0 0 x10 000000009e882070 x11 0000000000000008 E/TC:0 0 x12 0000000000000000 x13 000000009e8a3e60 E/TC:0 0 x14 0000000000000000 x15 0000000000000000 E/TC:0 0 x16 000000009e81cb90 x17 0000000000000000 E/TC:0 0 x18 0000000000000000 x19 000000009e8a41e0 E/TC:0 0 x20 000000009e8a41e8 x21 000000009e875000 E/TC:0 0 x22 000000009e875000 x23 000000009e875f00 E/TC:0 0 x24 000000009e874dc0 x25 0000000000000000 E/TC:0 0 x26 0000000000000000 x27 0000000000000000 E/TC:0 0 x28 0000000000000000 x29 000000009e8a4170 E/TC:0 0 x30 000000009e817350 elr 000000009e817360 E/TC:0 0 sp_el0 000000009e8a4170 E/TC:0 0 TEE load address @ 0x9e800000 E/TC:0 0 Call stack: E/TC:0 0 0x9e817360 E/TC:0 0 0x9e807ca0 E/TC:0 0 0x9e822530 E/TC:0 0 0x9e807e9c E/TC:0 0 Panic 'unhandled pageable abort' at /usr/src/debug/optee-os/4.2.0+git/core/arch/arm/kernel/abort.c:582 E/TC:0 0 TEE load address @ 0x9e800000 E/TC:0 0 Call stack: E/TC:0 0 0x9e80817c E/TC:0 0 0x9e81eff4 E/TC:0 0 0x9e807884 E/TC:0 0 0x9e804a68