U-Boot SPL 2026.01 (Jun 15 2026 - 15:34:48 +0530)
Resetting on cold boot to workaround ErrataID:i2331
Please resend tiboot3.bin in case of UART/DFU boot
resetting ...

U-Boot SPL 2026.01 (Jun 15 2026 - 15:34:48 +0530)
SYSFW ABI: 4.0 (firmware rev 0x000b '11.1.5--v11.01.05 (Fancy Rat)')
EEPROM not available at 0x50, trying to read at 0x51
Reading on-board EEPROM at 0x51 failed -121
Set clock rates for '/a53@0', CPU: 1000MHz at Speed Grade 'S'
SPL initial stack usage: 13552 bytes
Trying to boot from SPI
Authentication passed
Authentication passed
Loading Environment from nowhere... OK
Authentication passed
Authentication passed
Starting ATF on ARM64 core...

NOTICE:  BL31: v2.14.0(release):76500ceaeefcda967d8a1f4e30bb04f9fe0425a2
NOTICE:  BL31: Built : 14:26:48, Jun 13 2026

U-Boot SPL 2026.01 (Jun 16 2026 - 11:28:59 +0530)
SYSFW ABI: 4.0 (firmware rev 0x000b '11.1.5--v11.01.05 (Fancy Rat)')
EEPROM not available at 0x50, trying to read at 0x51
Reading on-board EEPROM at 0x51 failed -121
Trying to boot from SPI
Authentication passed
Authentication passed


U-Boot 2026.01 (Jun 16 2026 - 11:32:12 +0530)

SoC:   AM64X SR2.0 HS-FS
Reset reason: RST
Model: Texas Instruments AM642 EVM
EEPROM not available at 0x50, trying to read at 0x51
Reading on-board EEPROM at 0x51 failed -121
DRAM:  475 MiB (total 512 MiB)
Timed out in wait_for_bb: status=1000
Timed out in wait_for_bb: status=1000
Timed out in wait_for_bb: status=1000
pca953x gpio@22: Error reading output register
Core:  111 devices, 37 uclasses, devicetree: separate
MMC:   mmc@fa10000: 0, mmc@fa00000: 1
Loading Environment from nowhere... OK
In:    serial@2800000
Out:   serial@2800000
Err:   serial@2800000
EEPROM not available at 0x50, trying to read at 0x51
Reading on-board EEPROM at 0x51 failed -121
Net:   Could not get PHY for mdio@f00: addr 0
am65_cpsw_nuss_port ethernet@8000000port@1: phy_connect() failed

Warning: icssg1-eth-port@0 (eth2) using random MAC address - 22:99:f6:d3:f9:e9
eth2: icssg1-eth-port@0
Hit any key to stop autoboot:  0 
=> 
=> 
=> 
=> sf read ${loadaddr} 0x780000 0xA00000
No SPI flash selected. Please run `sf probe'
=> sf probe
SF: Detected w25q512jvfim with page size 256 Bytes, erase size 64 KiB, total 64 MiB
=> sf read ${loadaddr} 0x780000 0xA00000
device 0 offset 0x780000, size 0xa00000
SF: 10485760 bytes @ 0x780000 Read: OK
=> sf read ${fdtaddr} 0x1180000 0x40000
device 0 offset 0x1180000, size 0x40000
SF: 262144 bytes @ 0x1180000 Read: OK
=> setenv bootargs 'console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 root=/dev/mtdblock7 ro rootfstype=squashfs rootwait'
=> unzip ${loadaddr} 0x90000000
Uncompressed size: 19065344 = 0x122EA00
=> booti 0x90000000 - ${fdt
  ${fdt_addr_r} ${fdtaddr} ${fdtcontroladdr} ${fdtfile} ${fdtoverlay_addr_r}
=> booti 0x90000000 - ${fdtaddr} 
## Flattened Device Tree blob at 88000000
   Booting using the fdt blob at 0x88000000
Working FDT set to 88000000
   Loading Device Tree to 000000009a949000, end 000000009a95c01f ... OK
Working FDT set to 9a949000

Starting kernel ...

[    0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
[    0.000000] Linux version 6.18.13 (sqm@2sqmx4q2) (aarch64-buildroot-linux-gnu-gcc.br_real (Buildroot 2026.02) 14.3.0, GNU ld (GNU Binutils) 2.44) #4 SMP PREEMPT Mon Jun 15 12:46:33 IST 2026
[    0.000000] KASLR enabled
[    0.000000] Machine model: Texas Instruments AM642 EVM
[    0.000000] earlycon: ns16550a0 at MMIO32 0x0000000002800000 (options '')
[    0.000000] printk: legacy bootconsole [ns16550a0] enabled
[    0.000000] efi: UEFI not found.
[    0.000000] OF: reserved mem: 0x000000009e800000..0x000000009fffffff (24576 KiB) nomap non-reusable optee@9e800000
[    0.000000] Reserved memory: created DMA memory pool at 0x000000009c000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node memory@9c000000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x000000009c000000..0x000000009c0fffff (1024 KiB) nomap non-reusable memory@9c000000
[    0.000000] Reserved memory: created DMA memory pool at 0x000000009c100000, size 15 MiB
[    0.000000] OF: reserved mem: initialized node memory@9c100000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x000000009c100000..0x000000009cffffff (15360 KiB) nomap non-reusable memory@9c100000
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a1000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node memory@a1000000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000a1000000..0x00000000a10fffff (1024 KiB) nomap non-reusable memory@a1000000
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a1100000, size 15 MiB
[    0.000000] OF: reserved mem: initialized node memory@a1100000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000a1100000..0x00000000a1ffffff (15360 KiB) nomap non-reusable memory@a1100000
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a2000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node memory@a2000000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000a2000000..0x00000000a20fffff (1024 KiB) nomap non-reusable memory@a2000000
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a2100000, size 15 MiB
[    0.000000] OF: reserved mem: initialized node memory@a2100000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000a2100000..0x00000000a2ffffff (15360 KiB) nomap non-reusable memory@a2100000
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a3000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node memory@a3000000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000a3000000..0x00000000a30fffff (1024 KiB) nomap non-reusable memory@a3000000
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a3100000, size 15 MiB
[    0.000000] OF: reserved mem: initialized node memory@a3100000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000a3100000..0x00000000a3ffffff (15360 KiB) nomap non-reusable memory@a3100000
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a4000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node memory@a4000000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000a4000000..0x00000000a40fffff (1024 KiB) nomap non-reusable memory@a4000000
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a4100000, size 15 MiB
[    0.000000] OF: reserved mem: initialized node memory@a4100000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000a4100000..0x00000000a4ffffff (15360 KiB) nomap non-reusable memory@a4100000
[    0.000000] OF: reserved mem: 0x00000000a5000000..0x00000000a57fffff (8192 KiB) nomap non-reusable memory@a5000000
[    0.000000] Zone ranges:
[    0.000000]   DMA      [mem 0x0000000080000000-0x000000009fffffff]
[    0.000000]   DMA32    empty
[    0.000000]   Normal   empty
[    0.000000] Movable zone start for each node
[    0.000000] Early memory node ranges
[    0.000000]   node   0: [mem 0x0000000080000000-0x000000009bffffff]
[    0.000000]   node   0: [mem 0x000000009c000000-0x000000009cffffff]
[    0.000000]   node   0: [mem 0x000000009d000000-0x000000009e7fffff]
[    0.000000]   node   0: [mem 0x000000009e800000-0x000000009fffffff]
[    0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x000000009fffffff]
[    0.000000] cma: Reserved 32 MiB at 0x0000000098800000
[    0.000000] psci: probing for conduit method from DT.
[    0.000000] psci: PSCIv1.1 detected in firmware.
[    0.000000] psci: Using standard PSCI v0.2 function IDs
[    0.000000] psci: Trusted OS migration not required
[    0.000000] psci: SMC Calling Convention v1.5
[    0.000000] percpu: Embedded 22 pages/cpu s51160 r8192 d30760 u90112
[    0.000000] Detected VIPT I-cache on CPU0
[    0.000000] CPU features: detected: GICv3 CPU interface
[    0.000000] CPU features: kernel page table isolation forced ON by KASLR
[    0.000000] CPU features: detected: Kernel page table isolation (KPTI)
[    0.000000] CPU features: detected: ARM erratum 845719
[    0.000000] alternatives: applying boot alternatives
[    0.000000] Kernel command line: console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 root=/dev/mtdblock7 ro rootfstype=squashfs rootwait
[    0.000000] printk: log buffer data + meta data: 131072 + 458752 = 589824 bytes
[    0.000000] Dentry cache hash table entries: 65536 (order: 7, 524288 bytes, linear)
[    0.000000] Inode-cache hash table entries: 32768 (order: 6, 262144 bytes, linear)
[    0.000000] software IO TLB: SWIOTLB bounce buffer size adjusted to 0MB
[    0.000000] software IO TLB: area num 1.
[    0.000000] software IO TLB: mapped [mem 0x000000009dd40000-0x000000009ddc0000] (0MB)
[    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 131072
[    0.000000] mem auto-init: stack:all(zero), heap alloc:off, heap free:off
[    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
[    0.000000] rcu: Preemptible hierarchical RCU implementation.
[    0.000000] rcu: 	RCU event tracing is enabled.
[    0.000000] rcu: 	RCU restricting CPUs from NR_CPUS=512 to nr_cpu_ids=1.
[    0.000000] 	Trampoline variant of Tasks RCU enabled.
[    0.000000] 	Tracing variant of Tasks RCU enabled.
[    0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[    0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=1
[    0.000000] RCU Tasks: Setting shift to 0 and lim to 1 rcu_task_cb_adjust=1 rcu_task_cpu_ids=1.
[    0.000000] RCU Tasks Trace: Setting shift to 0 and lim to 1 rcu_task_cb_adjust=1 rcu_task_cpu_ids=1.
[    0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[    0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[    0.000000] GICv3: 256 SPIs implemented
[    0.000000] GICv3: 0 Extended SPIs implemented
[    0.000000] Root IRQ handler: gic_handle_irq
[    0.000000] GICv3: GICv3 features: 16 PPIs
[    0.000000] GICv3: GICD_CTLR.DS=0, SCR_EL3.FIQ=1
[    0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000001840000
[    0.000000] ITS [mem 0x01820000-0x0182ffff]
[    0.000000] GIC: enabling workaround for ITS: Socionext Synquacer pre-ITS
[    0.000000] ITS@0x0000000001820000: Devices Table too large, reduce ids 20->19
[    0.000000] ITS@0x0000000001820000: allocated 524288 Devices @80800000 (flat, esz 8, psz 64K, shr 0)
[    0.000000] ITS: using cache flushing for cmd queue
[    0.000000] GICv3: using LPI property table @0x0000000080030000
[    0.000000] GIC: using cache flushing for LPI property table
[    0.000000] GICv3: CPU0: using allocated LPI pending table @0x0000000080040000
[    0.000000] rcu: srcu_init: Setting srcu_struct sizes based on contention.
[    0.000000] arch_timer: cp15 timer running at 200.00MHz (phys).
[    0.000000] clocksource: arch_sys_counter: mask: 0x3ffffffffffffff max_cycles: 0x2e2049d3e8, max_idle_ns: 440795210634 ns
[    0.000001] sched_clock: 58 bits at 200MHz, resolution 5ns, wraps every 4398046511102ns
[    0.008837] Console: colour dummy device 80x25
[    0.013476] Calibrating delay loop (skipped), value calculated using timer frequency.. 400.00 BogoMIPS (lpj=800000)
[    0.024159] pid_max: default: 32768 minimum: 301
[    0.029018] LSM: initializing lsm=capability,selinux
[    0.034168] SELinux:  Initializing.
[    0.038363] Mount-cache hash table entries: 1024 (order: 1, 8192 bytes, linear)
[    0.045845] Mountpoint-cache hash table entries: 1024 (order: 1, 8192 bytes, linear)
[    0.056668] rcu: Hierarchical SRCU implementation.
[    0.061664] rcu: 	Max phase no-delay instances is 1000.
[    0.067953] EFI services will not be available.
[    0.072884] smp: Bringing up secondary CPUs ...
[    0.077566] smp: Brought up 1 node, 1 CPU
[    0.081706] SMP: Total of 1 processors activated.
[    0.086534] CPU: All CPU(s) started at EL2
[    0.090734] CPU features: detected: 32-bit EL0 Support
[    0.095991] CPU features: detected: CRC32 instructions
[    0.101257] CPU features: detected: PMUv3
[    0.105400] alternatives: applying system-wide alternatives
[    0.111968] Memory: 414252K/524288K available (11840K kernel code, 1210K rwdata, 4080K rodata, 1344K init, 558K bss, 71184K reserved, 32768K cma-reserved)
[    0.127049] devtmpfs: initialized
[    0.142299] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[    0.152373] posixtimers hash table entries: 512 (order: 1, 8192 bytes, linear)
[    0.159795] futex hash table entries: 256 (16384 bytes on 1 NUMA nodes, total 16 KiB, linear).
[    0.169496] 2G module region forced by RANDOMIZE_MODULE_REGION_FULL
[    0.176052] 0 pages in range for non-PLT usage
[    0.176060] 519472 pages in range for PLT usage
[    0.181040] pinctrl core: initialized pinctrl subsystem
[    0.191819] DMI not present or invalid.
[    0.198564] NET: Registered PF_NETLINK/PF_ROUTE protocol family
[    0.206013] DMA: preallocated 128 KiB GFP_KERNEL pool for atomic allocations
[    0.213804] DMA: preallocated 128 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
[    0.222340] DMA: preallocated 128 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
[    0.230538] audit: initializing netlink subsys (disabled)
[    0.236422] audit: type=2000 audit(0.144:1): state=initialized audit_enabled=0 res=1
[    0.244927] thermal_sys: Registered thermal governor 'step_wise'
[    0.244937] thermal_sys: Registered thermal governor 'power_allocator'
[    0.251166] cpuidle: using governor menu
[    0.262072] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[    0.269061] ASID allocator initialised with 32768 entries
[    0.283375] /bus@f4000/interrupt-controller@1800000: Fixed dependency cycle(s) with /bus@f4000/interrupt-controller@1800000
[    0.308450] HugeTLB: registered 1.00 GiB page size, pre-allocated 0 pages
[    0.315475] HugeTLB: 0 KiB vmemmap can be freed for a 1.00 GiB page
[    0.321888] HugeTLB: registered 32.0 MiB page size, pre-allocated 0 pages
[    0.328826] HugeTLB: 0 KiB vmemmap can be freed for a 32.0 MiB page
[    0.335234] HugeTLB: registered 2.00 MiB page size, pre-allocated 0 pages
[    0.342171] HugeTLB: 0 KiB vmemmap can be freed for a 2.00 MiB page
[    0.348578] HugeTLB: registered 64.0 KiB page size, pre-allocated 0 pages
[    0.355516] HugeTLB: 0 KiB vmemmap can be freed for a 64.0 KiB page
[    0.364176] k3-chipinfo 43000014.chipid: Family:AM64X rev:SR2.0 JTAGID[0x1bb3802f] Detected
[    0.376268] iommu: Default domain type: Translated
[    0.381327] iommu: DMA domain TLB invalidation policy: strict mode
[    0.388129] SCSI subsystem initialized
[    0.392278] usbcore: registered new interface driver usbfs
[    0.397931] usbcore: registered new interface driver hub
[    0.403409] usbcore: registered new device driver usb
[    0.409269] pps_core: LinuxPPS API ver. 1 registered
[    0.414361] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[    0.423715] PTP clock support registered
[    0.427764] EDAC MC: Ver: 3.0.0
[    0.431573] scmi_core: SCMI protocol bus registered
[    0.437092] FPGA manager framework
[    0.442337] clocksource: Switched to clocksource arch_sys_counter
[    0.457860] NET: Registered PF_INET protocol family
[    0.463219] IP idents hash table entries: 8192 (order: 4, 65536 bytes, linear)
[    0.471942] tcp_listen_portaddr_hash hash table entries: 256 (order: 0, 4096 bytes, linear)
[    0.480579] Table-perturb hash table entries: 65536 (order: 6, 262144 bytes, linear)
[    0.488520] TCP established hash table entries: 4096 (order: 3, 32768 bytes, linear)
[    0.496479] TCP bind hash table entries: 4096 (order: 5, 131072 bytes, linear)
[    0.504023] TCP: Hash tables configured (established 4096 bind 4096)
[    0.510683] UDP hash table entries: 256 (order: 2, 16384 bytes, linear)
[    0.517481] UDP-Lite hash table entries: 256 (order: 2, 16384 bytes, linear)
[    0.524909] NET: Registered PF_UNIX/PF_LOCAL protocol family
[    0.532463] Initialise system trusted keyrings
[    0.537534] workingset: timestamp_bits=46 max_order=17 bucket_order=0
[    0.544669] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[    0.620476] Key type asymmetric registered
[    0.624704] Asymmetric key parser 'x509' registered
[    0.629811] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 244)
[    0.637721] io scheduler mq-deadline registered
[    0.642398] io scheduler kyber registered
[    0.646552] io scheduler bfq registered
[    0.653818] pinctrl-single 4084000.pinctrl: 33 pins, size 132
[    0.660469] pinctrl-single f4000.pinctrl: 180 pins, size 720
[    0.668573] ledtrig-cpu: registered to indicate activity on CPUs
[    0.681588] Serial: 8250/16550 driver, 12 ports, IRQ sharing enabled
[    0.703538] loop: module loaded
[    0.713512] tun: Universal TUN/TAP device driver, 1.6
[    0.720267] VFIO - User Level meta-driver version: 0.3
[    0.727063] usbcore: registered new interface driver usb-storage
[    0.734043] i2c_dev: i2c /dev entries driver
[    0.739555] sdhci: Secure Digital Host Controller Interface driver
[    0.745970] sdhci: Copyright(c) Pierre Ossman
[    0.750821] sdhci-pltfm: SDHCI platform and OF driver helper
[    0.757435] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
[    0.766048] hw perfevents: enabled with armv8_cortex_a53 PMU driver, 7 (0,8000003f) counters available
[    0.776687] optee: probing for conduit method.
[    0.781349] optee: revision 4.9
[    0.781854] optee: dynamic shared memory is enabled
[    0.791417] random: crng init done
[    0.795124] optee: initialized driver
[    0.800965] Initializing XFRM netlink socket
[    0.805572] NET: Registered PF_PACKET protocol family
[    0.810814] Key type dns_resolver registered
[    0.823953] registered taskstats version 1
[    0.829358] Loading compiled-in X.509 certificates
[    0.850220] ti-sci 44043000.system-controller: ABI: 4.0 (firmware rev 0x000b '11.1.5--v11.01.05 (Fancy Rat)')
[    0.992882] pca953x 0-0038: supply vcc not found, using dummy regulator
[    1.000008] pca953x 0-0038: using no AI
[    1.018404] pca953x 0-0038: failed writing register: -121
[    1.024464] pca953x 0-0038: probe with driver pca953x failed with error -121
[    1.032196] omap_i2c 20000000.i2c: bus 0 rev0.12 at 400 kHz
[    1.040394] pca953x 1-0022: supply vcc not found, using dummy regulator
[    1.047506] pca953x 1-0022: using AI
[    2.058496] pca953x 1-0022: failed writing register: -16
[    2.064204] pca953x 1-0022: probe with driver pca953x failed with error -16
[    2.072075] omap_i2c 20010000.i2c: bus 1 rev0.12 at 400 kHz
[    2.078489] ti-sci-intr bus@f4000:interrupt-controller@a00000: Interrupt Router 3 domain created
[    2.088020] ti-sci-inta 48000000.interrupt-controller: Interrupt Aggregator domain 28 created
[    2.097646] ti-udma 485c0100.dma-controller: Number of rings: 68
[    2.105809] ti-udma 485c0100.dma-controller: Channels: 24 (bchan: 12, tchan: 6, rchan: 6)
[    2.116490] ti-udma 485c0000.dma-controller: Number of rings: 288
[    2.135552] ti-udma 485c0000.dma-controller: Channels: 44 (tchan: 29, rchan: 15)
[    2.147541] printk: legacy console [ttyS2] disabled
[    2.153252] 2800000.serial: ttyS2 at MMIO 0x2800000 (irq = 310, base_baud = 3000000) is a 8250
[    2.162219] printk: legacy console [ttyS2] enabled
[    2.162219] printk: legacy console [ttyS2] enabled
[    2.172010] printk: legacy bootconsole [ns16550a0] disabled
[    2.172010] printk: legacy bootconsole [ns16550a0] disabled
[    2.197829] spi-nor spi0.0: supply vcc not found, using dummy regulator
[    2.215951] 9 fixed-partitions partitions found on MTD device fc40000.spi.0
[    2.223052] Creating 9 MTD partitions on "fc40000.spi.0":
[    2.228486] 0x000000000000-0x000000100000 : "ospi.tiboot3"
[    2.236299] 0x000000100000-0x000000300000 : "ospi.tispl"
[    2.254764] 0x000000300000-0x000000700000 : "ospi.u-boot"
[    2.274724] 0x000000700000-0x000000740000 : "ospi.env"
[    2.282790] 0x000000740000-0x000000780000 : "ospi.env.backup"
[    2.294725] 0x000000780000-0x000001180000 : "ospi.kernel"
[    2.314763] 0x000001180000-0x0000011c0000 : "ospi.dtb"
[    2.321724] 0x0000011c0000-0x000003fc0000 : "ospi.rootfs"
[    2.342750] 0x000003fc0000-0x000004000000 : "ospi.phypattern"
[    2.351943] am65-cpsw-nuss 8000000.ethernet: initializing am65 cpsw nuss version 0x6BA00903, cpsw version 0x6BA80903 Ports: 3 quirks:00000006
[    2.364932] am65-cpsw-nuss 8000000.ethernet: RGMII mode without internal TX delay unsupported; please fix your Device Tree
[    2.376213] am65-cpsw-nuss 8000000.ethernet: RGMII mode without internal TX delay unsupported; please fix your Device Tree
[    2.387320] am65-cpsw-nuss 8000000.ethernet: Use random MAC address
[    2.394405] davinci_mdio 8000f00.mdio: Configuring MDIO in manual mode
[    2.434328] davinci_mdio 8000f00.mdio: davinci mdio revision 9.7, bus freq 1000000
[    2.442236] mdio_bus 8000f00.mdio: MDIO device at address 0 is missing.
[    2.449108] am65-cpsw-nuss 8000000.ethernet: initialized cpsw ale version 1.4
[    2.456276] am65-cpsw-nuss 8000000.ethernet: ALE Table size 512, Policers 32
[    2.464873] am65-cpsw-nuss 8000000.ethernet: CPTS ver 0x4e8a010c, freq:500000000, add_val:1 pps:1
[    2.486993] am65-cpsw-nuss 8000000.ethernet: set new flow-id-base 16
[    2.501444] am65-cpts 39000000.cpts: CPTS ver 0x4e8a010c, freq:500000000, add_val:1 pps:1
[    2.514161] mmc0: CQHCI version 5.10
[    2.534617] clk: Disabling unused clocks
[    2.560838] PM: genpd: Disabling unused power domains
[    2.566682] check access for rdinit=/init failed: -2, ignoring
[    2.572622] mmc0: SDHCI controller on fa10000.mmc [fa10000.mmc] using ADMA 64-bit
[    2.585239] VFS: Mounted root (squashfs filesystem) readonly on device 31:7.
[    2.595694] devtmpfs: mounted
[    2.599907] Freeing unused kernel memory: 1344K
[    2.604824] Run /sbin/init as init process
seedrng: can't create directory '/var/lib/seedrng': Read-only file system
Starting syslogd: OK
Starting klogd: OK
Running sysctl: OK
Starting udevd: OK
[    2.771713] mmc0: Failed to initialize a non-removable card
[    3.581135] udevd[88]: starting version 3.2.14
[    3.852344] udevd[88]: starting eudev-3.2.14
[    4.456152] at24 0-0050: supply vcc not found, using dummy regulator
[    4.494201] omap-mailbox 29020000.mailbox: omap mailbox rev 0x66fc9100
[    4.527325] omap-mailbox 29040000.mailbox: omap mailbox rev 0x66fc9100
[    4.559815] omap-mailbox 29060000.mailbox: omap mailbox rev 0x66fc9100
[    4.820081] davinci_mdio 300b2400.mdio: Configuring MDIO in manual mode
[    4.906434] davinci_mdio 300b2400.mdio: davinci mdio revision 1.7, bus freq 1000000
[    4.990551] k3-m4-rproc 5000000.m4fss: assigned reserved memory node memory@a4000000
[    5.010945] platform 78000000.r5f: configured R5F for remoteproc mode
[    5.027217] k3-m4-rproc 5000000.m4fss: configured M4F for remoteproc mode
[    5.041160] k3_r5_rproc bus@f4000:r5fss@78000000: split-mode not permitted, force configuring for single-cpu mode
[    5.076366] remoteproc remoteproc0: 5000000.m4fss is available
[    5.115831] platform 78000000.r5f: assigned reserved memory node memory@9c000000
[    5.158883] remoteproc remoteproc1: 78000000.r5f is available
[    5.191670] platform 78400000.r5f: configured R5F for remoteproc mode
[    5.232393] k3_r5_rproc bus@f4000:r5fss@78400000: split-mode not permitted, force configuring for single-cpu mode
[    5.278734] remoteproc remoteproc0: powering up 5000000.m4fss
[    5.294485] remoteproc remoteproc0: Booting fw image am64-mcu-m4f0_0-fw, size 88248
[    5.306874] remoteproc remoteproc1: powering up 78000000.r5f
[    5.324353] remoteproc remoteproc1: Booting fw image am64-main-r5f0_0-fw, size 94056
[    5.341267] rproc-virtio rproc-virtio.0.auto: assigned reserved memory node memory@a4000000
[    5.364157] remoteproc remoteproc1: bad phdr da 0xa0100000 mem 0x1000
[    5.379657] virtio_rpmsg_bus virtio0: rpmsg host is online
[    5.385270] virtio_rpmsg_bus virtio0: creating channel ti.ipc4.ping-pong addr 0xd
[    5.393024] virtio_rpmsg_bus virtio0: creating channel rpmsg_chrdev addr 0xe
[    5.406580] remoteproc remoteproc1: Failed to load program segments: -22
[    5.413612] rproc-virtio rproc-virtio.0.auto: registered virtio0 (type 7)
[    5.430918] remoteproc remoteproc0: remote processor 5000000.m4fss is now up
[    5.446642] platform 78400000.r5f: assigned reserved memory node memory@a2000000
[    5.479201] remoteproc remoteproc3: 78400000.r5f is available
[    5.522301] davinci_mdio 300b2400.mdio: phy[15]: device 300b2400.mdio:0f, driver unknown
[    5.629975] remoteproc remoteproc3: powering up 78400000.r5f
[    5.643250] remoteproc remoteproc3: Booting fw image am64-main-r5f1_0-fw, size 90216
[    5.666729] rproc-virtio rproc-virtio.1.auto: assigned reserved memory node memory@a2000000
[    5.686680] virtio_rpmsg_bus virtio1: rpmsg host is online
[    5.692249] virtio_rpmsg_bus virtio1: creating channel ti.ipc4.ping-pong addr 0xd
[    5.699961] virtio_rpmsg_bus virtio1: creating channel rpmsg_chrdev addr 0xe
[    5.714531] rproc-virtio rproc-virtio.1.auto: registered virtio1 (type 7)
[    5.727806] remoteproc remoteproc3: remote processor 78400000.r5f is now up
[    5.742818] Unable to handle kernel NULL pointer dereference at virtual address 0000000000000008
[    5.755461] remoteproc remoteproc5: 3000a000.txpru is available
[    5.766417] Mem abort info:
[    5.769222]   ESR = 0x0000000096000004
[    5.778554] remoteproc remoteproc6: 3000c000.txpru is available
[    5.789957]   EC = 0x25: DABT (current EL), IL = 32 bits
[    5.804570] remoteproc remoteproc7: 3008a000.txpru is available
[    5.815554] Unable to handle kernel NULL pointer dereference at virtual address 0000000000000008
[    5.824552]   SET = 0, FnV = 0
[    5.829031]   EA = 0, S1PTW = 0
[    5.833517] Unable to handle kernel NULL pointer dereference at virtual address 0000000000000008
[    5.846203] remoteproc remoteproc8: 3008c000.txpru is available
[    5.852650]   FSC = 0x04: level 0 translation fault
[    5.857657] Mem abort info:
[    5.864946]   ESR = 0x0000000096000004
[    5.869462] Data abort info:
[    5.872740] Mem abort info:
[    5.875974]   ISV = 0, ISS = 0x00000004, ISS2 = 0x00000000
[    5.882028]   EC = 0x25: DABT (current EL), IL = 32 bits
[    5.887838]   ESR = 0x0000000096000004
[    5.891934]   EC = 0x25: DABT (current EL), IL = 32 bits
[    5.897438]   SET = 0, FnV = 0
[    5.900853]   CM = 0, WnR = 0, TnD = 0, TagAccess = 0
[    5.906271]   EA = 0, S1PTW = 0
[    5.914351]   GCS = 0, Overlay = 0, DirtyBit = 0, Xs = 0
[    5.920015]   SET = 0, FnV = 0
[    5.923212]   FSC = 0x04: level 0 translation fault
[    5.930445]   EA = 0, S1PTW = 0
[    5.933600]   FSC = 0x04: level 0 translation fault
[    5.942545] user pgtable: 4k pages, 48-bit VAs, pgdp=0000000081bb8000
[    5.949345] Data abort info:
[    5.955725]   ISV = 0, ISS = 0x00000004, ISS2 = 0x00000000
[    5.965393] Data abort info:
[    5.968905] [0000000000000008] pgd=0000000000000000, p4d=0000000000000000
[    5.976157]   ISV = 0, ISS = 0x00000004, ISS2 = 0x00000000
[    5.982033]   CM = 0, WnR = 0, TnD = 0, TagAccess = 0
[    5.987462] Internal error: Oops: 0000000096000004 [#1]  SMP
[    5.993125] Modules linked in: icss_iep pru_rproc phy_can_transceiver phy_j721e_wiz cdns3_ti rti_wdt ti_k3_r5_remoteproc ti_k3_m4_remoteproc ti_k3_common sa2ul k3_j72xx_bandgap mux_ti_k3_event sha1 pruss omap_hwspinlock spi_omap2_mcspi omap_mailbox at24
[    6.015591] CPU: 0 UID: 0 PID: 88 Comm: udevd Not tainted 6.18.13 #4 PREEMPT 
[    6.022716] Hardware name: Texas Instruments AM642 EVM (DT)
[    6.028278] pstate: 40000005 (nZcv daif -PAN -UAO -TCO -DIT -SSBS BTYPE=--)
[    6.035228] pc : kernfs_dop_revalidate+0x2c/0x150
[    6.039940] lr : kernfs_dop_revalidate+0x2c/0x150
[    6.044637] sp : ffff800080a1ba80
[    6.047942] x29: ffff800080a1ba80 x28: 0000000000000000 x27: 2f2f2f2f2f2f2f2f
[    6.055074] x26: d0d0d0d0d0d0d0d0 x25: ffff800080a1bc30 x24: fefefefefefefeff
[    6.062206] x23: ffff000001cec07a x22: ffff800080a1bc40 x21: ffff000000532480
[    6.069337] x20: 0000000000000000 x19: ffff000000539e40 x18: 0000000000000000
[    6.076467] x17: 0000000000000000 x16: 0000000000000000 x15: 0000000000000000
[    6.083597] x14: ffff000001cec021 x13: ffff800080a1bc74 x12: 0000000000000003
[    6.090728] x11: 000000033b175d0d x10: 0000b50f01534e88 x9 : 0000000000000018
[    6.097859] x8 : 0101010101010101 x7 : ffff000000050490 x6 : 0000000000000006
[    6.104989] x5 : ffff000000539e40 x4 : ffffb50f00f86640 x3 : 0000000000000401
[    6.112119] x2 : ffff000000539e40 x1 : ffff000001ce0000 x0 : 0000000000000001
[    6.119250] Call trace:
[    6.121689]  kernfs_dop_revalidate+0x2c/0x150 (P)
[    6.126391]  lookup_fast+0x11c/0x140
[    6.129967]  walk_component+0x28/0x190
[    6.133715]  link_path_walk+0x1ec/0x3b0
[    6.137548]  path_openat+0x88/0x1000
[    6.141123]  do_filp_open+0xa8/0x170
[    6.144696]  do_sys_openat2+0x94/0x110
[    6.148443]  __arm64_sys_openat+0x64/0xc0
[    6.152448]  invoke_syscall+0x48/0x110
[    6.156200]  el0_svc_common.constprop.0+0x40/0xe0
[    6.160902]  do_el0_svc+0x1c/0x30
[    6.164215]  el0_svc+0x28/0x80
[    6.167273]  el0t_64_sync_handler+0xa0/0xf0
[    6.171450]  el0t_64_sync+0x198/0x19c
[    6.175116] Code: b40006a0 a9025bf5 f9412c14 97f5a826 (f9400680) 
[    6.181196] ---[ end trace 0000000000000000 ]---
[    6.188249]   GCS = 0, Overlay = 0, DirtyBit = 0, Xs = 0
[    6.194520]   CM = 0, WnR = 0, TnD = 0, TagAccess = 0
[    6.199728]   GCS = 0, Overlay = 0, DirtyBit = 0, Xs = 0
[    6.205138] user pgtable: 4k pages, 48-bit VAs, pgdp=0000000081a0f000
[    6.211692] user pgtable: 4k pages, 48-bit VAs, pgdp=0000000081b75000
[    6.218220] [0000000000000008] pgd=0000000000000000, p4d=0000000000000000
[    6.225124] [0000000000000008] pgd=0000000000000000, p4d=0000000000000000
[    6.232025] Internal error: Oops: 0000000096000004 [#2]  SMP
[    6.237679] Modules linked in: icss_iep pru_rproc phy_can_transceiver phy_j721e_wiz cdns3_ti rti_wdt ti_k3_r5_remoteproc ti_k3_m4_remoteproc ti_k3_common sa2ul k3_j72xx_bandgap mux_ti_k3_event sha1 pruss omap_hwspinlock spi_omap2_mcspi omap_mailbox at24
[    6.260145] CPU: 0 UID: 0 PID: 97 Comm: udevd Tainted: G      D             6.18.13 #4 PREEMPT 
[    6.268832] Tainted: [D]=DIE
[    6.271704] Hardware name: Texas Instruments AM642 EVM (DT)
[    6.277265] pstate: 40000005 (nZcv daif -PAN -UAO -TCO -DIT -SSBS BTYPE=--)
[    6.284216] pc : kernfs_dop_revalidate+0x2c/0x150
[    6.288927] lr : kernfs_dop_revalidate+0x2c/0x150
[    6.293624] sp : ffff800080acba80
[    6.296929] x29: ffff800080acba80 x28: 0000000000000000 x27: 2f2f2f2f2f2f2f2f
[    6.304060] x26: d0d0d0d0d0d0d0d0 x25: ffff800080acbc30 x24: fefefefefefefeff
[    6.311190] x23: ffff000001ce807a x22: ffff800080acbc40 x21: ffff000000532480
[    6.318320] x20: 0000000000000000 x19: ffff00000053a9c0 x18: 0000000000000000
[    6.325452] x17: 0000000000000000 x16: 0000000000000000 x15: 0000000000000000
[    6.332582] x14: ffff000001ce8021 x13: ffff800080acbc74 x12: 0000000000000003
[    6.339713] x11: 000000033b175d0d x10: 0000b50f01534e88 x9 : 0000000000000018
[    6.346845] x8 : 0101010101010101 x7 : ffff000000050490 x6 : 0000000000000006
[    6.353975] x5 : ffff00000053a9c0 x4 : ffffb50f00f86640 x3 : 0000000000000401
[    6.361105] x2 : ffff00000053a9c0 x1 : ffff0000019f6600 x0 : 0000000000000001
[    6.368237] Call trace:
[    6.370676]  kernfs_dop_revalidate+0x2c/0x150 (P)
[    6.375378]  lookup_fast+0x11c/0x140
[    6.378953]  walk_component+0x28/0x190
[    6.382701]  link_path_walk+0x1ec/0x3b0
[    6.386534]  path_openat+0x88/0x1000
[    6.390108]  do_filp_open+0xa8/0x170
[    6.393682]  do_sys_openat2+0x94/0x110
[    6.397429]  __arm64_sys_openat+0x64/0xc0
[    6.401433]  invoke_syscall+0x48/0x110
[    6.405185]  el0_svc_common.constprop.0+0x40/0xe0
[    6.409887]  do_el0_svc+0x1c/0x30
[    6.413202]  el0_svc+0x28/0x80
[    6.416260]  el0t_64_sync_handler+0xa0/0xf0
[    6.420437]  el0t_64_sync+0x198/0x19c
[    6.424103] Code: b40006a0 a9025bf5 f9412c14 97f5a826 (f9400680) 
[    6.430185] ---[ end trace 0000000000000000 ]---
[    6.436624] Internal error: Oops: 0000000096000004 [#3]  SMP
[    6.442286] Modules linked in: icss_iep pru_rproc phy_can_transceiver phy_j721e_wiz cdns3_ti rti_wdt ti_k3_r5_remoteproc ti_k3_m4_remoteproc ti_k3_common sa2ul k3_j72xx_bandgap mux_ti_k3_event sha1 pruss omap_hwspinlock spi_omap2_mcspi omap_mailbox at24
[    6.464749] CPU: 0 UID: 0 PID: 94 Comm: udevd Tainted: G      D             6.18.13 #4 PREEMPT 
[    6.473436] Tainted: [D]=DIE
[    6.476308] Hardware name: Texas Instruments AM642 EVM (DT)
[    6.481869] pstate: 40000005 (nZcv daif -PAN -UAO -TCO -DIT -SSBS BTYPE=--)
[    6.488820] pc : kernfs_dop_revalidate+0x2c/0x150
[    6.493528] lr : kernfs_dop_revalidate+0x2c/0x150
[    6.498225] sp : ffff800080a63a80
[    6.501530] x29: ffff800080a63a80 x28: 0000000000000000 x27: 2f2f2f2f2f2f2f2f
[    6.508663] x26: d0d0d0d0d0d0d0d0 x25: ffff800080a63c30 x24: fefefefefefefeff
[    6.515793] x23: ffff000001ce907a x22: ffff800080a63c40 x21: ffff000000532480
[    6.522923] x20: 0000000000000000 x19: ffff00000053b540 x18: 0000000000000000
[    6.530053] x17: 0000000000000000 x16: 0000000000000000 x15: 0000000000000000
[    6.537183] x14: ffff000001ce9021 x13: ffff800080a63c74 x12: 0000000000000003
[    6.544313] x11: 000000033b175d0d x10: 0000b50f01534e88 x9 : 0000000000000018
[    6.551443] x8 : 0101010101010101 x7 : ffff000000050490 x6 : 0000000000000006
[    6.558573] x5 : ffff00000053b540 x4 : ffffb50f00f86640 x3 : 0000000000000401
[    6.565704] x2 : ffff00000053b540 x1 : ffff000001ce5500 x0 : 0000000000000001
[    6.572834] Call trace:
[    6.575272]  kernfs_dop_revalidate+0x2c/0x150 (P)
[    6.579973]  lookup_fast+0x11c/0x140
[    6.583548]  walk_component+0x28/0x190
[    6.587295]  link_path_walk+0x1ec/0x3b0
[    6.591128]  path_openat+0x88/0x1000
[    6.594702]  do_filp_open+0xa8/0x170
[    6.598275]  do_sys_openat2+0x94/0x110
[    6.602022]  __arm64_sys_openat+0x64/0xc0
[    6.606027]  invoke_syscall+0x48/0x110
[    6.609777]  el0_svc_common.constprop.0+0x40/0xe0
[    6.614479]  do_el0_svc+0x1c/0x30
[    6.617793]  el0_svc+0x28/0x80
[    6.620850]  el0t_64_sync_handler+0xa0/0xf0
[    6.625027]  el0t_64_sync+0x198/0x19c
[    6.628693] Code: b40006a0 a9025bf5 f9412c14 97f5a826 (f9400680) 
[    6.634773] ---[ end trace 0000000000000000 ]---
[    6.719252] udevd[96]: failed to send result of seq 2133 to main daemon: Connection refused
[   16.779618] remoteproc remoteproc9: 30004000.rtu is available
[   16.787545] remoteproc remoteproc10: 30038000.pru is available
[   16.795361] remoteproc remoteproc11: 30006000.rtu is available
[   16.803179] remoteproc remoteproc12: 300b8000.pru is available
[   16.811060] remoteproc remoteproc13: 30086000.rtu is available
[   16.818886] remoteproc remoteproc14: 300b4000.pru is available
[   16.826615] remoteproc remoteproc15: 30084000.rtu is available
[   16.835409] remoteproc remoteproc16: 30034000.pru is available
[   16.847349] platform regulator-3: deferred probe pending: platform: supplier 1-0022 not ready
[   16.856061] platform fa00000.mmc: deferred probe pending: platform: supplier regulator-3 not ready
[   16.865473] platform icssg1-eth: deferred probe pending: icssg-prueth: netdev init port failed
[   16.874218] platform leds: deferred probe pending: leds-gpio: Failed to get GPIO '/leds/led-0'
[   16.883022] platform mdio-mux-1: deferred probe pending: mdio-mux-multiplexer: Failed to get mux
[   16.891925] platform can-phy0: deferred probe pending: platform: supplier 1-0022 not ready
[   16.900404] platform can-phy1: deferred probe pending: platform: supplier 1-0022 not ready
[   16.908872] ti_sci_pm_domains 44043000.system-controller:power-controller: sync_state() pending due to 20711000.can
[   16.919410] ti_sci_pm_domains 44043000.system-controller:power-controller: sync_state() pending due to 20701000.can
[   16.929929] ti_sci_pm_domains 44043000.system-controller:power-controller: sync_state() pending due to 23100000.pwm
[   16.940478] ti_sci_pm_domains 44043000.system-controller:power-controller: sync_state() pending due to f102000.pcie
[   16.951006] ti_sci_pm_domains 44043000.system-controller:power-controller: sync_state() pending due to fa00000.mmc





udevadm settle failed
Starting network: [   33.988996] Unable to handle kernel NULL pointer dereference at virtual address 0000000000000008
[   33.998090] Mem abort info:
[   34.001416]   ESR = 0x0000000096000004
[   34.005316]   EC = 0x25: DABT (current EL), IL = 32 bits
[   34.010721]   SET = 0, FnV = 0
[   34.013770]   EA = 0, S1PTW = 0
[   34.017040]   FSC = 0x04: level 0 translation fault
[   34.022005] Data abort info:
[   34.024979]   ISV = 0, ISS = 0x00000004, ISS2 = 0x00000000
[   34.030548]   CM = 0, WnR = 0, TnD = 0, TagAccess = 0
[   34.035681]   GCS = 0, Overlay = 0, DirtyBit = 0, Xs = 0
[   34.041074] user pgtable: 4k pages, 48-bit VAs, pgdp=0000000081a1f000
[   34.047595] [0000000000000008] pgd=0000000000000000, p4d=0000000000000000
[   34.054475] Internal error: Oops: 0000000096000004 [#4]  SMP
[   34.060127] Modules linked in: icssg_prueth sch_taprio sch_mqprio_lib hsr icssg icss_iep pru_rproc phy_can_transceiver phy_j721e_wiz cdns3_ti rti_wdt ti_k3_r5_remoteproc ti_k3_m4_remoteproc ti_k3_common sa2ul k3_j72xx_bandgap mux_ti_k3_event sha1 pruss omap_hwspinlock spi_omap2_mcspi omap_mailbox at24
[   34.086863] CPU: 0 UID: 0 PID: 119 Comm: wait_iface Tainted: G      D             6.18.13 #4 PREEMPT 
[   34.096071] Tainted: [D]=DIE
[   34.098944] Hardware name: Texas Instruments AM642 EVM (DT)
[   34.104505] pstate: 40000005 (nZcv daif -PAN -UAO -TCO -DIT -SSBS BTYPE=--)
[   34.111454] pc : kernfs_dop_revalidate+0x2c/0x150
[   34.116166] lr : kernfs_dop_revalidate+0x2c/0x150
[   34.120862] sp : ffff800080a7ba00
[   34.124166] x29: ffff800080a7ba00 x28: 0000000000000000 x27: 2f2f2f2f2f2f2f2f
[   34.131297] x26: d0d0d0d0d0d0d0d0 x25: ffff800080a7bb30 x24: fefefefefefefeff
[   34.138428] x23: ffff000001ceb02b x22: ffff800080a7bb40 x21: ffff0000017dff00
[   34.145560] x20: 0000000000000000 x19: ffff000000536a80 x18: 0000000000000000
[   34.152690] x17: 0000000000000000 x16: 0000000000000000 x15: 0000000000000000
[   34.159820] x14: ffff000001ceb021 x13: ffff800080a7bb74 x12: 0000000000000003
[   34.166950] x11: 000000033b175d0d x10: 0000000000000002 x9 : 0000000000000003
[   34.174081] x8 : ffff0000017df600 x7 : ffff000000050490 x6 : 0000000000000005
[   34.181212] x5 : ffff000000536a80 x4 : ffffb50f00f86640 x3 : 0000000000000401
[   34.188342] x2 : ffff000000536a80 x1 : ffff000001cd2200 x0 : 0000000000000001
[   34.195473] Call trace:
[   34.197912]  kernfs_dop_revalidate+0x2c/0x150 (P)
[   34.202614]  lookup_fast+0x11c/0x140
[   34.206190]  walk_component+0x28/0x190
[   34.209938]  link_path_walk+0x1ec/0x3b0
[   34.213771]  path_lookupat+0x6c/0x190
[   34.217431]  filename_lookup+0xbc/0x1d0
[   34.221265]  vfs_statx+0x80/0x190
[   34.224576]  vfs_fstatat+0x64/0xe0
[   34.227973]  __do_sys_newfstatat+0x5c/0xb0
[   34.232063]  __arm64_sys_newfstatat+0x20/0x30
[   34.236414]  invoke_syscall+0x48/0x110
[   34.240167]  el0_svc_common.constprop.0+0x40/0xe0
[   34.244869]  do_el0_svc+0x1c/0x30
[   34.248182]  el0_svc+0x28/0x80
[   34.251241]  el0t_64_sync_handler+0xa0/0xf0
[   34.255419]  el0t_64_sync+0x198/0x19c
[   34.259084] Code: b40006a0 a9025bf5 f9412c14 97f5a826 (f9400680) 
[   34.265166] ---[ end trace 0000000000000000 ]---
run-parts: /etc/network/if-pre-up.d/wait_iface: exit status 139
[   34.285656] Unable to handle kernel NULL pointer dereference at virtual address 0000000000000008
[   34.294705] Mem abort info:
[   34.297493]   ESR = 0x0000000096000004
[   34.301621]   EC = 0x25: DABT (current EL), IL = 32 bits
[   34.307136]   SET = 0, FnV = 0
[   34.310184]   EA = 0, S1PTW = 0
[   34.313475]   FSC = 0x04: level 0 translation fault
[   34.318462] Data abort info:
[   34.321335]   ISV = 0, ISS = 0x00000004, ISS2 = 0x00000000
[   34.327019]   CM = 0, WnR = 0, TnD = 0, TagAccess = 0
[   34.332165]   GCS = 0, Overlay = 0, DirtyBit = 0, Xs = 0
[   34.337579] user pgtable: 4k pages, 48-bit VAs, pgdp=0000000081b92000
[   34.344119] [0000000000000008] pgd=0000000000000000, p4d=0000000000000000
[   34.351041] Internal error: Oops: 0000000096000004 [#5]  SMP
[   34.356693] Modules linked in: icssg_prueth sch_taprio sch_mqprio_lib hsr icssg icss_iep pru_rproc phy_can_transceiver phy_j721e_wiz cdns3_ti rti_wdt ti_k3_r5_remoteproc ti_k3_m4_remoteproc ti_k3_common sa2ul k3_j72xx_bandgap mux_ti_k3_event sha1 pruss omap_hwspinlock spi_omap2_mcspi omap_mailbox at24
[   34.383430] CPU: 0 UID: 0 PID: 121 Comm: wait_iface Tainted: G      D             6.18.13 #4 PREEMPT 
[   34.392638] Tainted: [D]=DIE
[   34.395509] Hardware name: Texas Instruments AM642 EVM (DT)
[   34.401070] pstate: 40000005 (nZcv daif -PAN -UAO -TCO -DIT -SSBS BTYPE=--)
[   34.408022] pc : kernfs_dop_revalidate+0x2c/0x150
[   34.412734] lr : kernfs_dop_revalidate+0x2c/0x150
[   34.417431] sp : ffff80008091ba00
[   34.420737] x29: ffff80008091ba00 x28: 0000000000000000 x27: 2f2f2f2f2f2f2f2f
[   34.427869] x26: d0d0d0d0d0d0d0d0 x25: ffff80008091bb30 x24: fefefefefefefeff
[   34.435001] x23: ffff000001cea02b x22: ffff80008091bb40 x21: ffff0000017dff00
[   34.442132] x20: 0000000000000000 x19: ffff000000536a80 x18: 0000000000000000
[   34.449262] x17: 0000000000000000 x16: 0000000000000000 x15: 0000000000000000
[   34.456391] x14: ffff000001cea021 x13: ffff80008091bb74 x12: 0000000000000003
[   34.463522] x11: 000000033b175d0d x10: 0000000000000002 x9 : 0000000000000003
[   34.470652] x8 : ffff0000017df600 x7 : ffff000000050490 x6 : 0000000000000005
[   34.477782] x5 : ffff000000536a80 x4 : ffffb50f00f86640 x3 : 0000000000000401
[   34.484912] x2 : ffff000000536a80 x1 : ffff000001de6600 x0 : 0000000000000001
[   34.492044] Call trace:
[   34.494484]  kernfs_dop_revalidate+0x2c/0x150 (P)
[   34.499185]  lookup_fast+0x11c/0x140
[   34.502760]  walk_component+0x28/0x190
[   34.506508]  link_path_walk+0x1ec/0x3b0
[   34.510342]  path_lookupat+0x6c/0x190
[   34.514001]  filename_lookup+0xbc/0x1d0
[   34.517834]  vfs_statx+0x80/0x190
[   34.521144]  vfs_fstatat+0x64/0xe0
[   34.524541]  __do_sys_newfstatat+0x5c/0xb0
[   34.528632]  __arm64_sys_newfstatat+0x20/0x30
[   34.532983]  invoke_syscall+0x48/0x110
[   34.536735]  el0_svc_common.constprop.0+0x40/0xe0
[   34.541436]  do_el0_svc+0x1c/0x30
[   34.544751]  el0_svc+0x28/0x80
[   34.547809]  el0t_64_sync_handler+0xa0/0xf0
[   34.551986]  el0t_64_sync+0x198/0x19c
[   34.555652] Code: b40006a0 a9025bf5 f9412c14 97f5a826 (f9400680) 
[   34.561733] ---[ end trace 0000000000000000 ]---
run-parts: /etc/network/if-pre-up.d/wait_iface: exit status 139
[   34.582164] Unable to handle kernel NULL pointer dereference at virtual address 0000000000000008
[   34.591217] Mem abort info:
[   34.594006]   ESR = 0x0000000096000004
[   34.598126]   EC = 0x25: DABT (current EL), IL = 32 bits
[   34.603631]   SET = 0, FnV = 0
[   34.606772]   EA = 0, S1PTW = 0
[   34.609906]   FSC = 0x04: level 0 translation fault
[   34.614931] Data abort info:
[   34.617805]   ISV = 0, ISS = 0x00000004, ISS2 = 0x00000000
[   34.623441]   CM = 0, WnR = 0, TnD = 0, TagAccess = 0
[   34.628578]   GCS = 0, Overlay = 0, DirtyBit = 0, Xs = 0
[   34.633990] user pgtable: 4k pages, 48-bit VAs, pgdp=0000000081abc000
[   34.640531] [0000000000000008] pgd=0000000000000000, p4d=0000000000000000
[   34.647429] Internal error: Oops: 0000000096000004 [#6]  SMP
[   34.653081] Modules linked in: icssg_prueth sch_taprio sch_mqprio_lib hsr icssg icss_iep pru_rproc phy_can_transceiver phy_j721e_wiz cdns3_ti rti_wdt ti_k3_r5_remoteproc ti_k3_m4_remoteproc ti_k3_common sa2ul k3_j72xx_bandgap mux_ti_k3_event sha1 pruss omap_hwspinlock spi_omap2_mcspi omap_mailbox at24
[   34.679818] CPU: 0 UID: 0 PID: 123 Comm: wait_iface Tainted: G      D             6.18.13 #4 PREEMPT 
[   34.689025] Tainted: [D]=DIE
[   34.691897] Hardware name: Texas Instruments AM642 EVM (DT)
[   34.697457] pstate: 40000005 (nZcv daif -PAN -UAO -TCO -DIT -SSBS BTYPE=--)
[   34.704408] pc : kernfs_dop_revalidate+0x2c/0x150
[   34.709119] lr : kernfs_dop_revalidate+0x2c/0x150
[   34.713816] sp : ffff800080a7ba00
[   34.717122] x29: ffff800080a7ba00 x28: 0000000000000000 x27: 2f2f2f2f2f2f2f2f
[   34.724254] x26: d0d0d0d0d0d0d0d0 x25: ffff800080a7bb30 x24: fefefefefefefeff
[   34.731385] x23: ffff000001cee02b x22: ffff800080a7bb40 x21: ffff0000017dff00
[   34.738516] x20: 0000000000000000 x19: ffff000000536a80 x18: 0000000000000000
[   34.745647] x17: 0000000000000000 x16: 0000000000000000 x15: 0000000000000000
[   34.752777] x14: ffff000001cee021 x13: ffff800080a7bb74 x12: 0000000000000003
[   34.759908] x11: 000000033b175d0d x10: 0000000000000002 x9 : 0000000000000003
[   34.767038] x8 : ffff0000017df600 x7 : ffff000000050490 x6 : 0000000000000005
[   34.774168] x5 : ffff000000536a80 x4 : ffffb50f00f86640 x3 : 0000000000000401
[   34.781298] x2 : ffff000000536a80 x1 : ffff000001cd2200 x0 : 0000000000000001
[   34.788429] Call trace:
[   34.790869]  kernfs_dop_revalidate+0x2c/0x150 (P)
[   34.795570]  lookup_fast+0x11c/0x140
[   34.799146]  walk_component+0x28/0x190
[   34.802894]  link_path_walk+0x1ec/0x3b0
[   34.806727]  path_lookupat+0x6c/0x190
[   34.810387]  filename_lookup+0xbc/0x1d0
[   34.814220]  vfs_statx+0x80/0x190
[   34.817531]  vfs_fstatat+0x64/0xe0
[   34.820928]  __do_sys_newfstatat+0x5c/0xb0
[   34.825019]  __arm64_sys_newfstatat+0x20/0x30
[   34.829370]  invoke_syscall+0x48/0x110
[   34.833122]  el0_svc_common.constprop.0+0x40/0xe0
[   34.837822]  do_el0_svc+0x1c/0x30
[   34.841135]  el0_svc+0x28/0x80
[   34.844194]  el0t_64_sync_handler+0xa0/0xf0
[   34.848372]  el0t_64_sync+0x198/0x19c
[   34.852037] Code: b40006a0 a9025bf5 f9412c14 97f5a826 (f9400680) 
[   34.858117] ---[ end trace 0000000000000000 ]---
run-parts: /etc/network/if-pre-up.d/wait_iface: exit status 139
[   34.879004] Unable to handle kernel NULL pointer dereference at virtual address 0000000000000008
[   34.887992] Mem abort info:
[   34.891200]   ESR = 0x0000000096000004
[   34.895091]   EC = 0x25: DABT (current EL), IL = 32 bits
[   34.900492]   SET = 0, FnV = 0
[   34.903649]   EA = 0, S1PTW = 0
[   34.906867]   FSC = 0x04: level 0 translation fault
[   34.911837] Data abort info:
[   34.914804]   ISV = 0, ISS = 0x00000004, ISS2 = 0x00000000
[   34.920389]   CM = 0, WnR = 0, TnD = 0, TagAccess = 0
[   34.925526]   GCS = 0, Overlay = 0, DirtyBit = 0, Xs = 0
[   34.930940] user pgtable: 4k pages, 48-bit VAs, pgdp=0000000081b0f000
[   34.937465] [0000000000000008] pgd=0000000000000000, p4d=0000000000000000
[   34.944366] Internal error: Oops: 0000000096000004 [#7]  SMP
[   34.950018] Modules linked in: icssg_prueth sch_taprio sch_mqprio_lib hsr icssg icss_iep pru_rproc phy_can_transceiver phy_j721e_wiz cdns3_ti rti_wdt ti_k3_r5_remoteproc ti_k3_m4_remoteproc ti_k3_common sa2ul k3_j72xx_bandgap mux_ti_k3_event sha1 pruss omap_hwspinlock spi_omap2_mcspi omap_mailbox at24
[   34.976754] CPU: 0 UID: 0 PID: 125 Comm: wait_iface Tainted: G      D             6.18.13 #4 PREEMPT 
[   34.985963] Tainted: [D]=DIE
[   34.988835] Hardware name: Texas Instruments AM642 EVM (DT)
[   34.994395] pstate: 40000005 (nZcv daif -PAN -UAO -TCO -DIT -SSBS BTYPE=--)
[   35.001346] pc : kernfs_dop_revalidate+0x2c/0x150
[   35.006058] lr : kernfs_dop_revalidate+0x2c/0x150
[   35.010756] sp : ffff80008091ba00
[   35.014060] x29: ffff80008091ba00 x28: 0000000000000000 x27: 2f2f2f2f2f2f2f2f
[   35.021193] x26: d0d0d0d0d0d0d0d0 x25: ffff80008091bb30 x24: fefefefefefefeff
[   35.028324] x23: ffff000001cef02b x22: ffff80008091bb40 x21: ffff0000017dff00
[   35.035454] x20: 0000000000000000 x19: ffff000000536a80 x18: 0000000000000000
[   35.042584] x17: 0000000000000000 x16: 0000000000000000 x15: 0000000000000000
[   35.049715] x14: ffff000001cef021 x13: ffff80008091bb74 x12: 0000000000000003
[   35.056845] x11: 000000033b175d0d x10: 0000000000000002 x9 : 0000000000000003
[   35.063975] x8 : ffff0000017df600 x7 : ffff000000050490 x6 : 0000000000000005
[   35.071105] x5 : ffff000000536a80 x4 : ffffb50f00f86640 x3 : 0000000000000401
[   35.078236] x2 : ffff000000536a80 x1 : ffff000001de6600 x0 : 0000000000000001
[   35.085367] Call trace:
[   35.087809]  kernfs_dop_revalidate+0x2c/0x150 (P)
[   35.092510]  lookup_fast+0x11c/0x140
[   35.096086]  walk_component+0x28/0x190
[   35.099834]  link_path_walk+0x1ec/0x3b0
[   35.103667]  path_lookupat+0x6c/0x190
[   35.107327]  filename_lookup+0xbc/0x1d0
[   35.111161]  vfs_statx+0x80/0x190
[   35.114473]  vfs_fstatat+0x64/0xe0
[   35.117870]  __do_sys_newfstatat+0x5c/0xb0
[   35.121961]  __arm64_sys_newfstatat+0x20/0x30
[   35.126312]  invoke_syscall+0x48/0x110
[   35.130064]  el0_svc_common.constprop.0+0x40/0xe0
[   35.134765]  do_el0_svc+0x1c/0x30
[   35.138078]  el0_svc+0x28/0x80
[   35.141137]  el0t_64_sync_handler+0xa0/0xf0
[   35.145315]  el0t_64_sync+0x198/0x19c
[   35.148981] Code: b40006a0 a9025bf5 f9412c14 97f5a826 (f9400680) 
[   35.155062] ---[ end trace 0000000000000000 ]---
run-parts: /etc/network/if-pre-up.d/wait_iface: exit status 139
FAIL
Starting crond: OK

Welcome to Buildroot
am64xx-evm login: root   
# cat /sys/c[   57.321831] Unable to handle kernel NULL pointer dereference at virtual address 0000000000000008
[   57.330686] Mem abort info:
[   57.333472]   ESR = 0x0000000096000004
[   57.337739]   EC = 0x25: DABT (current EL), IL = 32 bits
[   57.343179]   SET = 0, FnV = 0
[   57.346229]   EA = 0, S1PTW = 0
[   57.349503]   FSC = 0x04: level 0 translation fault
[   57.354466] Data abort info:
[   57.357339]   ISV = 0, ISS = 0x00000004, ISS2 = 0x00000000
[   57.363008]   CM = 0, WnR = 0, TnD = 0, TagAccess = 0
[   57.368146]   GCS = 0, Overlay = 0, DirtyBit = 0, Xs = 0
[   57.373549] user pgtable: 4k pages, 48-bit VAs, pgdp=0000000081b8b000
[   57.380071] [0000000000000008] pgd=0000000000000000, p4d=0000000000000000
[   57.387061] Internal error: Oops: 0000000096000004 [#8]  SMP
[   57.392714] Modules linked in: icssg_prueth sch_taprio sch_mqprio_lib hsr icssg icss_iep pru_rproc phy_can_transceiver phy_j721e_wiz cdns3_ti rti_wdt ti_k3_r5_remoteproc ti_k3_m4_remoteproc ti_k3_common sa2ul k3_j72xx_bandgap mux_ti_k3_event sha1 pruss omap_hwspinlock spi_omap2_mcspi omap_mailbox at24
[   57.419450] CPU: 0 UID: 0 PID: 130 Comm: sh Tainted: G      D             6.18.13 #4 PREEMPT 
[   57.427965] Tainted: [D]=DIE
[   57.430837] Hardware name: Texas Instruments AM642 EVM (DT)
[   57.436398] pstate: 40000005 (nZcv daif -PAN -UAO -TCO -DIT -SSBS BTYPE=--)
[   57.443347] pc : kernfs_dop_revalidate+0x2c/0x150
[   57.448058] lr : kernfs_dop_revalidate+0x2c/0x150
[   57.452756] sp : ffff800080c4ba60
[   57.456061] x29: ffff800080c4ba60 x28: ffff0000019f6600 x27: 0000000000000000
[   57.463193] x26: 0000000000000000 x25: 0000000000000001 x24: ffff0000010ac000
[   57.470324] x23: 00000000ffffff9c x22: ffff800080c4bb40 x21: ffff0000017dff00
[   57.477456] x20: 0000000000000000 x19: ffff000000536a80 x18: 0000000000000000
[   57.484586] x17: 0000000000000000 x16: 0000000000000000 x15: 0000000000000000
[   57.491716] x14: ffff0000010ac021 x13: ffff800080c4bb74 x12: 0000000000000003
[   57.498846] x11: 000000033b175d0d x10: 0000000000000002 x9 : 0000000000000003
[   57.505978] x8 : ffff0000017df600 x7 : ffff000000050490 x6 : 0000000000000005
[   57.513107] x5 : ffff000000536a80 x4 : ffffb50f00f86640 x3 : 0000000000000001
[   57.520238] x2 : ffff000000536a80 x1 : ffff0000019f6600 x0 : 0000000000000001
[   57.527369] Call trace:
[   57.529808]  kernfs_dop_revalidate+0x2c/0x150 (P)
[   57.534510]  lookup_fast+0x11c/0x140
[   57.538085]  walk_component+0x28/0x190
[   57.541833]  path_lookupat+0x58/0x190
[   57.545494]  filename_lookup+0xbc/0x1d0
[   57.549327]  vfs_statx+0x80/0x190
[   57.552637]  vfs_fstatat+0x64/0xe0
[   57.556035]  __do_sys_newfstatat+0x5c/0xb0
[   57.560126]  __arm64_sys_newfstatat+0x20/0x30
[   57.564477]  invoke_syscall+0x48/0x110
[   57.568229]  el0_svc_common.constprop.0+0x40/0xe0
[   57.572930]  do_el0_svc+0x1c/0x30
[   57.576243]  el0_svc+0x28/0x80
[   57.579301]  el0t_64_sync_handler+0xa0/0xf0
[   57.583478]  el0t_64_sync+0x198/0x19c
[   57.587144] Code: b40006a0 a9025bf5 f9412c14 97f5a826 (f9400680) 
[   57.593223] ---[ end trace 0000000000000000 ]---

Welcome to Buildroot
am64xx-evm login: root
# cat /sys/c[   64.004759] Unable to handle kernel NULL pointer dereference at virtual address 0000000000000008
[   64.013654] Mem abort info:
[   64.016901]   ESR = 0x0000000096000004
[   64.020790]   EC = 0x25: DABT (current EL), IL = 32 bits
[   64.026187]   SET = 0, FnV = 0
[   64.029333]   EA = 0, S1PTW = 0
[   64.032560]   FSC = 0x04: level 0 translation fault
[   64.037523] Data abort info:
[   64.040489]   ISV = 0, ISS = 0x00000004, ISS2 = 0x00000000
[   64.046146]   CM = 0, WnR = 0, TnD = 0, TagAccess = 0
[   64.051296]   GCS = 0, Overlay = 0, DirtyBit = 0, Xs = 0
[   64.056704] user pgtable: 4k pages, 48-bit VAs, pgdp=0000000081afd000
[   64.063230] [0000000000000008] pgd=0000000000000000, p4d=0000000000000000
[   64.070112] Internal error: Oops: 0000000096000004 [#9]  SMP
[   64.075763] Modules linked in: icssg_prueth sch_taprio sch_mqprio_lib hsr icssg icss_iep pru_rproc phy_can_transceiver phy_j721e_wiz cdns3_ti rti_wdt ti_k3_r5_remoteproc ti_k3_m4_remoteproc ti_k3_common sa2ul k3_j72xx_bandgap mux_ti_k3_event sha1 pruss omap_hwspinlock spi_omap2_mcspi omap_mailbox at24
[   64.102501] CPU: 0 UID: 0 PID: 132 Comm: sh Tainted: G      D             6.18.13 #4 PREEMPT 
[   64.111015] Tainted: [D]=DIE
[   64.113887] Hardware name: Texas Instruments AM642 EVM (DT)
[   64.119448] pstate: 40000005 (nZcv daif -PAN -UAO -TCO -DIT -SSBS BTYPE=--)
[   64.126398] pc : kernfs_dop_revalidate+0x2c/0x150
[   64.131109] lr : kernfs_dop_revalidate+0x2c/0x150
[   64.135806] sp : ffff80008090ba60
[   64.139112] x29: ffff80008090ba60 x28: ffff0000019f6600 x27: 0000000000000000
[   64.146244] x26: 0000000000000000 x25: 0000000000000001 x24: ffff0000010af000
[   64.153374] x23: 00000000ffffff9c x22: ffff80008090bb40 x21: ffff0000017dff00
[   64.160506] x20: 0000000000000000 x19: ffff000000536a80 x18: 0000000000000000
[   64.167636] x17: 0000000000000000 x16: 0000000000000000 x15: 0000000000000000
[   64.174767] x14: ffff0000010af021 x13: ffff80008090bb74 x12: 0000000000000003
[   64.181897] x11: 000000033b175d0d x10: 0000000000000002 x9 : 0000000000000003
[   64.189027] x8 : ffff0000017df600 x7 : ffff000000050490 x6 : 0000000000000005
[   64.196158] x5 : ffff000000536a80 x4 : ffffb50f00f86640 x3 : 0000000000000001
[   64.203288] x2 : ffff000000536a80 x1 : ffff0000019f6600 x0 : 0000000000000001
[   64.210420] Call trace:
[   64.212859]  kernfs_dop_revalidate+0x2c/0x150 (P)
[   64.217561]  lookup_fast+0x11c/0x140
[   64.221138]  walk_component+0x28/0x190
[   64.224886]  path_lookupat+0x58/0x190
[   64.228546]  filename_lookup+0xbc/0x1d0
[   64.232379]  vfs_statx+0x80/0x190
[   64.235690]  vfs_fstatat+0x64/0xe0
[   64.239088]  __do_sys_newfstatat+0x5c/0xb0
[   64.243179]  __arm64_sys_newfstatat+0x20/0x30
[   64.247530]  invoke_syscall+0x48/0x110
[   64.251282]  el0_svc_common.constprop.0+0x40/0xe0
[   64.255984]  do_el0_svc+0x1c/0x30
[   64.259297]  el0_svc+0x28/0x80
[   64.262357]  el0t_64_sync_handler+0xa0/0xf0
[   64.266534]  el0t_64_sync+0x198/0x19c
[   64.270200] Code: b40006a0 a9025bf5 f9412c14 97f5a826 (f9400680) 
[   64.276282] ---[ end trace 0000000000000000 ]---

Welcome to Buildroot
am64xx-evm login: