beaglebone login: U-Boot SPL 2016.11-rc3-dirty (Dec 07 2016 - 13:35:56) Trying to boot from MMC1 U-Boot 2016.11-rc3-dirty (Dec 07 2016 - 13:35:56 +0000) CPU : AM335X-GP rev 2.1 I2C: ready DRAM: 512 MiB Reset Source: Power-on reset has occurred. == init vfd == set vfd MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1 Using default environment Board: BeagleBone Black not set. Validating first E-fuse MAC Net: eth0: MII MODE Could not get PHY for cpsw: addr 0 cpsw Press SPACE to abort autoboot in 2 seconds board_name=[A335BNLT] ... board_rev=[000B] ... switch to partitions #0, OK mmc0 is current device SD/MMC found on device 0 ** Bad device 0:2 0x82000000 ** ** Bad device 0:2 0x82000000 ** switch to partitions #0, OK mmc0 is current device Scanning mmc 0:1... gpio: pin 56 (gpio 56) value is 0 gpio: pin 55 (gpio 55) value is 0 gpio: pin 54 (gpio 54) value is 0 gpio: pin 53 (gpio 53) value is 1 switch to partitions #0, OK mmc0 is current device gpio: pin 54 (gpio 54) value is 1 Checking for: /uEnv.txt ... reading uEnv.txt 1179 bytes read in 5 ms (229.5 KiB/s) gpio: pin 55 (gpio 55) value is 1 Loaded environment from /uEnv.txt Importing environment from mmc ... Checking if uenvcmd is set ... gpio: pin 56 (gpio 56) value is 1 Running uenvcmd ... 1712 bytes read in 35 ms (46.9 KiB/s) debug: [/boot/vmlinuz-3.8.13-bone79] ... 5644336 bytes read in 384 ms (14 MiB/s) debug: [/boot/initrd.img-3.8.13-bone79] ... 2880457 bytes read in 212 ms (13 MiB/s) debug: [/boot/dtbs/3.8.13-bone79/am335x-boneblack.dtb] ... 25938 bytes read in 54 ms (468.8 KiB/s) debug: [console=tty0 console=ttyO0,115200n8 capemgr.disable_partno=BB-BONELT-HDMI,BB-BONELT-HDMIN capemgr.enable_partno=BB-UART1 root=/dev/mmcblk0p2 rootfstype=ext4 rootwait coherent_pool=1M quiet init=/lib/systemd/systemd cape_universal=enable] ... debug: [bootz 0x82000000 0x88080000:2bf3c9 0x88000000] ... ## Flattened Device Tree blob at 88000000 Booting using the fdt blob at 0x88000000 Using Device Tree in place at 88000000, end 88009551 Starting kernel ... Uncompressing Linux... done, booting the kernel. [ 0.384658] omap2_mbox_probe: platform not supported [ 0.540245] tps65217-bl tps65217-bl: no platform data provided [ 0.603624] bone-capemgr bone_capemgr.9: slot #0: No cape found [ 0.640731] bone-capemgr bone_capemgr.9: slot #1: No cape found [ 0.677839] bone-capemgr bone_capemgr.9: slot #2: No cape found [ 0.714949] bone-capemgr bone_capemgr.9: slot #3: No cape found [ 0.735652] omap_hsmmc mmc.5: of_parse_phandle_with_args of 'reset' failed [ 0.771050] LDO3: operation not allowed [ 0.775104] omap_hsmmc mmc.11: could not set regulator OCR (-1) [ 0.807014] pinctrl-single 44e10800.pinmux: pin 44e10854 already requested by 44e10800.pinmux; cannot claim for gpio-leds.8 [ 0.818683] pinctrl-single 44e10800.pinmux: pin-21 (gpio-leds.8) status -22 [ 0.825958] pinctrl-single 44e10800.pinmux: could not request pin 21 on device pinctrl-single Loading, please wait... systemd-fsck[198]: rootfs: clean, 83840/211744 files, 539469/845568 blocks [ 5.688418] libphy: PHY 4a101000.mdio:03 not found [ 5.693485] net eth0: phy 4a101000.mdio:03 not found on slave 1 Debian GNU/Linux 7 beaglebone ttyO0 BeagleBoard.org Debian Image 2015-11-12 Support/FAQ: http://elinux.org/Beagleboard:BeagleBoneBlack_Debian default username:password is [debian:temppwd] beaglebone login: [ 26.816637] Unable to handle kernel NULL pointer dereference at virtual address 00000007 [ 26.825183] pgd = df350000 [ 26.828025] [00000007] *pgd=9e590831, *pte=00000000, *ppte=00000000 [ 26.834644] Internal error: Oops: 17 [#1] SMP THUMB2 [ 26.839821] Modules linked in: g_multi libcomposite mt7601Usta(O) [ 26.846197] CPU: 0 Tainted: G O (3.8.13-bone79 #1) [ 26.852481] PC is at start_this_handle+0x72/0x344 [ 26.857390] LR is at start_this_handle+0x4d/0x344 [ 26.862295] pc : [] lr : [] psr: a0000033 [ 26.862295] sp : de685c00 ip : 00000000 fp : c0045b31 [ 26.874268] r10: de684000 r9 : 00000008 r8 : c093ab80 [ 26.879714] r7 : de403c14 r6 : 00000008 r5 : ffffffff r4 : de403c00 [ 26.886528] r3 : 00000000 r2 : 00000000 r1 : c084e0c0 r0 : 00000000 [ 26.893338] Flags: NzCv IRQs on FIQs on Mode SVC_32 ISA Thumb Segment user [ 26.900967] Control: 50c5387d Table: 9f350019 DAC: 00000015 [ 26.906955] Process lc_main (pid: 907, stack limit = 0xde684240) [ 26.913219] Stack: (0xde685c00 to 0xde686000) [ 26.929707] 5c00: de685d04 00000000 ded253b0 00000050 de685c18 c04d5fdb 00000050 c00b6a2b [ 26.943548] 5c20: def3551c 00030002 def35510 def3551c de685c4c ded253b0 de403c00 de684000 [ 26.956721] 5c40: 00000008 c093ab80 00000000 00000000 de685d04 c0156ac3 def35418 00000050 [ 26.972859] 5c60: def35418 00000001 ded253b0 00000000 de685d38 c0124e45 de685d04 c0156e4f [ 27.001521] 5c80: 00000000 00000000 def3550c 00000001 00000001 de520800 00000000 00000001 [ 27.020055] 5ca0: 00000000 00000000 00000000 00000000 00000000 00000000 def35418 00000000 [ 27.039068] 5cc0: 00000000 00000000 00001000 00000221 00000000 00000001 de685d38 00000001 [ 27.055846] 5ce0: 00000001 00000000 00000000 91827364 de130c00 de130c00 de685cf8 de685cf8 [ 27.070569] 5d00: 00000000 00000001 00000027 00000004 7fffffff 00000026 00000000 00000026 [ 27.082710] 5d20: 00000000 de403c00 00000000 c009a3a1 00000000 c009424d 7ffffffe 00000000 [ 27.093026] 5d40: 00000000 00000000 00000026 00000000 00000001 00000000 00000027 00000001 [ 27.104666] 5d60: def3550c 00000000 00000000 c00942e1 00000026 00000000 00000001 def3550c [ 27.117444] 5d80: 00000027 def35418 df68ec00 00000026 00000000 00000000 00000000 c011df93 [ 27.128161] 5da0: 00000026 00000000 00000000 00000000 c011df41 00000027 00000026 00000000 [ 27.140869] 5dc0: 00000000 00000000 00000000 c00d814b 00000026 00000000 00000000 c04d526d [ 27.151776] 5de0: def35418 00000001 df68ec00 de685f40 00000001 c0094811 00000027 00000000 [ 27.164319] 5e00: 00101042 df68ec00 00000001 de685f40 df68ec00 de685ec0 de685fa8 00000000 [ 27.176914] 5e20: 00000000 c011dc71 00000000 00000000 de685f00 def32758 80000000 c00c2f7d [ 27.191777] 5e40: def33bd0 c00b6a49 df68ec00 def2d088 00000000 00000001 00000000 def32758 [ 27.209228] 5e60: c0892300 df016d50 00000000 00000000 df68ec00 00f32758 00000009 df68ec00 [ 27.222013] 5e80: de685f00 de685ecc de685f78 de685eb8 00000000 df68ec00 fffffdee c04f6a80 [ 27.234818] 5ea0: de685fa8 df767840 de685fa8 00000000 00000000 c00bbe11 00000000 00000000 [ 27.248283] 5ec0: 00000000 00000000 00000000 00000001 ffffffff df68ec00 00000000 00000000 [ 27.261083] 5ee0: 00000000 00000000 df767840 00000000 00000000 00000000 00000027 00000000 [ 27.273156] 5f00: 00000000 00000000 00000027 00000000 00000027 00000000 00000000 00000000 [ 27.287378] 5f20: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000 [ 27.297544] 5f40: be81b6d4 00000027 de684000 00000027 df68ec00 c00bbda9 be81b6d4 c00bc2e3 [ 27.310792] 5f60: df68ec00 00000020 df68ec08 df68ec00 00000000 be81b6d4 00000027 c000c9e4 [ 27.320806] 5f80: de684000 c00bc59d de685fb0 00000000 be821d38 00000000 00000000 00000000 [ 27.334224] 5fa0: 000000b5 c000c841 00000000 00000000 00000004 be81b6d4 00000027 00000000 [ 27.346417] 5fc0: 00000000 00000000 00000000 000000b5 00000000 00000000 b6f38000 00000000 [ 27.360212] 5fe0: 000000b5 be81b668 b6efc193 b6efd416 40000030 00000004 00000000 00000000 [ 27.368933] [] (start_this_handle+0x72/0x344) from [] (jbd2__journal_start+0x6b/0x94) [ 27.378949] [] (jbd2__journal_start+0x6b/0x94) from [] (ext4_da_writepages+0x211/0x3f8) [ 27.389159] [] (ext4_da_writepages+0x211/0x3f8) from [] (do_writepages+0x11/0x20) [ 27.398826] [] (do_writepages+0x11/0x20) from [] (__filemap_fdatawrite_range+0x35/0x38) [ 27.409027] [] (__filemap_fdatawrite_range+0x35/0x38) from [] (filemap_write_and_wait_range+0x29/0x44) [ 27.420589] [] (filemap_write_and_wait_range+0x29/0x44) from [] (ext4_sync_file+0x53/0x224) [ 27.431148] [] (ext4_sync_file+0x53/0x224) from [] (generic_write_sync+0x5b/0x78) [ 27.440794] [] (generic_write_sync+0x5b/0x78) from [] (generic_file_aio_write+0x7d/0x98) [ 27.451070] [] (generic_file_aio_write+0x7d/0x98) from [] (ext4_file_write+0x9d/0x36c) [ 27.461175] [] (ext4_file_write+0x9d/0x36c) from [] (do_sync_write+0x69/0x94) [ 27.470459] [] (do_sync_write+0x69/0x94) from [] (vfs_write+0x67/0xfc) [ 27.479092] [] (vfs_write+0x67/0xfc) from [] (sys_pwrite64+0x45/0x58) [ 27.487652] [] (sys_pwrite64+0x45/0x58) from [] (ret_fast_syscall+0x1/0x46) [ 27.500206] Code: 6d25 2d00 f000 80b0 (68aa) 2a01 [ 27.505316] ---[ end trace 648907737b2d3903 ]--- [ 27.510167] ------------[ cut here ]------------ [ 27.515022] WARNING: at kernel/exit.c:713 do_exit+0x37/0x68c() [ 27.521126] Modules linked in: g_multi libcomposite mt7601Usta(O) [ 27.527573] [] (unwind_backtrace+0x1/0x9c) from [] (warn_slowpath_common+0x33/0x48) [ 27.537395] [] (warn_slowpath_common+0x33/0x48) from [] (warn_slowpath_null+0x11/0x14) [ 27.547487] [] (warn_slowpath_null+0x11/0x14) from [] (do_exit+0x37/0x68c) [ 27.556501] [] (do_exit+0x37/0x68c) from [] (die+0x2a9/0x2c8) [ 27.564335] [] (die+0x2a9/0x2c8) from [] (__do_kernel_fault.part.8+0x37/0x54) [ 27.573623] [] (__do_kernel_fault.part.8+0x37/0x54) from [] (do_page_fault+0x15f/0x2ac) [ 27.583804] [] (do_page_fault+0x15f/0x2ac) from [] (do_DataAbort+0x2b/0x68) [ 27.592910] [] (do_DataAbort+0x2b/0x68) from [] (__dabt_svc+0x35/0x60) [ 27.601551] Exception stack(0xde685bb8 to 0xde685c00) [ 27.608304] 5ba0: 00000000 c084e0c0 [ 27.617334] 5bc0: 00000000 00000000 de403c00 ffffffff 00000008 de403c14 c093ab80 00000008 [ 27.626238] 5be0: de684000 c0045b31 00000000 de685c00 c0156689 c01566ae a0000033 ffffffff [ 27.634854] [] (__dabt_svc+0x35/0x60) from [] (start_this_handle+0x72/0x344) [ 27.644070] [] (start_this_handle+0x72/0x344) from [] (jbd2__journal_start+0x6b/0x94) [ 27.654082] [] (jbd2__journal_start+0x6b/0x94) from [] (ext4_da_writepages+0x211/0x3f8) [ 27.664288] [] (ext4_da_writepages+0x211/0x3f8) from [] (do_writepages+0x11/0x20) [ 27.673937] [] (do_writepages+0x11/0x20) from [] (__filemap_fdatawrite_range+0x35/0x38) [ 27.684130] [] (__filemap_fdatawrite_range+0x35/0x38) from [] (filemap_write_and_wait_range+0x29/0x44) [ 27.695665] [] (filemap_write_and_wait_range+0x29/0x44) from [] (ext4_sync_file+0x53/0x224) [ 27.706223] [] (ext4_sync_file+0x53/0x224) from [] (generic_write_sync+0x5b/0x78) [ 27.715873] [] (generic_write_sync+0x5b/0x78) from [] (generic_file_aio_write+0x7d/0x98) [ 27.726147] [] (generic_file_aio_write+0x7d/0x98) from [] (ext4_file_write+0x9d/0x36c) [ 27.736246] [] (ext4_file_write+0x9d/0x36c) from [] (do_sync_write+0x69/0x94) [ 27.745522] [] (do_sync_write+0x69/0x94) from [] (vfs_write+0x67/0xfc) [ 27.754165] [] (vfs_write+0x67/0xfc) from [] (sys_pwrite64+0x45/0x58) [ 27.762726] [] (sys_pwrite64+0x45/0x58) from [] (ret_fast_syscall+0x1/0x46) [ 27.771821] ---[ end trace 648907737b2d3904 ]--- [ 28.021785] IPv6: ADDRCONF(NETDEV_UP): usb0: link is not ready [ 56.035278] BUG: soft lockup - CPU#0 stuck for 23s! [jbd2/mmcblk0p2-:172] [ 56.042538] Modules linked in: g_multi libcomposite mt7601Usta(O) [ 56.049073] [ 56.050678] Pid: 172, comm: jbd2/mmcblk0p2- [ 56.055599] CPU: 0 Tainted: G D W O (3.8.13-bone79 #1) [ 56.062012] PC is at do_raw_write_lock+0x34/0x80 [ 56.066949] LR is at kjournald2+0x137/0x198 [ 56.071412] pc : [] lr : [] psr: 20000033 [ 56.071412] sp : de419f00 ip : de418040 fp : c084e0c0 [ 56.083601] r10: c08f9aac r9 : de403c8c r8 : de403eb8 [ 56.089159] r7 : de418000 r6 : de403cbc r5 : de418000 r4 : de403c14 [ 56.096090] r3 : 80000000 r2 : 00000001 r1 : 00000000 r0 : de403c14 [ 56.103033] Flags: nzCv IRQs on FIQs on Mode SVC_32 ISA Thumb Segment kernel [ 56.110991] Control: 50c5387d Table: 9f674019 DAC: 00000015 [ 56.117147] [] (unwind_backtrace+0x1/0x9c) from [] (watchdog_timer_fn+0xc7/0xfc) [ 56.126888] [] (watchdog_timer_fn+0xc7/0xfc) from [] (__run_hrtimer+0x4b/0x154) [ 56.136526] [] (__run_hrtimer+0x4b/0x154) from [] (hrtimer_interrupt+0xcf/0x1fc) [ 56.146268] [] (hrtimer_interrupt+0xcf/0x1fc) from [] (omap2_gp_timer_interrupt+0x1f/0x24) [ 56.156924] [] (omap2_gp_timer_interrupt+0x1f/0x24) from [] (handle_irq_event_percpu+0x3b/0x188) [ 56.168118] [] (handle_irq_event_percpu+0x3b/0x188) from [] (handle_irq_event+0x29/0x3c) [ 56.178583] [] (handle_irq_event+0x29/0x3c) from [] (handle_level_irq+0x53/0x8c) [ 56.188307] [] (handle_level_irq+0x53/0x8c) from [] (generic_handle_irq+0x13/0x1c) [ 56.198220] [] (generic_handle_irq+0x13/0x1c) from [] (handle_IRQ+0x23/0x60) [ 56.207578] [] (handle_IRQ+0x23/0x60) from [] (omap3_intc_handle_irq+0x51/0x5c) [ 56.217229] [] (omap3_intc_handle_irq+0x51/0x5c) from [] (__irq_svc+0x3b/0x5c) [ 56.226751] Exception stack(0xde419eb8 to 0xde419f00)