****** Server exec ***** Link is not ready! ***** Link is not ready! ***** Link is not ready! ***** Link is not ready! ***** Link is not ready! ***** Link is not ready! ***** Link is not ready! ***** Link is not ready! ***** Link is not ready! ***** Link is not ready! ***** Link is not ready! ***** Link is not ready! ***** Link is not ready! ***** Link is not ready! ***** Link is not ready! ***** Link is not ready! ***** Link is not ready! ***** Link is not ready! ***** Link is not ready! ***** Link is not ready! ***** Link is not ready! ***** Link is not ready! ***** Link is not ready! ***** Link is not ready! ***** Link is not ready! ***** Link is not ready! ***** Link is not ready! ***** Link is not ready! ***** Link is not ready! ***** Link is not ready! ***** Link is not ready! [Server_exec] MPU-DSP IF Mem Init Done. (0x2c768) [Server_exec] Send Cmd 1, SolverInit Start! SolverInit End! ********************************************** * PCIe Test Start * * RC mode * ********************************************** Version #: 0x02020007; string PCIE LLD Revision: 02.02.00.07:Dec 13 2016:16:54:46 ********* edma3init() Passed! edma3Id = 1 PCIe Power Up. ***** Link is not ready!