C67x DSP Library Installation
(C) Copyright 2005 Texas Instruments Incorporated
All rights reserved worldwide.
-------------------------------------------------

Contents
--------
- ZIPFILE CONTENTS
- INSTALLATION INFORMATION
- CONTACTING TI


ZIPFILE CONTENTS
----------------
C67xDSPLIB_v200.exe - Contains the installation program for the C67x DSP Library
Readme.txt - This file.


INSTALLATION INFORMATION
------------------------
To run the TI C67x DSP Library Installation, follow the directions below:

Windows 98, Windows NT, Windows 2000, Windows XP
1. Unzip the C67xDSPLIb_v100.exe file to a temp directory
2. Double Click the file to launch the Install Shield Wizard
3. Answer all remaining questions presented in Install Shield dialog boxes

NOTES: 
1) If you DO NOT accept the software license agreement the library WILL NOT be installed. 
2) The default location to install the software is C:\CCStudio\, which will install the code into c:\CCStudio\c6700\dsplib and the docs into c:\CCStudio\docs\pdf.  If the existing tools are not installed in the default location you need to know the correct location to complete the installation of the DSP Library.

CONTACTING TI
-------------
Texas Instruments Incorporated
Post Office Box 655303
Dallas, Texas  75265  USA

Phone: +1(972) 644-5580
Fax: +1(214) 480-7800
Internet: dsph@ti.com
World Wide Web: http://www.ti.com/sc/support