U-Boot SPL 2016.11-rc3-dirty (Dec 07 2016 - 13:35:56) Trying to boot from MMC1 U-Boot 2016.11-rc3-dirty (Dec 07 2016 - 13:35:56 +0000) CPU : AM335X-GP rev 2.1 I2C: ready DRAM: 512 MiB Reset Source: Power-on reset has occurred. == init vfd == set vfd MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1 Using default environment Board: BeagleBone Black not set. Validating first E-fuse MAC Net: eth0: MII MODE cpsw Press SPACE to abort autoboot in 2 seconds board_name=[A335BNLT] ... board_rev=[000B] ... switch to partitions #0, OK mmc0 is current device SD/MMC found on device 0 ** Bad device 0:2 0x82000000 ** ** Bad device 0:2 0x82000000 ** switch to partitions #0, OK mmc0 is current device Scanning mmc 0:1... gpio: pin 56 (gpio 56) value is 0 gpio: pin 55 (gpio 55) value is 0 gpio: pin 54 (gpio 54) value is 0 gpio: pin 53 (gpio 53) value is 1 switch to partitions #0, OK mmc0 is current device gpio: pin 54 (gpio 54) value is 1 Checking for: /uEnv.txt ... reading uEnv.txt 1179 bytes read in 4 ms (287.1 KiB/s) gpio: pin 55 (gpio 55) value is 1 Loaded environment from /uEnv.txt Importing environment from mmc ... Checking if uenvcmd is set ... gpio: pin 56 (gpio 56) value is 1 Running uenvcmd ... 1712 bytes read in 34 ms (48.8 KiB/s) debug: [/boot/vmlinuz-3.8.13-bone79] ... 5644336 bytes read in 383 ms (14.1 MiB/s) debug: [/boot/initrd.img-3.8.13-bone79] ... 2880457 bytes read in 211 ms (13 MiB/s) debug: [/boot/dtbs/3.8.13-bone79/am335x-boneblack.dtb] ... 25938 bytes read in 54 ms (468.8 KiB/s) debug: [console=tty0 console=ttyO0,115200n8 capemgr.disable_partno=BB-BONELT-HDMI,BB-BONELT-HDMIN capemgr.enable_partno=BB-UART1 root=/dev/mmcblk0p2 rootfstype=ext4 rootwait coherent_pool=1M quiet init=/lib/systemd/systemd cape_universal=enable] ... debug: [bootz 0x82000000 0x88080000:2bf3c9 0x88000000] ... ## Flattened Device Tree blob at 88000000 Booting using the fdt blob at 0x88000000 Using Device Tree in place at 88000000, end 88009551 Starting kernel ... Uncompressing Linux... done, booting the kernel. [ 0.384642] omap2_mbox_probe: platform not supported [ 0.540287] tps65217-bl tps65217-bl: no platform data provided [ 0.603544] bone-capemgr bone_capemgr.9: slot #0: No cape found [ 0.640651] bone-capemgr bone_capemgr.9: slot #1: No cape found [ 0.677760] bone-capemgr bone_capemgr.9: slot #2: No cape found [ 0.714869] bone-capemgr bone_capemgr.9: slot #3: No cape found [ 0.735645] omap_hsmmc mmc.5: of_parse_phandle_with_args of 'reset' failed [ 0.770966] LDO3: operation not allowed [ 0.775029] omap_hsmmc mmc.11: could not set regulator OCR (-1) [ 0.806924] pinctrl-single 44e10800.pinmux: pin 44e10854 already requested by 44e10800.pinmux; cannot claim for gpio-leds.8 [ 0.818578] pinctrl-single 44e10800.pinmux: pin-21 (gpio-leds.8) status -22 [ 0.825853] pinctrl-single 44e10800.pinmux: could not request pin 21 on device pinctrl-single Loading, please wait... systemd-fsck[198]: rootfs: clean, 83832/211744 files, 539505/845568 blocks [ 5.531667] libphy: PHY 4a101000.mdio:01 not found [ 5.536739] net eth0: phy 4a101000.mdio:01 not found on slave 1 Debian GNU/Linux 7 beaglebone ttyO0 BeagleBoard.org Debian Image 2015-11-12 Support/FAQ: http://elinux.org/Beagleboard:BeagleBoneBlack_Debian default username:password is [debian:temppwd] beaglebone login: [ 34.796264] BUG: spinlock lockup suspected on CPU#0, apache2/909 [ 34.802555] lock: 0xde354800, .magic: dead4ead, .owner: /-1, .owner_cpu: -1