U-Boot 2017.01-00360-gfde06f6-dirty (Dec 01 2017 - 15:45:50 +0530) CPU: 66AK2Ex SR1.0 Model: Texas Instruments Keystone 2 Edison EVM I2C: ready DRAM: Detected DDR3 DDR3 speed 1600 DRAM: 4 GiB Clear entire DDR3 memory to enable ECC 2 GiB NAND: 1024 MiB Net: K2E_EMAC0 connected to Marvell 88E1510 K2E_EMAC1 connected to Marvell 88E1510 Could not get PHY for ethernet-mdio: addr 2 Could not get PHY for ethernet-mdio: addr 3 Could not get PHY for ethernet-mdio: addr 4 Could not get PHY for ethernet-mdio: addr 5 Could not get PHY for ethernet-mdio: addr 6 Could not get PHY for ethernet-mdio: addr 7 K2E_EMAC0, K2E_EMAC1 Warning: K2E_EMAC1 (eth1) using random MAC address - 8a:58:d2:15:b8:34 , K2E_EMAC2 Warning: K2E_EMAC2 (eth2) using random MAC address - 6e:5f:91:50:47:a0 , K2E_EMAC3 Warning: K2E_EMAC3 (eth3) using random MAC address - 66:57:b8:2a:cb:ac , K2E_EMAC4 Warning: K2E_EMAC4 (eth4) using random MAC address - 7e:0d:80:c5:f3:74 , K2E_EMAC5 Warning: K2E_EMAC5 (eth5) using random MAC address - 16:06:ee:f6:b4:8b , K2E_EMAC6 Warning: K2E_EMAC6 (eth6) using random MAC address - 8a:b7:e3:23:e9:de , K2E_EMAC7 Warning: K2E_EMAC7 (eth7) using random MAC address - a2:be:0f:16:b4:02 DHANUSH GPIO PCIE260bf08 : 0 Hit any key to stop autoboot: 0 starting USB... USB0: Register 2001040 NbrPorts 2 Starting the controller USB XHCI 1.00 scanning bus 0 for devices... 2 USB Device(s) found scanning usb for storage devices... 1 Storage Device(s) found reading keystone-k2e-evm.dtb 35534 bytes read in 45 ms (770.5 KiB/s) reading skern-k2e.bin 32832 bytes read in 44 ms (728.5 KiB/s) reading uImage 4498216 bytes read in 2379 ms (1.8 MiB/s) DEBUG: Message2 from Secure Mode: Core freq - 233333333Hz K2_BM_15. 07-nogit SoC:k2e built:15:13:44, Dec 1 2017 ## installed monitor @ 0xc1f0000, freq [233333333], status 203358208 ## Booting kernel from Legacy Image at 88000000 ... Image Name: Linux-4.9.41-ge3a80a1c5c Created: 2017-12-04 7:19:11 UTC Image Type: ARM Linux Kernel Image (uncompressed) Data Size: 4498152 Bytes = 4.3 MiB Load Address: 80008000 Entry Point: 80008000 Verifying Checksum ... OK ## Flattened Device Tree blob at 87000000 Booting using the fdt blob at 0x87000000 Loading Kernel Image ... OK Using Device Tree in place at 87000000, end 8700bacd Starting kernel ... Uncompressing Linux... done, booting the kernel. DEBUG: >>>> skern_poweron_cpu(1) >>>> DEBUG: >>>> skern_poweron_cpu(2) >>>> DEBUG: >>>> skern_poweron_cpu(3) >>>> [ 0.000000] Booting Linux on physical CPU 0x0 [ 0.000000] Linux version 4.9.41-ge3a80a1c5c (sathish.v@sathish) (gcc version 4.7.3 20130226 (prerelease) (crosstool-NG linaro-1.13.1-4.7-2013.03-20130313 - Linaro GCC 2013.03) ) #12 SMP Mon Dec 4 12:47:39 IST 2017 [ 0.000000] CPU: ARMv7 Processor [412fc0f4] revision 4 (ARMv7), cr=30c5387d [ 0.000000] CPU: div instructions available: patching division code [ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, PIPT instruction cache [ 0.000000] OF: fdt:Machine model: Texas Instruments Keystone 2 Edison EVM [ 0.000000] Switching physical address space to 0x800000000 [ 0.000000] Reserved memory: created DMA memory pool at 0x0000000820000000, size 256 MiB [ 0.000000] OF: reserved mem: initialized node dsp_common_mpm_pool@820000000, compatible id shared-dma-pool [ 0.000000] Memory policy: Data cache writealloc [ 0.000000] psci: probing for conduit method from DT. [ 0.000000] psci: Using PSCI v0.1 Function IDs from DT [ 0.000000] percpu: Embedded 14 pages/cpu @dd7a3000 s27520 r8192 d21632 u57344 [ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 752640 [ 0.000000] Kernel command line: console=ttyS0,115200n8 rootwait=1 rootfstype=ext4 root=/dev/sda2 rw rootdelay=10 [ 0.000000] log_buf_len individual max cpu contribution: 4096 bytes [ 0.000000] log_buf_len total cpu_extra contributions: 12288 bytes [ 0.000000] log_buf_len min size: 16384 bytes [ 0.000000] log_buf_len: 32768 bytes [ 0.000000] early log buf free: 14404(87%) [ 0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes) [ 0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes) [ 0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes) [ 0.000000] Memory: 2969184K/3014656K available (6144K kernel code, 379K rwdata, 2028K rodata, 2048K init, 209K bss, 45472K reserved, 0K cma-reserved, 2490368K highmem) [ 0.000000] Virtual kernel memory layout: [ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB) [ 0.000000] fixmap : 0xffc00000 - 0xfff00000 (3072 kB) [ 0.000000] vmalloc : 0xe0800000 - 0xff800000 ( 496 MB) [ 0.000000] lowmem : 0xc0000000 - 0xe0000000 ( 512 MB) [ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB) [ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB) [ 0.000000] .text : 0xc0008000 - 0xc0800000 (8160 kB) [ 0.000000] .init : 0xc0c00000 - 0xc0e00000 (2048 kB) [ 0.000000] .data : 0xc0e00000 - 0xc0e5ef14 ( 380 kB) [ 0.000000] .bss : 0xc0e60000 - 0xc0e94768 ( 210 kB) [ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1 [ 0.000000] Hierarchical RCU implementation. [ 0.000000] Build-time adjustment of leaf fanout to 32. [ 0.000000] NR_IRQS:16 nr_irqs:16 16 [ 0.000000] GIC: Using split EOI/Deactivate mode [ 0.000000] arm_arch_timer: Architected cp15 timer(s) running at 233.33MHz (phys). [ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x6ba0ac50b7, max_idle_ns: 881590427583 ns [ 0.000002] sched_clock: 56 bits at 233MHz, resolution 4ns, wraps every 4398046511102ns [ 0.000009] Switching to timer-based delay loop, resolution 4ns [ 0.000114] keystone timer clock @233333333 Hz [ 0.000280] Console: colour dummy device 80x30 [ 0.000295] Calibrating delay loop (skipped), value calculated using timer frequency.. 466.66 BogoMIPS (lpj=2333333) [ 0.000304] pid_max: default: 4096 minimum: 301 [ 0.000359] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes) [ 0.000365] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes) [ 0.000678] CPU: Testing write buffer coherency: ok [ 0.000821] /cpus/cpu@0 missing clock-frequency property [ 0.000837] /cpus/cpu@1 missing clock-frequency property [ 0.000853] /cpus/cpu@2 missing clock-frequency property [ 0.000870] /cpus/cpu@3 missing clock-frequency property [ 0.000876] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000 [ 0.000886] Setting up static identity map for 0x80200000 - 0x80200138 [ 1.040584] CPU1: failed to come online [ 2.081552] CPU2: failed to come online [ 3.122922] CPU3: failed to come online [ 3.122983] Brought up 1 CPUs [ 3.122995] SMP: Total of 1 processors activated (466.66 BogoMIPS). [ 3.123007] CPU: All CPU(s) started in HYP mode. [ 3.123017] CPU: Virtualization extensions available. [ 3.123420] devtmpfs: initialized [ 3.138061] VFP support v0.3: implementor 41 architecture 4 part 30 variant f rev 0 [ 3.138412] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns [ 3.138428] futex hash table entries: 16 (order: -2, 1024 bytes) [ 3.138486] pinctrl core: initialized pinctrl subsystem [ 3.138895] NET: Registered protocol family 16 [ 3.139053] DMA: preallocated 256 KiB pool for atomic coherent allocations [ 3.140823] No ATAGs? [ 3.140840] hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers. [ 3.140852] hw-breakpoint: maximum watchpoint size is 8 bytes. [ 3.152431] irq: no irq domain found for /soc/keystone_irq@26202a0 ! [ 3.207134] vgaarb: loaded [ 3.207376] SCSI subsystem initialized [ 3.208470] usbcore: registered new interface driver usbfs [ 3.208564] usbcore: registered new interface driver hub [ 3.208671] usbcore: registered new device driver usb [ 3.218923] clocksource: Switched to clocksource arch_sys_counter [ 3.292971] NET: Registered protocol family 2 [ 3.293492] TCP established hash table entries: 4096 (order: 2, 16384 bytes) [ 3.293528] TCP bind hash table entries: 4096 (order: 3, 32768 bytes) [ 3.293584] TCP: Hash tables configured (established 4096 bind 4096) [ 3.293630] UDP hash table entries: 256 (order: 1, 8192 bytes) [ 3.293653] UDP-Lite hash table entries: 256 (order: 1, 8192 bytes) [ 3.293863] NET: Registered protocol family 1 [ 3.294778] RPC: Registered named UNIX socket transport module. [ 3.294791] RPC: Registered udp transport module. [ 3.294803] RPC: Registered tcp transport module. [ 3.294814] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 3.295277] hw perfevents: enabled with armv7_cortex_a15 PMU driver, 7 counters available [ 3.296481] platform alarmtimer: set dma_pfn_offset00780000 [ 3.301245] workingset: timestamp_bits=30 max_order=20 bucket_order=0 [ 3.322343] Installing knfsd (copyright (C) 1996 okir@monad.swb.de). [ 3.322488] ntfs: driver 2.1.32 [Flags: R/O]. [ 3.322868] jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc. [ 3.328143] NET: Registered protocol family 38 [ 3.328194] bounce: pool size: 64 pages [ 3.328429] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 252) [ 3.328443] io scheduler noop registered [ 3.328455] io scheduler deadline registered [ 3.328656] io scheduler cfq registered (default) [ 3.490357] Serial: 8250/16550 driver, 4 ports, IRQ sharing disabled [ 3.490490] platform serial8250: set dma_pfn_offset00780000 [ 3.495502] console [ttyS0] disabled [ 3.495547] 2530c00.serial: ttyS0 at MMIO 0x2530c00 (irq = 26, base_baud = 14583333) is a TI DA8xx/66AK2x [ 4.144269] console [ttyS0] enabled [ 4.150078] 2531000.serial: ttyS1 at MMIO 0x2531000 (irq = 27, base_baud = 14583333) is a TI DA8xx/66AK2x [ 4.170970] loop: module loaded [ 4.203097] spi_davinci 21000400.spi: DMA is not supported (-19) [ 4.210274] spi_davinci 21000400.spi: Controller at 0xe092d400 [ 4.216492] spi_davinci 21000600.spi: DMA is not supported (-19) [ 4.223277] spi_davinci 21000600.spi: Controller at 0xe092f600 [ 4.229753] spi_davinci 21000800.spi: DMA is not supported (-19) [ 4.236425] spi_davinci 21000800.spi: Controller at 0xe0931800 [ 4.243078] platform Fixed MDIO bus.0: set dma_pfn_offset00780000 [ 4.249460] libphy: Fixed MDIO Bus: probed [ 4.254168] tun: Universal TUN/TAP device driver, 1.6 [ 4.259260] tun: (C) 1999-2004 Max Krasnyansky [ 4.318881] davinci_mdio 24200f00.mdio: davinci mdio revision 1.7 [ 4.324996] libphy: 24200f00.mdio: probed [ 4.330108] davinci_mdio 24200f00.mdio: phy[0]: device 24200f00.mdio:00, driver Marvell 88E1510 [ 4.338835] davinci_mdio 24200f00.mdio: phy[1]: device 24200f00.mdio:01, driver Marvell 88E1510 [ 4.349720] platform xhci-hcd.0.auto: set dma_pfn_offset00780000 [ 4.356557] dwc3 25010000.dwc3: Configuration mismatch. dr_mode forced to host [ 4.364008] platform xhci-hcd.1.auto: set dma_pfn_offset00780000 [ 4.371388] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller [ 4.376914] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 1 [ 4.384759] xhci-hcd xhci-hcd.0.auto: hcc params 0x0298f06d hci version 0x100 quirks 0x02010010 [ 4.393524] xhci-hcd xhci-hcd.0.auto: irq 34, io mem 0x02690000 [ 4.401320] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002 [ 4.408133] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1 [ 4.415413] usb usb1: Product: xHCI Host Controller [ 4.420335] usb usb1: Manufacturer: Linux 4.9.41-ge3a80a1c5c xhci-hcd [ 4.426796] usb usb1: SerialNumber: xhci-hcd.0.auto [ 4.432630] hub 1-0:1.0: USB hub found [ 4.436622] hub 1-0:1.0: 1 port detected [ 4.441452] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller [ 4.446969] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 2 [ 4.454943] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM. [ 4.463357] usb usb2: New USB device found, idVendor=1d6b, idProduct=0003 [ 4.470202] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1 [ 4.477450] usb usb2: Product: xHCI Host Controller [ 4.482372] usb usb2: Manufacturer: Linux 4.9.41-ge3a80a1c5c xhci-hcd [ 4.488833] usb usb2: SerialNumber: xhci-hcd.0.auto [ 4.494670] hub 2-0:1.0: USB hub found [ 4.498666] hub 2-0:1.0: 1 port detected [ 4.503324] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller [ 4.508884] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 3 [ 4.516701] xhci-hcd xhci-hcd.1.auto: hcc params 0x0298f06d hci version 0x100 quirks 0x02010010 [ 4.525467] xhci-hcd xhci-hcd.1.auto: irq 69, io mem 0x25010000 [ 4.531745] usb usb3: New USB device found, idVendor=1d6b, idProduct=0002 [ 4.538556] usb usb3: New USB device strings: Mfr=3, Product=2, SerialNumber=1 [ 4.545858] usb usb3: Product: xHCI Host Controller [ 4.550776] usb usb3: Manufacturer: Linux 4.9.41-ge3a80a1c5c xhci-hcd [ 4.557237] usb usb3: SerialNumber: xhci-hcd.1.auto [ 4.563171] hub 3-0:1.0: USB hub found [ 4.567167] hub 3-0:1.0: 1 port detected [ 4.571715] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller [ 4.577236] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 4 [ 4.585106] usb usb4: We don't know the algorithms for LPM for this host, disabling LPM. [ 4.593579] usb usb4: New USB device found, idVendor=1d6b, idProduct=0003 [ 4.600426] usb usb4: New USB device strings: Mfr=3, Product=2, SerialNumber=1 [ 4.607672] usb usb4: Product: xHCI Host Controller [ 4.612598] usb usb4: Manufacturer: Linux 4.9.41-ge3a80a1c5c xhci-hcd [ 4.619083] usb usb4: SerialNumber: xhci-hcd.1.auto [ 4.625066] hub 4-0:1.0: USB hub found [ 4.629116] hub 4-0:1.0: 1 port detected [ 4.633823] usbcore: registered new interface driver usb-storage [ 4.640623] mousedev: PS/2 mouse device common for all mice [ 4.646391] i2c /dev entries driver [ 4.651696] davinci-wdt 22f0080.wdt: heartbeat 60 sec [ 4.658490] usbcore: registered new interface driver usbhid [ 4.664144] usbhid: USB HID core driver [ 4.668348] platform oprofile-perf.0: set dma_pfn_offset00780000 [ 4.674726] oprofile: using timer interrupt. [ 4.679187] ipip: IPv4 and MPLS over IPv4 tunneling driver [ 4.685382] gre: GRE over IPv4 demultiplexor driver [ 4.690299] ip_gre: GRE over IPv4 tunneling driver [ 4.696465] Initializing XFRM netlink socket [ 4.701505] NET: Registered protocol family 10 [ 4.711483] NET: Registered protocol family 17 [ 4.715965] NET: Registered protocol family 15 [ 4.720522] bridge: filtering via arp/ip/ip6tables is no longer available by default. Update your scripts to load br_netfilter if you need this. [ 4.733539] 8021q: 802.1Q VLAN Support v1.8 [ 4.737803] sctp: Hash tables configured (bind 512/512) [ 4.743420] Registering SWP/SWPB emulation handler [ 4.805677] Waiting 10 sec before mounting root device... [ 4.858887] usb 1-1: new high-speed USB device number 2 using xhci-hcd [ 5.029331] usb 1-1: New USB device found, idVendor=0781, idProduct=557d [ 5.036057] usb 1-1: New USB device strings: Mfr=1, Product=2, SerialNumber=3 [ 5.043237] usb 1-1: Product: Cruzer Force [ 5.047348] usb 1-1: Manufacturer: SanDisk [ 5.051480] usb 1-1: SerialNumber: 4C530006910727111293 [ 5.057595] usb-storage 1-1:1.0: USB Mass Storage device detected [ 5.064213] scsi host0: usb-storage 1-1:1.0 [ 6.089929] scsi 0:0:0:0: Direct-Access SanDisk Cruzer Force 1.27 PQ: 0 ANSI: 6 [ 6.099506] sd 0:0:0:0: Attached scsi generic sg0 type 0 [ 6.106013] sd 0:0:0:0: [sda] 30529536 512-byte logical blocks: (15.6 GB/14.6 GiB) [ 6.114868] sd 0:0:0:0: [sda] Write Protect is off [ 6.120061] sd 0:0:0:0: [sda] Write cache: disabled, read cache: enabled, doesn't support DPO or FUA [ 6.146188] sda: sda1 sda2 [ 6.151668] sd 0:0:0:0: [sda] Attached SCSI removable disk [ 15.281756] EXT4-fs (sda2): mounted filesystem with ordered data mode. Opts: (null) [ 15.289495] VFS: Mounted root (ext4 filesystem) on device 8:2. [ 15.303000] devtmpfs: mounted [ 15.307591] Freeing unused kernel memory: 2048K (c0c00000 - c0e00000) [ 15.385342] random: fast init done INIT: version 2.88 booting Starting udev [ 15.879262] udevd[1260]: starting version 182 [ 18.701739] FAT-fs (sda1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck. Starting Bootlog daemon: bootlogd. [ 18.902323] EXT4-fs (sda2): re-mounted. Opts: (null) Configuring network interfaces... ifconfig: SIOCGIFFLAGS: No such device done. net.ipv4.conf.default.rp_filter = 1 net.ipv4.conf.all.rp_filter = 1 Sat Mar 28 16:54:00 UTC 2015 INIT: Entering runlevel: 5 Starting system message bus: dbus. ##################Sathish############## Starting Dropbear SSH server: dropbear. cppi library link established for device : k2e hyplnk library link established for device : k2e qmss library link established for device : k2e Starting mpmsrv daemon. platform: k2e-evm Starting softhsm daemon. Starting telnet daemon. #>>>>> LCD 12 IP Address: ifconfig: eth0: error fetching interface information: Device not found Starting tiipclad daemon Opened log file: lad.txt Setting base cluster id to 0 id = 0 baseId= 0 Spawned daemon: /usr/bin/lad_66ak2e . Starting syslog-ng:. Starting thttpd. Starting Lighttpd Web Server: lighttpd. * starting FTP Server: vsftpd... 2015-03-28 16:54:02: (log.c.166) server started done. *************************************************************** *************************************************************** NOTICE: This file system contains the followin GPLv3 packages: autoconf binutils-symlinks binutils coreutils cpp-symlinks cpp g++-symlinks g++ gcc-symlinks gcc gdb gdbserver libgmp10 libmpfr4 m4 make If you do not wish to distribute GPLv3 components please remove the above packages prior to distribution. This can be done using the opkg remove command. i.e.: opkg remove Where is the name printed in the list above NOTE: If the package is a dependency of another package you will be notified of the dependent packages. You should use the --force-removal-of-dependent-packages option to also remove the dependent packages as well *************************************************************** *************************************************************** Stopping Bootlog daemon: bootlogd. _____ _____ _ _ | _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_ | | _| .'| . | . | | __| _| . | | | -_| _| _| |__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_| |___| |___| Arago Project http://arago-project.org k2e-evm ttyS0 Arago 2013.12 k2e-evm ttyS0 k2e-evm login: root [ 26.121190] random: crng init done root@k2e-evm:~#