|
|
This report summarizes results from two software quality assessment tools used to analyze the software in this product:
Unless noted below, all source code, both .c and .h files, for embedded target libraries was analyzed using these tools.
This report summarizes the Static Program Analysis results. The listing provides:
This report summarizes the MISRA-C:2004 Program Analysis results. The listing provides:
There are several rules in MISRA-C:2004 that are contrary to long-standing coding standards used in this product, and, hence will not be addressed in the product source code. These rules are listed in the table below. The corresponding checks were explicitly disabled in the tool when the source code was analyzed.
| MISRA C Id | Brief Summary | Exemption Rationale | Exemption Type |
|---|---|---|---|
| 5.1/Required | Identifier is longer than 31 characters. | Coding convention | Blanket |
| 5.6/Advisory | Type and variable/function with the same name. | Coding convention | Blanket |
| 5.7/Advisory | Identifier clashes with other identifier. | Coding convention | Blanket |
| 6.3/Advisory | Built-in numeric type is used. | Coding convention | Blanket |
| 11.3/Advisory | Cast converts pointer to integral type. | Coding convention | Case-by-case |
| 11.4/Advisory | Cast between a pointer to object type and a different pointer to object type. | Coding convention | Case-by-case |
| 12.6/Advisory | Operand of logical operator is not effectively boolean. | Coding convention | Case-by-case |
| 13.2/Advisory | Non-boolean expression is implicitly tested against zero. | Tool reports false positives | Blanket |
| 14.7/Required (Advisory in MISRA-C:2012) | Return is not the last statement in a function. | Coding convention | Case-by-case |
| 16.7/Advisory | Pointer parameter is not used to modify the addressed object but is not declared as pointer to const. | Coding convention, required to match externally specified function interfaces | Case-by-case |
| 19.7/Advisory | Function-like macro definition. | Coding convention | Case-by-case |
Justification for Not Addressing MISRA-C:2004 Violations