/****************************************************************************/ /* 66AK2Gxx.lds */ /* Copyright (c) 2016 Texas Instruments Incorporated */ /* Author: Rafael de Souza */ /* */ /* Description: This file is a sample linker command file that can be */ /* used for linking programs built with the GCC compiler */ /* and running the resulting .out file on a 66AK2Gxx device.*/ /* Use it as a guideline. You will want to */ /* change the memory layout to match your specific */ /* target system. You may want to change the allocation */ /* scheme according to the size of your program. */ /* */ /****************************************************************************/ MEMORY { MSMC_SRAM : o = 0x0C000000, l = 0x00200000 /* 2MB MSMC Shared SRAM */ DDR0 : o = 0x80000000, l = 0x40000000 /* 1GB external DDR0 */ } /* Linker script to place sections and symbol values. Should be used together * with other linker script that defines memory region DDR0. * It references following symbols, which must be defined in code: * Entry : Entry of reset handler * * It defines following symbols, which code can use without definition: * __exidx_start * __exidx_end * __etext * __data_start__ * __preinit_array_start * __preinit_array_end * __init_array_start * __init_array_end * __fini_array_start * __fini_array_end * __data_end__ * __bss_start__ * __bss_end__ * __end__ * end * __HeapLimit * __HeapBase - To be compatible with Linaro's semihosting support * __StackLimit * __StackTop * __StackBase - To be compatible with Linaro's semihosting support * __stack */ ENTRY(Entry) SECTIONS { .rsthand : { . = ALIGN(0x10000); KEEP(*(.isr_vector)) *startup_ARMCA15.o (.text) } > DDR0 . = ALIGN(4); .text : { *(.text*) /* KEEP(*(.init)) KEEP(*(.fini)) */ /* .ctors */ /* *crtbegin.o(.ctors) *crtbegin?.o(.ctors) *(EXCLUDE_FILE(*crtend?.o *crtend.o) .ctors) *(SORT(.ctors.*)) *(.ctors) */ /* .dtors */ /* *crtbegin.o(.dtors) *crtbegin?.o(.dtors) *(EXCLUDE_FILE(*crtend?.o *crtend.o) .dtors) *(SORT(.dtors.*)) *(.dtors) */ *(.rodata*) /* KEEP(*(.eh_frame*)) */ } > DDR0 .ARM.extab : { *(.ARM.extab* .gnu.linkonce.armextab.*) } > DDR0 __exidx_start = .; .ARM.exidx : { *(.ARM.exidx* .gnu.linkonce.armexidx.*) } > DDR0 __exidx_end = .; .data : { . = ALIGN(4); __data_start__ = .; *(vtable) *(.data*) . = ALIGN(4); /* preinit data */ PROVIDE_HIDDEN (__preinit_array_start = .); KEEP(*(.preinit_array)) PROVIDE_HIDDEN (__preinit_array_end = .); . = ALIGN(4); /* init data */ PROVIDE_HIDDEN (__init_array_start = .); KEEP(*(SORT(.init_array.*))) KEEP(*(.init_array)) PROVIDE_HIDDEN (__init_array_end = .); . = ALIGN(4); /* finit data */ PROVIDE_HIDDEN (__fini_array_start = .); KEEP(*(SORT(.fini_array.*))) KEEP(*(.fini_array)) PROVIDE_HIDDEN (__fini_array_end = .); . = ALIGN(4); /* All data end */ __data_end__ = .; } > DDR0 .bss : { . = ALIGN(4); __bss_start__ = .; *(.bss*) *(COMMON) __bss_end__ = .; } > DDR0 .heap (NOLOAD): { /* The line below can be used to FILL the memory with a known value and * debug any stack overruns. For this to work, the specifier (NOLOAD) above * must be removed at the expense of an increase in the output binary size */ FILL(0xDEADBEEF) . = ALIGN(4); __end__ = .; end = __end__; /* The line below created to be compatible with Linaro's semihosting support */ __HeapBase = __end__; *(.heap*) . = . + HEAPSIZE; __HeapLimit = .; } > DDR0 /* .stack section doesn't contain any symbols. It is only * used for linker to calculate size of stack sections, and assign * values to stack symbols later */ .stack (NOLOAD): { /* The line below can be used to FILL the memory with a known value and * debug any stack overruns. For this to work, the specifier (NOLOAD) above * must be removed at the expense of an increase in the output binary size */ FILL(0xBAD0BAD0) . = ALIGN(4); __StackLimit = . ; *(.stack*) . = . + STACKSIZE; __StackTop = . ; /* The line below created to be compatible with Linaro's semihosting support */ __StackBase = . ; } > DDR0 PROVIDE(__stack = __StackTop); } /**************************************************************************/