U-Boot SPL 2020.01 (May 23 2022 - 09:41:13 +0800) SYSFW ABI: 3.1 (firmware rev 0x0016 '22.1.1--v2022.01 (Terrific Llam') Reading on-board EEPROM at 0x50 failed 1 Trying to boot from MMC2 Starting ATF on ARM64 core... NOTICE: BL31: v2.3():07.01.00.004-1-g52c334fc3-dirty NOTICE: BL31: Built : 04:16:36, Nov 26 2020 U-Boot SPL 2020.01 (May 23 2022 - 09:39:58 +0800) SYSFW ABI: 3.1 (firmware rev 0x0016 '22.1.1--v2022.01 (Terrific Llam') Reading on-board EEPROM at 0x50 failed -19 Trying to boot from MMC2 U-Boot 2020.01 (May 23 2022 - 09:39:58 +0800) SoC: AM65X SR2.0 Model: Texas Instruments AM654 Base Board Reading on-board EEPROM at 0x50 failed -19 Board: AM6-COMPROCEVM rev E3 DRAM: 1 GiB MMC: sdhci@4f80000: 0, sdhci@4fa0000: 1 Loading Environment from MMC... OK In: serial Out: serial Err: serial Reading on-board EEPROM at 0x50 failed 1 led_gpio_control error led value=1 ax58100_rst_control value=0 ecat2_phy_rst value=0 ax58100_phy_rst value=0 eth0_phy_rst value=0 eth1_phy_rst value=0 i2c0_switch_init value=0 ser_comm_init value=0 SetSerdesReg for usb2.0 ... Net: eth0: ethernet@46000000 Hit any key to stop autoboot: 0 switch to partitions #0, OK mmc1 is current device SD/MMC found on device 1 1011 bytes read in 4 ms (246.1 KiB/s) Loaded env from uEnv.txt Importing environment from mmc1 ... Running uenvcmd ... 17142272 bytes read in 715 ms (22.9 MiB/s) 67225 bytes read in 8 ms (8 MiB/s) ## Flattened Device Tree blob at 88000000 Booting using the fdt blob at 0x88000000 Loading Device Tree to 000000008feec000, end 000000008fffffff ... OK Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034] [ 0.000000] Linux version 5.10.100-rt62-g204ec708dc (erichsieh@ubuntu) (aarch64-none-linux-gnu-gcc (GNU Toolchain for the A-profile Architecture 9.2-2019.12 (arm-9.10)) 9.2.1 20191025, GNU ld (GNU Toolchain for the A-profile Architecture 9.2-2019.12 (arm-9.10)) 2.33.1.20191209) #11 SMP PREEMPT_RT Thu Jul 7 17:54:23 CST 2022 [ 0.000000] Machine model: Texas Instruments AM654 Base Board [ 0.000000] earlycon: ns16550a0 at MMIO32 0x0000000002800000 (options '') [ 0.000000] printk: bootconsole [ns16550a0] enabled [ 0.000000] efi: UEFI not found. [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a0000000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a0000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a0100000, size 15 MiB [ 0.000000] OF: reserved mem: initialized node r5f-memory@a0100000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a1000000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a1000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a1100000, size 15 MiB [ 0.000000] OF: reserved mem: initialized node r5f-memory@a1100000, compatible id shared-dma-pool [ 0.000000] Zone ranges: [ 0.000000] DMA [mem 0x0000000080000000-0x00000000bfffffff] [ 0.000000] DMA32 empty [ 0.000000] Normal empty [ 0.000000] Movable zone start for each node [ 0.000000] Early memory node ranges [ 0.000000] node 0: [mem 0x0000000080000000-0x000000009e7fffff] [ 0.000000] node 0: [mem 0x000000009e800000-0x00000000a21fffff] [ 0.000000] node 0: [mem 0x00000000a2200000-0x00000000bfffffff] [ 0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000000bfffffff] [ 0.000000] On node 0 totalpages: 262144 [ 0.000000] DMA zone: 4096 pages used for memmap [ 0.000000] DMA zone: 0 pages reserved [ 0.000000] DMA zone: 262144 pages, LIFO batch:63 [ 0.000000] cma: Reserved 24 MiB at 0x00000000bc800000 [ 0.000000] psci: probing for conduit method from DT. [ 0.000000] psci: PSCIv1.1 detected in firmware. [ 0.000000] psci: Using standard PSCI v0.2 function IDs [ 0.000000] psci: Trusted OS migration not required [ 0.000000] psci: SMC Calling Convention v1.2 [ 0.000000] percpu: Embedded 18 pages/cpu s34752 r8192 d30784 u73728 [ 0.000000] pcpu-alloc: s34752 r8192 d30784 u73728 alloc=18*4096 [ 0.000000] pcpu-alloc: [0] 0 [0] 1 [0] 2 [0] 3 [ 0.000000] Detected VIPT I-cache on CPU0 [ 0.000000] CPU features: detected: ARM erratum 845719 [ 0.000000] CPU features: detected: GIC system register CPU interface [ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 258048 [ 0.000000] Kernel command line: console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 isolcpus=1-3 mtdparts=47040000.spi.0:512k(ospi.tiboot3),2m(ospi.tispl),4m(ospi.u-boot),128k(ospi.env),128k(ospi.env.backup),1m(ospi.sysfw),57216k@8m(ospi.rootfs),128k(ospi.phypattern) root=PARTUUID=9284c0bb-02 rw rootfstype=ext4 rootwait [ 0.000000] Dentry cache hash table entries: 131072 (order: 8, 1048576 bytes, linear) [ 0.000000] Inode-cache hash table entries: 65536 (order: 7, 524288 bytes, linear) [ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off [ 0.000000] Memory: 926900K/1048576K available (9984K kernel code, 1124K rwdata, 3872K rodata, 1664K init, 430K bss, 97100K reserved, 24576K cma-reserved) [ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1 [ 0.000000] rcu: Preemptible hierarchical RCU implementation. [ 0.000000] rcu: RCU event tracing is enabled. [ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=4. [ 0.000000] rcu: RCU priority boosting: priority 1 delay 500 ms. [ 0.000000] rcu: RCU_SOFTIRQ processing moved to rcuc kthreads. [ 0.000000] No expedited grace period (rcu_normal_after_boot). [ 0.000000] Trampoline variant of Tasks RCU enabled. [ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies. [ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4 [ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0 [ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode [ 0.000000] GICv3: 960 SPIs implemented [ 0.000000] GICv3: 0 Extended SPIs implemented [ 0.000000] GICv3: Distributor has no Range Selector support [ 0.000000] GICv3: 16 PPIs implemented [ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000001880000 [ 0.000000] ITS [mem 0x01820000-0x0182ffff] [ 0.000000] GIC: enabling workaround for ITS: Socionext Synquacer pre-ITS [ 0.000000] ITS@0x0000000001820000: Devices Table too large, reduce ids 20->19 [ 0.000000] ITS@0x0000000001820000: allocated 524288 Devices @80800000 (flat, esz 8, psz 64K, shr 0) [ 0.000000] ITS: using cache flushing for cmd queue [ 0.000000] GICv3: using LPI property table @0x0000000080040000 [ 0.000000] GIC: using cache flushing for LPI property table [ 0.000000] GICv3: CPU0: using allocated LPI pending table @0x0000000080050000 [ 0.000000] random: get_random_bytes called from start_kernel+0x320/0x4c8 with crng_init=0 [ 0.000000] arch_timer: cp15 timer(s) running at 200.00MHz (phys). [ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x2e2049d3e8, max_idle_ns: 440795210634 ns [ 0.000000] sched_clock: 56 bits at 200MHz, resolution 5ns, wraps every 4398046511102ns [ 0.008566] Console: colour dummy device 80x25 [ 0.013166] Calibrating delay loop (skipped), value calculated using timer frequency.. 400.00 BogoMIPS (lpj=800000) [ 0.023863] pid_max: default: 32768 minimum: 301 [ 0.028690] LSM: Security Framework initializing [ 0.033468] Mount-cache hash table entries: 2048 (order: 2, 16384 bytes, linear) [ 0.041060] Mountpoint-cache hash table entries: 2048 (order: 2, 16384 bytes, linear) [ 0.050810] rcu: Hierarchical SRCU implementation. [ 0.056245] Platform MSI: msi-controller@1820000 domain created [ 0.062574] PCI/MSI: /bus@100000/interrupt-controller@1800000/msi-controller@1820000 domain created [ 0.071962] EFI services will not be available. [ 0.076897] smp: Bringing up secondary CPUs ... [ 0.082697] Detected VIPT I-cache on CPU1 [ 0.086834] GICv3: CPU1: found redistributor 1 region 0:0x00000000018a0000 [ 0.093879] GICv3: CPU1: using allocated LPI pending table @0x0000000080060000 [ 0.101321] CPU1: Booted secondary processor 0x0000000001 [0x410fd034] [ 0.109384] Detected VIPT I-cache on CPU2 [ 0.113539] GICv3: CPU2: found redistributor 100 region 0:0x00000000018c0000 [ 0.120775] GICv3: CPU2: using allocated LPI pending table @0x0000000080070000 [ 0.128231] CPU2: Booted secondary processor 0x0000000100 [0x410fd034] [ 0.136220] Detected VIPT I-cache on CPU3 [ 0.140349] GICv3: CPU3: found redistributor 101 region 0:0x00000000018e0000 [ 0.147577] GICv3: CPU3: using allocated LPI pending table @0x0000000080080000 [ 0.155006] CPU3: Booted secondary processor 0x0000000101 [0x410fd034] [ 0.161846] smp: Brought up 1 node, 4 CPUs [ 0.166071] SMP: Total of 4 processors activated. [ 0.170907] CPU features: detected: 32-bit EL0 Support [ 0.176183] CPU features: detected: CRC32 instructions [ 0.193808] CPU: All CPU(s) started at EL2 [ 0.198037] alternatives: patching kernel code [ 0.203543] devtmpfs: initialized [ 0.217230] KASLR disabled due to lack of seed [ 0.221991] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns [ 0.232014] futex hash table entries: 1024 (order: 5, 131072 bytes, linear) [ 0.240233] pinctrl core: initialized pinctrl subsystem [ 0.246176] DMI not present or invalid. [ 0.250628] NET: Registered protocol family 16 [ 0.257240] DMA: preallocated 128 KiB GFP_KERNEL pool for atomic allocations [ 0.264621] DMA: preallocated 128 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations [ 0.272717] DMA: preallocated 128 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations [ 0.281440] thermal_sys: Registered thermal governor 'step_wise' [ 0.282013] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers. [ 0.295239] ASID allocator initialised with 65536 entries [ 0.336141] HugeTLB registered 1.00 GiB page size, pre-allocated 0 pages [ 0.343060] HugeTLB registered 32.0 MiB page size, pre-allocated 0 pages [ 0.349955] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages [ 0.356851] HugeTLB registered 64.0 KiB page size, pre-allocated 0 pages [ 0.365025] cryptd: max_cpu_qlen set to 1000 [ 0.373317] k3-chipinfo 43000014.chipid: Family:AM65X rev:SR2.0 JTAGID[0x1bb5a02f] Detected [ 0.382858] iommu: Default domain type: Translated [ 0.388242] SCSI subsystem initialized [ 0.392910] pps_core: LinuxPPS API ver. 1 registered [ 0.398019] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti [ 0.407668] PTP clock support registered [ 0.411744] EDAC MC: Ver: 3.0.0 [ 0.416091] FPGA manager framework [ 0.420638] clocksource: Switched to clocksource arch_sys_counter [ 0.427195] VFS: Disk quotas dquot_6.6.0 [ 0.431275] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes) [ 0.444496] NET: Registered protocol family 2 [ 0.449142] IP idents hash table entries: 16384 (order: 5, 131072 bytes, linear) [ 0.457871] tcp_listen_portaddr_hash hash table entries: 512 (order: 3, 32768 bytes, linear) [ 0.466668] TCP established hash table entries: 8192 (order: 4, 65536 bytes, linear) [ 0.474710] TCP bind hash table entries: 8192 (order: 6, 458752 bytes, linear) [ 0.482635] TCP: Hash tables configured (established 8192 bind 8192) [ 0.489442] UDP hash table entries: 512 (order: 4, 65536 bytes, linear) [ 0.496359] UDP-Lite hash table entries: 512 (order: 4, 65536 bytes, linear) [ 0.503855] NET: Registered protocol family 1 [ 0.508914] RPC: Registered named UNIX socket transport module. [ 0.515021] RPC: Registered udp transport module. [ 0.519837] RPC: Registered tcp transport module. [ 0.524666] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 0.531276] PCI: CLS 0 bytes, default 64 [ 0.536436] hw perfevents: enabled with armv8_cortex_a53 PMU driver, 7 counters available [ 0.549816] Initialise system trusted keyrings [ 0.554591] workingset: timestamp_bits=46 max_order=18 bucket_order=0 [ 0.566579] squashfs: version 4.0 (2009/01/31) Phillip Lougher [ 0.573618] NFS: Registering the id_resolver key type [ 0.578851] Key type id_resolver registered [ 0.583171] Key type id_legacy registered [ 0.587372] nfs4filelayout_init: NFSv4 File Layout Driver Registering... [ 0.594274] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering... [ 0.602054] 9p: Installing v9fs 9p2000 file system support [ 0.647422] Key type asymmetric registered [ 0.651628] Asymmetric key parser 'x509' registered [ 0.656702] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 244) [ 0.664285] io scheduler mq-deadline registered [ 0.668992] io scheduler kyber registered [ 0.675582] pinctrl-single 4301c000.pinctrl: 70 pins, size 280 [ 0.682176] pinctrl-single 11c000.pinctrl: 185 pins, size 740 [ 0.688369] pinctrl-single 11c2e8.pinctrl: 9 pins, size 36 [ 0.699816] k3-ringacc 2b800000.ringacc: Failed to get MSI domain [ 0.706208] k3-ringacc 3c000000.ringacc: Failed to get MSI domain [ 0.716275] Serial: 8250/16550 driver, 10 ports, IRQ sharing enabled [ 0.739193] brd: module loaded [ 0.751622] loop: module loaded [ 0.755766] megasas: 07.714.04.00-rc1 [ 0.763092] tun: Universal TUN/TAP device driver, 1.6 [ 0.768493] igbvf: Intel(R) Gigabit Virtual Function Network Driver [ 0.774963] igbvf: Copyright (c) 2009 - 2012 Intel Corporation. [ 0.781975] VFIO - User Level meta-driver version: 0.3 [ 0.788103] i2c /dev entries driver [ 0.793014] sdhci: Secure Digital Host Controller Interface driver [ 0.799375] sdhci: Copyright(c) Pierre Ossman [ 0.804485] sdhci-pltfm: SDHCI platform and OF driver helper [ 0.811719] ti-sci bus@100000:bus@28380000:bus@42040000:dmsc: invalid resource [ 0.819286] SMCCC: SOC_ID: ARCH_FEATURES(ARCH_SOC_ID) returned error: fffffffffffffffd [ 0.828747] optee: probing for conduit method. [ 0.833325] optee: revision 3.8 (199fca17) [ 0.833875] optee: initialized driver [ 0.843221] NET: Registered protocol family 17 [ 0.848008] 9pnet: Installing 9P2000 support [ 0.852481] Key type dns_resolver registered [ 0.857172] printk: bootconsole [ns16550a0]: printing thread started [ 0.857217] Loading compiled-in X.509 certificates [ 0.866157] k3-ringacc 2b800000.ringacc: Failed to get MSI domain [ 0.866389] k3-ringacc 3c000000.ringacc: Failed to get MSI domain [ 0.880522] ti-sci bus@100000:bus@28380000:bus@42040000:dmsc: invalid resource [ 0.884858] ti-sci bus@100000:bus@28380000:bus@42040000:dmsc: ABI: 3.1 (firmware rev 0x0016 '22.1.1--v2022.01 (Terrific Llam') [ 0.958750] random: fast init done [ 0.985756] omap_i2c 42120000.i2c: bus 0 rev0.12 at 100 kHz [ 0.986680] omap_i2c 40b00000.i2c: bus 1 rev0.12 at 100 kHz [ 0.988113] omap_i2c 2000000.i2c: bus 2 rev0.12 at 100 kHz [ 1.005608] omap_i2c 2010000.i2c: bus 3 rev0.12 at 100 kHz [ 1.013155] omap_i2c 2020000.i2c: bus 4 rev0.12 at 100 kHz [ 1.019723] omap_i2c 2030000.i2c: bus 5 rev0.12 at 100 kHz [ 1.020962] ti-sci-intr bus@100000:bus@28380000:bus@42040000:interrupt-controller2: Interrupt Router 156 domain created [ 1.036677] printk: console [ttyS2]: printing thread started [ 1.036694] printk: console [ttyS2] enabled [ 1.036699] printk: bootconsole [ns16550a0] disabled [ 1.058121] printk: bootconsole [ns16550a0]: printing thread stopped [ 1.059459] omap8250 2810000.serial: unable to register 8250 port [ 1.059473] omap8250 2810000.serial: PM domain pd:147 will not be powered off [ 1.060374] 2820000.serial: ttyS4 at MMIO 0x2820000 (irq = 31, base_baud = 3000000) is a 8250 [ 1.069835] [drm] Initialized tidss 1.0.0 20180215 for 4a00000.dss on minor 0 [ 1.152664] davinci_mdio 46000f00.mdio: davinci mdio revision 9.7, bus freq 1000000 [ 1.155261] davinci_mdio 46000f00.mdio: phy[3]: device 46000f00.mdio:03, driver TI DP83822 [ 1.155362] am65-cpsw-nuss 46000000.ethernet: initializing am65 cpsw nuss version 0x6BA00102, cpsw version 0x6BA80102 Ports: 2 quirks:00000000 [ 1.180718] am65-cpts 310d0000.cpts: CPTS ver 0x4e8a010b, freq:200000000, add_val:4 pps:0 [ 1.181492] thermal thermal_zone1: failed to read out thermal zone (-22) [ 1.183784] mmc0: CQHCI version 5.10 [ 1.194963] omap-mailbox 31f80000.mailbox: omap mailbox rev 0x66fc7100 [ 1.195479] omap-mailbox 31f81000.mailbox: omap mailbox rev 0x66fc7100 [ 1.197231] ti-udma 285c0000.dma-controller: Channels: 28 (tchan: 14, rchan: 14, gp-rflow: 16) [ 1.201956] mmc1: CQHCI version 5.10 [ 1.205837] ti-udma 31150000.dma-controller: Channels: 119 (tchan: 53, rchan: 66, gp-rflow: 64) [ 1.226383] 2810000.serial: ttyS3 at MMIO 0x2810000 (irq = 30, base_baud = 3000000) is a 8250 [ 1.275059] mmc0: SDHCI controller on 4f80000.mmc [4f80000.mmc] using ADMA 64-bit [ 1.290260] spi-nor spi9.0: unrecognized JEDEC id bytes: 00 00 00 00 00 00 [ 1.290291] spi-nor: probe of spi9.0 failed with error -2 [ 1.328647] davinci_mdio 46000f00.mdio: davinci mdio revision 9.7, bus freq 1000000 [ 1.331259] davinci_mdio 46000f00.mdio: phy[3]: device 46000f00.mdio:03, driver TI DP83822 [ 1.331361] am65-cpsw-nuss 46000000.ethernet: initializing am65 cpsw nuss version 0x6BA00102, cpsw version 0x6BA80102 Ports: 2 quirks:00000000 [ 1.335967] am65-cpsw-nuss 46000000.ethernet: set new flow-id-base 48 [ 1.336883] am65-cpsw-nuss 46000000.ethernet: initialized cpsw ale version 1.4 [ 1.336892] am65-cpsw-nuss 46000000.ethernet: ALE Table size 64 [ 1.348648] mmc0: mmc_select_hs200 failed, error -110 [ 1.348662] mmc0: error -110 whilst initialising MMC card [ 1.356720] am65-cpsw-nuss 46000000.ethernet: CPTS ver 0x4e8a010b, freq:200000000, add_val:4 pps:0 [ 1.373064] debugfs: Directory 'pd:121' with parent 'pm_genpd' already present! [ 1.373140] debugfs: Directory 'pd:120' with parent 'pm_genpd' already present! [ 1.458523] mmc0: switch to bus width 8 failed [ 1.466830] mmc0: mmc_select_hs200 failed, error -110 [ 1.466842] mmc0: error -110 whilst initialising MMC card [ 1.592134] mmc0: mmc_select_hs200 failed, error -110 [ 1.592142] mmc0: error -110 whilst initialising MMC card [ 1.759560] mmc0: switch to bus width 4 failed [ 1.765084] mmc0: mmc_select_hs200 failed, error -110 [ 1.765091] mmc0: error -110 whilst initialising MMC card [ 2.251689] mmc1: SDHCI controller on 4fa0000.mmc [4fa0000.mmc] using ADMA 64-bit [ 2.252118] Waiting for root device PARTUUID=9284c0bb-02... [ 2.332279] mmc1: new ultra high speed DDR50 SDHC card at address e624 [ 2.339539] mmcblk1: mmc1:e624 SU16G 14.8 GiB [ 2.342648] mmcblk1: p1 p2 [ 2.760423] EXT4-fs (mmcblk1p2): recovery complete [ 2.762192] EXT4-fs (mmcblk1p2): mounted filesystem with ordered data mode. Opts: (null) [ 2.762279] VFS: Mounted root (ext4 filesystem) on device 179:2. [ 2.769342] devtmpfs: mounted [ 2.770585] Freeing unused kernel memory: 1664K [ 2.770726] Run /sbin/init as init process [ 3.002394] systemd[1]: System time before build time, advancing clock. [ 3.080913] NET: Registered protocol family 10 [ 3.081934] Segment Routing with IPv6 [ 3.111990] systemd[1]: systemd 244.5+ running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR -SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN2 -IDN -PCRE2 default-hierarchy=hybrid) [ 3.112489] systemd[1]: Detected architecture arm64. Welcome to Arago 2021.09! [ 3.165997] systemd[1]: Set hostname to . [ 3.565639] systemd[1]: /lib/systemd/system/docker.socket:6: ListenStream= references a path below legacy directory /var/run/, updating /var/run/docker.sock → /run/docker.sock; please update the unit file accordingly. [ 3.692928] random: systemd: uninitialized urandom read (16 bytes read) [ 3.693218] systemd[1]: system-getty.slice: unit configures an IP firewall, but the local system does not support BPF/cgroup firewalling. [ OK ] Created slice system-getty.slice 3.693234] systemd[1]: (This warning is only shown for the first unit using IP firewalling.) m. [ 3.709225] systemd[1]: Created slice system-getty.slice. [ OK ] Created slice system-serial\x2dgett[ 3.740806] random: systemd: uninitialized urandom read (16 bytes read) y.slice. [ 3.742587] systemd[1]: Created slice system-serial\x2dgetty.slice. [ OK ] Created slice User and Session Slic[ 3.764776] random: systemd: uninitialized urandom read (16 bytes read) e. [ 3.766291] systemd[1]: Created slice User and Session Slice. [ OK ] Started Dispatch Password …ts to [ 3.789074] systemd[1]: Started Dispatch Password Requests to Console Directory Watch. Console Directory Watch. [ OK ] Started Forward Password R…uests [ 3.812934] systemd[1]: Started Forward Password Requests to Wall Directory Watch. to Wall Directory Watch. [ OK ] Reached target Paths.[ 3.836884] systemd[1]: Reached target Paths. [ OK ] Reached target Remote File Systems systemd[1]: Reached target Remote File Systems. [0m. [ OK ] Reached target Slices.[ 3.876748] systemd[1]: Reached target Slices. [ OK ] Reached target Swap.[ 3.896761] systemd[1]: Reached target Swap. [ OK ] Listening on RPCbind Server Activat[ 3.928225] systemd[1]: Listening on RPCbind Server Activation Socket. ion Socket. [ OK ] Reached target RPC Port Mapper.[ 3.952877] systemd[1]: Reached target RPC Port Mapper. [ OK ] Listening on Process Core Dump Sock[ 3.978076] systemd[1]: Listening on Process Core Dump Socket. et. [ OK ] Listening on initctl Compatibility [ 4.001059] systemd[1]: Listening on initctl Compatibility Named Pipe. Named Pipe. [ OK ] Listening on Journal Socket (/dev/l[ 4.037381] systemd[1]: Condition check resulted in Journal Audit Socket being skipped. og). [ 4.038134] systemd[1]: Listening on Journal Socket (/dev/log). [ OK ] Listening on Journal Socket.[ 4.061409] systemd[1]: Listening on Journal Socket. [ OK ] Listening on Network Service Netlin[ 4.081428] systemd[1]: Listening on Network Service Netlink Socket. k Socket. [ OK ] Listening on udev Control Socket 4.105206] systemd[1]: Listening on udev Control Socket. m. [ OK ] Listening on udev Kernel Socket[ 4.125045] systemd[1]: Listening on udev Kernel Socket. . Mounting Huge Pages File System...[ 4.150012] systemd[1]: Mounting Huge Pages File System... Mounting POSIX Message Queue File System... [ 4.181822] systemd[1]: Mounting POSIX Message Queue File System... Mounting Kernel Debug File System... [ 4.205900] systemd[1]: Mounting Kernel Debug File System... Mounting Temporary Directory (/tmp)...[ 4.230682] systemd[1]: Mounting Temporary Directory (/tmp)... Starting Create list of st…odes for the current kernel...[ 4.258285] systemd[1]: Starting Create list of static device nodes for the current kernel... Starting Start psplash boot splash screen.[ 4.289626] systemd[1]: Starting Start psplash boot splash screen... .. Starting RPC Bind...[ 4.319773] systemd[1]: Starting RPC Bind... Starting Journal Service...[ 4.341308] systemd[1]: Condition check resulted in File System Check on Root Device being skipped. [ 4.348299] systemd[1]: Starting Journal Service... Starting Load Kernel Modules...[ 4.397763] systemd[1]: Starting Load Kernel Modules... Starting Remount Root and Kernel File Systems systemd[1]: Starting Remount Root and Kernel File Systems... [0m... Starting udev Coldplug all Devices...[ 4.453717] systemd[1]: Starting udev Coldplug all Devices... [ OK ] Started RPC Bind.[ 4.483575] systemd[1]: Started RPC Bind. [ OK ] Mounted Huge Pages File System.[ 4.501909] systemd[1]: Mounted Huge Pages File System. [ 4.517081] cryptodev: loading out-of-tree module taints kernel. [ OK ] Mounted POSIX Message Queue File Sy[ 4.517526] cryptodev: disagrees about version of symbol crypto_skcipher_encrypt stem. [ 4.517533] cryptodev: Unknown symbol crypto_skcipher_encrypt (err -22) [ 4.517619] cryptodev: disagrees about version of symbol fd_install [ 4.517622] cryptodev: Unknown symbol fd_install (err -22) [ OK ] Mounted Kernel Debug File System 4.517663] cryptodev: disagrees about version of symbol __wake_up m. [ OK ] Mounted Temporary Directory (/tmp) cryptodev: Unknown symbol __wake_up (err -22) [0m. [ 4.517678] cryptodev: disagrees about version of symbol crypto_skcipher_setkey [ 4.517682] cryptodev: Unknown symbol crypto_skcipher_setkey (err -22) [ 4.517728] cryptodev: disagrees about version of symbol crypto_skcipher_decrypt [ OK ] Started Create list of sta… nodes[ 4.517732] cryptodev: Unknown symbol crypto_skcipher_decrypt (err -22) for the current kernel. [FAILED] Failed to start Start psplash boo[ 4.517754] cryptodev: disagrees about version of symbol __close_fd t splash screen. [ 4.517758] cryptodev: Unknown symbol __close_fd (err -22) See 'systemctl status psplash-start.service' for details.[ 4.517792] cryptodev: disagrees about version of symbol __init_waitqueue_head [DEPEND] Dependency failed for Star▒[ 4.517796] cryptodev: Unknown symbol __init_waitqueue_head (err -22) ▒▒progress communication helper. [ 4.517842] cryptodev: disagrees about version of symbol proc_dointvec [FAILED] Failed to start Load Kernel Modul[ 4.517846] cryptodev: Unknown symbol proc_dointvec (err -22) es. See 'systemctl status systemd-modules-load.service' for details.[ 4.517879] cryptodev: disagrees about version of symbol crypto_alloc_skcipher [ OK ] Started Journal Service.[ 4.519273] cryptodev: Unknown symbol crypto_alloc_skcipher (err -22) [ 4.527987] systemd[1]: Mounted POSIX Message Queue File System. [ 4.580612] systemd[1]: Mounted Kernel Debug File System. [ 4.617942] systemd[1]: Mounted Temporary Directory (/tmp). [ 4.636614] EXT4-fs (mmcblk1p2): re-mounted. Opts: (null) [ OK ] Started Remount Root and Kernel Fil[ 4.677922] systemd[1]: Started Create list of static device nodes for the current kernel. e Systems. [ 4.711887] systemd[1]: psplash-start.service: Main process exited, code=exited, status=255/EXCEPTION [ 4.712461] systemd[1]: psplash-start.service: Failed with result 'exit-code'. Mounting Kernel Configuration File System.[ 4.715116] systemd[1]: Failed to start Start psplash boot splash screen. .. [ 4.773443] systemd[1]: Dependency failed for Start psplash-systemd progress communication helper. Starting Flush Journal to Persistent Storage 4.813095] systemd[1]: psplash-systemd.service: Job psplash-systemd.service/start failed with result 'dependency'. 0m... [ 4.815691] systemd[1]: systemd-modules-load.service: Main process exited, code=exited, status=1/FAILURE Starting Apply Kernel Variables...[ 4.816194] systemd[1]: systemd-modules-load.service: Failed with result 'exit-code'. Starting Create Static Device Nodes in /dev 4.819168] systemd[1]: Failed to start Load Kernel Modules. m... [ 4.873888] systemd[1]: Started Journal Service. [ OK ] Mounted Kernel Configuration File S[ 5.073116] systemd-journald[216]: Received client request to flush runtime journal. ystem. [ OK ] Started Flush Journal to Persistent Storage. [ OK ] Started Apply Kernel Variables. [ OK ] Started Create Static Device Nodes in /dev. [ OK ] Reached target Local File Systems (Pre). Mounting /media/ram... Mounting /var/volatile... Starting udev Kernel Device Manager... [ OK ] Mounted /media/ram. [ OK ] Mounted /var/volatile. Starting Load/Save Random Seed... [ OK ] Reached target Local File Systems. Starting Create Volatile Files and Directories... [ OK ] Started Create Volatile Files and Directories. Starting Network Time Synchronization... Starting Update UTMP about System Boot/Shutdown... [ OK ] Started Update UTMP about System Boot/Shutdown. [ OK ] Started udev Kernel Device Manager. [ OK ] Started Network Time Synchronization. [ OK ] Started udev Coldplug all Devices. [ OK ] Reached target System Time Set. [ OK ] Reached target System Time Synchronized. Starting udev Wait for Complete Device Initialization... [ 7.458907] at24 2-0050: supply vcc not found, using dummy regulator [ 7.513007] at24 2-0050: 2048 byte 24c16 EEPROM, writable, 16 bytes/write [ 7.756694] random: crng init done [ 7.756711] random: 7 urandom warning(s) missed due to ratelimiting [ OK ] Started Load/Save Random Seed. [ 8.311749] pvrsrvkm: disagrees about version of symbol finish_wait [ 8.311773] pvrsrvkm: Unknown symbol finish_wait (err -22) [ 8.311829] pvrsrvkm: disagrees about version of symbol prepare_to_wait [ 8.311833] pvrsrvkm: Unknown symbol prepare_to_wait (err -22) [ 8.311894] pvrsrvkm: disagrees about version of symbol __wake_up [ 8.311897] pvrsrvkm: Unknown symbol __wake_up (err -22) [ 8.312073] pvrsrvkm: disagrees about version of symbol _dev_err [ 8.312076] pvrsrvkm: Unknown symbol _dev_err (err -22) [ 8.312236] pvrsrvkm: disagrees about version of symbol __init_waitqueue_head [ 8.312240] pvrsrvkm: Unknown symbol __init_waitqueue_head (err -22) [ 8.585577] pvrsrvkm: disagrees about version of symbol finish_wait [ 8.585599] pvrsrvkm: Unknown symbol finish_wait (err -22) [ 8.585654] pvrsrvkm: disagrees about version of symbol prepare_to_wait [ 8.585658] pvrsrvkm: Unknown symbol prepare_to_wait (err -22) [ 8.585718] pvrsrvkm: disagrees about version of symbol __wake_up [ 8.585721] pvrsrvkm: Unknown symbol __wake_up (err -22) [ 8.585896] pvrsrvkm: disagrees about version of symbol _dev_err [ 8.585899] pvrsrvkm: Unknown symbol _dev_err (err -22) [ 8.586058] pvrsrvkm: disagrees about version of symbol __init_waitqueue_head [ 8.586062] pvrsrvkm: Unknown symbol __init_waitqueue_head (err -22) [ 8.857781] CAN device driver interface [ 8.885072] m_can_platform 40528000.mcan: m_can device registered (irq=23, version=32) [ 8.970938] m_can_platform 40568000.mcan: m_can device registered (irq=25, version=32) [ 9.008679] davinci_mdio b132400.mdio: davinci mdio revision 1.7, bus freq 1000000 [ 9.118569] davinci_mdio b132400.mdio: phy[1]: device b132400.mdio:01, driver TI DP83867 [ 9.118592] davinci_mdio b132400.mdio: phy[7]: device b132400.mdio:07, driver TI DP83822 [ 9.184715] davinci_mdio b232400.mdio: davinci mdio revision 1.7, bus freq 1000000 [ 9.213589] davinci_mdio b232400.mdio: phy[2]: device b232400.mdio:02, driver TI DP83867 [ 9.480306] platform 41000000.r5f: configured R5F for remoteproc mode [ 9.490865] platform 41000000.r5f: assigned reserved memory node r5f-dma-memory@a0000000 [ 9.491217] remoteproc remoteproc0: 41000000.r5f is available [ 9.525999] remoteproc remoteproc0: powering up 41000000.r5f [ 9.526028] remoteproc remoteproc0: Booting fw image am65x-mcu-r5f0_0-fw, size 82412 [ 9.551452] remoteproc0#vdev0buffer: assigned reserved memory node r5f-dma-memory@a0000000 [ 9.551901] virtio_rpmsg_bus virtio0: rpmsg host is online [ 9.551943] remoteproc0#vdev0buffer: registered virtio0 (type 7) [ 9.551952] remoteproc remoteproc0: remote processor 41000000.r5f is now up [ 9.571913] virtio_rpmsg_bus virtio0: creating channel ti.ipc4.ping-pong addr 0xd [ 9.572166] virtio_rpmsg_bus virtio0: creating channel rpmsg_chrdev addr 0xe [ 10.984444] remoteproc remoteproc1: b034000.pru is available [ 10.992003] remoteproc remoteproc2: b004000.rtu is available [ 10.992417] remoteproc remoteproc3: b00a000.txpru is available [ 11.002526] remoteproc remoteproc4: b038000.pru is available [ 11.003031] remoteproc remoteproc5: b006000.rtu is available [ 11.025027] remoteproc remoteproc6: b00c000.txpru is available [ 11.025440] remoteproc remoteproc7: b134000.pru is available [ 11.055948] remoteproc remoteproc8: b104000.rtu is available [ 11.081105] remoteproc remoteproc9: b10a000.txpru is available [ 11.092046] remoteproc remoteproc10: b138000.pru is available [ 11.099642] remoteproc remoteproc11: b106000.rtu is available [ 11.107764] remoteproc remoteproc12: b10c000.txpru is available [ 11.133095] remoteproc remoteproc13: b234000.pru is available [ 11.143984] remoteproc remoteproc14: b204000.rtu is available [ 11.201120] remoteproc remoteproc15: b20a000.txpru is available [ 11.201523] remoteproc remoteproc16: b238000.pru is available [ 11.201928] remoteproc remoteproc17: b206000.rtu is available [ 11.202339] remoteproc remoteproc18: b20c000.txpru is available [ OK ] Created slice system-systemd\x2dfsck.slice. [ 13.948894] omap_rng 4e10000.rng: Random Number Generator ver. 241b34c [ 13.989170] icssg-prueth icssg1-eth: port 1: using random MAC addr: 9a:90:79:d4:58:00 [ 14.008890] icssg-prueth icssg1-eth: port 2: using random MAC addr: 42:f9:ac:b6:f0:e5 [ 14.010465] icssg-prueth icssg1-eth: TI PRU ethernet driver initialized: dual EMAC mode [ 14.029021] icssg-prueth icssg2-eth: port 1: using random MAC addr: 36:d8:b8:39:7a:48 [ 14.029852] icssg-prueth icssg2-eth: TI PRU ethernet driver initialized: single EMAC mode [ OK ] Found device /dev/mmcblk1p1. Starting File System Check on /dev/mmcblk1p1... [ OK ] Started File System Check on /dev/mmcblk1p1. Mounting /run/media/mmcblk1p1... [ OK ] Mounted /run/media/mmcblk1p1. [ OK ] Reached target Hardware activated USB gadget. [ 15.766836] usbcore: registered new interface driver usbfs [ 15.766899] usbcore: registered new interface driver hub [ 15.766968] usbcore: registered new device driver usb [ 15.881228] xhci-hcd xhci-hcd.2.auto: xHCI Host Controller [ 15.896847] xhci-hcd xhci-hcd.2.auto: new USB bus registered, assigned bus number 1 [ 15.897011] xhci-hcd xhci-hcd.2.auto: hcc params 0x0298fe6d hci version 0x110 quirks 0x0000000000010010 [ 15.936796] xhci-hcd xhci-hcd.2.auto: irq 599, io mem 0x04030000 [ 15.948303] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 5.10 [ 15.948325] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1 [ 15.948332] usb usb1: Product: xHCI Host Controller [ 15.948337] usb usb1: Manufacturer: Linux 5.10.100-rt62-g204ec708dc xhci-hcd [ 15.948343] usb usb1: SerialNumber: xhci-hcd.2.auto [ 15.964111] hub 1-0:1.0: USB hub found [ 15.964156] hub 1-0:1.0: 1 port detected [ 15.967652] xhci-hcd xhci-hcd.2.auto: xHCI Host Controller [ 15.967680] xhci-hcd xhci-hcd.2.auto: new USB bus registered, assigned bus number 2 [ 15.967698] xhci-hcd xhci-hcd.2.auto: Host supports USB 3.0 SuperSpeed [ 15.974805] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM. [ 15.993616] usb usb2: New USB device found, idVendor=1d6b, idProduct=0003, bcdDevice= 5.10 [ 15.993635] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1 [ 15.993642] usb usb2: Product: xHCI Host Controller [ 15.993647] usb usb2: Manufacturer: Linux 5.10.100-rt62-g204ec708dc xhci-hcd [ 15.993653] usb usb2: SerialNumber: xhci-hcd.2.auto [ 16.004727] hub 2-0:1.0: USB hub found [ 16.018671] hub 2-0:1.0: 1 port detected [ OK ] Started udev Wait for Complete Device Initialization. [ OK ] Started Hardware RNG Entropy Gatherer Daemon. [ OK ] Reached target System Initialization. [ OK ] Started Daily rotation of log files. [ OK ] Started Daily Cleanup of Temporary Directories. [ OK ] Reached target Timers. [ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket. [ OK ] Listening on D-Bus System Message Bus Socket. Starting Docker Socket for the API. [ OK ] Listening on dropbear.socket. Starting Reboot and dump vmcore via kexec... [ OK ] Listening on Docker Socket for the API. [ OK ] Reached target Sockets. [ OK ] Reached target Basic System. [ OK ] Started Job spooling tools. [ OK ] Started Periodic Command Scheduler. [ OK ] Started D-Bus System Message Bus. Starting Print notice about GPLv3 packages... Starting IPv6 Packet Filtering Framework... Starting IPv4 Packet Filtering Framework... [ OK ] Started irqbalance daemon. Starting Telephony service... Starting rc.pvr.service... Starting Login Service... [ OK ] Started TEE Supplicant. [ OK ] Started Reboot and dump vmcore via kexec. [ OK ] Started IPv6 Packet Filtering Framework. [ OK ] Started IPv4 Packet Filtering Framework. [ OK ] Reached target Network (Pre). Starting Network Service... [ 17.144915] optee: PTA_CMD_GET_DEVICES invoke function err: ffff0009 [ 17.145037] ------------[ cut here ]------------ [ 17.145042] WARNING: CPU: 0 PID: 40 at drivers/tee/optee/core.c:217 optee_bus_scan+0x24/0x38 [ 17.145066] Modules linked in: xhci_plat_hcd rpmsg_char xhci_hcd usbcore ti_am335x_adc kfifo_buf irq_pruss_intc omap_rng rng_core dwc3 udc_core roles usb_common crct10dif_ce icssg_prueth pru_rproc icss_iep ti_k3_r5_remoteproc virtio_rpmsg_bus ti_am335x_tscadc m_can_platform m_can can_dev pruss sa2ul sha512_generic authenc phy_omap_usb2 dwc3_keystone at24 sch_fq_codel ipv6 [ 17.145160] CPU: 0 PID: 40 Comm: kworker/0:1 Tainted: G O 5.10.100-rt62-g204ec708dc #11 [ 17.145168] Hardware name: Texas Instruments AM654 Base Board (DT) [ 17.145175] Workqueue: optee_bus_scan optee_bus_scan [ 17.145185] pstate: 60000005 (nZCv daif -PAN -UAO -TCO BTYPE=--) [ 17.145192] pc : optee_bus_scan+0x24/0x38 [ 17.145198] lr : optee_bus_scan+0x14/0x38 [ 17.145205] sp : ffff800011313d90 [ 17.145208] x29: ffff800011313d90 x28: ffff800010f49000 [ 17.145216] x27: ffff80001114bcc8 x26: ffff0000002d3748 [ 17.145223] x25: 0000000000000000 x24: ffff000001358960 [ 17.145230] x23: fffffdffbffb0500 x22: 0000000000000000 [ 17.145237] x21: ffff00003fd8edc0 x20: ffff0000002c9f00 [ 17.145244] x19: ffff000001358958 x18: 0000000000000020 [ 17.145251] x17: 000000005a2cfb92 x16: 00000000d396ecd0 [ 17.145259] x15: ffff0000001c22c0 x14: ffffffffffffffff [ 17.145266] x13: ffff80001106c58c x12: ffff800011165000 [ 17.145273] x11: 0000000000000004 x10: 0000000000000000 [ 17.145280] x9 : 0000000000000040 x8 : 0000000000000000 [ 17.145287] x7 : ffff800011165038 x6 : ffff000001350c20 [ 17.145293] x5 : ffff000001350c20 x4 : 0000000000000000 [ 17.145300] x3 : ffff000001350c08 x2 : 0000000000000000 [ 17.145307] x1 : 1c7c1eb0f4e03d00 x0 : 00000000ffffffea [ 17.145315] Call trace: [ 17.145319] optee_bus_scan+0x24/0x38 [ OK ] Started Telephony service.[ 17.145325] process_one_work+0x1a0/0x328 [ 17.145338] worker_thread+0x4c/0x420 [ 17.145347] kthread+0x174/0x198 [ 17.145355] ret_from_fork+0x10/0x34 [ 17.145365] ---[ end trace 0000000000000002 ]--- [ OK ] Listening on Load/Save RF …itch S[ 18.272968] pvrsrvkm: disagrees about version of symbol finish_wait tatus /dev/rfkill Watch. [ 18.272988] pvrsrvkm: Unknown symbol finish_wait (err -22) [ 18.273045] pvrsrvkm: disagrees about version of symbol prepare_to_wait [ 18.273049] pvrsrvkm: Unknown symbol prepare_to_wait (err -22) [ 18.273112] pvrsrvkm: disagrees about version of symbol __wake_up [ 18.273115] pvrsrvkm: Unknown symbol __wake_up (err -22) [ 18.273297] pvrsrvkm: disagrees about version of symbol _dev_err [ 18.273300] pvrsrvkm: Unknown symbol _dev_err (err -22) [ 18.273463] pvrsrvkm: disagrees about version of symbol __init_waitqueue_head [ 18.273467] pvrsrvkm: Unknown symbol __init_waitqueue_head (err -22) [ 18.607485] Bluetooth: Core ver 2.22 [ 18.607659] NET: Registered protocol family 31 [ 18.607664] Bluetooth: HCI device and connection manager initialized [ 18.607687] Bluetooth: HCI socket layer initialized [ 18.607698] Bluetooth: L2CAP socket layer initialized [ 18.607719] Bluetooth: SCO socket layer initialized [ OK ] Started Network Service. Starting Wait for Network to be Configured... Starting Network Name Resolution... [ 19.623191] remoteproc remoteproc13: powering up b234000.pru [ 19.634071] remoteproc remoteproc13: Booting fw image ti-pruss/am65x-sr2-pru0-prueth-fw.elf, size 37264 [ 19.634107] remoteproc remoteproc13: unsupported resource 5 [ 19.634136] remoteproc remoteproc13: remote processor b234000.pru is now up [ 19.634174] remoteproc remoteproc14: powering up b204000.rtu [ 19.649232] remoteproc remoteproc14: Booting fw image ti-pruss/am65x-sr2-rtu0-prueth-fw.elf, size 30832 [ 19.649279] remoteproc remoteproc14: remote processor b204000.rtu is now up [ 19.649314] remoteproc remoteproc15: powering up b20a000.txpru [ 19.652496] remoteproc remoteproc15: Booting fw image ti-pruss/am65x-sr2-txpru0-prueth-fw.elf, size 36656 [ 19.652542] remoteproc remoteproc15: remote processor b20a000.txpru is now up [ 19.656893] pps pps0: new PPS source ptp2 [ 19.699559] TI DP83867 b232400.mdio:02: attached PHY driver [TI DP83867] (mii_bus:phy_addr=b232400.mdio:02, irq=POLL) [ 19.699814] net eth3: started [ 19.836948] remoteproc remoteproc10: powering up b138000.pru [ 19.839989] remoteproc remoteproc10: Booting fw image ti-pruss/am65x-sr2-pru1-prueth-fw.elf, size 37540 [ 19.840022] remoteproc remoteproc10: unsupported resource 5 [ 19.840048] remoteproc remoteproc10: remote processor b138000.pru is now up [ 19.840085] remoteproc remoteproc11: powering up b106000.rtu [ 19.864513] remoteproc remoteproc11: Booting fw image ti-pruss/am65x-sr2-rtu1-prueth-fw.elf, size 30088 [ 19.864558] remoteproc remoteproc11: remote processor b106000.rtu is now up [ 19.864592] remoteproc remoteproc12: powering up b10c000.txpru [ 19.868254] remoteproc remoteproc12: Booting fw image ti-pruss/am65x-sr2-txpru1-prueth-fw.elf, size 35264 [ 19.868306] remoteproc remoteproc12: remote processor b10c000.txpru is now up [ 19.875477] icssg-prueth icssg1-eth: settime timeout [ 19.898968] pps pps1: new PPS source ptp3 [ 19.919773] TI DP83822 b132400.mdio:07: attached PHY driver [TI DP83822] (mii_bus:phy_addr=b132400.mdio:07, irq=POLL) [ 19.925929] net eth2: started [ 20.023948] remoteproc remoteproc7: powering up b134000.pru [ 20.024180] remoteproc remoteproc7: Booting fw image ti-pruss/am65x-sr2-pru0-prueth-fw.elf, size 37264 [ 20.024206] remoteproc remoteproc7: unsupported resource 5 [ 20.024234] remoteproc remoteproc7: remote processor b134000.pru is now up [ 20.024264] remoteproc remoteproc8: powering up b104000.rtu [ 20.024410] remoteproc remoteproc8: Booting fw image ti-pruss/am65x-sr2-rtu0-prueth-fw.elf, size 30832 [ 20.024438] remoteproc remoteproc8: remote processor b104000.rtu is now up [ 20.024458] remoteproc remoteproc9: powering up b10a000.txpru [ 20.024590] remoteproc remoteproc9: Booting fw image ti-pruss/am65x-sr2-txpru0-prueth-fw.elf, size 36656 [ 20.045474] remoteproc remoteproc9: remote processor b10a000.txpru is now up [ 20.068126] TI DP83867 b132400.mdio:01: attached PHY driver [TI DP83867] (mii_bus:phy_addr=b132400.mdio:01, irq=POLL) [ 20.068385] net eth1: started [ 20.209561] TI DP83822 46000f00.mdio:03: attached PHY driver [TI DP83822] (mii_bus:phy_addr=46000f00.mdio:03, irq=POLL) [ 20.217645] am65-cpsw-nuss 46000000.ethernet eth0: Link is Down [ OK ] Started Login Service. [ OK ] Started Network Name Resolution. [ OK ] Reached target Network. [ OK ] Reached target Host and Network Name Lookups. Starting Avahi mDNS/DNS-SD Stack... Starting Enable and configure wl18xx bluetooth stack... [ OK ] Started NFS status monitor for NFSv2/3 locking.. Starting Simple Network Ma…ent Protocol (SNMP) Daemon.... Starting Permit User Sessions... [ OK ] Started Permit User Sessions. [ OK ] Started Getty on tty1. [ OK ] Started Serial Getty on ttyS1. [ OK ] Started Serial Getty on ttyS2. [ OK ] Reached target Login Prompts. Starting Synchronize System and HW clocks... [FAILED] Failed to start Synchronize System and HW clocks. See 'systemctl status sync-clocks.service' for details. [ OK ] Started Enable and configure wl18xx bluetooth stack. [ OK ] Started Avahi mDNS/DNS-SD Stack. [ OK ] Started Simple Network Man…ement Protocol (SNMP) Daemon.. [ 22.993546] icssg-prueth icssg1-eth eth2: Link is Up - 100Mbps/Full - flow control off [ 22.993632] IPv6: ADDRCONF(NETDEV_CHANGE): eth2: link becomes ready [ 23.290930] pvrsrvkm: disagrees about version of symbol finish_wait [ 23.290955] pvrsrvkm: Unknown symbol finish_wait (err -22) [ 23.291010] pvrsrvkm: disagrees about version of symbol prepare_to_wait [ 23.291014] pvrsrvkm: Unknown symbol prepare_to_wait (err -22) [ OK ] Started rc.pvr.service. Starting weston.service...[ 23.291074] pvrsrvkm: disagrees about version of symbol __wake_up [ 23.291078] pvrsrvkm: Unknown symbol __wake_up (err -22) [ 23.291255] pvrsrvkm: disagrees about version of symbol _dev_err [ 23.291258] pvrsrvkm: Unknown symbol _dev_err (err -22) [ 23.291414] pvrsrvkm: disagrees about version of symbol __init_waitqueue_head [ 23.291418] pvrsrvkm: Unknown symbol __init_waitqueue_head (err -22) [ 24.178307] icssg-prueth icssg1-eth eth1: Link is Up - 1Gbps/Full - flow control off [ 24.178396] IPv6: ADDRCONF(NETDEV_CHANGE): eth1: link becomes ready *************************************************************** *************************************************************** NOTICE: This file system contains the following GPLv3 packages: autoconf bash-dev bash bc binutils cifs-utils coreutils-stdbuf coreutils cpio cpp-symlinks cpp dosfstools elfutils g++-symlinks g++ gawk gcc-symlinks gcc gdb gdbserver gettext glmark2 gstreamer1.0-libav-dev gstreamer1.0-libav gzip less libasm1 libbfd libdw1 libelf1 libgdbm-compat4 libgdbm-dev libgdbm6 libgettextlib libgettextsrc libgmp-dev libgmp10 libgmpxx4 libidn2-0 libidn2-dev libmpc3 libmpfr6 libreadline-dev libreadline8 libunistring-dev libunistring2 m4-dev m4 make nettle-dev nettle parted pdm-anomaly-detection python3-rfc3987 python3-strict-rfc3339 tar which zeromq If you do not wish to distribute GPLv3 components please remove the above packages prior to distribution. This can be done using the opkg remove command. i.e.: opkg remove Where is the name printed in the list above NOTE: If the package is a dependency of another package you will be notified of the dependent packages. You should use the --force-removal-of-dependent-packages option to also remove the dependent packages as well *************************************************************** *************************************************************** _____ _____ _ _ | _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_ | | _| .'| . | . | | __| _| . | | | -_| _| _| |__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_| |___| |___| Arago Project http://arago-project.org am65xx-evm ttyS2 Arago 2021.09 am65xx-evm ttyS2 am65xx-evm login: am65xx-evm login: am65xx-evm login: am65xx-evm login: root root@am65xx-evm:~# ifconfig eth0: flags=4099 mtu 1500 metric 1 ether 40:2e:71:44:b0:88 txqueuelen 1000 (Ethernet) RX packets 0 bytes 0 (0.0 B) RX errors 0 dropped 0 overruns 0 frame 0 TX packets 0 bytes 0 (0.0 B) TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0 eth1: flags=4163 mtu 1500 metric 1 inet6 fe80::d8f9:a8ff:fe4e:4624 prefixlen 64 scopeid 0x20 ether da:f9:a8:4e:46:24 txqueuelen 1000 (Ethernet) RX packets 184 bytes 19827 (19.3 KiB) RX errors 0 dropped 0 overruns 0 frame 0 TX packets 24 bytes 4116 (4.0 KiB) TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0 eth2: flags=4163 mtu 1500 metric 1 inet6 fe80::b029:8ff:fe66:51b8 prefixlen 64 scopeid 0x20 ether b2:29:08:66:51:b8 txqueuelen 1000 (Ethernet) RX packets 0 bytes 0 (0.0 B) RX errors 0 dropped 0 overruns 0 frame 0 TX packets 25 bytes 4186 (4.0 KiB) TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0 eth3: flags=4099 mtu 1500 metric 1 ether ce:ce:bc:0e:67:4d txqueuelen 1000 (Ethernet) RX packets 0 bytes 0 (0.0 B) RX errors 0 dropped 0 overruns 0 frame 0 TX packets 0 bytes 0 (0.0 B) TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0 lo: flags=73 mtu 65536 metric 1 inet 127.0.0.1 netmask 255.0.0.0 inet6 ::1 prefixlen 128 scopeid 0x10 loop txqueuelen 1000 (Local Loopback) RX packets 82 bytes 6220 (6.0 KiB) RX errors 0 dropped 0 overruns 0 frame 0 TX packets 82 bytes 6220 (6.0 KiB) TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0 root@am65xx-evm:~# [ 52.849744] icssg-prueth icssg1-eth eth1: Link is Down [ 56.946212] icssg-prueth icssg1-eth eth1: Link is Up - 1Gbps/Full - flow control off root@am65xx-evm:~# root@am65xx-evm:~# root@am65xx-evm:~# ifconfig eth1 192.168.1.5 up root@am65xx-evm:~# [ 73.169337] icssg-prueth icssg1-eth eth2: Link is Down [ 76.241550] icssg-prueth icssg1-eth eth2: Link is Up - 100Mbps/Full - flow control off root@am65xx-evm:~# root@am65xx-evm:~# ethtool eth2 Settings for eth2: Supported ports: [ TP MII ] Supported link modes: 10baseT/Full 100baseT/Full Supported pause frame use: No Supports auto-negotiation: Yes Supported FEC modes: Not reported Advertised link modes: 10baseT/Full 100baseT/Full Advertised pause frame use: No Advertised auto-negotiation: Yes Advertised FEC modes: Not reported Link partner advertised link modes: 10baseT/Half 10baseT/Full 100baseT/Half 100baseT/Full Link partner advertised pause frame use: No Link partner advertised auto-negotiation: Yes Link partner advertised FEC modes: Not reported Speed: 100Mb/s Duplex: Full Auto-negotiation: on Port: Twisted Pair PHYAD: 7 Transceiver: external MDI-X: Unknown Current message level: 0x00007fff (32767) drv probe link timer ifdown ifup rx_err tx_err tx_queued intr tx_done rx_status pktdata hw wol Link detected: yes root@am65xx-evm:~# ethtool eth2 Settings for eth2: Supported ports: [ TP MII ] Supported link modes: 10baseT/Full 100baseT/Full Supported pause frame use: No Supports auto-negotiation: Yes Supported FEC modes: Not reported Advertised link modes: 10baseT/Full 100baseT/Full Advertised pause frame use: No Advertised auto-negotiation: Yes Advertised FEC modes: Not reported Link partner advertised link modes: 10baseT/Half 10baseT/Full 100baseT/Half 100baseT/Full Link partner advertised pause frame use: No Link partner advertised auto-negotiation: Yes Link partner advertised FEC modes: Not reported Speed: 100Mb/s Duplex: Full Auto-negotiation: on Port: Twisted Pair PHYAD: 7 Transceiver: external MDI-X: Unknown Current message level: 0x00007fff (32767) drv probe link timer ifdown ifup rx_err tx_err tx_queued intr tx_done rx_status pktdata hw wol Link detected: yes root@am65xx-evm:~# [ 140.889180] Initializing XFRM netlink socket [ 144.588154] process 'docker/tmp/qemu-check188148612/check' started with executable stack root@am65xx-evm:~# root@am65xx-evm:~# ethtool -S eth2 NIC statistics: rx_good_frames: 0 rx_broadcast_frames: 13 rx_multicast_frames: 13 rx_crc_error_frames: 45 rx_mii_error_frames: 0 rx_odd_nibble_frames: 0 rx_frame_max_size: 2000 rx_max_size_error_frames: 0 rx_frame_min_size: 64 rx_min_size_error_frames: 45 rx_overrun_frames: 0 rx_class0_hits: 45 rx_class1_hits: 0 rx_class2_hits: 0 rx_class3_hits: 0 rx_class4_hits: 0 rx_class5_hits: 0 rx_class6_hits: 0 rx_class7_hits: 0 rx_class8_hits: 45 rx_class9_hits: 45 rx_class10_hits: 0 rx_class11_hits: 0 rx_class12_hits: 0 rx_class13_hits: 0 rx_class14_hits: 0 rx_class15_hits: 0 rx_smd_frags: 0 rx_bucket1_size: 64 rx_bucket2_size: 128 rx_bucket3_size: 256 rx_bucket4_size: 512 rx_64B_frames: 0 rx_bucket1_frames: 45 rx_bucket2_frames: 0 rx_bucket3_frames: 0 rx_bucket4_frames: 0 rx_bucket5_frames: 0 rx_total_bytes: 507 rx_tx_total_bytes: 8925 tx_good_frames: 45 tx_broadcast_frames: 13 tx_multicast_frames: 45 tx_odd_nibble_frames: 0 tx_underflow_errors: 0 tx_frame_max_size: 2000 tx_max_size_error_frames: 0 tx_frame_min_size: 64 tx_min_size_error_frames: 0 tx_bucket1_size: 64 tx_bucket2_size: 128 tx_bucket3_size: 256 tx_bucket4_size: 512 tx_64B_frames: 0 tx_bucket1_frames: 0 tx_bucket2_frames: 24 tx_bucket3_frames: 8 tx_bucket4_frames: 13 tx_bucket5_frames: 0 tx_total_bytes: 8418 root@am65xx-evm:~# root@am65xx-evm:~# root@am65xx-evm:~# root@am65xx-evm:~# cd /home/ root@am65xx-evm:/home# ls 3_5_17_10 AX5root codesys root sdcard root@am65xx-evm:/home# cd 3_5_17_10/ root@am65xx-evm:/home/3_5_17_10# ls CODESYSControl.cfg PlcLogic SysFileMap.cfg cert codesyscontrol codesyscontrol.a root@am65xx-evm:/home/3_5_17_10# ./codesyscontrol & [1] 1231 root@am65xx-evm:/home/3_5_17_10# [ 219.375173] can: controller area network core [ 219.375284] NET: Registered protocol family 29 [ 219.395277] can: raw protocol _/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/ _/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/ _/_/_/_/ _/_/_/_/ _/_/_/_/_/ _/_/_/_/_/_/ _/_/_/_/_/ _/_/ _/_/ _/_/_/_/_/ _/ _/_/_/_/_/_/ _/_/_/_/_/_/ _/_/_/_/_/_/ _/_/_/_/_/_/ _/_/_/_/_/_/ _/_/ _/_/ _/_/_/_/_/_/ _/_/_/ _/_/ _/_/ _/_/ _/_/ _/_/ _/_/ _/_/ _/_/ _/_/ _/_/ _/_/ _/_/_/_/_/ _/_/ _/_/ _/_/ _/_/ _/_/ _/_/_/_/ _/_/_/_/ _/_/_/_/ _/_/_/_/ _/_/_/_/_/_/_/ _/_/ _/_/ _/_/ _/_/ _/_/ _/_/ _/_/ _/_/ _/_/ _/_/ _/_/_/_/_/ _/_/_/_/_/_/ _/_/_/_/_/_/ _/_/_/_/_/_/ _/_/_/_/_/_/ _/_/_/_/_/_/ _/_/ _/_/_/_/_/_/ _/_/_/ _/_/_/_/ _/_/_/_/ _/_/_/_/_/ _/_/_/_/_/_/ _/_/_/_/_/ _/_/ _/_/_/_/_/ _/ _/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/ _/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/ 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= System: CM, 0x00000001 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= System: CmpMemPool, 0x0000001e 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= System: CmpLog, 0x000[ 219.628963] device eth3 entered promiscuous mode 00013 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= System: CmpSettings, 0x0000001a 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= System: SysFile, 0x00000104 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= System: SysCom, 0x00000100 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= System: SysCpuHandling, 0x00000101 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= System: SysCrypto, 0x00000141 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= System: SysDir, 0x0000011b 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= System: SysEthernet, 0x0000011c 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= System: SysEvent, 0x00000102 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= System: SysExcept, 0x00000103 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= System: SysInternalLib, 0x00000107 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= System: SysMem, 0x00000108 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= System: SysModule, 0x00000109 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= System: SysMsgQ, 0x0000010a 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= System: SysMutex, 0x0000013a 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= System: SysOut, 0x0000010b 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= System: SysProcess, 0x0000010e 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= System: SysSem, 0x0000010f 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= System: SysSemCount, 0x00000139 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= System: SysSemProcess, 0x00000119 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= System: SysShm, 0x00000110 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= System: SysSocket, 0x00000111 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= System: SysTarget, 0x00000112 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= System: SysTask, 0x00000114 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= System: SysTime, 0x00000115 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= System: SysTimeRtc, 0x00000127 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= System: SysTimer, 0x00000116 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpAlarmManager, 0x0000007c 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpApp, 0x00000002 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpAppBP, 0x00000073 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpAppForce, 0x00000074 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpAsyncMgr, 0x0000005f 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpBinTagUtil, 0x00000004 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpBinTagUtilIec, 0x0000005c 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpBlkDrvCom, 0x00000006 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpBlkDrvTcp, 0x00000030 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpBlkDrvUdp, 0x00000007 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpCAAAsyncMan, 0x00004007 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpCAABehaviourModel, 0x00004015 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpCAACallback, 0x00004001 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpCAACanL2, 0x00004004 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpCAADTUtil, 0x00004013 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpCAAFile, 0x00004008 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpCAAMemBlockMan, 0x00004003 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpCAANetBaseServices, 0x00004018 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpCAARealTimeClock, 0x00004014 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpCAASdoClient, 0x00004011 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpCAASdoServer, 0x00004017 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpCAASegBufferMan, 0x00004019 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpCAASerialCom, 0x00004012 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpCAAStorage, 0x0000007e 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpCAATick, 0x00004009 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpCAATickUtil, 0x00004010 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpCAATimer, 0x00004016 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpCAATypes, 0x00004006 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpChannelClient, 0x00000008 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpChannelClientIec, 0x0000005d 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpChannelMgr, 0x00000009 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpChannelServer, 0x0000000a 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpCharDevice, 0x00000300 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpChecksum, 0x0000000b 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpCodeMeter, 0x0000007a 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpCommunicationLib, 0x0000000c 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpCoreDump, 0x00000083 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpCryptMD5, 0x0000006a 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpDevice, 0x0000000e 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpEL6751CanDrv, 0x00005f0b 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpEventMgr, 0x0000005b 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpFileTransfer, 0x0000005e 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpIecStringUtils, 0x0000007f 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpIecTask, 0x00000011 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpIecVarAccess, 0x00000060 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpIoDrvIec, 0x0000005a 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpIoMgr, 0x00000012 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpMonitor2, 0x00000032 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpNameServiceClient, 0x00000015 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpNameServiceClientIec, 0x0000011d 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpNameServiceServer, 0x00000016 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpOPCUAProviderIecVarAccess, 0x00000126 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpOPCUAServer, 0x00000124 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpOPCUAStack, 0x0000008d 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpObjectMgr, 0x00000080 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpOpenSSL, 0x00000033 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpPlcShell, 0x00000128 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpRetain, 0x00000017 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpRouter, 0x00000018 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpSchedule, 0x00000019 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpSecureChannel, 0x00000090 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpSecurityManager, 0x0000008e 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpSessionInformation, 0x00000097 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpSocketCanDrv, 0x00005f0d 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpSrv, 0x0000001c 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpTraceMgr, 0x00000070 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpUserDBFile, 0x00000098 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpUserGroupsDBFile, 0x00000099 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpUserMgr, 0x00000061 3.5.17.10 2022-03-24T05:21:59.360Z: Cmp=CM, Class=1, Error=0, Info=10, pszInfo= CmpUserObjectsDBFile, 0x0000009c 3.5.17.10 2022-03-24T05:21:59.589Z: Cmp=CmpBlkDrvUdp, Class=1, Error=0, Info=6, pszInfo= Network interface: 192.168.1.5, subnetmask 255.255.255.0 2022-03-24T05:21:59.589Z: Cmp=CmpRouter, Class=1, Error=0, Info=4, pszInfo= Network interface ether 2 at router 0 registered 2022-03-24T05:21:59.589Z: Cmp=CmpBlkDrvUdp, Class=1, Error=0, Info=6, pszInfo= Network interface: 172.17.0.1, subnetmask 255.255.0.0 2022-03-24T05:21:59.589Z: Cmp=CmpRouter, Class=1, Error=0, Info=4, pszInfo= Network interface ether 5 at router 1 registered 2022-03-24T05:21:59.589Z: Cmp=CmpChannelMgr, Class=1, Error=0, Info=2, pszInfo= Running as network server 2022-03-24T05:21:59.589Z: Cmp=CmpChannelMgr, Class=1, Error=0, Info=1, pszInfo= Running as network client 2022-03-24T05:21:59.591Z: Cmp=CmpChannelServer, Class=1, Error=0, Info=0, pszInfo= 4 channels available, each of the size 100000 Bytes 2022-03-24T05:21:59.649Z: Cmp=CmpBlkDrvTcp, Class=1, Error=0, Info=6, pszInfo= Local network address: 192.168.1.5 2022-03-24T05:21:59.649Z: Cmp=CmpRouter, Class=1, Error=0, Info=4, pszInfo= Network interface BlkDrvTcp at router 2 registered 2022-03-24T05:21:59.658Z: Cmp=CmpOPCUAServer, Class=1, Error=0, Info=0, pszInfo= No certificate for the OPC UA server available. 2022-03-24T05:21:59.658Z: Cmp=CmpOPCUAServer, Class=1, Error=0, Info=0, pszInfo= Security policy allows plain text communication. Secure communication is deactivated. 2022-03-24T05:21:59.659Z: Cmp=CmpOPCUAServer, Class=1, Error=0, Info=0, pszInfo= ************************************************************** 2022-03-24T05:21:59.659Z: Cmp=CmpOPCUAServer, Class=1, Error=0, Info=0, pszInfo= OPC UA Server Started: 2022-03-24T05:21:59.659Z: Cmp=CmpOPCUAServer, Class=1, Error=0, Info=0, pszInfo= Hostname: am65xx-evm, Port: 4840 2022-03-24T05:21:59.659Z: Cmp=CmpOPCUAServer, Class=1, Error=0, Info=0, pszInfo= URL: opc.tcp://am65xx-evm:4840 2022-03-24T05:21:59.659Z: Cmp=CmpOPCUAServer, Class=1, Error=0, Info=0, pszInfo= Loopbackadapter activated. 2022-03-24T05:21:59.659Z: Cmp=CmpOPCUAServer, Class=1, Error=0, Info=0, pszInfo= All available networkadapters are used. 2022-03-24T05:21:59.659Z: Cmp=CmpOPCUAServer, Class=1, Error=0, Info=0, pszInfo= ************************************************************** 2022-03-24T05:22:00.365Z: Cmp=CmpOPCUAServer, Class=1, Error=0, Info=0, pszInfo= Provider 'CODESYS_DefaultProvider' (version 0x305110a) registered at the OPC UA server. 2022-03-24T05:22:00.399Z: Cmp=CmpSocketCanDrv, Class=1, Error=0, Info=1, pszInfo= registered interface can0 as can network 0 2022-03-24T05:22:00.399Z: Cmp=CmpSocketCanDrv, Class=1, Error=0, Info=1, pszInfo= registered interface can1 as can network 1 2022-03-24T05:22:00.419Z: Cmp=CM, Class=1, Error=0, Info=0, pszInfo= ========================================================================= 2022-03-24T05:22:00.419Z: Cmp=CM, Class=1, Error=0, Info=4, pszInfo= Delta AX-516-ARM_64-Linux-SM 2022-03-24T05:22:00.419Z: Cmp=CM, Class=1, Error=0, Info=4, pszInfo= OS=Linux, CPU=ARM, Arch=64Bit, Coding=C 2022-03-24T05:22:00.419Z: Cmp=CM, Class=1, Error=0, Info=6, pszInfo= 3.5.17.10 Sep 27 2021 2022-03-24T05:22:00.419Z: Cmp=CM, Class=1, Error=0, Info=5, pszInfo= Copyright (c) 2017-2020 CODESYS Development GmbH, Copyright (c) 1994-2016 3S-Smart Software Solutions GmbH 2022-03-24T05:22:00.419Z: Cmp=CM, Class=1, Error=0, Info=0, pszInfo= ========================================================================= 2022-03-24T05:22:00.426Z: Cmp=CmpOPCUAServer, Class=1, Error=0, Info=0, pszInfo= Provider 'AddressSpaceFragment Provider' (version 0x305110a) registered at the OPC UA server. 2022-03-24T05:22:00.427Z: Cmp=CmpOPCUAServer, Class=1, Error=0, Info=0, pszInfo= Provider 'OPC UA for IEC-61131-3' (version 0x305110a) registered at the OPC UA server. 2022-03-24T05:22:00.427Z: Cmp=CmpOPCUAServer, Class=1, Error=0, Info=0, pszInfo= Provider 'AlarmManager' (version 0x305110a) registered at the OPC UA server. 2022-03-24T05:22:00.560Z: Cmp=OnlineLicenseManager, Class=4, Error=0, Info=0, pszInfo=**** License file missing. 2022-03-24T05:22:00.569Z: Cmp=CmpApp, Class=1, Error=0, Info=22, pszInfo= No retain area in bootproject of application [Application] 2022-03-24T05:22:00.569Z: Cmp=CmpApp, Class=1, Error=0, Info=6, pszInfo= Bootproject of application [Application] loaded 2022-03-24T05:22:00.579Z: Cmp=CmpRouter, Class=1, Error=0, Info=1, pszInfo= Setting router 0 address to
(0005)
2022-03-24T05:22:00.579Z: Cmp=CmpRouter, Class=1, Error=0, Info=1, pszInfo= Setting router 1 address to
(0000:0001)
2022-03-24T05:22:00.579Z: Cmp=CmpRouter, Class=1, Error=0, Info=1, pszInfo= Setting router 2 address to
(2ddc:c0a8:0105)
2022-03-24T05:22:00.590Z: Cmp=CmpApp, Class=1, Error=0, Info=10, pszInfo= Application [Application] started 2022-03-24T05:22:00.594Z: Cmp=CM, Class=1, Error=0, Info=34, pszInfo= CODESYS Control ready 2022-03-24T05:22:00.626Z: Cmp=IoDrvEtherCAT, Class=1, Error=0, Info=0, pszInfo= Networkadapter opened 2022-03-24T05:22:00.626Z: Cmp=IoDrvEtherCAT, Class=1, Error=0, Info=0, pszInfo= Preparation successfull 2022-03-24T05:22:00.629Z: Cmp=OnlineLicenseManager, Class=4, Error=0, Info=0, pszInfo=**** Demo mode for ETCStack started. Will expire and stop! 2022-03-24T05:22:04.631Z: Cmp=IoDrvEtherCAT, Class=4, Error=0, Info=0, pszInfo=**** Checking slaves: perhaps slave(s) missing, mismatch to configuration or no communication at all. Use scan for devices to check! [ 247.403452] device eth3 left promiscuous mode 2022-03-24T05:22:29.035Z: Cmp=OnlineLicenseManager, Class=4, Error=0, Info=0, pszInfo=**** License file missing. 2022-03-24T05:22:29.042Z: Cmp=CmpApp, Class=1, Error=0, Info=2, pszInfo= Application [Application] loaded via [Download] [ 251.185062] device eth2 entered promiscuous mode 2022-03-24T05:22:32.152Z: Cmp=IoDrvEtherCAT, Class=1, Error=0, Info=0, pszInfo= No slaves added to the master 2022-03-24T05:22:32.183Z: Cmp=IoDrvEtherCAT, Class=1, Error=0, Info=0, pszInfo= Networkadapter opened 2022-03-24T05:22:32.183Z: Cmp=IoDrvEtherCAT, Class=1, Error=0, Info=0, pszInfo= Preparation successfull 2022-03-24T05:22:32.190Z: Cmp=OnlineLicenseManager, Class=4, Error=0, Info=0, pszInfo=**** Demo mode for ETCStack started. Will expire and stop! 2022-03-24T05:22:35.755Z: Cmp=IoDrvEtherCAT, Class=2, Error=0, Info=0, pszInfo=!!!! ScanModules: no slaves found 2022-03-24T05:22:36.190Z: Cmp=IoDrvEtherCAT, Class=4, Error=0, Info=0, pszInfo=**** Checking slaves: perhaps slave(s) missing, mismatch to configuration or no communication at all. Use scan for devices to check! 2022-03-24T05:22:42.134Z: Cmp=IoDrvEtherCAT, Class=2, Error=0, Info=0, pszInfo=!!!! ScanModules: no slaves found root@am65xx-evm:/home/3_5_17_10# root@am65xx-evm:/home/3_5_17_10# root@am65xx-evm:/home/3_5_17_10# root@am65xx-evm:/home/3_5_17_10# ethtool eth2 Settings for eth2: Supported ports: [ TP MII ] Supported link modes: 10baseT/Full 100baseT/Full Supported pause frame use: No Supports auto-negotiation: Yes Supported FEC modes: Not reported Advertised link modes: 10baseT/Full 100baseT/Full Advertised pause frame use: No Advertised auto-negotiation: Yes Advertised FEC modes: Not reported Link partner advertised link modes: 10baseT/Half 10baseT/Full 100baseT/Half 100baseT/Full Link partner advertised pause frame use: No Link partner advertised auto-negotiation: Yes Link partner advertised FEC modes: Not reported Speed: 100Mb/s Duplex: Full Auto-negotiation: on Port: Twisted Pair PHYAD: 7 Transceiver: external MDI-X: Unknown Current message level: 0x00007fff (32767) drv probe link timer ifdown ifup rx_err tx_err tx_queued intr tx_done rx_status pktdata hw wol Link detected: yes root@am65xx-evm:/home/3_5_17_10# ethtool -S eth2 NIC statistics: rx_good_frames: 304 rx_broadcast_frames: 319 rx_multicast_frames: 319 rx_crc_error_frames: 48 rx_mii_error_frames: 0 rx_odd_nibble_frames: 0 rx_frame_max_size: 2000 rx_max_size_error_frames: 0 rx_frame_min_size: 64 rx_min_size_error_frames: 48 rx_overrun_frames: 0 rx_class0_hits: 352 rx_class1_hits: 0 rx_class2_hits: 0 rx_class3_hits: 0 rx_class4_hits: 0 rx_class5_hits: 0 rx_class6_hits: 0 rx_class7_hits: 0 rx_class8_hits: 352 rx_class9_hits: 352 rx_class10_hits: 0 rx_class11_hits: 0 rx_class12_hits: 0 rx_class13_hits: 0 rx_class14_hits: 0 rx_class15_hits: 0 rx_smd_frags: 0 rx_bucket1_size: 64 rx_bucket2_size: 128 rx_bucket3_size: 256 rx_bucket4_size: 512 rx_64B_frames: 0 rx_bucket1_frames: 48 rx_bucket2_frames: 304 rx_bucket3_frames: 0 rx_bucket4_frames: 0 rx_bucket5_frames: 0 rx_total_bytes: 21257 rx_tx_total_bytes: 53553 tx_good_frames: 352 tx_broadcast_frames: 319 tx_multicast_frames: 352 tx_odd_nibble_frames: 0 tx_underflow_errors: 0 tx_frame_max_size: 2000 tx_max_size_error_frames: 0 tx_frame_min_size: 64 tx_min_size_error_frames: 0 tx_bucket1_size: 64 tx_bucket2_size: 128 tx_bucket3_size: 256 tx_bucket4_size: 512 tx_64B_frames: 0 tx_bucket1_frames: 0 tx_bucket2_frames: 329 tx_bucket3_frames: 8 tx_bucket4_frames: 15 tx_bucket5_frames: 0 tx_total_bytes: 32296 root@am65xx-evm:/home/3_5_17_10#