/******************************************************************************/
/* This GEL file is loaded on the command line of Code Composer               */
/* The StartUp() function is called every time you start                      */
/* Code Composer.  You can customize this function to                         */
/* initialize wait states or to perform other initialization.                 */
/*                                                                            */
/* File       :AM571x_DDR_Config.gel                                          */
/* Description:DDR3 initialization sequences for AM571x IDK EVM               */
/*                                                                            */
/* Revision history                                                           */
/* ===========================================================================*/
/* Version   Date      Change from previous version                           */
/* ===========================================================================*/
/* 0.5       20150424  Add HW Leveling support.                               */
/*                     Programming sequence clean-up and sync for AM57x       */
/* ===========================================================================*/
/* IMPORTANT:                                                                 */
/* 1. us_delay() is a dummy implementation - SW must implement it correctly   */
/* 2. Phy reset is required if you come back from a warm reset.               */
/*    GEL file does not modify the PRM_RSTST - Any SW implementation should   */
/*    take care of clearing this status so that a stale value is not used.    */
/* 3. EMIF_DDR3_UpdateHWLevelOutput() function is required only if HW leveling*/
/*    is used and if CORE can go in and out of INACTIVE / CSWR modes          */
/* 4. ENABLE_ECC is Reserved for future use, if set when ECC memories         */
/*    are not available will result in HW 									  */
/*    leveling time-out error                                                 */
/******************************************************************************/

#define HW_LEVELING_ENABLED      (1)
#define ENABLE_ECC               (0) /* If ECC memories are not available,
                                      * setting this to 1 will cause HW
                                      * leveling to time-out
                                      * PG1.0 - ECC must be disabled due to Errata i882
                                      */

menuitem "DDR Memory config"

/*
 * Following registers are derived from other parameters and should not be
 * defined
 * directly:
 * EXT_PHY_CTRL_1
 * DDR_PHY_CTRL_1
 * EXT_PHY_CTRL_22
 * EXT_PHY_CTRL_23
 * EXT_PHY_CTRL_24
 * EXT_PHY_CTRL_25
 */
static uint32_t SDRAM_TIM_1;
static uint32_t SDRAM_TIM_2;
static uint32_t SDRAM_TIM_3;
static uint32_t PWR_MGMT_CTRL;
static uint32_t OCP_CONFIG;
static uint32_t IODFT_TLGC;
static uint32_t DLL_CALIB_CTRL;
static uint32_t ZQ_CONFIG;
static uint32_t RDWR_LVL_RMP_WIN;
static uint32_t DDR_PHY_CTRL_2;
static uint32_t PRI_COS_MAP;
static uint32_t CONNID_COS_1_MAP;
static uint32_t CONNID_COS_2_MAP;
static uint32_t RD_WR_EXEC_THRSH;
static uint32_t COS_CONFIG;
static uint32_t EXT_PHY_CTRL_2;
static uint32_t EXT_PHY_CTRL_3;
static uint32_t EXT_PHY_CTRL_4;
static uint32_t EXT_PHY_CTRL_5;
static uint32_t EXT_PHY_CTRL_6;
static uint32_t EXT_PHY_CTRL_7;
static uint32_t EXT_PHY_CTRL_8;
static uint32_t EXT_PHY_CTRL_9;
static uint32_t EXT_PHY_CTRL_10;
static uint32_t EXT_PHY_CTRL_11;
static uint32_t EXT_PHY_CTRL_12;
static uint32_t EXT_PHY_CTRL_13;
static uint32_t EXT_PHY_CTRL_14;
static uint32_t EXT_PHY_CTRL_15;
static uint32_t EXT_PHY_CTRL_16;
static uint32_t EXT_PHY_CTRL_17;
static uint32_t EXT_PHY_CTRL_18;
static uint32_t EXT_PHY_CTRL_19;
static uint32_t EXT_PHY_CTRL_20;
static uint32_t EXT_PHY_CTRL_21;
static uint32_t EXT_PHY_CTRL_26;
static uint32_t EXT_PHY_CTRL_27;
static uint32_t EXT_PHY_CTRL_28;
static uint32_t EXT_PHY_CTRL_29;
static uint32_t EXT_PHY_CTRL_30;
static uint32_t EXT_PHY_CTRL_31;
static uint32_t EXT_PHY_CTRL_32;
static uint32_t EXT_PHY_CTRL_33;
static uint32_t EXT_PHY_CTRL_34;
static uint32_t EXT_PHY_CTRL_35;
static uint32_t EXT_PHY_CTRL_36;

static uint32_t SDRAM_REF_CTRL;
/* Example calculation:
 * For 7.8us at 666MHz : Value = 7.8u*666M = 0x144A
 */

static uint32_t SDRAM_CONFIG_2;
static uint32_t SDRAM_CONFIG;

/* Fields in DDR_PHY_CTRL_1 */
/* Bit[21] - calculated using DataMacro/MDLL clock ratio
 * Set to 1 for 666M, so that PHY DLL runs at 333M.
 * Set to 0 for 400M, so that PHY DLL runs at 400M.
 * Ensure PHY DLL lower limit of 266M is not violated.
 */
static uint32_t EMIF_PHY_HALF_DELAY_MODE;
static uint32_t EMIF_PHY_DIS_CALIB_RST;    /* Bit[19]    */
static uint32_t EMIF_PHY_INVERT_CLKOUT;    /* Bit[18]    */
static uint32_t EMIF_PHY_DLL_LOCK_DIFF;    /* Bit[17:10] */
static uint32_t EMIF_PHY_FAST_DLL_LOCK;    /* Bit[9]     */
static uint32_t EMIF_PHY_READ_LATENCY;     /* Bit[4:0], Typically >= (CL + 4) */

static uint32_t EMIF_PHY_USE_RANK0_DELAYS; /* Set to 1 if using ddr1_csn[0]
                                            * only.
                                            * Set to 0 otherwise.
                                            * ddr1_csn[1] is not supported on
                                            * AM572x.
                                            */
static uint32_t EMIF_PHY_CTRL_SLAVE_RATIO;
static uint32_t EMIF_PHY_DQ_OFFSET;
static uint32_t EMIF_PHY_GATELVL_INIT_MODE;
static uint32_t EMIF_PHY_FIFO_WE_IN_DELAY;    /* Only for DLL_OVERRIDE = 1 */
static uint32_t EMIF_PHY_CTRL_SLAVE_DELAY;    /* Only for DLL_OVERRIDE = 1 */
static uint32_t EMIF_PHY_RD_DQS_SLAVE_DELAY;  /* Only for DLL_OVERRIDE = 1 */
static uint32_t EMIF_PHY_WR_DQS_SLAVE_DELAY;  /* Only for DLL_OVERRIDE = 1 */
static uint32_t EMIF_PHY_WR_DATA_SLAVE_DELAY; /* Only for DLL_OVERRIDE = 1 */

/* SDRAM_REF_CTRL_INIT:
 * For DDR3:   value used initially to get 500us delay between
 *             RESET de-assertion to CKE assertion after power-up
 * Example calculation:
 * For 500us delay at 666MHz : Value = 500u*666M/16 = 0x514C
 */
static uint32_t SDRAM_REF_CTRL_INIT;

/* Following three values are applicable only when HW_LEVELING_ENABLED == 1.
 * These allows us to use a combination of HW leveling and SW leveling.
 * Currently only for debug.
 * If DISABLE_READ_LEVELING == 1
 *      Set EMIF_PHY_RD_DQS_SLAVE_RATIO registers with SW Leveling values
 * If DISABLE_READ_GATE_LEVELING == 1
 *      Set EMIF_PHY_FIFO_WE_SLAVE_RATIO registers with SW Leveling values
 * If DISABLE_WRITE_LEVELING == 1
 *      Set EMIF_PHY_WR_DQS_SLAVE_RATIO registers with SW Leveling values
 */
static uint32_t DISABLE_READ_LEVELING;
static uint32_t DISABLE_READ_GATE_LEVELING;
static uint32_t DISABLE_WRITE_LEVELING;

/* This is dummy function - GEL does not work real-time.
 * If GELs are imported to C code, this function must be implemented a loop of
 * "delay" microseconds
 */
static void us_delay(uint32_t delay)
{
    uint32_t loop;
    for (loop = 0; loop < delay * 100; loop++)
    {
        loop = loop;
    }
}

/* Wrapper function to simplify importing GEL file to a C code */
printf(char *temp)
{
    GEL_TextOut(temp);
}

static void AM571x_reset_emif_params_ddr3_666(uint32_t base_addr)
{
    uint32_t temp;

    EMIF_PHY_HALF_DELAY_MODE     = 1U;
    EMIF_PHY_DIS_CALIB_RST       = 0U;
    EMIF_PHY_INVERT_CLKOUT       = 1U;
    EMIF_PHY_DLL_LOCK_DIFF       = 0x10U;
    EMIF_PHY_FAST_DLL_LOCK       = 0U;
    EMIF_PHY_READ_LATENCY        = 0xDU;

    EMIF_PHY_USE_RANK0_DELAYS    = 1U; 

    EMIF_PHY_CTRL_SLAVE_RATIO    = 0x80U;
    EMIF_PHY_DQ_OFFSET           = 0x40U;
    EMIF_PHY_GATELVL_INIT_MODE   = 0x01U;
    EMIF_PHY_FIFO_WE_IN_DELAY    = 0x00U;
    EMIF_PHY_CTRL_SLAVE_DELAY    = 0x00U;
    EMIF_PHY_RD_DQS_SLAVE_DELAY  = 0x20U;
    EMIF_PHY_WR_DQS_SLAVE_DELAY  = 0x60U;
    EMIF_PHY_WR_DATA_SLAVE_DELAY = 0x80U;

    SDRAM_TIM_1         = 0xD113781C;
    SDRAM_TIM_2         = 0x30B37FE3;
    SDRAM_TIM_3         = 0x409F8AD8;
    
    PWR_MGMT_CTRL      = 0x00000000U;
    OCP_CONFIG         = 0x0A500000U;
    IODFT_TLGC         = HW_RD_REG32(base_addr +
                                     EMIF_IODFT_TLGC);
    DLL_CALIB_CTRL     = 0x00050000U;
    ZQ_CONFIG          = 0x5007190BU;
	
    RDWR_LVL_RMP_WIN   = HW_RD_REG32(base_addr +
                                     EMIF_READ_WRITE_LEVELING_RAMP_WINDOW);

    DDR_PHY_CTRL_2     = HW_RD_REG32(base_addr +
                                     EMIF_DDR_PHY_CONTROL_2);
    PRI_COS_MAP        = 0x00000000U;
    CONNID_COS_1_MAP   = 0x00000000U;
    CONNID_COS_2_MAP   = 0x00000000U;
    RD_WR_EXEC_THRSH   = 0x00000305U;
    COS_CONFIG         = 0x00FFFFFFU;

    /* EMIF_PHY_FIFO_WE_SLAVE_RATIO (RD_DQS_GATE) */
    temp = 0xBBU;
    EXT_PHY_CTRL_2     = (temp << 16U) | (temp << 0U);
    EXT_PHY_CTRL_3     = (temp << 16U) | (temp << 0U);
    EXT_PHY_CTRL_4     = (temp << 16U) | (temp << 0U);
    EXT_PHY_CTRL_5     = (temp << 16U) | (temp << 0U);
    EXT_PHY_CTRL_6     = (temp << 16U) | (temp << 0U);

    /* EMIF_PHY_RD_DQS_SLAVE_RATIO */
    temp = 0x44U;
    EXT_PHY_CTRL_7     = (temp << 16U) | (temp << 0U);
    EXT_PHY_CTRL_8     = (temp << 16U) | (temp << 0U);
    EXT_PHY_CTRL_9     = (temp << 16U) | (temp << 0U);
    EXT_PHY_CTRL_10    = (temp << 16U) | (temp << 0U);
    EXT_PHY_CTRL_11    = (temp << 16U) | (temp << 0U);

    /* EMIF_PHY_WR_DATA_SLAVE_RATIO */
    temp = 0x7FU;
    EXT_PHY_CTRL_12    = (temp << 16U) | (temp << 0U);
    EXT_PHY_CTRL_13    = (temp << 16U) | (temp << 0U);
    EXT_PHY_CTRL_14    = (temp << 16U) | (temp << 0U);
    EXT_PHY_CTRL_15    = (temp << 16U) | (temp << 0U);
    EXT_PHY_CTRL_16    = (temp << 16U) | (temp << 0U);

    /* EMIF_PHY_WR_DQS_SLAVE_RATIO */
    temp = 0x60U;
    EXT_PHY_CTRL_17    = (temp << 16U) | (temp << 0U);
    EXT_PHY_CTRL_18    = (temp << 16U) | (temp << 0U);
    EXT_PHY_CTRL_19    = (temp << 16U) | (temp << 0U);
    EXT_PHY_CTRL_20    = (temp << 16U) | (temp << 0U);
    EXT_PHY_CTRL_21    = (temp << 16U) | (temp << 0U);

    /* EMIF_PHY_GATELVL_INIT_RATIO */
    temp = 0U;
    EXT_PHY_CTRL_26    = (temp << 16U) | (temp << 0U);
    EXT_PHY_CTRL_27    = (temp << 16U) | (temp << 0U);
    EXT_PHY_CTRL_28    = (temp << 16U) | (temp << 0U);
    EXT_PHY_CTRL_29    = (temp << 16U) | (temp << 0U);
    EXT_PHY_CTRL_30    = (temp << 16U) | (temp << 0U);

    /* EMIF_PHY_WRLVL_INIT_RATIO */
    temp = 0U;
    EXT_PHY_CTRL_31    = (temp << 16U) | (temp << 0U);
    EXT_PHY_CTRL_32    = (temp << 16U) | (temp << 0U);
    EXT_PHY_CTRL_33    = (temp << 16U) | (temp << 0U);
    EXT_PHY_CTRL_34    = (temp << 16U) | (temp << 0U);
    EXT_PHY_CTRL_35    = (temp << 16U) | (temp << 0U);

    EXT_PHY_CTRL_36    = HW_RD_REG32(base_addr +
                                     EMIF_EXT_PHY_CONTROL_36);
    EXT_PHY_CTRL_36    = HW_RD_REG32(base_addr +
                                     EMIF_EXT_PHY_CONTROL_36_SHADOW);

    SDRAM_REF_CTRL     = 0x0000144AU;
    SDRAM_CONFIG_2     = 0x08000000U;
    SDRAM_CONFIG       = 0x61862B32U;

    DISABLE_READ_LEVELING      = 0U;
    DISABLE_READ_GATE_LEVELING = 0U;
    DISABLE_WRITE_LEVELING     = 0U;
}

static void AM571x_set_emif1_params_ddr3_666(uint32_t base_addr)
{
    SDRAM_TIM_1         = 0xD113781C;
    SDRAM_TIM_2         = 0x30B37FE3;
    SDRAM_TIM_3         = 0x409F8AD8;

    SDRAM_REF_CTRL      = 0x0000144AU;
    SDRAM_CONFIG        = 0x61862B32U;
    SDRAM_REF_CTRL_INIT = 0x0000514CU;

    /* EMIF_PHY_FIFO_WE_SLAVE_RATIO (RD_DQS_GATE) */
    EXT_PHY_CTRL_2     = 0x00A400A4U;
    EXT_PHY_CTRL_3     = 0x00A900A9U;
    EXT_PHY_CTRL_4     = 0x00B000B0U;
    EXT_PHY_CTRL_5     = 0x00B000B0U;
    EXT_PHY_CTRL_6     = 0x00A400A4U;

    /* EMIF_PHY_RD_DQS_SLAVE_RATIO */
    EXT_PHY_CTRL_7     = 0x002F002FU;
    EXT_PHY_CTRL_8     = 0x002F002FU;
    EXT_PHY_CTRL_9     = 0x002F002FU;
    EXT_PHY_CTRL_10    = 0x002F002FU;
    EXT_PHY_CTRL_11    = 0x002F002FU;

    /* EMIF_PHY_WR_DQS_SLAVE_RATIO */
    EXT_PHY_CTRL_17    = 0x004D004DU;
    EXT_PHY_CTRL_18    = 0x00430043U;
    EXT_PHY_CTRL_19    = 0x00560056U;
    EXT_PHY_CTRL_20    = 0x00540054U;
    EXT_PHY_CTRL_21    = 0x00600060U;
}

static void AM571x_set_lisa_maps()
{
    /* MA_LISA_MAP_i */
    HW_WR_REG32(SOC_MA_MPU_CONF_REGS_BASE + LISA_MAP_0, 0x80600100U);
    HW_WR_REG32(SOC_MA_MPU_CONF_REGS_BASE + LISA_MAP_1, 0x00000000U);
    HW_WR_REG32(SOC_MA_MPU_CONF_REGS_BASE + LISA_MAP_2, 0x00000000U);
    HW_WR_REG32(SOC_MA_MPU_CONF_REGS_BASE + LISA_MAP_3, 0x00000000U);
    /* DMM_LISA_MAP_i */
    HW_WR_REG32(SOC_DMM_CONF_REGS_BASE + LISA_MAP_0, 0x80600100U);
    HW_WR_REG32(SOC_DMM_CONF_REGS_BASE + LISA_MAP_1, 0x00000000U);
    HW_WR_REG32(SOC_DMM_CONF_REGS_BASE + LISA_MAP_2, 0x00000000U);
    HW_WR_REG32(SOC_DMM_CONF_REGS_BASE + LISA_MAP_3, 0x00000000U);
}

static void AM571x_CM_DDRIO_Config()
{
    /* DLL_OVERRIDE: No Override = 0; Override = 1
     * Value 1 is only for debug
     */
    HW_WR_REG32(SOC_CKGEN_CM_CORE_AON_BASE + CM_DLL_CTRL, 0);
    
	/* CTRL_CORE_CONTROL_DDRCACH1_0
	 * - Impedance = 40ohm (34ohm for DDRCH1_PART6)/
	 *   SlewRate = fastest / No pulls */
	/* CTRL_CORE_CONTROL_DDRCH1_0
	 * - Impedance = 40ohm / SlewRate = fastest / No pulls */
	/* CTRL_CORE_CONTROL_DDRCH1_1
	 * - Impedance = 40ohm / SlewRate = fastest / No pulls */
	/* CTRL_CORE_CONTROL_DDRCH1_2
	 * - Impedance = 40ohm / SlewRate = fastest / No pulls */
	HW_WR_REG32(SOC_CTRL_MODULE_CORE_CORE_PAD_REGISTERS_BASE +
				CTRL_CORE_CONTROL_DDRCACH1_0,
				0x60606080U);
	HW_WR_REG32(SOC_CTRL_MODULE_CORE_CORE_PAD_REGISTERS_BASE +
				CTRL_CORE_CONTROL_DDRCH1_0,
				0x40404040U);
	HW_WR_REG32(SOC_CTRL_MODULE_CORE_CORE_PAD_REGISTERS_BASE +
				CTRL_CORE_CONTROL_DDRCH1_1,
				0x40404040U);
	HW_WR_REG32(SOC_CTRL_MODULE_CORE_CORE_PAD_REGISTERS_BASE +
				CTRL_CORE_CONTROL_DDRCH1_2,
				0x00404000U);

	/* CTRL_CORE_CONTROL_DDRIO_0
	 * - DDRCH1_VREF_DQ0/1_INT_EN = 0, reset values for other fields */
	/* CTRL_CORE_CONTROL_DDRIO_0
	 * - DDRCH2_VREF_DQ0/1_INT_EN = 0, reset values for other fields */
	HW_WR_REG32(SOC_CTRL_MODULE_CORE_CORE_PAD_REGISTERS_BASE +
				CTRL_CORE_CONTROL_DDRIO_0,
				0x00094A40U);
   
    /* CTRL_WKUP_EMIF1/2_SDRAM_CONFIG_EXT
     * - EMIF1_REG_PHY_NUM_OF_SAMPLES = 3
     * - EMIF1_REG_PHY_ALL_DQ_MPR_RD_RESP = 0
     * - EMIF1_PHY_RD_LOCAL_ODT = 60ohms
     * - EMIF1_SDRAM_DISABLE_RESET = 0
	 *   Always set to 1, this is needed for suspend-to-ram use-cases.
     *   There is no impact of setting this to 1 even if ECC memory is not
     *   available on the system.
     * - Reset values for other fields.
     */
     HW_WR_REG32(SOC_CTRL_MODULE_WKUP_CORE_REGISTERS_BASE +
                 CTRL_WKUP_EMIF1_SDRAM_CONFIG_EXT,
                 0x0001C127U);

}

static void EMIF_DDR3_UpdateHWLevelOutput(uint32_t base_addr)
{
    /* Following function is needed for whenever CORE can go in and out of
     * INACTIVE/CSWR */
    printf("       Updating slave ratios in PHY_STATUSx registers\n");
    printf("       as per HW leveling output\n");

    if(0U == DISABLE_READ_GATE_LEVELING)
    {
        /* EMIF_PHY_FIFO_WE_SLAVE_RATIO (RD_DQS_GATE) */
        HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_2,
                    HW_RD_REG32(base_addr + EMIF_PHY_STATUS_12));
        HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_2_SHADOW,
                    HW_RD_REG32(base_addr + EMIF_PHY_STATUS_12));
        HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_3,
                    HW_RD_REG32(base_addr + EMIF_PHY_STATUS_13));
        HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_3_SHADOW,
                    HW_RD_REG32(base_addr + EMIF_PHY_STATUS_13));
        HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_4,
                    HW_RD_REG32(base_addr + EMIF_PHY_STATUS_14));
        HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_4_SHADOW,
                    HW_RD_REG32(base_addr + EMIF_PHY_STATUS_14));
        HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_5,
                    HW_RD_REG32(base_addr + EMIF_PHY_STATUS_15));
        HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_5_SHADOW,
                    HW_RD_REG32(base_addr + EMIF_PHY_STATUS_15));
        HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_6,
                    HW_RD_REG32(base_addr + EMIF_PHY_STATUS_16));
        HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_6_SHADOW,
                    HW_RD_REG32(base_addr + EMIF_PHY_STATUS_16));
    }

    if(0U == DISABLE_READ_LEVELING)
    {
        /* EMIF_PHY_RD_DQS_SLAVE_RATIO */
        HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_7,
                    HW_RD_REG32(base_addr + EMIF_PHY_STATUS_7));
        HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_7_SHADOW,
                    HW_RD_REG32(base_addr + EMIF_PHY_STATUS_7));
        HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_8,
                    HW_RD_REG32(base_addr + EMIF_PHY_STATUS_8));
        HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_8_SHADOW,
                    HW_RD_REG32(base_addr + EMIF_PHY_STATUS_8));
        HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_9,
                    HW_RD_REG32(base_addr + EMIF_PHY_STATUS_9));
        HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_9_SHADOW,
                    HW_RD_REG32(base_addr + EMIF_PHY_STATUS_9));
        HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_10,
                    HW_RD_REG32(base_addr + EMIF_PHY_STATUS_10));
        HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_10_SHADOW,
                    HW_RD_REG32(base_addr + EMIF_PHY_STATUS_10));
        HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_11,
                    HW_RD_REG32(base_addr + EMIF_PHY_STATUS_11));
        HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_11_SHADOW,
                    HW_RD_REG32(base_addr + EMIF_PHY_STATUS_11));
    }

    if(0U == DISABLE_WRITE_LEVELING)
    {
        /* EMIF_PHY_WR_DATA_SLAVE_RATIO */
        HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_12,
                    HW_RD_REG32(base_addr + EMIF_PHY_STATUS_17));
        HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_12_SHADOW,
                    HW_RD_REG32(base_addr + EMIF_PHY_STATUS_17));
        HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_13,
                    HW_RD_REG32(base_addr + EMIF_PHY_STATUS_18));
        HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_13_SHADOW,
                    HW_RD_REG32(base_addr + EMIF_PHY_STATUS_18));
        HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_14,
                    HW_RD_REG32(base_addr + EMIF_PHY_STATUS_19));
        HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_14_SHADOW,
                    HW_RD_REG32(base_addr + EMIF_PHY_STATUS_19));
        HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_15,
                    HW_RD_REG32(base_addr + EMIF_PHY_STATUS_20));
        HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_15_SHADOW,
                    HW_RD_REG32(base_addr + EMIF_PHY_STATUS_20));
        HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_16,
                    HW_RD_REG32(base_addr + EMIF_PHY_STATUS_21));
        HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_16_SHADOW,
                    HW_RD_REG32(base_addr + EMIF_PHY_STATUS_21));

        /* EMIF_PHY_WR_DQS_SLAVE_RATIO */
        HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_17,
                    HW_RD_REG32(base_addr + EMIF_PHY_STATUS_22));
        HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_17_SHADOW,
                    HW_RD_REG32(base_addr + EMIF_PHY_STATUS_22));
        HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_18,
                    HW_RD_REG32(base_addr + EMIF_PHY_STATUS_23));
        HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_18_SHADOW,
                    HW_RD_REG32(base_addr + EMIF_PHY_STATUS_23));
        HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_19,
                    HW_RD_REG32(base_addr + EMIF_PHY_STATUS_24));
        HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_19_SHADOW,
                    HW_RD_REG32(base_addr + EMIF_PHY_STATUS_24));
        HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_20,
                    HW_RD_REG32(base_addr + EMIF_PHY_STATUS_25));
        HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_20_SHADOW,
                    HW_RD_REG32(base_addr + EMIF_PHY_STATUS_25));
        HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_21,
                    HW_RD_REG32(base_addr + EMIF_PHY_STATUS_26));
        HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_21_SHADOW,
                    HW_RD_REG32(base_addr + EMIF_PHY_STATUS_26));
    }

    HW_WR_REG32(base_addr + EMIF_DDR_PHY_CONTROL_1,
                (HW_RD_REG32(base_addr + EMIF_DDR_PHY_CONTROL_1) |
                 EMIF_DDR_PHY_CONTROL_1_WRLVL_MASK_MASK |
                 EMIF_DDR_PHY_CONTROL_1_RDLVLGATE_MASK_MASK |
                 EMIF_DDR_PHY_CONTROL_1_RDLVL_MASK_MASK));
    HW_WR_REG32(base_addr + EMIF_DDR_PHY_CONTROL_1_SHADOW,
                (HW_RD_REG32(base_addr + EMIF_DDR_PHY_CONTROL_1_SHADOW) |
                 EMIF_DDR_PHY_CONTROL_1_WRLVL_MASK_MASK |
                 EMIF_DDR_PHY_CONTROL_1_RDLVLGATE_MASK_MASK |
                 EMIF_DDR_PHY_CONTROL_1_RDLVL_MASK_MASK));
    HW_WR_REG32(base_addr + EMIF_READ_WRITE_LEVELING_RAMP_CONTROL, 0U);

    printf("       HW leveling is now disabled. Using slave ratios from \n");
    printf("       PHY_STATUSx registers\n");
}

static void EMIF_Config(uint32_t base_addr,
                        uint32_t isHwLevelingEnabledInput,
                        uint32_t isEccEnabled)
{
    uint32_t EXT_PHY_CTRL_1;
    uint32_t DDR_PHY_CTRL_1;
    uint32_t EXT_PHY_CTRL_22;
    uint32_t EXT_PHY_CTRL_23;
    uint32_t EXT_PHY_CTRL_24;
    uint32_t EXT_PHY_CTRL_25;
    uint32_t RDWR_LVL_RMP_CTRL;
    uint32_t EMIF_PHY_LEVLELING_DISABLED;
    uint32_t isHwLevelingEnabled;

    isHwLevelingEnabled = isHwLevelingEnabledInput;   

    if (1U == isHwLevelingEnabled)
    {
        EMIF_PHY_LEVLELING_DISABLED = 0U;
        if(1U == DISABLE_READ_LEVELING)
        {
            EMIF_PHY_LEVLELING_DISABLED |=
                EMIF_DDR_PHY_CONTROL_1_RDLVL_MASK_MASK;
        }
        if(1U == DISABLE_READ_GATE_LEVELING)
        {
            EMIF_PHY_LEVLELING_DISABLED |=
                EMIF_DDR_PHY_CONTROL_1_RDLVLGATE_MASK_MASK;
        }
        if(1U == DISABLE_WRITE_LEVELING)
        {
            EMIF_PHY_LEVLELING_DISABLED |=
                EMIF_DDR_PHY_CONTROL_1_WRLVL_MASK_MASK;
        }

        RDWR_LVL_RMP_CTRL =
            EMIF_READ_WRITE_LEVELING_RAMP_CONTROL_RDWRLVL_EN_MASK;
    }
    else
    {
        EMIF_PHY_LEVLELING_DISABLED =
            EMIF_DDR_PHY_CONTROL_1_WRLVL_MASK_MASK |
            EMIF_DDR_PHY_CONTROL_1_RDLVLGATE_MASK_MASK |
            EMIF_DDR_PHY_CONTROL_1_RDLVL_MASK_MASK;

        RDWR_LVL_RMP_CTRL = 0U;
    }

    DDR_PHY_CTRL_1  = (EMIF_PHY_READ_LATENCY        <<  0U)|
                      (EMIF_PHY_FAST_DLL_LOCK       <<  9U)|
                      (EMIF_PHY_DLL_LOCK_DIFF       << 10U)|
                      (EMIF_PHY_INVERT_CLKOUT       << 18U)|
                      (EMIF_PHY_DIS_CALIB_RST       << 19U)|
                      (EMIF_PHY_HALF_DELAY_MODE     << 21U)|
                      (EMIF_PHY_LEVLELING_DISABLED);
    EXT_PHY_CTRL_22 = (EMIF_PHY_FIFO_WE_IN_DELAY    << 16U)|
                      (EMIF_PHY_CTRL_SLAVE_DELAY    <<  0U);
    EXT_PHY_CTRL_23 = (EMIF_PHY_WR_DQS_SLAVE_DELAY  << 16U)|
                      (EMIF_PHY_RD_DQS_SLAVE_DELAY  <<  0U);
    EXT_PHY_CTRL_24 = (EMIF_PHY_DQ_OFFSET           << 24U)|
                      (EMIF_PHY_GATELVL_INIT_MODE   << 16U)|
                      (EMIF_PHY_USE_RANK0_DELAYS    << 12U)|
                      (EMIF_PHY_WR_DATA_SLAVE_DELAY <<  0U);
    EXT_PHY_CTRL_25 = (EMIF_PHY_DQ_OFFSET           << 21U)|
                      (EMIF_PHY_DQ_OFFSET           << 14U)|
                      (EMIF_PHY_DQ_OFFSET           <<  7U)|
                      (EMIF_PHY_DQ_OFFSET           <<  0U);

    if (0U != HW_RD_REG32(SOC_DEVICE_PRM_BASE + PRM_RSTST) &
        (PRM_RSTST_GLOBAL_WARM_SW_RST_MASK | PRM_RSTST_EXTERNAL_WARM_RST_MASK))
    {
        /* Phy reset is required if you are coming back from a warm reset */
        HW_WR_REG32(base_addr + EMIF_IODFT_TLGC,
                    HW_RD_REG32(base_addr + EMIF_IODFT_TLGC) | 0x400U);
    }

    if (1U == EMIF_PHY_INVERT_CLKOUT)
    {
        EXT_PHY_CTRL_1 = ((EMIF_PHY_CTRL_SLAVE_RATIO + 0x80U) << 20U) |
                         ((EMIF_PHY_CTRL_SLAVE_RATIO + 0x80U) << 10U) |
                         ((EMIF_PHY_CTRL_SLAVE_RATIO + 0x80U) << 0U);
    }
    else
    {
        EXT_PHY_CTRL_1 = (EMIF_PHY_CTRL_SLAVE_RATIO << 20U) |
                         (EMIF_PHY_CTRL_SLAVE_RATIO << 10U) |
                         (EMIF_PHY_CTRL_SLAVE_RATIO << 0U);
    }
    HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_1,
                EXT_PHY_CTRL_1);
    HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_1_SHADOW,
                EXT_PHY_CTRL_1);
    
	if (((1U == isHwLevelingEnabled) &&
		 (1U == DISABLE_READ_GATE_LEVELING)) ||
		(0U == isHwLevelingEnabled))
	{
		/* EMIF_PHY_FIFO_WE_SLAVE_RATIO (RD_DQS_GATE) */
		HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_2,
					EXT_PHY_CTRL_2);
		HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_2_SHADOW,
					EXT_PHY_CTRL_2);
		HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_3,
					EXT_PHY_CTRL_3);
		HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_3_SHADOW,
					EXT_PHY_CTRL_3);
		HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_4,
					EXT_PHY_CTRL_4);
		HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_4_SHADOW,
					EXT_PHY_CTRL_4);
		HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_5,
					EXT_PHY_CTRL_5);
		HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_5_SHADOW,
					EXT_PHY_CTRL_5);
		HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_6,
					EXT_PHY_CTRL_6);
		HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_6_SHADOW,
					EXT_PHY_CTRL_6);
	}

	if (((1U == isHwLevelingEnabled) &&
		 (1U == DISABLE_READ_LEVELING)) ||
		(0U == isHwLevelingEnabled))
	{
		/* EMIF_PHY_RD_DQS_SLAVE_RATIO */
		HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_7,
					EXT_PHY_CTRL_7);
		HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_7_SHADOW,
					EXT_PHY_CTRL_7);
		HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_8,
					EXT_PHY_CTRL_8);
		HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_8_SHADOW,
					EXT_PHY_CTRL_8);
		HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_9,
					EXT_PHY_CTRL_9);
		HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_9_SHADOW,
					EXT_PHY_CTRL_9);
		HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_10,
					EXT_PHY_CTRL_10);
		HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_10_SHADOW,
					EXT_PHY_CTRL_10);
		HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_11,
					EXT_PHY_CTRL_11);
		HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_11_SHADOW,
					EXT_PHY_CTRL_11);
	}

	if (((1U == isHwLevelingEnabled) &&
		 (1U == DISABLE_WRITE_LEVELING)) ||
		(0U == isHwLevelingEnabled))
	{
		/* EMIF_PHY_WR_DATA_SLAVE_RATIO */
		HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_12,
					EXT_PHY_CTRL_12);
		HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_12_SHADOW,
					EXT_PHY_CTRL_12);
		HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_13,
					EXT_PHY_CTRL_13);
		HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_13_SHADOW,
					EXT_PHY_CTRL_13);
		HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_14,
					EXT_PHY_CTRL_14);
		HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_14_SHADOW,
					EXT_PHY_CTRL_14);
		HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_15,
					EXT_PHY_CTRL_15);
		HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_15_SHADOW,
					EXT_PHY_CTRL_15);
		HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_16,
					EXT_PHY_CTRL_16);
		HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_16_SHADOW,
					EXT_PHY_CTRL_16);

		/* EMIF_PHY_WR_DQS_SLAVE_RATIO */
		HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_17,
					EXT_PHY_CTRL_17);
		HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_17_SHADOW,
					EXT_PHY_CTRL_17);
		HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_18,
					EXT_PHY_CTRL_18);
		HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_18_SHADOW,
					EXT_PHY_CTRL_18);
		HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_19,
					EXT_PHY_CTRL_19);
		HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_19_SHADOW,
					EXT_PHY_CTRL_19);
		HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_20,
					EXT_PHY_CTRL_20);
		HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_20_SHADOW,
					EXT_PHY_CTRL_20);
		HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_21,
					EXT_PHY_CTRL_21);
		HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_21_SHADOW,
					EXT_PHY_CTRL_21);
	}    

    HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_22,
                EXT_PHY_CTRL_22);
    HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_22_SHADOW,
                EXT_PHY_CTRL_22);
    HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_23,
                EXT_PHY_CTRL_23);
    HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_23_SHADOW,
                EXT_PHY_CTRL_23);
    HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_24,
                EXT_PHY_CTRL_24);
    HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_24_SHADOW,
                EXT_PHY_CTRL_24);
    HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_25,
                EXT_PHY_CTRL_25);
    HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_25_SHADOW,
                EXT_PHY_CTRL_25);

    if (1U == isHwLevelingEnabled)
    {
        HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_26,
                    EXT_PHY_CTRL_26);
        HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_26_SHADOW,
                    EXT_PHY_CTRL_26);
        HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_27,
                    EXT_PHY_CTRL_27);
        HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_27_SHADOW,
                    EXT_PHY_CTRL_27);
        HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_28,
                    EXT_PHY_CTRL_28);
        HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_28_SHADOW,
                    EXT_PHY_CTRL_28);
        HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_29,
                    EXT_PHY_CTRL_29);
        HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_29_SHADOW,
                    EXT_PHY_CTRL_29);
        HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_30,
                    EXT_PHY_CTRL_30);
        HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_30_SHADOW,
                    EXT_PHY_CTRL_30);

        HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_31,
                    EXT_PHY_CTRL_31);
        HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_31_SHADOW,
                    EXT_PHY_CTRL_31);
        HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_32,
                    EXT_PHY_CTRL_32);
        HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_32_SHADOW,
                    EXT_PHY_CTRL_32);
        HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_33,
                    EXT_PHY_CTRL_33);
        HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_33_SHADOW,
                    EXT_PHY_CTRL_33);
        HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_34,
                    EXT_PHY_CTRL_34);
        HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_34_SHADOW,
                    EXT_PHY_CTRL_34);
        HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_35,
                    EXT_PHY_CTRL_35);
        HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_35_SHADOW,
                    EXT_PHY_CTRL_35);
    }

    HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_36,
                EXT_PHY_CTRL_36);
    HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_36_SHADOW,
                EXT_PHY_CTRL_36);

    HW_WR_REG32(base_addr + EMIF_SDRAM_REFRESH_CONTROL_SHADOW,
                (EMIF_SDRAM_REFRESH_CONTROL_INITREF_DIS_MASK |
                 SDRAM_REF_CTRL_INIT));
    HW_WR_REG32(base_addr + EMIF_SDRAM_REFRESH_CONTROL,
                (EMIF_SDRAM_REFRESH_CONTROL_INITREF_DIS_MASK |
                 SDRAM_REF_CTRL_INIT));

    HW_WR_REG32(base_addr + EMIF_SDRAM_TIMING_1,
                SDRAM_TIM_1);
    HW_WR_REG32(base_addr + EMIF_SDRAM_TIMING_1_SHADOW,
                SDRAM_TIM_1);
    HW_WR_REG32(base_addr + EMIF_SDRAM_TIMING_2,
                SDRAM_TIM_2);
    HW_WR_REG32(base_addr + EMIF_SDRAM_TIMING_2_SHADOW,
                SDRAM_TIM_2);
    HW_WR_REG32(base_addr + EMIF_SDRAM_TIMING_3,
                SDRAM_TIM_3);
    HW_WR_REG32(base_addr + EMIF_SDRAM_TIMING_3_SHADOW,
                SDRAM_TIM_3);
    HW_WR_REG32(base_addr + EMIF_POWER_MANAGEMENT_CONTROL,
                PWR_MGMT_CTRL);
    HW_WR_REG32(base_addr + EMIF_POWER_MANAGEMENT_CONTROL_SHADOW,
                PWR_MGMT_CTRL);
    HW_WR_REG32(base_addr + EMIF_OCP_CONFIG,
                OCP_CONFIG);
    HW_WR_REG32(base_addr + EMIF_IODFT_TLGC,
                IODFT_TLGC);
    HW_WR_REG32(base_addr + EMIF_DLL_CALIB_CTRL,
                DLL_CALIB_CTRL);
    HW_WR_REG32(base_addr + EMIF_DLL_CALIB_CTRL_SHADOW,
                DLL_CALIB_CTRL);
    HW_WR_REG32(base_addr + EMIF_SDRAM_OUTPUT_IMPEDANCE_CALIBRATION_CONFIG,
                ZQ_CONFIG);
    HW_WR_REG32(base_addr + EMIF_READ_WRITE_LEVELING_RAMP_WINDOW,
                RDWR_LVL_RMP_WIN);
    HW_WR_REG32(base_addr + EMIF_READ_WRITE_LEVELING_RAMP_CONTROL,
                RDWR_LVL_RMP_CTRL);
    HW_WR_REG32(base_addr + EMIF_READ_WRITE_LEVELING_CONTROL,
                0U);

    HW_WR_REG32(base_addr + EMIF_DDR_PHY_CONTROL_1,
                DDR_PHY_CTRL_1);
    HW_WR_REG32(base_addr + EMIF_DDR_PHY_CONTROL_1_SHADOW,
                DDR_PHY_CTRL_1);

    HW_WR_REG32(base_addr + EMIF_DDR_PHY_CONTROL_2,
                DDR_PHY_CTRL_2);
    HW_WR_REG32(base_addr + EMIF_PRIORITY_TO_CLASS_OF_SERVICE_MAPPING,
                PRI_COS_MAP);
    HW_WR_REG32(base_addr + EMIF_CONNECTION_ID_TO_CLASS_OF_SERVICE_1_MAPPING,
                CONNID_COS_1_MAP);
    HW_WR_REG32(base_addr + EMIF_CONNECTION_ID_TO_CLASS_OF_SERVICE_2_MAPPING,
                CONNID_COS_2_MAP);
    HW_WR_REG32(base_addr + EMIF_READ_WRITE_EXECUTION_THRESHOLD,
                RD_WR_EXEC_THRSH);
    HW_WR_REG32(base_addr + EMIF_COS_CONFIG,
                COS_CONFIG);

    HW_WR_REG32(base_addr + EMIF_SDRAM_REFRESH_CONTROL_SHADOW,
                SDRAM_REF_CTRL_INIT);
    HW_WR_REG32(base_addr + EMIF_SDRAM_REFRESH_CONTROL,
                SDRAM_REF_CTRL_INIT);
    HW_WR_REG32(base_addr + EMIF_SDRAM_CONFIG_2,
                SDRAM_CONFIG_2);
    HW_WR_REG32(base_addr + EMIF_SDRAM_CONFIG,
                SDRAM_CONFIG);
				
    /* If delay is not present, interconnect can throw a false error */
    us_delay(1000U);    

    HW_WR_REG32(base_addr + EMIF_SDRAM_REFRESH_CONTROL_SHADOW,
                SDRAM_REF_CTRL);
    HW_WR_REG32(base_addr + EMIF_SDRAM_REFRESH_CONTROL,
                SDRAM_REF_CTRL);
    
    if (1U == isHwLevelingEnabled)
    {
        /* This is required for leveling of ECC macros */
        if ((1U == isEccEnabled) && (SOC_EMIF1_CONF_REGS_BASE == base_addr))
        {
            /* Configuration ensures ECC calculation does not happen */
            HW_WR_REG32(base_addr + EMIF_ECC_ADDRESS_RANGE_1,
                        0U);
            HW_WR_REG32(base_addr + EMIF_ECC_ADDRESS_RANGE_2,
                        0U);
            HW_WR_REG32(base_addr + EMIF_ECC_CTRL_REG,
                        (EMIF_ECC_CTRL_REG_REG_ECC_EN_MASK |
                         EMIF_ECC_CTRL_REG_REG_ECC_ADDR_RGN_PROT_MASK));
        }

        printf("       Launch full leveling\n");

        /* clear error status - FIFO_WE_IN_MISALIGNED */
        HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_36,
                    (HW_RD_REG32(base_addr + EMIF_EXT_PHY_CONTROL_36) |
                     0x00000100U));
        HW_WR_REG32(base_addr + EMIF_EXT_PHY_CONTROL_36_SHADOW,
                    (HW_RD_REG32(base_addr + EMIF_EXT_PHY_CONTROL_36_SHADOW) |
                     0x00000100U));

        /* Disable SDRAM refreshes before leveling */
        HW_WR_REG32(base_addr + EMIF_SDRAM_REFRESH_CONTROL,
                    (HW_RD_REG32(base_addr + EMIF_SDRAM_REFRESH_CONTROL) |
                     EMIF_SDRAM_REFRESH_CONTROL_INITREF_DIS_MASK));

        /* RDWR_LVL_CTRL - Launch full leveling */
        HW_WR_REG32(base_addr + EMIF_READ_WRITE_LEVELING_CONTROL,
                    EMIF_READ_WRITE_LEVELING_CONTROL_RDWRLVLFULL_START_MASK);
        /* If delay is not present, interconnect can throw a false error */
        us_delay(300U);

        /* Wait for the leveling procedure to complete */
        while ((HW_RD_REG32(base_addr + EMIF_READ_WRITE_LEVELING_CONTROL) &
                EMIF_READ_WRITE_LEVELING_CONTROL_RDWRLVLFULL_START_MASK) !=
                0U) ;

        /* Enable SDRAM refreshes after leveling */
        HW_WR_REG32(base_addr + EMIF_SDRAM_REFRESH_CONTROL,
                    (HW_RD_REG32(base_addr + EMIF_SDRAM_REFRESH_CONTROL) &
                     ~EMIF_SDRAM_REFRESH_CONTROL_INITREF_DIS_MASK));

        if ((HW_RD_REG32(base_addr + EMIF_STATUS) & 0x70) != 0U)
        {
            printf("ERROR: HW-Leveling time-out\n");
        }
        else
        {
            /* Following function is needed for whenever CORE can
             * go in and out of INACTIVE/CSWR */
            EMIF_DDR3_UpdateHWLevelOutput(base_addr);
        }

        /* This is done since ECC configuration is handled
         * in separate function */
        HW_WR_REG32(base_addr + EMIF_ECC_CTRL_REG, 0U);
    }
}

hotmenu AM571x_DDR3_666MHz_Config()
{
    printf("--->>> DDR3 Initialization is in progress ... <<<---\n");

    /* DDR PLL config */
    dpll_ddr_config(666);

    AM571x_CM_DDRIO_Config();

    AM571x_reset_emif_params_ddr3_666(SOC_EMIF1_CONF_REGS_BASE);
    AM571x_set_emif1_params_ddr3_666(SOC_EMIF1_CONF_REGS_BASE);
    EMIF_Config(SOC_EMIF1_CONF_REGS_BASE,             
                HW_LEVELING_ENABLED,
                ENABLE_ECC);

    AM571x_set_lisa_maps();

    printf("--->>> DDR3 Initialization is DONE! <<<---\n");
}

hotmenu EMIF_DDR3_UpdateHWLevelOutput_EMIF1()
{
    EMIF_DDR3_UpdateHWLevelOutput(SOC_EMIF1_CONF_REGS_BASE);
}

hotmenu AM571x_EMIF1_ECC_Configuration()
{
    printf("--->>> EMIF1 ECC Initialization is in progress ... <<<---\n");
    printf("DEBUG: Ensure all memory browsers and watch windows accessing\n");
    printf("       DDR are closed!!\n");

    HW_WR_REG32(0x4AE0C144, (HW_RD_REG32(0x4AE0C144)|0x00010000));

    /* EMIF_ECC_ADDRESS_RANGE_1 - 0x80000000 to 0x90000000 */
    HW_WR_REG32(0x4C000114, 0x0FFF0000);
    /* EMIF_ECC_ADDRESS_RANGE_2 - 0x90000000 to 0xA0000000 */
    HW_WR_REG32(0x4C000118, 0x1FFF1000);

    /* EMIF_ECC_CTRL_REG - Enable ECC on both ranges */
    HW_WR_REG32(0x4C000110, 0xC0000003);

    printf("DEBUG: Init all ECC enabled memory before any read access!!\n");
    printf("--->>> EMIF1 ECC Initialization is DONE! <<<---\n");
}

hotmenu AM571x_EMIF1_Enable_Narrow_Mode()
{
    printf("--->>> EMIF1 Narrow Mode config is in progress ... <<<---\n");

    HW_WR_REG32(0x4C000008, (HW_RD_REG32(0x4C000008)|0x00004000));

    printf("--->>> EMIF1 Narrow Mode config is DONE! <<<---\n");
}

hotmenu print_hw_leveling_output_EMIF1() {print_hw_leveling_output(SOC_EMIF1_CONF_REGS_BASE);}
print_hw_leveling_output(uint32_t base_addr)
{
    GEL_TextOut("EMIF_PHY_FIFO_WE_SLAVE_RATIO Macro 0: %x\n",,,,,HW_RD_REG32(base_addr + 0x00000170) & 0xFF);
    GEL_TextOut("EMIF_PHY_FIFO_WE_SLAVE_RATIO Macro 1: %x\n",,,,,HW_RD_REG32(base_addr + 0x00000174) & 0xFF);
    GEL_TextOut("EMIF_PHY_FIFO_WE_SLAVE_RATIO Macro 2: %x\n",,,,,HW_RD_REG32(base_addr + 0x00000178) & 0xFF);
    GEL_TextOut("EMIF_PHY_FIFO_WE_SLAVE_RATIO Macro 3: %x\n",,,,,HW_RD_REG32(base_addr + 0x0000017c) & 0xFF);
    GEL_TextOut("EMIF_PHY_FIFO_WE_SLAVE_RATIO Macro 4: %x\n",,,,,HW_RD_REG32(base_addr + 0x00000180) & 0xFF);
    GEL_TextOut("\n");
    GEL_TextOut("EMIF_PHY_RD_DQS_SLAVE_RATIO  Macro 0: %x\n",,,,,HW_RD_REG32(base_addr + 0x0000015C) & 0xFF);
    GEL_TextOut("EMIF_PHY_RD_DQS_SLAVE_RATIO  Macro 1: %x\n",,,,,HW_RD_REG32(base_addr + 0x00000160) & 0xFF);
    GEL_TextOut("EMIF_PHY_RD_DQS_SLAVE_RATIO  Macro 2: %x\n",,,,,HW_RD_REG32(base_addr + 0x00000164) & 0xFF);
    GEL_TextOut("EMIF_PHY_RD_DQS_SLAVE_RATIO  Macro 3: %x\n",,,,,HW_RD_REG32(base_addr + 0x00000168) & 0xFF);
    GEL_TextOut("EMIF_PHY_RD_DQS_SLAVE_RATIO  Macro 4: %x\n",,,,,HW_RD_REG32(base_addr + 0x0000016c) & 0xFF);
    GEL_TextOut("\n");
    GEL_TextOut("EMIF_PHY_WR_DATA_SLAVE_RATIO Macro 0: %x\n",,,,,HW_RD_REG32(base_addr + 0x00000184) & 0xFF);
    GEL_TextOut("EMIF_PHY_WR_DATA_SLAVE_RATIO Macro 1: %x\n",,,,,HW_RD_REG32(base_addr + 0x00000188) & 0xFF);
    GEL_TextOut("EMIF_PHY_WR_DATA_SLAVE_RATIO Macro 2: %x\n",,,,,HW_RD_REG32(base_addr + 0x0000018c) & 0xFF);
    GEL_TextOut("EMIF_PHY_WR_DATA_SLAVE_RATIO Macro 3: %x\n",,,,,HW_RD_REG32(base_addr + 0x00000190) & 0xFF);
    GEL_TextOut("EMIF_PHY_WR_DATA_SLAVE_RATIO Macro 4: %x\n",,,,,HW_RD_REG32(base_addr + 0x00000194) & 0xFF);
    GEL_TextOut("\n");
    GEL_TextOut("EMIF_PHY_WR_DQS_SLAVE_RATIO  Macro 0: %x\n",,,,,HW_RD_REG32(base_addr + 0x00000198) & 0xFF);
    GEL_TextOut("EMIF_PHY_WR_DQS_SLAVE_RATIO  Macro 1: %x\n",,,,,HW_RD_REG32(base_addr + 0x0000019c) & 0xFF);
    GEL_TextOut("EMIF_PHY_WR_DQS_SLAVE_RATIO  Macro 2: %x\n",,,,,HW_RD_REG32(base_addr + 0x000001A0) & 0xFF);
    GEL_TextOut("EMIF_PHY_WR_DQS_SLAVE_RATIO  Macro 3: %x\n",,,,,HW_RD_REG32(base_addr + 0x000001A4) & 0xFF);
    GEL_TextOut("EMIF_PHY_WR_DQS_SLAVE_RATIO  Macro 4: %x\n",,,,,HW_RD_REG32(base_addr + 0x000001A8) & 0xFF);
    GEL_TextOut("\n");
}