U-Boot 2021.01-g44a87e3ab8 (Aug 20 2024 - 21:54:41 +0000) CPU : AM437X-GP rev 1.2 Model: TI AM437x GP EVM DRAM: 1 GiB PMIC: TPS65218 NAND: 1024 MiB MMC: OMAP SD/MMC: 0 Loading Environment from FAT... MMC: no card present Net: Could not get PHY for ethernet@4a100000: addr 0 eth2: ethernet@4a100000 Hit any key to stop autoboot: 0 MMC: no card present MMC: no card present MMC: no card present MMC: no card present starting USB... Bus usb@483d0000: Register 2000440 NbrPorts 2 Starting the controller USB XHCI 1.00 scanning bus usb@483d0000 for devices... 2 USB Device(s) found scanning usb for storage devices... 0 Storage Device(s) found Device 0: unknown device Booting from nand ... NAND read: device 0 offset 0x100000, size 0x80000 524288 bytes read: OK NAND read: device 0 offset 0x300000, size 0x700000 omap-elm: uncorrectable ECC errors omap-elm: uncorrectable ECC errors NAND read from offset 300000 failed -74 0 bytes read: ERROR ## Flattened Device Tree blob at 88000000 Booting using the fdt blob at 0x88000000 Loading Device Tree to 8ffe2000, end 8ffffbaf ... OK Starting kernel ... It will freeze at this point. Sometimes it will start without any errors.