GSG:CCSv5 Running for the first time

From Texas Instruments Wiki
Jump to: navigation, search

Running Code Composer Studio for the first time



Defining the workspace directory[edit]

The first thing CCSv5 asks is to define a workspace - a directory that holds all elements (projects, links to projects, possibly source code) used in the development.

  • Differently than CCSv4, by default the workspace is created under the C:\Users\<user> or C:\Documents and Settings\<user> directory, but its location is arbitrary.
  • Every time CCSv5 is executed it will ask for the workspace directory. If you plan to use just a single directory for all your projects, just check the option Use this as the default and do not ask again. The workspace can always be changed later from inside CCSv5.
Fig. 1: selecting the workspace location



Choosing the license[edit]

1. Update as of Dec 2016 CCSv5 full license can be downloaded from the link below. There are no restrictions in regards to time, code size, debug probe or target used.

CCS Full License


2. In the pop up license screen, select Activate and then click on Next button

Fig. 2: License options



3. Click on Browse under Specify a License File. Point to the place where you saved the license file downloaded above. Click Finish.

Fig. 3: activate license file



All of the below (collapsed) information is now legacy information.


Expand

Old licensing information (Obsolete)

The welcome screen[edit]

After the license process is finished, CCS will show the Welcome Screen and is ready to use.

Fig. 11: Welcome to Code Composer Studio v5!


What's next?[edit]

Now that you have finished the license activation of Code Composer Studio v5, please continue on to the Working with CCS section of the CCSv5 Getting Started Guide.



E2e.jpg {{
  1. switchcategory:MultiCore=
  • For technical support on MultiCore devices, please post your questions in the C6000 MultiCore Forum
  • For questions related to the BIOS MultiCore SDK (MCSDK), please use the BIOS Forum

Please post only comments related to the article GSG:CCSv5 Running for the first time here.

Keystone=
  • For technical support on MultiCore devices, please post your questions in the C6000 MultiCore Forum
  • For questions related to the BIOS MultiCore SDK (MCSDK), please use the BIOS Forum

Please post only comments related to the article GSG:CCSv5 Running for the first time here.

C2000=For technical support on the C2000 please post your questions on The C2000 Forum. Please post only comments about the article GSG:CCSv5 Running for the first time here. DaVinci=For technical support on DaVincoplease post your questions on The DaVinci Forum. Please post only comments about the article GSG:CCSv5 Running for the first time here. MSP430=For technical support on MSP430 please post your questions on The MSP430 Forum. Please post only comments about the article GSG:CCSv5 Running for the first time here. OMAP35x=For technical support on OMAP please post your questions on The OMAP Forum. Please post only comments about the article GSG:CCSv5 Running for the first time here. OMAPL1=For technical support on OMAP please post your questions on The OMAP Forum. Please post only comments about the article GSG:CCSv5 Running for the first time here. MAVRK=For technical support on MAVRK please post your questions on The MAVRK Toolbox Forum. Please post only comments about the article GSG:CCSv5 Running for the first time here. For technical support please post your questions at http://e2e.ti.com. Please post only comments about the article GSG:CCSv5 Running for the first time here.

}}

Hyperlink blue.png Links

Amplifiers & Linear
Audio
Broadband RF/IF & Digital Radio
Clocks & Timers
Data Converters

DLP & MEMS
High-Reliability
Interface
Logic
Power Management

Processors

Switches & Multiplexers
Temperature Sensors & Control ICs
Wireless Connectivity