U-Boot SPL 2017.01-00319-g7752743-dirty (Aug 04 2017 - 17:05:22)
Trying to boot from NAND
Card did not respond to voltage select!
** Bad device mmc 0 **
Using default environment



U-Boot 2017.01-00319-g7752743-dirty (Aug 04 2017 - 17:05:22 +0300)

CPU  : AM335X-GP rev 1.0
Model: UniPOS AM335x Base Module
DRAM:  512 MiB
NAND:  256 MiB
MMC:   OMAP SD/MMC: 0
Card did not respond to voltage select!
** Bad device mmc 0 **
Using default environment

EM3027 charger already enabled
Net:   <ethaddr> not set. Validating first E-fuse MAC
usb_ether
Hit any key to stop autoboot:  0
Card did not respond to voltage select!
Card did not respond to voltage select!
Card did not respond to voltage select!
Card did not respond to voltage select!
Booting from nand ...

NAND read: device 0 offset 0x80000, size 0x40000
 262144 bytes read: OK

NAND read: device 0 offset 0x200000, size 0x600000
 6291456 bytes read: OK
## Flattened Device Tree blob at 88000000
   Booting using the fdt blob at 0x88000000
   Loading Device Tree to 8fff3000, end 8ffffda9 ... OK

Starting kernel ...

[    0.000000] Booting Linux on physical CPU 0x0
[    0.000000] Linux version 4.9.28-geed43d1050 (peter@ubuntu64) (gcc version 6.2.1 20161016 (Linaro GCC 6.2-2016.11) ) #1 PREEMPT Fri Aug 4 17:16:52 EEST 2017
[    0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c5387d
[    0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[    0.000000] OF: fdt:Machine model: UniPOS AM335x Base Module
[    0.000000] efi: Getting EFI parameters from FDT:
[    0.000000] efi: UEFI not found.
[    0.000000] cma: Reserved 48 MiB at 0x9d000000
[    0.000000] Memory policy: Data cache writeback
[    0.000000] CPU: All CPU(s) started in SVC mode.
[    0.000000] AM335X ES1.0 (neon)
[    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 129920
[    0.000000] Kernel command line: console=ttyO0,115200n8 root=ubi0:rootfs rw ubi.mtd=NAND.file-system,2048 rootfstype=ubifs rootwait=1
[    0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes)
[    0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
[    0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
[    0.000000] Memory: 457972K/524288K available (7168K kernel code, 280K rwdata, 2372K rodata, 1024K init, 272K bss, 17164K reserved, 49152K cma-reserved, 0K highmem)
[    0.000000] Virtual kernel memory layout:
[    0.000000]     vector  : 0xffff0000 - 0xffff1000   (   4 kB)
[    0.000000]     fixmap  : 0xffc00000 - 0xfff00000   (3072 kB)
[    0.000000]     vmalloc : 0xe0800000 - 0xff800000   ( 496 MB)
[    0.000000]     lowmem  : 0xc0000000 - 0xe0000000   ( 512 MB)
[    0.000000]     pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)
[    0.000000]     modules : 0xbf000000 - 0xbfe00000   (  14 MB)
[    0.000000]       .text : 0xc0008000 - 0xc0800000   (8160 kB)
[    0.000000]       .init : 0xc0b00000 - 0xc0c00000   (1024 kB)
[    0.000000]       .data : 0xc0c00000 - 0xc0c46210   ( 281 kB)
[    0.000000]        .bss : 0xc0c46210 - 0xc0c8a5b4   ( 273 kB)
[    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
[    0.000000] Preemptible hierarchical RCU implementation.
[    0.000000]  Build-time adjustment of leaf fanout to 32.
[    0.000000] NR_IRQS:16 nr_irqs:16 16
[    0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
[    0.000000] OMAP clockevent source: timer2 at 24000000 Hz
[    0.000016] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 89478484971ns
[    0.000040] clocksource: timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 79635851949 ns
[    0.000052] OMAP clocksource: timer1 at 24000000 Hz
[    0.000249] clocksource_probe: no matching clocksources found
[    0.000434] Console: colour dummy device 80x30
[    0.000469] Calibrating delay loop... 718.02 BogoMIPS (lpj=3590144)
[    0.119003] pid_max: default: 32768 minimum: 301
[    0.119147] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
[    0.119160] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
[    0.120016] CPU: Testing write buffer coherency: ok
[    0.120410] Setting up static identity map for 0x80100000 - 0x80100060
[    0.121347] EFI services will not be available.
[    0.122856] devtmpfs: initialized
[    0.136521] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[    0.136897] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[    0.136925] futex hash table entries: 256 (order: -1, 3072 bytes)
[    0.140860] pinctrl core: initialized pinctrl subsystem
[    0.142220] NET: Registered protocol family 16
[    0.144351] DMA: preallocated 256 KiB pool for atomic coherent allocations
[    0.160661] omap_hwmod: debugss: _wait_target_disable failed
[    0.239005] cpuidle: using governor ladder
[    0.268990] cpuidle: using governor menu
[    0.275922] OMAP GPIO hardware version 0.1
[    0.291139] omap-gpmc 50000000.gpmc: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/nandflash_pins_default, deferring probe
[    0.293316] hw-breakpoint: debug architecture 0x4 unsupported.
[    0.338014] edma 49000000.edma: TI EDMA DMA engine driver
[    0.341890] omap_i2c 44e0b000.i2c: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/pinmux_i2c0_pins, deferring probe
[    0.342037] media: Linux media interface: v0.10
[    0.342101] Linux video capture interface: v2.00
[    0.342149] pps_core: LinuxPPS API ver. 1 registered
[    0.342158] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[    0.342185] PTP clock support registered
[    0.342229] EDAC MC: Ver: 3.0.0
[    0.343454] omap-mailbox 480c8000.mailbox: omap mailbox rev 0x400
[    0.343820] Advanced Linux Sound Architecture Driver Initialized.
[    0.345208] clocksource: Switched to clocksource timer1
[    0.357017] NET: Registered protocol family 2
[    0.357892] TCP established hash table entries: 4096 (order: 2, 16384 bytes)
[    0.357952] TCP bind hash table entries: 4096 (order: 2, 16384 bytes)
[    0.358004] TCP: Hash tables configured (established 4096 bind 4096)
[    0.358078] UDP hash table entries: 256 (order: 0, 4096 bytes)
[    0.358100] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[    0.358257] NET: Registered protocol family 1
[    0.358712] RPC: Registered named UNIX socket transport module.
[    0.358729] RPC: Registered udp transport module.
[    0.358736] RPC: Registered tcp transport module.
[    0.358744] RPC: Registered tcp NFSv4.1 backchannel transport module.
[    0.359745] hw perfevents: enabled with armv7_cortex_a8 PMU driver, 5 counters available
[    0.362267] workingset: timestamp_bits=14 max_order=17 bucket_order=3
[    0.371071] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[    0.372136] NFS: Registering the id_resolver key type
[    0.372178] Key type id_resolver registered
[    0.372187] Key type id_legacy registered
[    0.372239] ntfs: driver 2.1.32 [Flags: R/O].
[    0.372570] jffs2: version 2.2. (NAND) (SUMMARY)   2001-2006 Red Hat, Inc.
[    0.374995] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 246)
[    0.375018] io scheduler noop registered
[    0.375027] io scheduler deadline registered
[    0.375314] io scheduler cfq registered (default)
[    0.376366] pinctrl-single 44e10800.pinmux: please update dts to use #pinctrl-cells = <1>
[    0.376877] pinctrl-single 44e10800.pinmux: 142 pins at pa f9e10800 size 568
[    0.447894] Serial: 8250/16550 driver, 10 ports, IRQ sharing disabled
[    0.452215] omap_uart 44e09000.serial: no wakeirq for uart0
[    0.452451] 44e09000.serial: ttyO0 at MMIO 0x44e09000 (irq = 158, base_baud = 3000000) is a OMAP UART0
[    1.076523] console [ttyO0] enabled
[    1.080810] omap_uart 481a6000.serial: no wakeirq for uart3
[    1.086941] 481a6000.serial: ttyO3 at MMIO 0x481a6000 (irq = 159, base_baud = 3000000) is a OMAP UART3
[    1.097266] omap_uart 481a8000.serial: no wakeirq for uart4
[    1.103298] 481a8000.serial: ttyO4 at MMIO 0x481a8000 (irq = 160, base_baud = 3000000) is a OMAP UART4
[    1.114433] omap_rng 48310000.rng: OMAP Random Number Generator ver. 20
[    1.121541] [drm] Initialized
[    1.139848] brd: module loaded
[    1.150220] loop: module loaded
[    1.156880] m25p80 spi1.0: s25fl016k (2048 Kbytes)
[    1.161934] 1 ofpart partitions found on MTD device spi1.0
[    1.167796] Creating 1 MTD partitions on "spi1.0":
[    1.172821] 0x000000000000-0x000000200000 : "SPIFLASH.file-system"
[    1.181715] libphy: Fixed MDIO Bus: probed
[    1.255300] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6
[    1.261696] davinci_mdio 4a101000.mdio: detected phy mask fffffff7
[    1.269205] libphy: 4a101000.mdio: probed
[    1.273418] davinci_mdio 4a101000.mdio: phy[3]: device 4a101000.mdio:03, driver Micrel KSZ9031 Gigabit PHY
[    1.284436] cpsw 4a100000.ethernet: Detected MACID = c8:a0:30:89:f2:c5
[    1.291523] cpsw 4a100000.ethernet: cpts: overflow check period 500 (jiffies)
[    1.300931] mousedev: PS/2 mouse device common for all mice
[    1.307292] i2c /dev entries driver
[    1.312872] cpuidle: enable-method property 'ti,am3352' found operations
[    1.321133] omap_hsmmc 48060000.mmc: Got CD GPIO
[    1.357898] ledtrig-cpu: registered to indicate activity on CPUs
[    1.366658] NET: Registered protocol family 10
[    1.372778] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[    1.380138] NET: Registered protocol family 17
[    1.385071] Key type dns_resolver registered
[    1.389927] omap_voltage_late_init: Voltage driver support not added
[    1.402450] omap-gpmc 50000000.gpmc: GPMC revision 6.0
[    1.408015] gpmc_mem_init: disabling cs 0 mapped at 0x0-0x1000000
[    1.416441] nand: device found, Manufacturer ID: 0x2c, Chip ID: 0xda
[    1.423098] nand: Micron MT29F2G08ABAEAH4
[    1.427403] nand: 256 MiB, SLC, erase size: 128 KiB, page size: 2048, OOB size: 64
[    1.435399] nand: using OMAP_ECC_BCH8_CODE_HW ECC scheme
[    1.441057] 10 ofpart partitions found on MTD device 8000000.nand
[    1.447456] Creating 10 MTD partitions on "8000000.nand":
[    1.453113] 0x000000000000-0x000000020000 : "NAND.SPL"
[    1.460064] 0x000000020000-0x000000040000 : "NAND.SPL.backup1"
[    1.467575] 0x000000040000-0x000000060000 : "NAND.SPL.backup2"
[    1.475016] 0x000000060000-0x000000080000 : "NAND.SPL.backup3"
[    1.482584] 0x000000080000-0x0000000c0000 : "NAND.u-boot-spl-os"
[    1.490284] 0x0000000c0000-0x0000001c0000 : "NAND.u-boot"
[    1.497637] 0x0000001c0000-0x0000001e0000 : "NAND.u-boot-env"
[    1.504886] 0x0000001e0000-0x000000200000 : "NAND.u-boot-env.backup1"
[    1.512942] 0x000000200000-0x000000800000 : "NAND.kernel"
[    1.521947] 0x000000800000-0x000010000000 : "NAND.file-system"
[    1.645474] tps65910 0-002d: No interrupt support, no core IRQ
[    1.653771] vrtc: supplied by vbat
[    1.661208] vio: supplied by vbat
[    1.666274] vdd1: supplied by vbat
[    1.671731] vdd2: supplied by vbat
[    1.676945] random: fast init done
[    1.682162] vdig1: supplied by vbat
[    1.687315] vdig2: supplied by vbat
[    1.692414] vpll: supplied by vbat
[    1.697450] vdac: supplied by vbat
[    1.702455] vaux1: supplied by vbat
[    1.707578] vaux2: supplied by vbat
[    1.712688] vaux33: supplied by vbat
[    1.717906] vmmc: supplied by vbat
[    1.722928] vbb: supplied by vbat
[    1.728587] rtc-em3027 0-0056: rtc core: registered rtc-em3027 as rtc0
[    1.736080] at24 0-0050: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
[    1.743408] omap_i2c 44e0b000.i2c: bus 0 rev0.11 at 400 kHz
[    1.751161] omap_hsmmc 48060000.mmc: Got CD GPIO
[    1.815926] ubi0: attaching mtd10
[    2.799353] ubi0: scanning is finished
[    2.812622] ubi0: attached mtd10 (name "NAND.file-system", size 248 MiB)
[    2.819744] ubi0: PEB size: 131072 bytes (128 KiB), LEB size: 126976 bytes
[    2.826959] ubi0: min./max. I/O unit sizes: 2048/2048, sub-page size 512
[    2.833973] ubi0: VID header offset: 2048 (aligned 2048), data offset: 4096
[    2.841271] ubi0: good PEBs: 1982, bad PEBs: 2, corrupted PEBs: 0
[    2.847660] ubi0: user volume: 1, internal volumes: 1, max. volumes count: 128
[    2.855242] ubi0: max/mean erase counter: 1/0, WL threshold: 4096, image sequence number: 1291566592
[    2.864802] ubi0: available PEBs: 0, total reserved PEBs: 1982, PEBs reserved for bad PEB handling: 38
[    2.874566] ubi0: background thread "ubi_bgt0d" started, PID 79
[    2.881577] rtc-em3027 0-0056: setting system clock to 2017-08-07 07:08:08 UTC (1502089688)
[    2.891105] ALSA device list:
[    2.894221]   No soundcards found.
[    2.905325] UBIFS (ubi0:0): background thread "ubifs_bgt0_0" started, PID 80
[    2.936232] UBIFS (ubi0:0): recovery needed
[    3.061597] UBIFS (ubi0:0): recovery completed
[    3.066422] UBIFS (ubi0:0): UBIFS: mounted UBI device 0, volume 0, name "rootfs"
[    3.074168] UBIFS (ubi0:0): LEB size: 126976 bytes (124 KiB), min./max. I/O unit sizes: 2048 bytes/2048 bytes
[    3.084575] UBIFS (ubi0:0): FS size: 244936704 bytes (233 MiB, 1929 LEBs), journal size 9023488 bytes (8 MiB, 72 LEBs)
[    3.095786] UBIFS (ubi0:0): reserved for root: 0 bytes (0 KiB)
[    3.101893] UBIFS (ubi0:0): media format: w4/r0 (latest is w4/r0), UUID 016022B2-7C18-4376-BD29-F9CE18937068, small LPT model
[    3.115268] VFS: Mounted root (ubifs filesystem) on device 0:14.
[    3.122380] devtmpfs: mounted
[    3.127160] Freeing unused kernel memory: 1024K (c0b00000 - c0c00000)
[    3.432350] systemd[1]: systemd 230 running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR +SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN)
[    3.452679] systemd[1]: Detected architecture arm.

Welcome to Arago 2017.05!

[    3.486786] systemd[1]: Set hostname to <unipos-am335x>.
[    4.197290] systemd[1]: sysinit.target: Found ordering cycle on sysinit.target/start
[    4.205619] systemd[1]: sysinit.target: Found dependency on alignment.service/start
[    4.213666] systemd[1]: sysinit.target: Found dependency on basic.target/start
[    4.221269] systemd[1]: sysinit.target: Found dependency on sockets.target/start
[    4.229042] systemd[1]: sysinit.target: Found dependency on avahi-daemon.socket/start
[    4.237265] systemd[1]: sysinit.target: Found dependency on sysinit.target/start
[    4.245019] systemd[1]: sysinit.target: Breaking ordering cycle by deleting job alignment.service/start
[ SKIP ] Ordering cycle found, skipping alignment.service
[  OK  ] Listening on Syslog Socket.
[  OK  ] Started Dispatch Password Requests to Console Directory Watch.
[  OK  ] Listening on udev Kernel Socket.
[  OK  ] Listening on Network Service Netlink Socket.
[  OK  ] Listening on /dev/initctl Compatibility Named Pipe.
[  OK  ] Reached target Remote File Systems.
[  OK  ] Created slice System Slice.
[  OK  ] Created slice system-serial\x2dgetty.slice.
[  OK  ] Listening on udev Control Socket.
[  OK  ] Created slice User and Session Slice.
[  OK  ] Reached target Slices.
[  OK  ] Listening on Journal Socket (/dev/log).
[  OK  ] Reached target Swap.
[  OK  ] Started Forward Password Requests to Wall Directory Watch.
[  OK  ] Reached target Paths.
[  OK  ] Listening on Journal Socket.
         Starting Remount Root and Kernel File Systems...
         Starting Journal Service...
         Starting Load Kernel Modules...
         Starting Setup Virtual Console...
[    5.020881] cryptodev: loading out-of-tree module taints kernel.
         Mounting Debug File System...
[    5.061450] cryptodev: driver 1.8 loaded.
         Starting Create list of required st... nodes for the current kernel...
         Mounting Temporary Directory...
         Mounting POSIX Message Queue File System...
[  OK  ] Mounted Debug File System.
[  OK  ] Mounted POSIX Message Queue File System.
[  OK  ] Mounted Temporary Directory.
[  OK  ] Started Journal Service.
[  OK  ] Started Remount Root and Kernel File Systems.
[  OK  ] Started Load Kernel Modules.
[  OK  ] Started Setup Virtual Console.
[  OK  ] Started Create list of required sta...ce nodes for the current kernel.
         Starting Create Static Device Nodes in /dev...
         Starting Apply Kernel Variables...
         Mounting Configuration File System...
         Starting udev Coldplug all Devices...
         Starting Flush Journal to Persistent Storage...
[  OK  ] Mounted Configuration File System.
[  OK  ] Started Create Static Device Nodes in /dev.
[  OK  ] Started Apply Kernel Variables.
[    5.904631] systemd-journald[95]: Received request to flush runtime journal from PID 1
[  OK  ] Started Flush Journal to Persistent Storage.
         Starting udev Kernel Device Manager...
[  OK  ] Reached target Local File Systems (Pre).
         Mounting /media/ram...
         Mounting /var/volatile...
[  OK  ] Mounted /var/volatile.
[  OK  ] Mounted /media/ram.
[  OK  ] Started udev Kernel Device Manager.
         Starting Load/Save Random Seed...
[  OK  ] Started Load/Save Random Seed.
[  OK  ] Found device /dev/ttyO0.
[    7.810735] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[  OK  ] Started udev Coldplug all Devices.
[    8.314639] CAN device driver interface
[    8.473882] c_can_platform 481cc000.can: c_can_platform device registered (regs=fa1cc000, irq=164)
[    8.544509] c_can_platform 481d0000.can: c_can_platform device registered (regs=fa1d0000, irq=165)
[    8.756042] omap_hwmod: pruss: _wait_target_ready failed: -16
[    8.875484] pruss-soc-bus 4a326000.pruss-soc-bus: use pm_runtime_put_sync_suspend() in driver?
[    8.884535] pruss-soc-bus 4a326000.pruss-soc-bus: couldn't enable module
[    9.016578] pruss-soc-bus: probe of 4a326000.pruss-soc-bus failed with error -16
[    9.024783] omap-sham 53100000.sham: hw accel on OMAP rev 4.3
[    9.132127] omap-aes 53500000.aes: OMAP AES hw accel rev: 3.2
[    9.158492] omap-aes 53500000.aes: will run requests pump with realtime priority
[  OK  ] Found device /dev/mtdblock0.
         Mounting /media/flash...
[    9.934485] wkup_m3_ipc 44e11324.wkup_m3_ipc: could not get rproc handle
[    9.944794] remoteproc remoteproc0: wkup_m3 is available
[   10.141138] PM: Cannot get wkup_m3_ipc handle
[   10.148086] remoteproc remoteproc0: powering up wkup_m3
[   10.172955] jffs2: notice: (295) jffs2_build_xattr_subsystem: complete building xattr subsystem, 0 of xdatum (0 unchecked, 0 orphan) and 0 of xref (0 dead, 0 orphan) found.
[   10.339686] remoteproc remoteproc0: Booting fw image am335x-pm-firmware.elf, size 224344
[   10.339946] remoteproc remoteproc0: remote processor wkup_m3 is now up
[   10.339974] wkup_m3_ipc 44e11324.wkup_m3_ipc: CM3 Firmware Version = 0x192
[  OK  ] Mounted /media/flash.
[   10.667356] PM: no-rtc available, rtc-only mode disabled.
[  OK  ] Reached target Local File Systems.
         Starting Create Volatile Files and Directories...
[  OK  ] Started Create Volatile Files and Directories.
[  OK  ] Listening on Load/Save RF Kill Switch Status /dev/rfkill Watch.
         Starting Network Time Synchronization...
         Starting Update UTMP about System Boot/Shutdown...
[  OK  ] Started Network Time Synchronization.
[  OK  ] Started Update UTMP about System Boot/Shutdown.
         Starting Synchronize System and HW clocks...
[  OK  ] Reached target System Time Synchronized.
[  OK  ] Started Synchronize System and HW clocks.
[  OK  ] Reached target System Initialization.
[  OK  ] Listening on RPCbind Server Activation Socket.
[  OK  ] Listening on dropbear.socket.
[  OK  ] Listening on D-Bus System Message Bus Socket.
[  OK  ] Started Daily Cleanup of Temporary Directories.
[  OK  ] Reached target Timers.
[  OK  ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
[  OK  ] Reached target Sockets.
[  OK  ] Reached target Basic System.
         Starting telnetd.service...
[  OK  ] Started D-Bus System Message Bus.
         Starting Login Service...
[  OK  ] Started Kernel Logging Service.
         Starting Print notice about GPLv3 packages...
[   14.439025] 47401300.usb-phy supply vcc not found, using dummy regulator
[  OK  ] Started System Logging Service.
         [   14.656226] 47401b00.usb-phy supply vcc not found, using dummy regulator
Starting Avahi mDNS/DNS-SD Stack...
         Starting Network Service...
         Starting Start power button service...
[  OK  ] Started telnetd.service.
[   15.004519] usbcore: registered new interface driver usbfs
[   15.118915] usbcore: registered new interface driver hub
[   15.174495] usbcore: registered new device driver usb
[  OK  ] Started Start power button service.
[   15.484879] musb-hdrc musb-hdrc.0: MUSB HDRC host driver
[   15.565610] musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus number 1
[   15.586835] hub 1-0:1.0: USB hub found
[   15.625442] hub 1-0:1.0: 1 port detected
[   15.714922] musb-hdrc musb-hdrc.1: MUSB HDRC host driver
[   15.767581] musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 2
[   15.824109] hub 2-0:1.0: USB hub found
[   15.841120] hub 2-0:1.0: 1 port detected
[  OK  ] Started Network Service.
[   16.317829] net eth0: initializing cpsw version 1.12 (0)
[   16.323419] net eth0: initialized cpsw ale version 1.4
[   16.391354] net eth0: ALE Table size 1024
[   16.517942] Micrel KSZ9031 Gigabit PHY 4a101000.mdio:03: attached PHY driver [Micrel KSZ9031 Gigabit PHY] (mii_bus:phy_addr=4a101000.mdio:03, irq=-1)
[   16.589384] libphy: PHY  not found
[   16.592972] net eth0: phy "" not found on slave 1, err -19
[   16.645168] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
[  OK  ] Started Avahi mDNS/DNS-SD Stack.
[  OK  ] Started Login Service.
         Starting Start USB gadget...
[  OK  ] Reached target Network.
         Starting Network Name Resolution...
         Starting Lightning Fast Webserver With Light System Requirements...
         Starting Simple Network Management Protocol (SNMP) Daemon....
         Starting Enable and configure wl18xx bluetooth stack...
         Starting Permit User Sessions...
         Starting busybox-udhcpd.service...
         Starting thttpd.service...
[  OK  ] Started Permit User Sessions.
[  OK  ] Started Serial Getty on ttyO0.
[  OK  ] Started Enable and configure wl18xx bluetooth stack.
[  OK  ] Started busybox-udhcpd.service.
[   18.546983] g_serial gadget: Gadget Serial v2.4
[   18.551751] g_serial gadget: g_serial ready
[  OK  ] Found device /dev/ttyGS0.
[  OK  ] Started Start USB gadget.
[   18.646573] cpsw 4a100000.ethernet eth0: Link is Up - 100Mbps/Full - flow control rx/tx
[   18.655043] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
[  OK  ] Started thttpd.service.
         Starting SYSV: The kdump script provides the support:...
[  OK  ] Started Serial Getty on ttyGS0.
[  OK  ] Reached target Login Prompts.
[  OK  ] Started Lightning Fast Webserver With Light System Requirements.
[  OK  ] Started Network Name Resolution.
[FAILED] Failed to start SYSV: The kdump script provides the support:.
See 'systemctl status kdump.service' for details.
         Starting thermal-zone-init.service...
         Starting parse-ip.service...
[  OK  ] Started thermal-zone-init.service.
[  OK  ] Started parse-ip.service.
[  OK  ] Started Simple Network Management Protocol (SNMP) Daemon..
***************************************************************
***************************************************************
NOTICE: This file system contains the following GPLv3 packages:
        binutils
        dosfstools
        gawk
        gdb
        gdbserver
        hidapi
        libcairo-perf-utils
        libgmp10
        libidn11
        libmpc3
        libmpfr4
        libreadline6
        m4
        nettle

If you do not wish to distribute GPLv3 components please remove
the above packages prior to distribution.  This can be done using
the opkg remove command.  i.e.:
    opkg remove <package>
Where <package> is the name printed in the list above

NOTE: If the package is a dependency of another package you
      will be notified of the dependent packages.  You should
      use the --force-removal-of-dependent-packages option to
      also remove the dependent packages as well
***************************************************************
***************************************************************
[  OK  ] Started Print notice about GPLv3 packages.
[  OK  ] Reached target Multi-User System.
[  OK  ] Started 7000M panel application service.
         Starting Update UTMP about System Runlevel Changes...
[  OK  ] Started Update UTMP about System Runlevel Changes.

 _____                    _____           _         _
|  _  |___ ___ ___ ___   |  _  |___ ___  |_|___ ___| |_
|     |  _| .'| . | . |  |   __|  _| . | | | -_|  _|  _|
|__|__|_| |__,|_  |___|  |__|  |_| |___|_| |___|___|_|
              |___|                    |___|

Arago Project http://arago-project.org unipos-am335x ttyO0

Arago 2017.05 unipos-am335x ttyO0

unipos-am335x login: