This sample demonstrates how to write driver for a generic PCI device using Windows Driver Framework. The target hardware for this driver is PLX9656/9653RDK-LITE board. The product kit and the hardware specification are available at http://www.plxtech.com.
For more information, see Peripheral Component Interconnect (PCI) Bus Drivers.
The device is a PCI device with port, memory, interrupt and DMA resources. Device can be stopped and started at run-time and also supports low power states. The driver is capable of doing concurrent read and write operations to the device but it can handle only one read or write request at any time. The following lists the driver framework interfaces demonstrated in this sample:
- Handling PnP & Power Events
- Registering a Device Interface
- Hardware resource mapping: Port, Memory & Interrupt
- DMA Interfaces
- Serialized Default Queue for Write requests
- Serialized custom Queue for Read requests
- Handling Interrupt & DPC
This sample driver is a minimal driver meant to demonstrate the usage of the Windows Driver Framework. It is not intended for use in a production environment.
Note
To build this sample, you can use Microsoft Visual Studio 2013 (Express, Professional, or Ultimate) and Windows Driver Kit (WDK) 8.1 Update. You can get Visual Studio 2013 and WDK 8.1 Update here.
You can also build this sample with Visual Studio 2013 (Professional or Ultimate) and Windows Driver Kit (WDK) 8.1.
For Windows Driver Kit (WDK) 8 samples, download the WDK 8 samples pack. The samples in the WDK 8 samples pack will build only with Microsoft Visual Studio Professional 2012 (Professional or Ultimate) and WDK 8.
Operating system requirements
| Client | |
|---|---|
| Server |
Build the sample
For information on how to build a driver solution using Microsoft Visual Studio, see Building a Driver.