|
Id |
Component |
Headline |
Additional Details |
Workaround (if applicable) |
Planned Resolution |
|
SDSCM00050559 |
IDE |
Register view cannot export registers if group has more than 100
registers in it |
The register export function does not support exporting register
groups that have more than 100 registers in them |
|
|
|
SDSCM00050556 |
IDE |
Memory Usage View should support GCC |
The Memory Usage View is currently only supported for TI build
tools. It is important to support GCC due the growing popularity
... |
|
|
|
SDSCM00050555 |
IDE |
Memory Usage View should state that a non-TI compiler is not
supported |
Memory Usage View should state that a non-TI compiler is not
supported. Currently is displays a misleading message about
setting... |
|
|
|
SDSCM00050552 |
IDE |
assembly source debug for PRU does not work |
Assembly source debug with the PRU does not seem to work well.
The debugger is unable to correlate the assembly source file
with... |
|
|
|
SDSCM00050521 |
IDE |
Autoformat (ctrl + shift + F) can alter formatting of source
files which can cause compiler errors. |
Autoformat (ctrl + shift + F) can alter formatting of source
files which can cause compiler errors. Related to combination
of #... |
|
|
|
SDSCM00050510 |
IDE |
Hide the 'RemoteSystemsTempFile' project as an option when
browsing projects in the workspace |
The RSE plugin comes with CCSv6 by default. Because of that, a
folder called 'RemoteSystemsTempFile' appears in the workspace
w... |
|
CCS 6.2.0 |
|
SDSCM00050509 |
IDE |
PRU projects/executables are not recognized when trying to load
a PRU program via 'Browse Projects' |
PRU projects/executables are not recognized when trying to load
a PRU program via 'Browse Projects'. |
Manually browse to the executable via the 'Browse' button. |
CCS 6.1.0 |
|
SDSCM00050491 |
IDE |
Manual-mode MPU Project-Property Settings don't persist |
|
|
CCS 6.1.0 |
|
SDSCM00050489 |
IDE |
Once launch configuration has been created, can't switch from
load symbols back to load program |
|
|
CCS 6.1.0 |
|
SDSCM00050372 |
IDE |
CCS needs to interpret .debug_macinfo (GCC support) |
In some cases, adding a symbol found in the source window to the
watch window results in an error: identifier not found. This
ha... |
Inspect the generated map file for the program. Look for the
symbol name and note its fully qualified name. Use the long name
in... |
CCS 6.1.0 |
|
SDSCM00050356 |
IDE |
DSS documentation for the description for memory.loadData2() API
has typos. |
DSS documentation for the description for memory.loadData2() API
has typos. Part of the description is: This is an API for
sup... |
|
CCS 6.1.0 |
|
SDSCM00050353 |
IDE |
Scanner config builder is very slow for projects where many
files override build-settings |
|
|
CCS 6.1.0 |
|
SDSCM00050342 |
IDE |
When trying to manually load an executable to a PRU core, Browse
project returns no hits |
The automatic detection of PRU-compatible projects of the option
Load Program is not working for PRU cores. This happens with
... |
Use the Browse button instead |
CCS 6.1.0 |
|
SDSCM00050324 |
IDE |
Switching between Linaro GNU and TI compiler does not
include/exclude linker command file and startup file properly |
Switching between Linaro GNU and TI compiler for TivaC projects
does not automatically include/exclude the proper linker
command... |
|
CCS 6.1.0 |
|
SDSCM00050293 |
IDE |
Spell-checker in the editor does not work |
Spell-checker in the editor does not work despite the feature
being enabled. |
|
CCS 6.2.0 |
|
SDSCM00050275 |
IDE |
License location is lost after an update |
The list of locations CCS checks for licenses is currently
stored in a temporary folder location. This folder is being
deleted d... |
Manually restore the locations in the GUI. |
CCS 6.1.0 |
|
SDSCM00050230 |
IDE |
Browse box of Debug Server log is missing the filename
designator |
When trying to select a file to save the Debug server log, the
browser box that opens does not have a filename designator
field.... |
Create a blank .log file in the desired location: user@host:~$
touch my_log.log Then use the box to select this file |
CCS 6.1.0 |
|
SDSCM00050229 |
IDE |
The ability to set file specific linker options should not be
exposed |
If you have a .lib in your project you can right click on it and
CCS will let you set file specific options for the linker.
How... |
|
CCS 6.2.0 |
|
SDSCM00050201 |
IDE |
Removing file should remove all associated settings |
|
|
CCS 6.2.0 |
|
SDSCM00050189 |
IDE |
Scroll bars missing on Getting Started View |
When the Getting Started View is resized the buttons at the top
are often not visible. However no scroll bars are present so
th... |
Maximize the window |
CCS 6.1.0 |
|
SDSCM00050137 |
IDE |
A basic new project for Tiva does not run to main when built
with Linaro GCC |
A basic new project for Tiva does not run to main when built
with Linaro GCC |
|
CCS 6.1.0 |
|
SDSCM00050132 |
IDE |
Dependency Checker having issues with libusb on CentOS 6.5 |
On CentOS 6.4 and 6.5 the dependency checker in the CCS
installer detects that libusb is missing. However after
installing libu... |
Install libusb1.i686 and then create a soft link that matches
the exact library that is needed. sudo ln -s
/usr/lib/libusb-1.0.... |
CCS 6.1.0 |
|
SDSCM00050110 |
IDE |
Imported TivaWare project missing links files on CCS Linux |
When importing a TivaWare example into CCS 6.0 on Linux, all
broken links are missing in the project. Inspecting the original
.p... |
Manually add missing linked files |
CCS 6.1.0 |
|
SDSCM00050108 |
IDE |
If a GUI Composer app already contains appInitDS.js file, then
it should be used during export |
GUI Composer application export always uses an internal default
appInitDS.js file. This can break existing applications that
had... |
After export, replace appInitDS.js file with file from previous
version of the app. |
CCS 6.1.0 |
|
SDSCM00050102 |
IDE |
Changing part should trigger reindexing |
|
|
CCS 6.1.0 |
|
SDSCM00049988 |
IDE |
Switching compiler tools from Red Hat GNU to TI does not set
linker command file properly |
Switching compiler tools from Red Hat GNU to TI does not set
linker command file properly |
|
CCS 6.1.0 |
|
SDSCM00049947 |
IDE |
New CCS EVE project does not run out of the box |
|
|
CCS 6.1.0 |
|
SDSCM00049947 |
IDE |
New CCS EVE project does not run out of the box |
|
|
CCS 6.1.0 |
|
SDSCM00049946 |
IDE |
EVE CCS/Load Program/Browse Project not working |
|
|
|
|
SDSCM00049946 |
IDE |
EVE CCS/Load Program/Browse Project not working |
|
|
|
|
SDSCM00049946 |
IDE |
EVE CCS/Load Program/Browse Project not working |
|
|
|
|
SDSCM00049917 |
IDE |
Error when using editor feature 'Open Declaration' to jump to
declaration of an array |
Error when using editor feature 'Open Declaration' to jump to
declaration of an array. An internal error occurred during:
"Ope... |
|
|
|
SDSCM00049910 |
IDE |
Adding a source look up from Debug View context menu does not
works |
|
|
CCS 6.1.0 |
|
SDSCM00049901 |
IDE |
Blank line shown above editor area when editors are open side by
side |
When viewing source files side by side you get a blank line
above the editor area. |
|
|
|
SDSCM00049856 |
IDE |
CCSv6 experiences high CPU usage when chromium based tool is
opened |
If GUI Composer feature is installed in Linux, then CCS will
experience high CPU usage for the rest of CCS session. There is
no ... |
|
CCS 6.1.0 |
|
SDSCM00049845 |
IDE |
App Center search should search the title as well |
Currently the app center search looks in the keywords and
description. It should also look in the title. |
|
CCS 6.1.0 |
|
SDSCM00049804 |
IDE |
CCS fails in the presence of VMWare shared folders |
|
Disable VMware shares when installing CCS. |
CCS 6.1.0 |
|
SDSCM00049786 |
IDE |
GC: support bi-directional char array binding |
|
|
CCS 6.1.0 |
|
SDSCM00049763 |
IDE |
headless project import: Add option to auto-import dependant
projects |
When importing projects via CCS GUI, there is an option
"Automatically import referenced projects" which will then
auto-import a... |
|
CCS 6.1.0 |
|
SDSCM00049742 |
IDE |
Pop up a warning dialog when 1 day is left on eval license |
Implement a dialog box that pops up when only 1 day is left on
the evaluation license. |
|
CCS 6.1.0 |
|
SDSCM00049613 |
IDE |
case sensitive mismatch when importing v3 projects to v5 |
If a CCSv3.3 pjt references a source file with a path where the
case of the path is different than the actual folder, it works
f... |
Modify pjt to be case sensitive |
CCS 6.1.0 |
|
SDSCM00049607 |
IDE |
Enhance Codan plug-in with the ability to create custom rules |
Enhance Codan plug-in with the ability to define and create
custom rules. Codan is an Eclipse plug-in and any
modifications wo... |
Use other 3rd party Code Analysis plug-ins that support this
feature |
|
|
SDSCM00049589 |
IDE |
variables decalred in annoymous namspace cannot be accessed
(GCC compiler ) |
|
|
CCS 6.1.0 |
|
SDSCM00049562 |
IDE |
Renaming widget ID causes existing binding to disappear. |
|
|
CCS 6.1.0 |
|
SDSCM00049540 |
IDE |
CCS GUI does not allow for compiler option --interrupt_threshold
with threshold value omitted |
In the CCS GUI, Compiler->Advanced Options->Runtime Model
Options, it does not allow enabling the --interrupt_threshold
option w... |
|
CCS 6.1.0 |
|
SDSCM00049538 |
IDE |
Digital Gauge rapaint issue when threshold value is small |
|
|
CCS 6.1.0 |
|
SDSCM00049537 |
IDE |
Installation dialog shows "Not Responding" |
When installing CCSv6 beta, you have the option to choose
additional components to be installed (GCC, GUI composer, etc).
After ... |
|
CCS 6.1.0 |
|
SDSCM00049534 |
IDE |
Windows ERRORLEVEL code is not set for headless project import
error |
When using the headless command to import a project which
already exists in the workspace, an error occurs. However the
ERRORLEV... |
|
CCS 6.1.0 |
|
SDSCM00049478 |
IDE |
CCSv6 should be integrated in Ubuntu's Dash menu |
Historically CCS and Blackhawk/Spectrum Digital always created
desktop icons in Ubuntu. This is fine for Ubuntu releases 10.10
... |
N/A. |
CCS 6.1.0 |
|
SDSCM00049404 |
IDE |
msp430 emulation logic not restored on a hard reset |
|
|
CCS 6.1.0 |
|
SDSCM00049303 |
IDE |
C6671 device file specifies 2 C66x cores when it should be one |
The device xml file for C6671 is incorrect (C6671.xml). It
specifies 2 C66x cores instead of one. |
|
CCS 6.1.0 |
|
SDSCM00049211 |
IDE |
Need erase flash option for MSP430 |
There should be an action available from the flash options to
just erase the flash. |
|
CCS 6.1.0 |
|
SDSCM00049095 |
IDE |
The wrench/push-pin icon that denotes a file with file specific
options does not appear when expected |
The wrench/push-pin icon that denotes that a file has file
specific options does not appear when expected |
|
CCS 6.1.0 |
|
SDSCM00049080 |
IDE |
Hovering the mouse cursor over messages in Problems and Advice
views show truncated by the column width |
When hovering the mouse over a message in the Problems or Advice
views, the message tool tip is truncated by the width of the
De... |
N/A. |
|
|
SDSCM00049004 |
IDE |
MSP430 GTI driver is getting installed even when MSP is not
installed |
The MSP430 GTI driver is getting installed into
ccs_base/DebugServer/drivers even when MSP430 support is not
installed. |
|
|
|
SDSCM00048600 |
IDE |
CCS needs to interpret .debug_macinfo ( was: Symbol not found
when adding expression ) |
In some cases, adding a symbol found in the source window to the
watch window results in an error: identifier not found. This
ha... |
Inspect the generated map file for the program. Look for the
symbol name and note its fully qualified name. Use the long name
in... |
CCS 6.1.0 |
|
SDSCM00048029 |
IDE |
CCS flash programmer fails with message "Timed out while writing
to Flash memory" |
CCS flash programmer fails with message "Timed out while writing
to Flash memory" |
Change the Flash Erase option from "Necessary Pages Only" to
"Use the Erase Options Specified Below", which will erase Entire
Fl... |
CCS 6.1.0 |
|
SDSCM00047828 |
IDE |
Enhancement to use last specified data format for new views. |
Would like ability to use last specified data format for new
memory views rather than a fixed default. |
|
CCS 6.1.0 |
|
SDSCM00047827 |
IDE |
Would like ability to rename memory view "tabs" to user
specified name |
Enhancement request to provide ability to rename memory view
tabs |
|
CCS 6.1.0 |
|
SDSCM00047723 |
IDE |
In the Target Configuration Editor, changing the "Device" or the
"Connection" should not reset to all defaults |
Whenever creating a Target Configuration using the Editor, any
changes to either the Connection or the Device reset all
settings... |
N/A. |
CCS 6.2.0 |
|
SDSCM00047490 |
IDE |
Rebuild of index for updating macro expansions does not permeate
through multiple levels of include files |
Rebuild of index for updating macro expansions does not permeate
through multiple levels of include files |
|
|
|
SDSCM00047442 |
IDE |
New project wizard should only create one default build
configuration |
When a new project is created in CCS, two build configurations
are created by default - 'Debug' and 'Release'. This has been
the... |
|
|
|
SDSCM00047370 |
IDE |
Add support for easily leveraging build variables when setting
build properties |
It would be helpful to improve the usability in specifying build
variables when setting build options. For example, it is very
c... |
|
CCS 6.1.0 |
|
SDSCM00047368 |
IDE |
Ability to import/export project and workspace level variables
(to/from a file) |
Ability to import/export project and workspace level variables
(to/from a file). This includes both linked resource path
variabl... |
|
CCS 6.1.0 |
|
SDSCM00047366 |
IDE |
Improve usability for setting linked resource path variables and
build variables |
People are often confused with setting Linked Resource Path
Variables and Build Variables. The main confusion is the need
for ha... |
|
CCS 6.1.0 |
|
SDSCM00047285 |
IDE |
Support Linux OS Aware Debug |
This feature existed with CCSv4 but was not ported to CCSv5 for
a variety of reasons (compatibility issues with stock Eclipse,
l... |
|
|
|
SDSCM00047055 |
IDE |
Support for debugging RealView Compiler output including
Semi-hosting |
Would like to be able to use CIO functions like printf when
debugging code generated by the RealView compiler in CCS. |
|
CCS 6.1.0 |
|
SDSCM00046736 |
IDE |
Eclipse won't start when there are unusual characters in the
platform path |
Eclipse and hence CCS will not start if a folder contains #!$
characters in the path. As a workaround CCS installer is
detecting... |
Don't use a User or Install path that includes characters like #
or $. |
|
|
SDSCM00046255 |
IDE |
JLink: loading and running program in a debug session on
LM3S9D92 behaves oddly |
1. connect to lm3s9d92 using JLink v0.1.0.3 and after 2. load
blinky.out from stellarisware 3. run, the execution will stop
aft... |
After loading and running once, reset the device (menu Run -->
Reset --> Core Reset) to properly run the code. |
CCS 6.1.0 |
|
SDSCM00045764 |
IDE |
Renaming linked files causes invalid duplicate links in another
workspace that is sharing the same file |
When the file is renamed in CCS (hence updating the .project
file), the rename is not getting handled properly by other
workspac... |
Remove the project from the workspaces that exhibit the issue
and re-import it. This will correctly update the Project
Explorer ... |
|
|
SDSCM00044613 |
IDE |
XDC Content Assist is triggering a lot exceptions in customer
workspace logs |
Clicking on certain variables may trigger exceptions in
workspace log. There does not appear to be a user impact beyond
exceptio... |
|
CCS 6.1.0 |
|
SDSCM00042650 |
IDE |
[TISB] Project Manager should add the RTSC Platform file to the
Project Explorer view |
|
|
|
|
SDSCM00042329 |
IDE |
Support ISA aware dynamic support for view menu |
The MMU Page Table View should be listed on the view menu. |
|
CCS 6.1.0 |
|
SDSCM00042270 |
IDE |
Linker - Cmd mapping should be introduced when a user changes
defaults for RTSC projects. |
|
|
CCS 6.1.0 |
|
SDSCM00041325 |
IDE |
Library projects for non-default build configurations must have
'lib' for the Artifact Extension |
Library projects for non-default build configurations must have
'lib' for the Artifact Extension. The default 'Debug' and
'Relea... |
|
|
|
SDSCM00040708 |
IDE |
For header files outside the project folder double clicking on
compile errors in the Problems view does not jump to error |
When a compilation error occurs in a header file that is outside
the project (e.g. system header file or even user header file
l... |
|
|
|
SDSCM00040262 |
IDE |
MMU Page table view should be listed on the view menu |
The MMU Page Table View should be listed on the view menu. |
|
|
|
SDSCM00040259 |
IDE |
Merge the two CCS project import wizards |
Today we have separate wizards for importing eclipse based CCS
projects and legacy CCSv3.x projects. We could have them be a
si... |
|
|
|
SDSCM00040045 |
IDE |
NullPointerException when renaming project |
Sometimes when renaming an imported project you will get a
dialog complaining of a null pointer exception. |
|
|
|
SDSCM00040028 |
IDE |
Import wizard should prompt user to change compiler version if
needed |
If I am importing a project that uses a different version of the
compiler than what I have installed the wizard should inform
me... |
|
|
|
SDSCM00039559 |
IDE |
Would like ability to adjust file specific options on multiple
selected files. |
Would like ability to be able to apply file specific options on
multiple files. |
|
|
|
SDSCM00038857 |
IDE |
EASY: Simplified Build Options Dialog |
Today the build options dialog is quite cluttered and it can be
overwhelming to use. Creating the Basic options helped a bit
bu... |
|
|
|
SDSCM00038571 |
IDE |
Need excluded files filter for the Project Explorer |
In the Project Explorer, which will be the default project view
in CCSv5 instead of the C/C++ Projects View, there is a list of
... |
|
|
|
SDSCM00034673 |
IDE |
CCS v4 allows usage of 1 hardware breakpoint less than CCS 3.3
for BIOS programs |
CCS v4.0x allows user to set only 1 hardware breakpoint when
debugging BIOS programs in Flash |
|
|
|
SDSCM00050410 |
DVT |
Request to add commas to timestamps in RTOS Analyzer views to
make it easier to analyze the numbers |
Request to add commas to timestamps in RTOS Analyzer views to
make it easier to analyze the numbers |
|
|
|
SDSCM00050409 |
DVT |
Request for a way to be able to adjust and save column settings
in system analyzer data views |
Request for a way to be able to customize and save column
settings in system analyzer data views so they are preserved for
futur... |
|
|
|
SDSCM00050408 |
DVT |
Request for a way to clear the printf log data without having to
close the view |
Request for a way to clear the printf log data without having to
close the view |
|
|
|
SDSCM00050087 |
DVT |
Ability to show user events in Execution Graph |
|
|
CCS 6.1.0 |
|
SDSCM00050080 |
DVT |
Support dynamic TSK/HWI/SWI name in System Analyzer |
|
|
CCS 6.1.0 |
|
SDSCM00050047 |
DVT |
System Analyzer/UIA data transfer via JTAG should have a
progress bar |
When using UIA in JTAG stop mode, this stage is preceded by the
time when the JTAG reads data from the target. If the logger
buf... |
N/A. |
|
|
SDSCM00048808 |
DVT |
Trace Analysis Features are not filtered by device |
Analysis features shown in the Trace Viewer should only show
those features applicable to the selected device. |
|
CCS 6.2.0 |
|
SDSCM00046280 |
DVT |
Image Analyzer does not process 8bit data read in big endian for
RGB correctly |
Ther is a problem with viewing RGB data with 8bit Data Read. See
forum post for details.
http://e2e.ti.com/support/development_... |
Customer was able to workaround this using 32bit Data Read. See
Forum Post for details:
http://e2e.ti.com/support/development_t... |
CCS 6.1.0 |
|
SDSCM00045827 |
DVT |
Using JTAGRunMode with stairstep example on LM4F232 results in
"trouble reading memory block" error |
RTA does not work reliably when using JTAGRunMode on LM4F232 and
results in "trouble reading memory block" errors. |
|
CCS 6.2.0 |
|
SDSCM00043762 |
DVT |
The format display for Y axis does not show 64-bit values
correctly |
When displaying graphs with 64-bit data, the Y axis shows
invalid data when using Display Format as General, Decimal or
Scientif... |
Use Hexadecimal format instead. Right-click on the graph view
and select Display Properties --> Axes --> Y-axis --> set the
val... |
CCS 6.2.0 |
|
SDSCM00041756 |
DVT |
Add ability in image analyzer to flip the image on either axis:
up/down or left/right |
Request to add the ability in image analyzer to flip the image
on either axis: up/down or left/right |
|
|
|
SDSCM00041366 |
DVT |
Code Coverage coloring does not work for files that do not have
a CCS Project |
Line coloring works if coverage is done for an executable from a
CCS Project. Does not work E.g. if a .out file is directly
loa... |
|
|
|
SDSCM00040472 |
DVT |
Would like to pick out a range of data to display |
|
|
|
|
SDSCM00040471 |
DVT |
Show profile data in call graph |
|
|
|
|
SDSCM00040470 |
DVT |
Call graph with link back to raw data view |
|
|
|
|
SDSCM00040469 |
DVT |
Use profile data to compute CPU loading |
|
|
|
|
SDSCM00050465 |
Emulation |
XDS100v2 voltage detection circuit applies excessive voltage to
the FPGA's input pin |
The circuit diagram and some measurements show that USB's Vbus
(5V) is injected into pin 16 of the XC2C32A FPGA, which is void
b... |
The simplest way to workaround this is to add a 10k resistor in
the trace that connects R31 (5.1k) to pin 16 of the XC2C32A. Thi... |
CCS 6.1.0 |
|
SDSCM00050444 |
Emulation |
When two XDS100 emulators are connected to a USB3.0 Hub, only
one emulator is able to be connected to CCS |
CCS fails to connect to one of two XDS100 emulators when they
are plugged to the ports of a USB3.0 Hub. This causes problems
i... |
Use a USB2.0 port instead. |
|
|
SDSCM00050124 |
Emulation |
Unable to step over an ARM embedded BKPT instruction if it is
BKPT 123, works if it is BKPT #123 |
If you embed a breakpoint instruction like this: BKPT 123 The
debugger will halt at it but you cannot run or step past it.
Howe... |
Use # before the number |
CCS 6.1.0 |
|
SDSCM00049637 |
Emulation |
Remove/improve error messages displayed in CCS console when
accessing uninitialized peripherals |
Request to remove/improve error messages displayed in CCS
console when accessing uninitialized peripherals. |
|
CCS 6.1.0 |
|
SDSCM00047580 |
Emulation |
Linking MSP FETS and sessions |
|
|
|
|
SDSCM00047337 |
Emulation |
Request to separate out FPU registers into their own group |
Request to separate out FPU registers for Stellaris into their
own group so they are visible in the CCS registers view under
the... |
|
|
|
SDSCM00047129 |
Emulation |
Default heap size for MSP430 helloworld is too small for FR5739 |
The default heap size for the helloworld template is not being
enough for MSP4305739. |
Increase the heap size to 280 |
|
|
SDSCM00043910 |
Emulation |
MSP430 REGISTER view descriptions for SR.SCG0 and SR.SCG1
incorrect in CCSv5.1 |
|
|
|
|
SDSCM00042934 |
Emulation |
Improve the error message when attempting to connect to the
ethernet interface of XDS560v2 STM from multiple hosts |
Whenever two users attempt to connect to the ethernet interface
of a single XDS560v2 STM emulator, the error message thrown
show... |
N/A. |
CCS 6.1.0 |
|
SDSCM00050528 |
Trace |
Unable to set breakpoint while target is running on Tiva
LaunchPad |
When trying to set a (hardware) breakpoint on a running Tiva
LaunchPad, the below error occurs: "Error enabling this
function: ... |
Manually halt the target first |
|
|
SDSCM00050028 |
Trace |
Code coverage trace job freezes CCS |
When trying to gather the data for code coverage analysis trace
job, CCS freezes while processing the incoming data. This
issu... |
N/A |
|
|
SDSCM00050024 |
Trace |
Cache analysis trace job collapses CCS |
When trying to gather the data for cache analysis trace job, CCS
collapses without a trace. This is probably related to the
am... |
N/A |
|
|
SDSCM00049896 |
Trace |
Trace Server Crashes on Debugger Terminate after using ITM |
Trace server crashes after using ITM. CCS does not crash, just
the trace server. |
|
CCS 6.1.0 |
|
SDSCM00049598 |
Trace |
ETB Trace fails to collect data in CCSv6 for Linux |
ETB Trace fails to collect data on CortexA and ARM9 cores.
When setting a PC Trace job via ETB, the setup procedure goes
witho... |
N/A. |
CCS 6.1.0 |
|
SDSCM00049598 |
Trace |
ETB Trace fails to collect data in CCSv6 for Linux |
ETB Trace fails to collect data on CortexA and ARM9 cores.
When setting a PC Trace job via ETB, the setup procedure goes
witho... |
N/A. |
CCS 6.1.0 |
|
SDSCM00048813 |
Trace |
When simultaneously running two separate CCS debug session, one
instance may hang and crash |
When simultaneously running two separate CCS debug session, one
instance may hang and crash when trying to run both targets.
Th... |
Use a single target configuration that defines both emulators. |
CCS 6.1.0 |
|
SDSCM00048795 |
Trace |
Trace: "End at address" of the "Trace Range" parameter fails to
stop and display trace data |
Setting an end address to the "Trace Range" parameter fails to
stop the Trace data collection at the specified address and
cause... |
Use "Range" or "Start and stop at address" instead. |
CCS 6.1.0 |
|
SDSCM00044490 |
Trace |
Need to load installed libbz2.dll and not the first one found on
the windows path |
|
Remove the other version of the library from the windows path |
CCS 6.1.0 |