� U-Boot SPL 2018.01 (Feb 03 2020 - 11:22:17) DRA722-GP ES2.0 Trying to boot from MMC1 no pinctrl state for default mode no pinctrl state for default mode Card did not respond to voltage select! *** Warning - MMC init failed, using default environment U-Boot 2018.01 (Feb 03 2020 - 11:22:17 +0530) CPU : DRA722-GP ES2.0 Model: TI AM5718 IDK Board: AM571x IDK REV 1.3B DRAM: 1 GiB MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1 Card did not respond to voltage select! *** Warning - MMC init failed, using default environment Card did not respond to voltage select! invalid mmc device SCSI: SATA link 0 timeout. AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode flags: 64bit ncq stag pm led clo only pmp pio slum part ccc apst scanning bus for devices... Found 0 device(s). Net: Could not get PHY for ethernet@48484000: addr 0 Warning: ethernet@48484000 using MAC address from ROM eth0: ethernet@48484000 Hit any key to stop autoboot: 0 switch to partitions #0, OK mmc0 is current device SD/MMC found on device 0 ** Unable to read file boot.scr ** 1490 bytes read in 2 ms (727.5 KiB/s) Loaded env from uEnv.txt Importing environment from mmc0 ... Running uenvcmd ... 1 bytes read in 2 ms (0 Bytes/s) Already setup. switch to partitions #0, OK mmc0 is current device SD/MMC found on device 0 4026880 bytes read in 290 ms (13.2 MiB/s) 97137 bytes read in 56 ms (1.7 MiB/s) ## Flattened Device Tree blob at 88000000 Booting using the fdt blob at 0x88000000 Loading Device Tree to 8ffe5000, end 8ffffb70 ... OK Starting kernel ...