# # This file defines the modules included in $(MAKECONFIG) config # # Modules are split into, # - Use-cases specified in uc_cfg.mk # - Other system config/feature, specified in this file # # Any specific overrides are also specified in this file # Example, for TDA3x SoC EVE2/3/4 are not present and hence force marked as , i.e disabled # # # Additional config options # # # CPUs to included in build # PROC_IPU1_0_INCLUDE=yes PROC_IPU1_1_INCLUDE=yes PROC_IPU2_INCLUDE=yes PROC_A15_0_INCLUDE=yes PROC_DSP1_INCLUDE=yes PROC_DSP2_INCLUDE=yes PROC_EVE1_INCLUDE=yes PROC_EVE2_INCLUDE=yes VSDK_BOARD_TYPE=TDA2PX_EVM DUAL_A15_SMP_BIOS=no # Supported values: DDR_MEM_512M DDR_MEM=DDR_MEM_512M # Supported values: ipu1_0 ipu1_1 a15_0 none NDK_PROC_TO_USE=a15_0 #Used to control TFDTP stack (supported only when NDK_PROC_TO_USE = ipu1_1) NSP_TFDTP_INCLUDE=no # Supported values: ipu1_0 none FATFS_PROC_TO_USE=ipu1_0 # # Used to control building of algorithm source. # By default algorithm source not included in Vision SDK # BUILD_ALGORITHMS=no # # Applies profile to all cores # # Supported profiles: release debug #PROFILE=debug PROFILE ?= release PROFILE_ipu1_0 ?= $(PROFILE) PROFILE_ipu1_1 ?= $(PROFILE) PROFILE_ipu2 ?= $(PROFILE) PROFILE_c66xdsp_1 ?= $(PROFILE) PROFILE_c66xdsp_2 ?= $(PROFILE) PROFILE_arp32_1 ?= $(PROFILE) PROFILE_arp32_2 ?= $(PROFILE) PROFILE_a15_0 ?= $(PROFILE) # # For TDA2xx, TDA2Px & TDA2Ex - vision SDK can run on either IPU1 or IPU2 subsystem # For TDA3xx - We have only IPU1 and hence IPU1 is the only option # Select IPU primary core from the available IPU1 & IPU2 subsytems # # Supported values: ipu1_0 ipu2 IPU_PRIMARY_CORE=ipu1_0 IPU_SECONDARY_CORE=ipu2 # # Set A15_TARGET_OS # A15 can run Linux or Bios # # A15_TARGET_OS support # Platform BIOS Linux # # TDA2XX_EVM yes yes # TDA3XX_EVM yes no # TDA2EX_EVM yes yes # TDA2PX_EVM yes yes # # Supported values: Bios Linux A15_TARGET_OS=Bios IVAHD_INCLUDE=yes VPE_INCLUDE=yes DSS_INCLUDE=yes CAL_INCLUDE=yes ISS_INCLUDE=yes # # EMIF ECC and Freedom from Interference (FFI) are clubbed together as they # involve consolidated memory map changes # ECC_FFI_INCLUDE=yes is not supported for DDR_MEM_128M # If ECC_FFI_INCLUDE is set to no - memory map will match older versions. # Firewall configuration and DSP XMC configuration is enabled/disabled using this # flag # Vision SDK does not enable EMIF ECC but expects SBL to enable it. # Vision SDK sets up ECC error handlers irrespective of value of ECC_FFI_INCLUDE. # ECC_FFI_INCLUDE=no AVB_INCLUDE=no # # Enable below macro to enable DCAN integration into Vision SDK. # DCAN_INCLUDE=no # # Enable below macro to enable Radar integration into Vision SDK # RADAR_INCLUDE=no # # Enable below macro to enable OPENVX into Vision SDK # OPENVX_INCLUDE=no CIO_REDIRECT=yes CPU_IDLE_ENABLED=yes # # Enable below macro to view the bandwidth used by different IPs in the device # as a graphical plot on the display screen. # DATA_VIS_INCLUDE=no OPENCL_INCLUDE=no ENABLE_OPENCV=no HS_DEVICE=no # # Enable this macro to enable Ultra sonic based initialization # This is added as the power measurement and Ultra sonic use the same # pad on the device. Kindly note the Ultrasonic and power measurement # use the same GPIO6_14/15 pads with different functionalities. Ultrasonic configures # UART10 on those pads and power measurement configures I2C3. Hence when this # macro is yes the power measurement functionality is not supported. # ULTRASONIC_INCLUDE=no # Enable this macro to enable profiling features through system analyzer on CCS ENABLE_UIA_PROFILING=no # #Flag for task profiling # ENABLE_TASK_PROFILE_UTIL=yes include $($(MAKEAPPNAME)_PATH)/configs/$(MAKECONFIG)/uc_cfg.mk