![]() |
![]() |
Broadcast/multicast bandwidth limit configuration parameters. More...
#include <cpsw_ale.h>
Data Fields | |
uint32_t | portNum |
bool | enableBRateLimitForPort |
bool | enableMRateLimitForPort |
uint32_t | bcastLimitNumPktsPerSec |
uint32_t | mcastLimitNumPktsPerSec |
Broadcast/multicast bandwidth limit configuration parameters.
uint32_t CpswAle_PortBcastMcastRateLimitParams_s::bcastLimitNumPktsPerSec |
Broadcast packet limit per second
bool CpswAle_PortBcastMcastRateLimitParams_s::enableBRateLimitForPort |
Enable Broadcast Rate Limit for port. If set to TRUE, bcastLimitNumPktsPerSec should be non-zero
bool CpswAle_PortBcastMcastRateLimitParams_s::enableMRateLimitForPort |
Enable Multicast Rate Limit for port. If set to TRUE, mcastLimitNumPktsPerSec should be non-zero
uint32_t CpswAle_PortBcastMcastRateLimitParams_s::mcastLimitNumPktsPerSec |
Multicast packet limit per second
uint32_t CpswAle_PortBcastMcastRateLimitParams_s::portNum |
Port number for which broadcast/multicast rate limiting configuration is to be done