Table of Contents

Example Summary

This example demonstrates the various range of networking capabilities which the CC3220 device family provides.
For simplicity, We divide our Application’s functionality into four different silos:

Silo Description
Wlan Contains link layer functions like scan, connect, etc.
NetApp. Demonstrates the usage of networking applications.
Socket Shows variety of socket API and responsible for sending and receiving data.
Transceiver Gives the user a direct interface to the NWP radio for RF tests, raw sockets (L1) and more.

Each silo contains several commands, accessible by the user via command line interface,
which implemented using CC3220 user UART. Any events or application output, would be displayed over the UART terminal screen. Later on, in the Available Commands section, we’ll discuss in greater detail about each silo and the commands it includes.

Example Usage

The connection should have the following connection settings:

    Baud-rate:    115200
    Data bits:         8
    Stop bits:         1
    Parity:         None
    Flow Control:   None

Once the application has complete it’s initialization and the network processor is up,
the application banner would be displayed, showing version details:

        ============================================
           Network Terminal Example Ver: 1.0.1.0
        ============================================
         CHIP: 0x30000019
         MAC:  2.0.0.0
         PHY:  2.2.0.3
         NWP:  3.1.99.4
         ROM:  0
         HOST: 2.0.1.15
         MAC address: 70:ff:76:1c:2a:15
        ============================================

At this point, a menu showing the available commands would be printed followed by command prompt,
indicating that the application is ready for user input.

Application’s Overview

Network Terminal is a command line interface (cli) based application,
used to demonstrate the CC32XX/CC31XX networking capabilities. It does that by offering a list
of commands, fed to the application via UART and later parsed and dispatched.

The application starts with invoking cmd_prompt() which polls the UART input for a command.
Polling is completed once a cartridge return is detected. At this point in time, cmd_prompt possess
the command name, followed by the user’s choice of parameters. Once command is obtained,
cmd_prompt searches for the user’s command in the global command table, gCmdList.
For each command, this table stores three entries: the command string,
a callback which handles the command and a menu print callback that prints the help menu.

If the typed command matches a table entry, the handler is dispatched and the parameters
fed by the user are passed to the command callback.
All callback functions follow the same naming convention: cmd<command_name>Callback
and resides at the appropriate file. For example, all WLAN related callbacks are implemented in: wlan_cmd.c.

Inside each command callback, the first action is to parse the user’s input. This is achieved by
calling the corresponding parser function. A structure containing each command’s parameters
is also passed to the designated parser and returned filled with the parsed user’s parameters.
Later, the parsed structure is handled by the callback.
All command parser function follows the same naming convention: Parse<command_name>Cmd.
Parser functions resides in cmd_parser.c.

Once a dispatched callback finish it’s run, the application’s return to the cmd_prompt function,
ready of another input from the user.

Available Commands

Wlan commands:

  1. One shot: If background scans Aren’t set, the API call sl_getNetworkEntries() would result in return value
    of SL_ERROR_WLAN_GET_NETWORK_LIST_EAGAIN and the NWP triggers one scan only, in order to fill it’s cache with results.
    Upon calling sl_getNetworkEntries() once again, user can now retrieve these results and scans stays shut.

  2. Background: These kind of scans are issued on a regular time bases in the background, according to the scan policy.
    If user has set background scans, (using setpolicy command), invoking the API: sl_getNetworkEntries() would return the results collected in the NWP’s cache up to this point.

Usage: 
  scan [-help] [-n <number of APs to display>]
  
  -n        Maximum number of Scan results to show
  -help     Display this help.

Note: If no policy is set, scan command issue One-shot scan according to system persistent settings.

Once scan command has successfully completed, available devices would be printed to UART console.

Example:

scan -n 30

  1. Scan interval: times between consecutive scans.
  2. Hidden scan: If this option is set, scan results would include hidden SSIDs as well.
  3. Enabled Channels: This option uses HEX bitmask to determine the enabled scan channels.
  4. RSSI threshold: By setting an RSSI threshold, users can eliminate results with poor signal quality.
  5. Turn background scans off: This option would shut background scans immediately.
Usage: 
  setpolicy [-help] [-i <Scan interval in Sec>] [-h <hidden scan>]
            [-c <Channel Mask in HEX>] [-r <RSSI threshold>] [-o <Turn scans off>]
            
  -i      Sets scan interval in seconds (default is 10 seconds)
  -h      Scan for hidden AP as well (hidden scan = [YES, NO], default is NO)
  -c      Sets specific scan channels, using HEX base bitmask. (default is `0x1FFF` - all enabled)
  -r      Sets RSSI threshold for scan in dBm units (range: [-95,0] default: `-95`)
  -o      Turn scans off (YES = scans running in background would stop immediately)
  -help   Show Help regarding the setpolicy command.

Note: Once ‘setpolicy’ command has been executed, background scans would start immediately,
according to provided parameters. If no parameter is provided to this command, It would be using
it’s default values.

Note: calling ‘setpolicy’ command with -o YES parameter, would shut down scans
and would not set any other parameters given to this command.

After setting policy, calling Scan command would retrieve results from NWP cache, according to set settings.
Please note that the NWP cache has ageing time, so older retrieved results could violate the new policy.

Example:

setpolicy -i 30 -c 1D5 -r -48

  1. SSID: The requested SSID of the AP. Application expects this parameter to be inside quotation marks (" /“).
  2. Security Type: Device supports four modes: [OPEN, WPA/WPA2, WEP, WPS].
  3. Password: If needed, application expects this parameter to appear inside quotation marks (“/”).
  4. Static IP: User can decide to configure a static IP address. Application expect this parameter in dotted decimal format.
  5. Gateway: User can set it’s gw address statically. Unless provided, default parameter is set (IP address netmasked with 24).
  6. DNS: User can also set it’s dns address. Unless provided, default parameter is the gw address.
  7. Enterprise credentials: Enterprise user name needed in order to log in an enterprise network.
Usage: 
  wlanconnect [-help] [-s <"ssid name">] [-t <security type>] [-p <"password">]
  [-ip <static ip>] [-gw <static gw>] [-dns <static dns>] [-ent <"ent_username">]
  
    -s      SSID
    -t      Type of security (security type = [OPEN, WPA/WPA2, WEP, WPS])
    -p      Password in ascii character (pin in case of WPS)
    -ip     Static IP in '.' format for ipv4 and in ':' for ipv6
    -gw     Static Gateway (relevant in case of using a static IP)
    -dns    Static DNS (relevant in case of using a static IP)
    -ent    Enterprise user name credentials
  1. SL_WLAN_EVENT_CONNECT: This event signals that the NWP is connected to an AP. It also prints details
    about the connected AP, such as SSID and BSSID. Please Refer to SimpleLinkWlanEventHandler() implemented
    in network_terminal.c for more info.

  2. SL_DEVICE_EVENT_DROPPED_NETAPP_IPACQUIRED : This event signals that the device has an IP address.
    Event type is the same in both dynamic or static IP settings. Also, this event print useful information
    such as the leased IP, and the designated gateway. Please refer to SimpleLinkNetAppEventHandler()
    implemented in network_terminal.c for more info.

  3. SL_WLAN_EVENT_DISCONNECT : In case the device is already connected to an AP, before attempting to connect with the requested AP, the device would disconnect from the old one. Disconnect reason code would than be: SL_WLAN_DISCONNECT_USER_INITIATED. Please refer to SimpleLinkWlanEventHandler() implemented
    in network_terminal.c for more info.

Note: In this version, the only cypher used for enterprise Wlan connection is MSCHAPv2. Cypher option would be added in future releases.

Example:

wlanconnect -s "myhome network" -t WPA/WPA2 -p "password" -ip 10.123.45.11

Usage: 
    wlan_ap_start [-help] [-s <"ssid name">] [-t <security type>] 
    [-p <"password">][-h <hidden AP>][-txp <Tx power [0-15]>]
    [-c <Wlan channel [1-13]>] [-l <STA connection limit [1-4]>]
          
    -s      SSID
    -t      Type of security (security type = [OPEN, WPA/WPA2, WEP, WPS])
    -p      Password in ascii character (pin in case of WPS)
    -h      Start the AP in hidden mode (hidden mode = [YES, NO], Default is not hidden)
    -txp    Set Wlan Tx power (0 = Max Power, Default is Max)
    -c      Set channel for the AP (Default is channel 1)
    -l      Limit the number of connected stations
    -help   Display this help.
  1. SL_DEVICE_EVENT_DROPPED_NETAPP_IPACQUIRED : This event signals that the device has an IP address.
    This essentially states that device has started in AP mode, since it sets it’s own IP address.
    Also, this event print the leased IP, and the designated gateway (normally they’re the same).
    Please refer to SimpleLinkNetAppEventHandler() implemented in network_terminal.c for more info.

  2. SL_WLAN_EVENT_STA_ADDED : In case a station is connected to the device, this event is prompt. It than prints to the UART monitor the BSSID of the added station. Please refer to SimpleLinkNetAppEventHandler() implemented in network_terminal.c for more info.

  3. SL_WLAN_EVENT_STA_REMOVED : This event states that a connected station has disconnected.
    the BSSID of the disconnected station would also be displayed. Please refer to SimpleLinkNetAppEventHandler() implemented in network_terminal.c for more info.

Note: As mentioned in wlanconnect command, SSID and password parameters are expected to appear inside quotation marks.

Note: Invoking ‘wlan_ap_start’ when device is in p2p/station mode, would cause an NWP reset, and any ongoing connection would be disconnected.

Example:

wlan_ap_start -s "mySimpleLink" -t OPEN -l 1 -c 11 -txp 0 

  1. Drop: The packet which met the rule set by the filter, would be discarded.
  2. Pass: No action would be taken - this option is necessary in case of parent filter.
  3. Host event: Upon action, a user event would be triggered by the host driver.
  1. S_MAC: source mac, meaning set the match criteria according to packet’s source mac address.
  2. D_MAC: Destination mac address - following the same logic - match criteria is destination mac address.
  3. BSSID: This allows the user to filter packets according to the packet’s BSSID field.
  4. S_IP: Source Ip, meaning set the match criteria according to the packet source IP address.
  5. D_IP: Destination Ip, meaning set the match criteria according to the packet destination IP address.
  6. FRAME_TYPE: Set match rule according to frame types: Management, Control or Data.
  7. FRAME_SUBTYPE: Set match rule according to frame subtype field in packet header.
  8. PATTERN: Set match rule according to specific pattern in packet’s payload.

Moreover, aside from rule and action, filters must have two more important settings, which are ‘Mode’ and ‘comparison type’.
By mode, we let the filter know in which connection configuration it should operate and by comparison type we let the filter know what criteria the rule is being checked against.

  1. L4: Filter applies when device is in station mode.
  2. L4_CON: Filter applies when device is in station mode, but also connected to an AP.
  3. L1: Filter applies when device is in transceiver mode.
  1. Equals: Does the field in packet header equals to the set rule? If so, we have rule match.
  2. Not Equals: Does the field in packet header not equal to the set rule? If so, we have a rule match.

Once a filter has it’s set of rules, actions, mode and comparison type configured, it is ready to be enabled. There’s one more thing ‘create filter’ allows a user to do and that’s to combine filters in an hierarchy structure, specifically in a parent and son configuration. That issue would be covered in the parent filter section below.

Usage: 
  createfilter[-help] [-f <filter Type>] [-v <Compare value>] [-e <Compare type>]  
  [-a <Action type>] [-m <Mode>] [-o <Offset>] [-i <Parent filter ID>]
  
        -f      Filter Types:
                [S_MAC, D_MAC, BSSID, S_IP, D_IP, FRAME_TYPE, FRAME_SUBTYPE, PATTERN]
                [S - Source, D - Destination]
                [MAC - MAC address, Value: xx:xx:xx:xx:xx:xx]
                [BSSID - MAC address OF THE AP, Value: xx:xx:xx:xx:xx:xx]
                [IP - IP Address, Values: IPv4 - xxx.xxx.xxx.xxx, IPv6 - xxxx:xxxx:xxxx:xxxx:xxxx:xxxx:xxxx:xxxx]
                [FRAME_TYPE Values: management, control, data]

        -v      Comparison value used by the filter (sets the filter match criteria)
        -e      Compare type (Compare type = [equals, not equals])
        -a      Action on match (Action type = [event, drop, pass]), Either async event, drop the packet or let it pass
        -m      Filter Mode (Mode = [L4_CON, L4, L1])
                L4_CON - L4 connected to AP, L4 - L4 not connected to AP and  L1 - transceiver mode
        -o      Offset from L1 / L4 Header, according to chosen 'Mode' field (Valid only for 'PATTERN' filter Type)
        -i      Parent filter for a leaf filter, otherwise: 0

How to achieve this?
The answer is simple : We define two different filters, in a ‘parent - son’ configuration:

Example:

createfilter -f S_MAC -v XX:XX:XX:XX:XX:XX -e equals -a pass -m L4 -i 0

Filter Created successfully, filter's ID = 4

A message stating the filter was created successfully and it’s ID, should appear on screen.

Example:

createfilter -f PATTERN -v CAFE -e equals -a event -m L4 -o 20 -i 4

Please enter user ID, in range: [0,63] (needed for Host event action).
user@CC3220:

Since the action chosen is ‘event’, application would prompt you for host event ID.

Host event ID is used to indicate which filter has triggered the event. Elaborate explenation would follow.

user@CC3220:60
 Filter Created successfully, filters ID = 5

Finally, by setting the option -i 4, we’ve combined the two filters, such that each packet is checked first by the first filter, and upon match it would be checked against our second filter.

  1. SL_WLAN_EVENT_RXFILTER: This event prints the user Action ID bitmap. If bit i is set,
    host event ID number i has been triggered.

Note: Rx filters can have more advanced settings and filter combinations. Also, there are some limitations on which kind of filter can be a parent filter for another one. It’s highly advised to look at the RX filters section on programmers manual, before incorperating RX filters in your application.

Note: Rx filters are NOT supported for AP mode.

Note: ‘createfilter’ only creates a filter. In order to enable the filters, look at enablefilter.

Example:

createfilter -f D_IP -v 10.123.45.1 -e not equals -a drop -m L4_CON -i 0   

Usage: 
  enablefilter [-help] 
 
  -help     Display this help.

Note: TI recommends enable all filters at once, since enabling each filter at a time, could cause undefined behaviour in case we’re enabling combined filters / filters with parent.

Once enablefilter command has successfully completed, All filters are operational.

Example:

user@CC3220:enablefilter

Usage: 
  disablefilter [-help] 
 
  -help     Display this help.

Note: TI recommends disable all filters at once, since disabling each filter at a time, could cause undefined behaviour in case we’re disabling combined filters / filters with parent.

Once disablefilter command has successfully completed, All filters are shut.

Example:

user@CC3220:disablefilter

Usage: 
  deletefilter [-help] 
 
  -help     Display this help.

Note: TI recommends delete all filters at once, since deleting each filter at a time, could cause undefined behaviour in case we’re deleting combined filters / filters with parent.

Once deletefilter command has successfully completed, All filters are deleted.

Example:

user@CC3220:deletefilter

Usage: 
        enablewowlan[-help] [-v <"pattern value">] [-u <Action ID>] [-i <pattern offset>]
        
    -v      Pattern Value used by the Filter (string, of less than 16 characters)
    -u      WoWLAN filter Action ID, should be less than 255
    -i      Pattern offset in payload default 0
    -help   Display this help

Example:

enablewowlan -v Wake_up_str -u 5 -i 0

  1. SL_WLAN_EVENT_P2P_DEVFOUND: This event signals that a remote peer to peer device has been found. From this point on, the device is waiting for negotiation request. Please Refer to SimpleLinkWlanEventHandler() implemented
    in network_terminal.c for more info.

  2. SL_WLAN_EVENT_P2P_REQUEST : This event signals that the device got negotiation request. Here we save the remote p2p device SSID, in order to manually connect with it later.
    Please refer to SimpleLinkNetAppEventHandler() implemented in network_terminal.c for more info.

  3. SL_WLAN_EVENT_P2P_CONNECT : This event signify that device has successfully connected to a remote peer to peer device. At this event handler, we print the remote’s BSSID. Please Refer to SimpleLinkWlanEventHandler() implemented in network_terminal.c for more info.

  4. SL_DEVICE_EVENT_DROPPED_NETAPP_IPACQUIRED : This event signals that the device has an IP address.
    Event type is the same as in STA/AP mode. Also, this event print useful information
    such as the leased IP, and the designated gateway. Please refer to SimpleLinkNetAppEventHandler()
    implemented in network_terminal.c for more info.

  5. SL_WLAN_EVENT_P2P_DISCONNECT : Once the remote p2p device disconnects, this event is triggered.
    Please Refer to SimpleLinkWlanEventHandler() implemented in network_terminal.c for more info.

Note: At any point in the p2p connection process, user can type the command ‘p2pstop’ to exist p2p mode.

Usage: 
  p2pstart [-help] 
 
  -help     Show Help regarding the p2pstart command.

Example:

user@CC3220:p2pstart
Starting NWP in P2P role..

Device name: mysimplelink

User can stop the P2P connection process by typing 'p2pstop' command.

Socket commands:

This command allows user to open a udp or tcp sockets, and send packets in various configurations, which include the following:

  1. Run as server or client.
  2. Protocol: tcp or udp.
  3. Port number.
  4. Blocking vs. Non-blocking option.
  5. Number of packet to transmit.
  6. Use Ipv6 rather than Ipv4 (Default).
Usage:
        send [-help] [-c <server ip address>] [-u] [-p <port number>]  [-nb] [-n <number of packets>]  
        send [-help] [-s] [-u] [-p <port number>]  [-V] [-nb] [-n <number of packets>]
        
        -c      Run in client mode and connect to mentioned server - IP should be in '.' format for ipv4 and in ':' for ipv6
        -s      Run in server mode - (Note that for client, a server ip address is required.)
        -u      Use UDP rather than TCP
        -p      Port number to send/receive data (Default is 5001)
        -nb     Create non-blocking socket rather than blocking
        -n      Number of packets to transmit (Default is 1000)
        -V      Use IPv6 rather than IPv4

Once all packets have been sent, application would return to main menu.

Note: Make sure the server side is listening for incoming connections before sending packets as client.

Example:

send -c 10.123.45.6 -p 5050 -n 2000

This command allows user to open a udp or tcp sockets and receive packets in various configurations, which include the following:

  1. Run as server or client mode.
  2. Protocol: tcp or udp.
  3. Port number.
  4. Blocking vs. Non-blocking option.
  5. Number of packet to transmit.
  6. Use Ipv6 rather than Ipv4 (Default).
Usage:
        recv [-help] [-c <server ip address>] [-u] [-p <port number>]  [-nb] [-n <number of packets>]  
        recv [-help] [-s] [-u] [-p <port number>]  [-V] [-nb] [-n <number of packets>]
        
        -c      Run in client mode and connect to mentioned server - IP should be in '.' format for ipv4 and in ':' for ipv6
        -s      Run in server mode - (Note that for client, a server ip address is required.)
        -u      Use UDP rather than TCP
        -p      Port number to send/receive data (Default is 5001)
        -nb     Create non-blocking socket rather than blocking
        -n      Number of packets to transmit (Default is 1000)
        -V      Use IPv6 rather than IPv4

Once all packets have been received, application would exit.

Example:

recv -s -u -n 1000 

Netapp commands:

Usage: 
  ping [-help] [-h <host name or ip>] [-c <Num of packets>]  
  [-s <data size>] [-i <delay interval>] [-t <timeout>]
  
    -h      Host name or ip (In IPv4 '.' format)
    -c      Send <Num of packets> number of ECHO_REQUEST packets (Default is 10)
    -s      Specify the number of data bytes to be sent (Default is 56)
    -i      Wait <delay interval> time (in seconds) between sending each packet (Default is 1)
    -t      Specify a timeout (in seconds) before ping exits, (default is 3 seconds per ping packet)

Note: Application is blocked until ping timeout or ping ends successfully.

Example:

ping -h www.ti.com -c 30 -s 112 -t 10

Note: mDNS services are not persistent, i.e any advertised service would be lost after NWP reset, with one exception: the internal http server of the NWP.

Example:

user@CC3220:mdnsadvertise -n PC1 -so tcp -st ipp -ttl 3000 -p 5001
Setting service name: PC1
[mDNS advertise] : MDNS service started successfully
[mDNS advertise] : MDNS service name PC1._ipp._tcp.local registered successfully.

  1. One-Shot: The NWP issues one query, wait for the first result that comes up and exists.
  2. Continues: The NWP issue several queries, and store these results in the NWP cache.
Usage: 
    mdnsquery [-help] [-n <Device name>] [-st <Service type>] [-so <Service over>] [-o <Oneshot>]
   
    -n      Device name for query, should be character string (optional)
    -st     Service Type for query, should be character string (mandatory)
    -so     Set L4 protocol over which the service operates, should be character string (mandatory)
    -o      OneShot/Continues (Oneshot = [YES, NO (default)])
    -help   Display this help

User can query for a partial service name, or full. Meaning, query can be issued with partial service name.
For example,

mdnsquery -st ipp -so tcp

would query for any server who offers internet printer protocol service over tcp, whereas

mdnsquery -n PC1 -st ipp -so tcp

would query for the specific server named “PC1” who offers such service. On successful response, the service name and server’s port found would be printed to the screen.

Transceiver commands:

In order to start the device in transceiver mode, user can type the command: ‘radiotool’ to the UART terminal.
radiotool command lets the user run several radio related tests, for both RX and TX operations.

Once NWP has entered the device to transceiver mode, the following menu is printed:

     ------------------------------------------------
                   RadioTool Option Menu
      ------------------------------------------------
        |            Rx task options.            |
        |            Tx task options.            |
        |            Exit radio tool.            |
      ------------------------------------------------
        ------------------------------------------------
                     RX Task Option Menu
        ------------------------------------------------
        Choose Rx channel: [1,13]
        Enter Rx duration (in mSec units): [1,UINT32_MAX]
        Show Rx statistics? [Yes, No]

Once all Rx task parameters have been provided, the application is waiting for a key press, to give the user time to set up radio testing equipment:

Ready to start RX, press any key to continue...

If Rx statistics are configured, once RX task is finished a rate and RSSI histogram for received packets would appear:

*********************************Rx Statistics**********************************
Received Packets - 226
Average Rssi for management: -70  Average Rssi for other packets: -77
    -----------------------   RSSI Histogram   -----------------------
-40dBm to -87dBm (below and above RSSI will appear in the first and last cells]
           10   20   30   40   50   60   70   80   90   100
         |----+----+----+----+----+----+----+----+----+----|
  >-40dBm                                                  (0.00%)
         |----+----+----+----+----+----+----+----+----+----|
  -49dBm *                                                 (3.54%)
         |----+----+----+----+----+----+----+----+----+----|
  -58dBm *****                                             (11.06%)
         |----+----+----+----+----+----+----+----+----+----|
  -68dBm ***************************                       (55.75%)
         |----+----+----+----+----+----+----+----+----+----|
  -77dBm ***                                               (6.19%)
         |----+----+----+----+----+----+----+----+----+----|
<-87dBm  ***********                                       (23.45%)
         |----+----+----+----+----+----+----+----+----+----|
              10   20   30   40   50   60   70   80   90   100

    -----------------------   Rate Histogram   -----------------------

           10   20   30   40   50   60   70   80   90   100
         |----+----+----+----+----+----+----+----+----+----|
0        *************************************************  (99.56%)
         |----+----+----+----+----+----+----+----+----+----|
1                                                            (0.00%)
         |----+----+----+----+----+----+----+----+----+----|
2                                                            (0.00%)
         |----+----+----+----+----+----+----+----+----+----|
3                                                            (0.00%)
         |----+----+----+----+----+----+----+----+----+----|
4                                                            (0.44%)
         |----+----+----+----+----+----+----+----+----+----|
5                                                            (0.00%)
         |----+----+----+----+----+----+----+----+----+----|
6                                                            (0.00%)
         |----+----+----+----+----+----+----+----+----+----|
7                                                            (0.00%)
         |----+----+----+----+----+----+----+----+----+----|
8                                                            (0.00%)
         |----+----+----+----+----+----+----+----+----+----|
9                                                            (0.00%)
         |----+----+----+----+----+----+----+----+----+----|
10                                                           (0.00%)
         |----+----+----+----+----+----+----+----+----+----|
11                                                           (0.00%)
         |----+----+----+----+----+----+----+----+----+----|
12                                                           (0.00%)
         |----+----+----+----+----+----+----+----+----+----|
13                                                           (0.00%)
         |----+----+----+----+----+----+----+----+----+----|
14                                                           (0.00%)
         |----+----+----+----+----+----+----+----+----+----|
15                                                           (0.00%)
         |----+----+----+----+----+----+----+----+----+----|
16                                                           (0.00%)
         |----+----+----+----+----+----+----+----+----+----|
17                                                           (0.00%)
         |----+----+----+----+----+----+----+----+----+----|
18                                                           (0.00%)
         |----+----+----+----+----+----+----+----+----+----|
19                                                           (0.00%)
         |----+----+----+----+----+----+----+----+----+----|
              10   20   30   40   50   60   70   80   90   100
                     The data was sampled during 162109mSec
*******************************End Rx Statistics********************************
 Press any key to continue...

This mode expects the following parameters:

1. Destination MAC address that would appear in generated packet's header.
2. Packet size.
3. Tx channel.
4. Packet's payload pattern. Can be either:
    * All zeros.
    * All ones.
    * Incremental numbers.
    * Decremental numbers.
5. Tx duration.

Once all the above are provided to the application, user is prompt to enter PHY parameters.
User can choose between enter the parameters, or use defaults. for more information, refer to Radio parameters section in this document.

**Packetized Mode**: Transmitting fixed amount of packets, generated by Host processor.  

Each packet is sent one at a time from the Host processor to the NWP.

This mode expects the following parameters:

1. Destination MAC address that would appear in generated packet's header.
2. Packet size.
3. Tx channel.
4. Packet's payload pattern. Can be either:
    * All zeros.
    * All ones.
    * Incremental numbers.
    * Decremental numbers.
5. Amount of packets to transmit.

Once all the above are provided to the application, user is prompt to enter PHY parameters.
User can choose between enter the parameters, or use defaults. for more information, refer to Radio parameters section in this document.

**Carrier Wave (CW) Mode**: In this mode the device transmits an un-modulated RF tone. 
Choose Tx channel: [1,13] - This option determine the center frequency for the Carrier wave.
Tone offset: Specify desired Tone offset from center frequency. Value is in multiples of 312.5kHz In range: [-25,25].

Tone offset option can be explained by the following rule: for a tone offset of N, (N is a whole number in range [-25, 25] )

Carrier frequency = center frequency + N*312.5kHz.

Enter TX duration: [1,UINT_MAX] (in mSec)

Now, user is presented with key press screen to start the test. When the Tx duration time elapsed, application returns to the main radio tool option menu.


Note: override is recommended if the wireless environment is too congested in order to have a reliable periodic transmission.