/**
*  \file lwiplib.c
*
*  \brief lwip related initializations
*/
/*
 * Copyright (c) 2001-2004 Swedish Institute of Computer Science.
 * All rights reserved.
 *
 * Redistribution and use in source and binary forms, with or without modification,
 * are permitted provided that the following conditions are met:
 *
 * 1. Redistributions of source code must retain the above copyright notice,
 *    this list of conditions and the following disclaimer.
 * 2. Redistributions in binary form must reproduce the above copyright notice,
 *    this list of conditions and the following disclaimer in the documentation
 *    and/or other materials provided with the distribution.
 * 3. The name of the author may not be used to endorse or promote products
 *    derived from this software without specific prior written permission.
 *
 * THIS SOFTWARE IS PROVIDED BY THE AUTHOR ``AS IS'' AND ANY EXPRESS OR IMPLIED
 * WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES OF
 * MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT
 * SHALL THE AUTHOR BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
 * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT
 * OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS
 * INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN
 * CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING
 * IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY
 * OF SUCH DAMAGE.
 *
 * This file is part of the lwIP TCP/IP stack.
 *
 * Author: Adam Dunkels <adam@sics.se>
 *
*/

/*
** Copyright (C) 2010 Texas Instruments Incorporated - http://www.ti.com/
** ALL RIGHTS RESERVED
*/

/*
** lwIP Compile Time Options for SitaraWare.
*/
#include "lwiplib.h"

/*
** lwIP high-level API/Stack/IPV4/SNMP/Network Interface/PPP codes
*/
#include "src/api/api_lib.c"
#include "src/api/api_msg.c"
#include "src/api/err.c"
#include "src/api/netbuf.c"
#include "src/api/netdb.c"
#include "src/api/netifapi.c"
#include "src/api/tcpip.c"
#include "src/api/sockets.c"

#include "src/core/dhcp.c"
#include "src/core/dns.c"
#include "src/core/init.c"
#include "src/core/mem.c"
#include "src/core/memp.c"
#include "src/core/netif.c"
#include "src/core/pbuf.c"
#include "src/core/raw.c"
#include "src/core/stats.c"
#include "src/core/sys.c"
#include "src/core/tcp.c"
#include "src/core/tcp_in.c"
#include "src/core/tcp_out.c"
#include "src/core/udp.c"

#include "src/core/ipv4/autoip.c"
#include "src/core/ipv4/icmp.c"
#include "src/core/ipv4/igmp.c"
#include "src/core/ipv4/inet.c"
#include "src/core/ipv4/inet_chksum.c"
#include "src/core/ipv4/ip.c"
#include "src/core/ipv4/ip_addr.c"
#include "src/core/ipv4/ip_frag.c"

#include "src/core/snmp/asn1_dec.c"
#include "src/core/snmp/asn1_enc.c"
#include "src/core/snmp/mib2.c"
#include "src/core/snmp/mib_structs.c"
#include "src/core/snmp/msg_in.c"
#include "src/core/snmp/msg_out.c"

#include "src/netif/etharp.c"
#include "src/netif/loopif.c"

#include "src/netif/ppp/auth.c"
#include "src/netif/ppp/chap.c"
#include "src/netif/ppp/chpms.c"
#include "src/netif/ppp/fsm.c"
#include "src/netif/ppp/ipcp.c"
#include "src/netif/ppp/lcp.c"
#include "src/netif/ppp/magic.c"
#include "src/netif/ppp/md5.c"
#include "src/netif/ppp/pap.c"
#include "src/netif/ppp/ppp.c"
#include "src/netif/ppp/ppp_oe.c"
#include "src/netif/ppp/randm.c"
#include "src/netif/ppp/vj.c"

/*
** Sitara-specific lwIP interface/porting layer code.
*/
#include "ports/am1808/perf.c"
#include "ports/am1808/sys_arch.c"
#include "ports/am1808/netif/sitaraif.c"
#include "locator.c"

/******************************************************************************
**                       INTERNAL VARIABLE DEFINITIONS
******************************************************************************/
/*
** The lwIP network interface structure for the Sitara Ethernet MAC.
*/
static struct netif sitaraNetIF[MAX_EMAC_INSTANCE];

/******************************************************************************
**                          FUNCTION DEFINITIONS
******************************************************************************/
/**
 *
 * \brief Initializes the lwIP TCP/IP stack.
 *
 * \param instNum  The instance index of the EMAC module
 * \param macArray Pointer to the MAC Address
 * \param ipAddr   The IP address to be used 
 * \param netMask  The network mask to be used 
 * \param gwAddr   The Gateway address to be used 
 * \param ipMode   The IP Address Mode.
 *        ipMode can take the following values\n
 *             IPADDR_USE_STATIC - force static IP addressing to be used \n
 *             IPADDR_USE_DHCP - force DHCP with fallback to Link Local \n
 *             IPADDR_USE_AUTOIP - force  Link Local only
 *
 * This function performs initialization of the lwIP TCP/IP stack for the
 * Sitara EMAC, including DHCP and/or AutoIP, as configured.
 *
 * \return IP Address.
*/
unsigned int lwIPInit(unsigned int instNum, unsigned char *macArray,
                      unsigned int ipAddr, unsigned int netMask, 
                      unsigned int gwAddr, unsigned int ipMode)
{
    struct ip_addr ip_addr;
    struct ip_addr net_mask;
    struct ip_addr gw_addr;
    volatile unsigned char *state;
    unsigned int *ipAddrPtr;
    volatile unsigned int cnt = 0x3FFFFFFF;
 
    lwip_init();

    /* Setup the network address values. */
    if(ipMode == IPADDR_USE_STATIC)
    {
        ip_addr.addr = htonl(ipAddr);
        net_mask.addr = htonl(netMask);
        gw_addr.addr = htonl(gwAddr);
    }
   
    else
    {
        ip_addr.addr = 0;
        net_mask.addr = 0;
        gw_addr.addr = 0;
    }

    sitaraif_macaddrset(instNum, macArray);

    /*
    ** Create, configure and add the Ethernet controller interface with
    ** default settings.  ip_input should be used to send packets directly to
    ** the stack. The lwIP will internaly call the sitaraif_init function. 
    */
    if(NULL ==
       netif_add(&sitaraNetIF[instNum], &ip_addr, &net_mask, &gw_addr, &instNum, 
              sitaraif_init, ip_input))
    {
        return 0;
    };

    netif_set_default(&sitaraNetIF[instNum]);

    /* Start DHCP, if enabled. */
#if LWIP_DHCP
    if(ipMode == IPADDR_USE_DHCP)
    {
        dhcp_start(&sitaraNetIF[instNum]);
    }
#endif

    /* Start AutoIP, if enabled and DHCP is not. */
#if LWIP_AUTOIP
    if(ipMode == IPADDR_USE_AUTOIP)
    {
        autoip_start(&sitaraNetIF[instNum]);
    }
#endif

    if(ipMode != IPADDR_USE_STATIC) 
    {
        /* wait till the dynamic IP address is properly assigned */
        state = &(sitaraNetIF[instNum].dhcp->state);
      
        while((*state != DHCP_BOUND) && (cnt--));

        if(0 == cnt)
        {
            return 0;
        }
    }
    
    else
    {
       /* Bring the interface up */
       netif_set_up(&sitaraNetIF[instNum]);
    }
  
    ipAddrPtr = (unsigned int*)&(sitaraNetIF[instNum].ip_addr);

    return (*ipAddrPtr);
}

/*
 * \brief   Checks if the ethernet link is up
 *
 * \param   instNum  The instance number of EMAC module 
 *
 * \return  Interface status.
*/
unsigned int lwIPNetIfStatusGet(unsigned int instNum) 
{
    
    return (sitaraif_netif_status(&sitaraNetIF[instNum]));
}

/*
 * \brief   Checks if the ethernet link is up
 *
 * \param   instNum  The instance number of EMAC module 
 *
 * \return  The link status.
*/
unsigned int lwIPLinkStatusGet(unsigned int instNum) 
{
    return (sitaraif_link_status(&sitaraNetIF[instNum]));     
}

/**
 * \brief   Interrupt handler for Receive Interrupt. Directly calls the
 *          sitara interface receive interrupt handler.
 *
 * \param   instNum  The instance number of EMAC module for which receive 
 *                   interrupt happened
 *
 * \return  None.
*/
void lwIPRxIntHandler(unsigned int instNum) 
{
    sitaraif_rx_inthandler(&sitaraNetIF[instNum]);
}

/**
 * \brief   Interrupt handler for Transmit Interrupt. Directly calls the 
 *          sitara interface transmit interrupt handler.
 *
 * \param   instNum  The instance number of EMAC module for which transmit
 *                   interrupt happened
 *
 * \return  None.
*/
void lwIPTxIntHandler(unsigned int instNum)
{
    sitaraif_tx_inthandler(&sitaraNetIF[instNum]);
}

/***************************** End Of File ***********************************/