diff --git a/drivers/mtd/nand/raw/omap_gpmc.c b/drivers/mtd/nand/raw/omap_gpmc.c index f499d8611f..ea2dcbe1b9 100644 --- a/drivers/mtd/nand/raw/omap_gpmc.c +++ b/drivers/mtd/nand/raw/omap_gpmc.c @@ -284,7 +284,7 @@ static void __maybe_unused omap_enable_hwecc_bch(struct mtd_info *mtd, break; case OMAP_ECC_BCH8_CODE_HW: bch_type = 1; - nsectors = chip->ecc.steps; + nsectors = 1; if (mode == NAND_ECC_READ) { wr_mode = BCH_WRAPMODE_1; ecc_size0 = BCH8R_ECC_SIZE0; @@ -297,7 +297,7 @@ static void __maybe_unused omap_enable_hwecc_bch(struct mtd_info *mtd, break; case OMAP_ECC_BCH16_CODE_HW: bch_type = 0x2; - nsectors = chip->ecc.steps; + nsectors = 1; if (mode == NAND_ECC_READ) { wr_mode = 0x01; ecc_size0 = 52; /* ECC bits in nibbles per sector */ @@ -337,17 +337,16 @@ static void __maybe_unused omap_enable_hwecc_bch(struct mtd_info *mtd, #if defined(CONFIG_BCH) || defined(CONFIG_NAND_OMAP_ELM) /** - * _omap_calculate_ecc_bch - Generate BCH ECC bytes for one sector + * omap_calculate_ecc_bch - Generate BCH ECC bytes for one sector * @mtd: MTD device structure * @dat: The pointer to data on which ecc is computed * @ecc_code: The ecc_code buffer - * @sector: The sector number (for a multi sector page) * * Support calculating of BCH4/8/16 ECC vectors for one sector * within a page. Sector number is in @sector. */ -static int _omap_calculate_ecc_bch(struct mtd_info *mtd, const u8 *dat, - u8 *ecc_code, int sector) +static int omap_calculate_ecc_bch(struct mtd_info *mtd, const u8 *dat, + u8 *ecc_code) { struct nand_chip *chip = mtd_to_nand(mtd); struct omap_nand_info *info = nand_get_controller_data(chip); @@ -360,7 +359,7 @@ static int _omap_calculate_ecc_bch(struct mtd_info *mtd, const u8 *dat, case OMAP_ECC_BCH8_CODE_HW_DETECTION_SW: #endif case OMAP_ECC_BCH8_CODE_HW: - ptr = &gpmc_cfg->bch_result_0_3[sector].bch_result_x[3]; + ptr = &gpmc_cfg->bch_result_0_3[0].bch_result_x[3]; val = readl(ptr); ecc_code[i++] = (val >> 0) & 0xFF; ptr--; @@ -375,21 +374,21 @@ static int _omap_calculate_ecc_bch(struct mtd_info *mtd, const u8 *dat, break; case OMAP_ECC_BCH16_CODE_HW: - val = readl(&gpmc_cfg->bch_result_4_6[sector].bch_result_x[2]); + val = readl(&gpmc_cfg->bch_result_4_6[0].bch_result_x[2]); ecc_code[i++] = (val >> 8) & 0xFF; ecc_code[i++] = (val >> 0) & 0xFF; - val = readl(&gpmc_cfg->bch_result_4_6[sector].bch_result_x[1]); + val = readl(&gpmc_cfg->bch_result_4_6[0].bch_result_x[1]); ecc_code[i++] = (val >> 24) & 0xFF; ecc_code[i++] = (val >> 16) & 0xFF; ecc_code[i++] = (val >> 8) & 0xFF; ecc_code[i++] = (val >> 0) & 0xFF; - val = readl(&gpmc_cfg->bch_result_4_6[sector].bch_result_x[0]); + val = readl(&gpmc_cfg->bch_result_4_6[0].bch_result_x[0]); ecc_code[i++] = (val >> 24) & 0xFF; ecc_code[i++] = (val >> 16) & 0xFF; ecc_code[i++] = (val >> 8) & 0xFF; ecc_code[i++] = (val >> 0) & 0xFF; for (j = 3; j >= 0; j--) { - val = readl(&gpmc_cfg->bch_result_0_3[sector].bch_result_x[j] + val = readl(&gpmc_cfg->bch_result_0_3[0].bch_result_x[j] ); ecc_code[i++] = (val >> 24) & 0xFF; ecc_code[i++] = (val >> 16) & 0xFF; @@ -423,21 +422,6 @@ static int _omap_calculate_ecc_bch(struct mtd_info *mtd, const u8 *dat, return 0; } -/** - * omap_calculate_ecc_bch - ECC generator for 1 sector - * @mtd: MTD device structure - * @dat: The pointer to data on which ecc is computed - * @ecc_code: The ecc_code buffer - * - * Support calculating of BCH4/8/16 ECC vectors for one sector. This is used - * when SW based correction is required as ECC is required for one sector - * at a time. - */ -static int omap_calculate_ecc_bch(struct mtd_info *mtd, - const u_char *dat, u_char *ecc_calc) -{ - return _omap_calculate_ecc_bch(mtd, dat, ecc_calc, 0); -} #endif /* CONFIG_BCH || CONFIG_NAND_OMAP_ELM */ static inline void omap_nand_read_buf(struct mtd_info *mtd, uint8_t *buf, @@ -591,33 +575,6 @@ static void omap_nand_read_prefetch(struct mtd_info *mtd, uint8_t *buf, int len, #ifdef CONFIG_NAND_OMAP_ELM -/** - * omap_calculate_ecc_bch_multi - Generate ECC for multiple sectors - * @mtd: MTD device structure - * @dat: The pointer to data on which ecc is computed - * @ecc_code: The ecc_code buffer - * - * Support calculating of BCH4/8/16 ecc vectors for the entire page in one go. - */ -static int omap_calculate_ecc_bch_multi(struct mtd_info *mtd, - const u_char *dat, u_char *ecc_calc) -{ - struct nand_chip *chip = mtd_to_nand(mtd); - int eccbytes = chip->ecc.bytes; - unsigned long nsectors; - int i, ret; - - nsectors = ((readl(&gpmc_cfg->ecc_config) >> 4) & 0x7) + 1; - for (i = 0; i < nsectors; i++) { - ret = _omap_calculate_ecc_bch(mtd, dat, ecc_calc, i); - if (ret) - return ret; - - ecc_calc += eccbytes; - } - - return 0; -} /* * omap_reverse_list - re-orders list elements in reverse order [internal] @@ -744,32 +701,38 @@ static int omap_read_page_bch(struct mtd_info *mtd, struct nand_chip *chip, { int i, eccsize = chip->ecc.size; int eccbytes = chip->ecc.bytes; - int ecctotal = chip->ecc.total; int eccsteps = chip->ecc.steps; uint8_t *p = buf; uint8_t *ecc_calc = chip->buffers->ecccalc; uint8_t *ecc_code = chip->buffers->ecccode; uint32_t *eccpos = chip->ecc.layout->eccpos; uint8_t *oob = chip->oob_poi; + uint32_t data_pos; uint32_t oob_pos; + data_pos = 0; /* oob area start */ oob_pos = (eccsize * eccsteps) + chip->ecc.layout->eccpos[0]; oob += chip->ecc.layout->eccpos[0]; - /* Enable ECC engine */ - chip->ecc.hwctl(mtd, NAND_ECC_READ); + for (i = 0; eccsteps; eccsteps--, i += eccbytes, p += eccsize, + oob += eccbytes) { + /* Enable ECC engine */ + chip->ecc.hwctl(mtd, NAND_ECC_READ); - /* read entire page */ - chip->cmdfunc(mtd, NAND_CMD_RNDOUT, 0, -1); - chip->read_buf(mtd, buf, mtd->writesize, false); + /* read data */ + chip->cmdfunc(mtd, NAND_CMD_RNDOUT, data_pos, -1); + chip->read_buf(mtd, p, eccsize, false); - /* read all ecc bytes from oob area */ - chip->cmdfunc(mtd, NAND_CMD_RNDOUT, oob_pos, -1); - chip->read_buf(mtd, oob, ecctotal, false); + /* read respective ecc from oob area */ + chip->cmdfunc(mtd, NAND_CMD_RNDOUT, oob_pos, -1); + chip->read_buf(mtd, oob, eccbytes, false); + /* read syndrome */ + chip->ecc.calculate(mtd, p, &ecc_calc[i]); - /* Calculate ecc bytes */ - omap_calculate_ecc_bch_multi(mtd, buf, ecc_calc); + data_pos += eccsize; + oob_pos += eccbytes; + } for (i = 0; i < chip->ecc.total; i++) ecc_code[i] = chip->oob_poi[eccpos[i]]; @@ -937,6 +900,7 @@ static int omap_select_ecc_scheme(struct nand_chip *nand, nand->ecc.hwctl = omap_enable_hwecc_bch; nand->ecc.correct = omap_correct_data_bch_sw; nand->ecc.calculate = omap_calculate_ecc_bch; + nand->ecc.steps = eccsteps; /* define ecc-layout */ ecclayout->eccbytes = nand->ecc.bytes * eccsteps; ecclayout->eccpos[0] = BADBLOCK_MARKER_LENGTH; @@ -979,6 +943,7 @@ static int omap_select_ecc_scheme(struct nand_chip *nand, nand->ecc.correct = omap_correct_data_bch; nand->ecc.calculate = omap_calculate_ecc_bch; nand->ecc.read_page = omap_read_page_bch; + nand->ecc.steps = eccsteps; /* define ecc-layout */ ecclayout->eccbytes = nand->ecc.bytes * eccsteps; for (i = 0; i < ecclayout->eccbytes; i++) @@ -1012,6 +977,7 @@ static int omap_select_ecc_scheme(struct nand_chip *nand, nand->ecc.correct = omap_correct_data_bch; nand->ecc.calculate = omap_calculate_ecc_bch; nand->ecc.read_page = omap_read_page_bch; + nand->ecc.steps = eccsteps; /* define ecc-layout */ ecclayout->eccbytes = nand->ecc.bytes * eccsteps; for (i = 0; i < ecclayout->eccbytes; i++)