U-Boot SPL 2023.04-g24098ea90d (Jul 06 2023 - 12:59:40 +0000) SYSFW ABI: 3.1 (firmware rev 0x0009 '9.0.5--v09.00.05 (Kool Koala)') SPL initial stack usage: 13376 bytes Trying to boot from MMC2 Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Starting ATF on ARM64 core... NOTICE: BL31: v2.8(release):v2.8-226-g2fcd408bb3-dirty NOTICE: BL31: Built : 00:42:57, Jan 13 2023 U-Boot SPL 2023.04-g24098ea90d (Jul 06 2023 - 12:59:40 +0000) SYSFW ABI: 3.1 (firmware rev 0x0009 '9.0.5--v09.00.05 (Kool Koala)') SPL initial stack usage: 1856 bytes Trying to boot from MMC2 Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted !12Error: no valid bmp image at %lx SoC: AM62X SR1.0 GP Model: Texas Instruments AM625 SK EEPROM not available at 80, trying to read at 81 Reading on-board EEPROM at 0x51 failed -1 DRAM: 2 GiB Core: 70 devices, 30 uclasses, devicetree: separate MMC: mmc@fa10000: 0, mmc@fa00000: 1 Loading Environment from nowhere... OK In: serial Out: serial Err: serial EEPROM not available at 80, trying to read at 81 Reading on-board EEPROM at 0x51 failed -1 Net: eth0: ethernet@8000000port@1 Hit any key to stop autoboot: 0 switch to partitions #0, OK mmc1 is current device SD/MMC found on device 1 Failed to load 'boot.scr' 574 bytes read in 14 ms (40 KiB/s) Loaded env from uEnv.txt Importing environment from mmc1 ... ## Error: "main_cpsw0_qsgmii_phyinit" not defined 21064192 bytes read in 874 ms (23 MiB/s) 58770 bytes read in 19 ms (2.9 MiB/s) Working FDT set to 88000000 ## Flattened Device Tree blob at 88000000 Booting using the fdt blob at 0x88000000 Working FDT set to 88000000 ERROR: reserving fdt memory region failed (addr=ff700000 size=8ca000 flags=4) Loading Device Tree to 000000008feee000, end 000000008fffffff ... OK Working FDT set to 8feee000 System time before build time, advancing clock. systemd 250.5+ running in system mode (+PAM -AUDIT -SELINUX -APPARMOR +IMA -SMACK +SECCOMP -GCRYPT -GNUTLS -OPENSSL +ACL +BLKID -CURL -ELFUTILS -FIDO2 -IDN2 -IDN -IPTC +KMOD -LIBCRYPTSETUP +LIBFDISK -PCRE2 -PWQUALITY -P11KIT -QRENCODE -BZIP2 -LZ4 -XZ -ZLIB +ZSTD -BPF_FRAMEWORK +XKBCOMMON +UTMP +SYSVINIT default-hierarchy=hybrid) Detected architecture arm64. Hostname set to . /etc/systemd/system/sync-clocks.service:11: Standard output type syslog is obsolete, automatically updating to journal. Please update your unit file, and consider removing the setting altogether. Queued start job for default target Multi-User System. modprobe@configfs.service: Deactivated successfully. modprobe@drm.service: Deactivated successfully. modprobe@fuse.service: Deactivated successfully. psplash-start.service: Main process exited, code=exited, status=255/EXCEPTION psplash-start.service: Failed with result 'exit-code'. _____ _____ _ _ | _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_ | | _| .'| . | . | | __| _| . | | | -_| _| _| |__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_| |___| |___| Arago Project am62xx-evm - Arago 2023.04 am62xx-evm - am62xx-evm login: