root@j7-evm:/opt/vision_apps# ./vx_klk_isp_sith.out APP: Init ... !!! MEM: Init ... !!! MEM: Initialized DMA HEAP (fd=4) !!! MEM: Init ... Done !!! IPC: Init ... !!! IPC: Init ... Done !!! REMOTE_SERVICE: Init ... !!! REMOTE_SERVICE: Init ... Done !!! APP: Init ... Done !!! 58.916758 s: VX_ZONE_INIT:Enabled 58.916782 s: VX_ZONE_ERROR:Enabled 58.916795 s: VX_ZONE_WARNING:Enabled 58.917336 s: VX_ZONE_INIT:[tivxInit:71] Initialization Done !!! 58.917499 s: VX_ZONE_INIT:[tivxHostInit:48] Initialization Done for HOST !!! 58.918147 s: VX_ZONE_ERROR:[tivxAddKernelVpacCustomViss:567] tivxAddKernelTarget VPAC_CUSTOM_VISS ready //VX_PRINT 58.918161 s: VX_ZONE_ERROR:[tivxAddKernelVpacCustomCustom:246] tivxAddKernelTarget VPAC_CUSTOM ready //VX_PRINT 58.975125 s: VX_ZONE_WARNING:[tivxAddKernelVpacCustomVissValidate:85] tivxAddKernelVpacCustomVissValidate START 58.975143 s: VX_ZONE_WARNING:[tivxAddKernelVpacCustomVissValidate:439] tivxAddKernelVpacCustomVissValidate END 58.976150 s: VX_ZONE_ERROR:[ownContextSendCmd:782] Command ack message returned failure cmd_status: -7 58.976158 s: VX_ZONE_ERROR:[ownContextSendCmd:818] tivxEventWait() failed. 58.976164 s: VX_ZONE_ERROR:[ownNodeKernelInit:526] Target kernel, TIVX_CMD_NODE_CREATE failed 58.976169 s: VX_ZONE_ERROR:[ownNodeKernelInit:527] Please be sure the target callbacks have been registered for this core 58.976174 s: VX_ZONE_ERROR:[ownNodeKernelInit:528] If the target callbacks have been registered, please ensure no errors are occurring within the create callback of this kernel 58.976181 s: VX_ZONE_ERROR:[ownGraphNodeKernelInit:583] kernel init for node 0, kernel com.ti.hwa.vpac_custom ... failed !!! 58.976187 s: VX_ZONE_ERROR:[vxVerifyGraph:2014] Node kernel init failed 58.976201 s: VX_ZONE_ERROR:[vxVerifyGraph:2068] Graph verify failed 58.976460 s: VX_ZONE_WARNING:[tivxAddKernelVpacCustomVissValidate:85] tivxAddKernelVpacCustomVissValidate START 58.976477 s: VX_ZONE_WARNING:[tivxAddKernelVpacCustomVissValidate:439] tivxAddKernelVpacCustomVissValidate END 58.976560 s: VX_ZONE_WARNING:[tivxAddKernelVpacCustomVissInitialize:448] tivxAddKernelVpacCustomVissInitialize START 58.976565 s: VX_ZONE_WARNING:[tivxAddKernelVpacCustomVissInitialize:457] tivxAddKernelVpacCustomVissInitialize END 58.977237 s: VX_ZONE_ERROR:[ownContextSendCmd:782] Command ack message returned failure cmd_status: -7 58.977244 s: VX_ZONE_ERROR:[ownContextSendCmd:818] tivxEventWait() failed. 58.977249 s: VX_ZONE_ERROR:[ownNodeKernelInit:526] Target kernel, TIVX_CMD_NODE_CREATE failed 58.977254 s: VX_ZONE_ERROR:[ownNodeKernelInit:527] Please be sure the target callbacks have been registered for this core 58.977259 s: VX_ZONE_ERROR:[ownNodeKernelInit:528] If the target callbacks have been registered, please ensure no errors are occurring within the create callback of this kernel 58.977265 s: VX_ZONE_ERROR:[ownGraphNodeKernelInit:583] kernel init for node 0, kernel com.ti.hwa.vpac_custom_viss ... failed !!! 58.977271 s: VX_ZONE_ERROR:[vxVerifyGraph:2014] Node kernel init failed 58.977285 s: VX_ZONE_ERROR:[vxVerifyGraph:2068] Graph verify failed 58.977373 s: VX_ZONE_ERROR:[ownGraphScheduleGraphWrapper:807] graph is not in a state required to be scheduled 58.977379 s: VX_ZONE_ERROR:[vxProcessGraph:742] schedule graph failed 58.977383 s: VX_ZONE_ERROR:[vxProcessGraph:747] wait graph failed process doneYUV file name out.yuv [MCU2_0] 58.975863 s: VX_ZONE_ERROR:[tivxTargetKernelInstanceAlloc:114] kernel com.ti.hwa.vpac_custom_node has not been registered on this CPU [MCU2_0] 58.975936 s: VX_ZONE_ERROR:[tivxTargetKernelInstanceAlloc:115] Please register this kernel on the appropriate target core [MCU2_0] 58.975991 s: VX_ZONE_ERROR:[tivxTargetNodeDescNodeCreate:761] target_kernel_instance is NULL [MCU2_0] 58.977025 s: VX_ZONE_ERROR:[tivxTargetKernelInstanceAlloc:114] kernel com.ti.hwa.vpac_custom_viss has not been registered on this CPU [MCU2_0] 58.977095 s: VX_ZONE_ERROR:[tivxTargetKernelInstanceAlloc:115] Please register this kernel on the appropriate target core [MCU2_0] 58.977149 s: VX_ZONE_ERROR:[tivxTargetNodeDescNodeCreate:761] target_kernel_instance is NULL Written 1812480 bytes debug7 Processing time for Resolution 1280x944 is Time 7.79ms 58.983592 s: VX_ZONE_ERROR:[ownReleaseReferenceInt:307] Invalid reference 58.983771 s: VX_ZONE_WARNING:[vxReleaseContext:1011] Found a reference 0x5c0f40 of type 00000817 at external count 1, internal count 0, releasing it 58.983778 s: VX_ZONE_WARNING:[vxReleaseContext:1015] Unreleased reference name = raw_image_87 58.983783 s: VX_ZONE_WARNING:[vxReleaseContext:1017] Releasing reference now as a part of garbage collection 58.983792 s: VX_ZONE_WARNING:[vxReleaseContext:1011] Found a reference 0x637968 of type 00000813 at external count 1, internal count 0, releasing it 58.983798 s: VX_ZONE_WARNING:[vxReleaseContext:1015] Unreleased reference name = VISS_CONFIG 58.983803 s: VX_ZONE_WARNING:[vxReleaseContext:1017] Releasing reference now as a part of garbage collection 58.983842 s: VX_ZONE_INIT:[tivxHostDeInit:56] De-Initialization Done for HOST !!! 58.988165 s: VX_ZONE_INIT:[tivxDeInit:111] De-Initialization Done !!! APP: Deinit ... !!! REMOTE_SERVICE: Deinit ... !!! REMOTE_SERVICE: Deinit ... Done !!! IPC: Deinit ... !!! IPC: DeInit ... Done !!! MEM: Deinit ... !!! MEM: Alloc's: 6 alloc's of 6657496 bytes MEM: Free's : 6 free's of 6657496 bytes MEM: Open's : 0 allocs of 0 bytes MEM: Deinit ... Done !!! APP: Deinit ... Done !!! root@j7-evm:/opt/vision_apps#