U-Boot SPL 2019.01-ga141f7abfd (Jan 05 2020 - 03:55:36 +0000
                                                            SYSFW ABI: 2.7 (firmware rev 0x0013 '19.9.0-v2019.09 (TerrifiLlama')
Trying to boot from MMC2
Starting ATF on ARM64 core...

NOTICE:  BL31: v2.2(release):ti2019.05-rc1
NOTICE:  BL31: Bui : 03:29:45, Jan  5 2020
I/TC: 
I/TC: OP-TEE version: ti2019.05-rc1-dev (gcc version 8.3.0 (GNU Toolchain f the A-profile Architecture 8.3-2019.03 (arm-rel-8.36))) #1 SuJan  5 03:28:58 UTC 2020 aarch64
I/TC: Initialized

U-Boot SPL 2019.01-ga141f7abfd (Jan 05 2020 - 03:53:46 +0000
                                                            Trying to boot from MMC2


U-Boot 2019.01-ga141f7abfd (Jan 05 2020 - 03:53:46 +0000)
SoC:   AM654 PG 1.0
Model: Texas Instruments AM654 Base BoardBoard: AM6-COMPROCEVM rev E3
DRAM:  4 GiB
MMC:   sdhci@4f80000: 0, sdhci@04FA0000: 1
Loading Environment from C... OK
In:    serial
Out:   serial
Err:   serial
Net:   
Warning: cpsw_nuss@046000000 using MAC address from ROM
eth0: cpsw_nuss@046000000, eth1: pruss2_eth
Hit any key to stop autoboot:  0 
switch to partitions #0, OK
mmc1 is current device
SD/MMC found on device 1
** Unable to read file boot.scr **
1490 bytes read in 3 ms (4.4 KiB/s)
Loaded env from uEnv.txt
Importing environment frommc1 ...
Running uenvcmd ...
1 bytes read in 1 ms (1000 Bytes/s)
Alrdy setup.
12644360 bytes read in 1057 ms (11.4 MiB/s)
73168 bytes read in 10 ms (7 MiB/s)
## Flattened Device Tree ob at 82000000
   Booting using the fdt blob at 0x82000000
   Loading Device Tree to 000000fddb5000, end 00000000fdec9fff ... OK

Starting kernel ...

[    0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
[    0.0000] Linux version 4.19.79-rt28-g5baf382c8f (oe-user@oe-host) (gcversion 8.3.0 (GNU Toolchain for the A-profile Architecture 8.3-2019.03 (arm-rel-8.36))) #1 SMP PREEMPT RT Sun Jan 02:57:52 UTC 200
[    0.000000] Machine model: Texas Instrunts AM654 Base Board
[    0.000000] earlycon: ns16550a0 at MMIO32 0x0000000002800000 (options '')
[    0.000000] bootconsole [ns16550a0] enabled
[    0.000000] Reserv memory: created DMA memory pool at 0x00000000a0000000, size 1iB
[    0.000000] OF: reserved mem: initialized node r5f-dma-memory@a0000000, compatible id shared-dma-pool
[   .000000] Reserved memory: created DMA memory pool at 0x00000000100000, size 15 MiB
[    0.000000] OF: reserved mem: initialized node r5f-memory@a0100000, compatible id shared-a-pool
[    0.000000] Reserved memory: created DMA memory pooat 0x00000000a1000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node r5f-dma-memory@a1000000, compible id shared-dma-pool
[    0.000000] Reserved memory: creat DMA memory pool at 0x00000000a1100000, size 15 MiB
[    0.000000] OF: reserved mem: initialized node r5f-memory@100000, compatible id shared-dma-pool
[    0.000000] cma: Resved 24 MiB at 0x00000000fe800000
[    0.000000] psci: probing for conduit method from DT.
[    0.000000] psci: PIv1.1 detected in firmware.
[    0.000000] psci: Using standa PSCI v0.2 function IDs
[    0.000000] psci: Trusted OS migration not required
[    0.000000] psci: SMC Calling nvention v1.1
[    0.000000] random: get_random_bytes called om start_kernel+0x94/0x3ec with crng_init=0
[    0.000000] percpu: Embedded 22 pages/cpu s50560 r8192 d31360 u901
[    0.000000] Detected VIPT I-cache on CPU0
[    0.000000]PU features: enabling workaround for ARM erratum 845719
[    0.000000] Speculative Store Bypass Disable mitigationot required
[    0.000000] Built 1 zonelists, mobility groupg on.  Total pages: 1017344
[    0.000000] Kernel command line: console=ttyS2,115200n8 earlycon=ns16550a,mmio32,02800000 mtdparts=47040000.spi.0:512k(ospi.tiboot3),2m(ospi.tis),4m(ospi.u-boot),128k(ospi.env),128k(ospi.env.backup),1t
[    0.000000] Dentry cache hash tae entries: 524288 (order: 11, 8388608 bytes)
[    0.000000] Inode-cache hash table entries: 262144 (order: 9, 20952 bytes)
[    0.000000] software IO TLB: mapped [mem 0xf9db50-0xfddb5000] (64MB)
[    0.000000] Memory: 3954764K/4134912K available (8190K kernel code, 572K rwdata, 2948K rota, 576K init, 369K bss, 155572K reserved, 24576K cma-reserved
                                                                                                                                                          [    0.000000] SLUB: HWalign=64, Order=0-3, MinOb1
[    0.000000] rcu: Preemptible hierarical RCU implementation.
[    0.000000] rcu:     RCU restrictingPUs from NR_CPUS=64 to nr_cpu_ids=4.
[    0.000000] rcu:     RCU priority boosting: priority 1 delay 500 ms.
[    000000]    No expedited grace period (rcu_normal_after_boot).
[  0.000000]    Tasks RCU enabled.
[    0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
[    000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[    000000] GICv3: GIC: Using split EOI/Deactivate mode
[    0.000000] GICv3: Distributor has no Range Selector suppor
    0.000000] ITS [mem 0x01820000-0x0182ffff]                 [    0.000000] GICv3: no VLPI support, no direct LPI support
[    0.000000] GIC: enabling workaround for ITS: Socionext Synquacepre-ITS
[    0.000000] ITS@0x0000000001820000: Devices Table o large, reduce ids 20->19
[    0.000000] ITS@0x0000000001820000: allocated 524288 Devices @8fa400000 (flat, esz  psz 64K, shr 0)
[    0.000000] ITS: using cache flushing formd queue
[    0.000000] GIC: using LPI property table @0x00000008fac30000
[    0.000000] GICv3: CPU0: found redtributor 0 region 0:0x0000000001880000
[    0.000000] GIC: usg cache flushing for LPI property table
[    0.000000] GICv3: CPU0: using LPI pending table @0x00000008fac40000
   0.000000] arch_timer: cp15 timer(s) running at 200.00MHz (ps).
[    0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x2e2049d3e8, max_idle_ns: 4795210634 ns
[    0.000005] sched_clock: 56 bits at 200MHz, rolution 5ns, wraps every 4398046511102ns
[    0.000467] Console: colour dummy device 80x25
[    0.356794] Calibrating delay loop (skipped), value calculated using timer frequency.. 400.00 BogoMIPS (lpj=80000
[    0.356803] pid_max: default: 32768 minimum: 301
[    0.6920] Security Framework initialized
    0.357047] Mountpoint-cache hash table entries: 8192 (order4, 65536 bytes)
[    0.380341] ASID allocator initialised with 32768 entries
[    0.432393] rcu: Hierarchical SRCU implementation.
[    0.460583] Platform MSI: gic-its@1820000 domain created
[    0.466272] PCI/MSI: /interconnect@100000/interru-controller@1800000/gic-its@1820000 domain created
[    0.480525] smp: Bringing up secondary CPUs ...
[    0.541056] Detected VIPT I-cache on CPU1
[    0.541092] GCv3: CPU1: found redistributor 1 region 0:0x00000000018a0000
   0.541101] GICv3: CPU1: using LPI pending table @0x00000008f50000
[    0.541147] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
[    0.626830] Detected VIPT I-che on CPU2
[    0.626868] GICv3: CPU2: found redistributor 10region 0:0x00000000018c0000
[    0.626877] GICv3: CPU2: using LPI pending table @0x00000008fac60000
[    0.62692 CPU2: Booted secondary processor 0x0000000100 [0x410fd034]
[  0.683302] Detected VIPT I-cache on CPU3
[    0.683327] GICv3: CPU3: found redistributor 101 region 0:0x000000018e0000
[    0.683335] GICv3: CPU3: using LPI pending table @00000008fac70000
[    0.683362] CPU3: Booted secondary processor 0x0000000101 [0x410fd034]
[    0.683518] smp: Bught up 1 node, 4 CPUs
[    0.760952] SMP: Total of 4 processs activated.
[    0.765764] CPU features: detected: GIC system register CPU interface
[    0.772352] CPU feature detected: 32-bit EL0 Support
[    0.778065] CPU: All CPU(s) arted at EL2
[    0.782273] alternatives: patching kernel code
[    0.783768] devtmpfs: itialized
[    0.808500] clocksource: jiffies: mask: 0xffffffff max_cycl: 0xffffffff, max_idle_ns: 7645041785100000 ns
[    0.818488] futex hash table entries: 1024 (der: 4, 65536 bytes)
[    0.825932] pinctrl core: initializedinctrl subsystem
[    0.832464] NET: Registered protocol family 16
[    0.838523] vds 2 pages (1 code @ (____ptrval____), 1 data @ (____ptrval____)
                                                                                [    0.846099] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[    0.855436] DMApreallocated 256 KiB pool for atomic allocations
[    0.888243] HugeTLB registered 2.00 MiB page size, pre-alloted 0 pages
[    0.897954] SCSI subsystem initialized
[    0.902623] medi Linux media interface: v0.10
[    0.907327] videodev: Linux deo capture interface: v2.00
[    0.912986] pps_core: LinuxPPS API ver. 1 registered
[    018064] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodfo Giometti <giometti@linux.it>
[    0.927426] PTP clock support registered
[    0.931466] EDAC MC: Ver: 3.0.0
   0.936536] Advanced Linux Sound Architecture Driver Initialid.
[    0.943838] clocksource: Switched to clocksource arch_sys_counter
[    050285] VFS: Disk quotas dquot_6.6.0
[    0.954368] VFS: Dquotache hash table entries: 512 (order 0, 4096 bytes)
[    0.971903] NET: Registered protocol family 2
[    0.977299] tcp_listen_portaddr_hash hash table entries: 20 (order: 5, 131072 bytes)
[    0.985551] TCP established hashable entries: 32768 (order: 6, 262144 bytes)
[    0.993392] TCP bind hash table entries: 32768 (order: 8, 15008 bytes)
[    1.002064] TCP: Hash tables configured (estabshed 32768 bind 32768)
[    1.009096] UDP hash table entries: 2048 (order: 6, 262144 tes)
[    1.015614] UDP-Lite hash table entries: 2048 (order:, 262144 bytes)
[    1.022815] NET: Registered protocol family 1
[    1.028063] RPC: Registered named UX socket transport module.
[    1.034118] RPC: Registered udpransport module.
[    1.038927] RPC: Registered tcp transport module.
[    1.043755] RPC: Registered t NFSv4.1 backchannel transport module.
[    1.051540] hw perfents: enabled with armv8_pmuv3 PMU driver, 7 counters available
[    1.061594] Initialise system trted keyrings
[    1.066373] workingset: timestamp_bits=46 maxrder=20 bucket_order=0
[    1.081751] squashfs: version 4.0 (2009/01/31) Phillip Lougr
[    1.088629] NFS: Registering the id_resolver key type
[    1.0985] Key type id_resolver registered
[    1.098161] Key type ilegacy registered
[    1.102274] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[    1.109370] 9pInstalling v9fs 9p2000 file system support
[    1.120330] Key type asymmetric registered
[    1.124524] Asymmetr key parser 'x509' registered
[    1.129573] Block layer SCSIeneric (bsg) driver version 0.4 loaded (major 245)
[    1.137143] io scheduler noop registered
[    1.141154] iocheduler deadline registered
[    1.145706] io scheduler cfq gistered (default)
[    1.150532] io scheduler mq-deadline registered
[    1.155165] io scheduler kyber regisred
[    1.162298] pinctrl-single 4301c000.pinmux: 70 pins, se 280
[    1.168984] pinctrl-single 11c000.pinmux: 185 pins, size 740[    1.175000] pinctrl-single 11c2e8.pinmux: 9 pins, size 36
   1.181937] pinctrl-single a40000.timesync_router: 512 pins, size 2048
[    1.204574] Serial: 8250/16550 driver, 10 ports, IRQ sharinenabled
[    1.233242] brd: module loaded
[    1.248806] loop: module loaded
[    1.256505] libphy: Fixed IO Bus: probed
[    1.261558] tun: Universal TUN/TAP device driver, 1.6
[    1.267639] igbvf: Intel(R) Gigabit Virtu Function Network Driver - version 2.4.0-k
[    1.275700] igb: Copyright (c) 2009 - 2012 Intel Corporation.
[    1.281829] sky2: driver version 1.30
[    1.287801VFIO - User Level meta-driver version: 0.3
[    1.294461] i2cdev entries driver
[    1.300160] sdhci: Secure Digital Host Controllernterface driver
[    1.306480] sdhci: Copyright(c) Pierre Ossn
[    1.311705] sdhci-pltfm: SDHCI platform and OF driver helper
[    1.319414ti-sci interconnect@100000:interconnect@28380000:interconnect@040000:dmsc: invalid resource
[    1.331470] optee: probing for conduit method from DT.
[  1.336852] optee: revision 3.7 (5208e5c1)
[    1.337249] opte initialized driver
[    1.347518] NET: Registered protocol family 17
[    1.3528] 9pnet: Installing 9P2000 support
[    1.356735] Key type d_resolver registered
[    1.361981] registered taskstats version 1
[    1.366182] ading compiled-in X.509 certificates
[    1.390770] ti-sci interconnect@100000:interconnect@28380000:interconnect@42040000:dm: invalid resource
[    1.401011] ti-sci interconnect@100000:terconnect@28380000:interconnect@42040000:dmsc: ABI: 2.7 (firmware rev 0x0013 '19.9.0-v2019.09 (Terrific Llam)
[    1.438740] random: fast init done
[    2.003466] omap_i2c 42120000.i2c: bus 0 rev0.12 at 400 kHz[    2.010147] omap_i2c 40b00000.i2c: bus 1 rev0.12 at 100 kHz[    2.016910] pca953x 2-0021: 2-0021 supply vcc not found, usindummy regulator
[    2.024452] pca953x 2-0021: Linked as a coumer to regulator.0
    2.059174] omap_i2c 2010000.i2c: bus 3 rev0.12 at 400 kHzz
    2.072098] omap_i2c 2030000.i2c: bus 5 rev0.12 at 100 kHzz
[    2.084049] k3-ringacc 2b800000.ringacc: Ring Accelerator pbed rings:286, gp-rings[96,160] sci-dev-id:195
[    2.094020]3-ringacc 2b800000.ringacc: dma-ring-reset-quirk: enabled
[    2.100700] k3-rincc 2b800000.ringacc: RA Proxy rev. 66344100, num_proxies:64
[  2.108709] k3-ringacc 3c000000.ringacc: Ring Accelerator probed rings:818, gp-rings[304,464] sci-dev-id:18
                                                                                                            [    2.118822] k3-ringacc 3c000000.ringacc: dma-ring-reset-quk: enabled
[    2.125502] k3-ringacc 3c000000.ringacc: RA Proxy rev. 66344100, num_proxies:64
    2.141243] 40a00000.serial: ttyS1 at MMIO 0x40a00000 (irq = 8, base_baud = 6000000) is a 8250
[    151287] 2800000.serial: ttyS2 at MMIO 0x2800000 (irq = 18, basbaud = 3000000) is a 8250
[    2.160093] console [ttyS2] enabled
[    2.160093] consolettyS2] enabled
[    2.167149] bootconsole [ns16550a0] disable
                                              [    2.167149] bootconsole [ns16550a0] disabled
[    2.176811] 2810000.serial: ttyS3 at MMIO 0x2810000irq = 19, base_baud = 3000000) is a 8250
[    2.186307] 28200.serial: ttyS4 at MMIO 0x2820000 (irq = 20, base_baud = 3000000) is a 8250
[    2.198713] cadee-qspi 47040000.spi: mt35xu512aba (65536 Kbytes)
[    2.20490 7 cmdlinepart partitions found on MTD device 47040000.spi.0
[    2.2115] Creating 7 MTD partitions on "47040000.spi.0":
[    2.21699 0x000000000000-0x000000080000 : "ospi.tiboot3"
[    2.223677] 0x000000080000-0x000000280000 : "ospi.tispl"
[  2.230017] 0x000000280000-0x000000680000 : "ospi.u-boot"
[  2.236463] 0x000000680000-0x0000006a0000 : "ospi.env"
[    2.242618] 0x0000006a0000-0x00006c0000 : "ospi.env.backup"
[    2.249377] 0x0000006c0000-0000007c0000 : "ospi.sysfw"
[    2.255704] 0x000000800000-0x000004000000 : "ospi.rootfs"
[    2.488249] cadence-qspi 47040000.spi: Cadence QSPI NOR pro failed -517
[    2.506150] am65-cpsw-nuss 46000000.ethernet: rx-flow-id-base is not set -22
[    2.513248] am65-cpsw-nuss 4600000ethernet: initializing am65 cpsw nuss version 0x6BA07100, cpswersion 0x6BA80100 Ports: 2
[    2.524933] UDMA has not been proped
[    2.528508] am65-cpsw-nuss 46000000.ethern: Failed to request tx dma channel -517
[    2.538949] am65-cs 310d0000.cpts: CPTS ver 0x4e8a2109, freq:200000000, add_val:4 pps:0
[    2.547792] ermal thermal_zone1: failed to read out thermal zone (-22)
[  2.554507] thermal thermal_zone2: failed to read out thermal zone (-22)
[    2.562255] keystone-wdt 40610000.i: heartbeat 60 sec
[    2.568860] mmc0: Unknown controller vsion (4). You may experience problems.
[    2.607618] mmc0: SDHCI controller on 4f80000.sdhci [4f8000sdhci] using ADMA 64-bit
[    2.616547] mmc1: Unknown controlr version (4). You may experience problems.
[    2.655148] mmc1: SDHCI controller on 4fa0000.sdhci [4fa000sdhci] using ADMA 64-bit
[    2.672372] mmc0: new HS200 MMC card at address 0001
[    678780] mmcblk0: mmc0:0001 R1J56L 14.7 GiB 
[    2.685818] mmcblk0boot0: mmc0:0001 R1J56L partition 1 8.00 MiB
[    2.6530] mmcblk0boot1: mmc0:0001 R1J56L partition 2 8.00 MiB
[    2.697419] pca953x 0-0039: 0-0039 supply vcc not found,sing dummy regulator
[    2.707877] mmcblk0rpmb: mmc0:0001 R16L partition 3 4.00 MiB, chardev (243:0)
[    2.718538] pca953x 0-0039: Linked as a consumer to regulator.0
   2.726156]  mmcblk0: p1
[    2.749724] omap-mailbox 31f80000.mailbox: omap mailbox rev 0x66fc5900
[  2.756811] omap-mailbox 31f81000.mailbox: omap mailbox rev 0x6c5900
[    2.764599] ti-udma 285c0000.udmap: Channels: 96 (tchan: 48, echan: 0, rchan: 48, rflow96)
[    2.782513] ti-udma 31150000.udmap: Channels: 267 (tchan: 120, ecn: 32, rchan: 150, rflow: 300)
[    2.816806] cadence-qspi 47040000.spi: mt35xu512aba (65536 ytes)
[    2.822997] 7 cmdlinepart partitions found on MTD dece 47040000.spi.0
[    2.829600] Creating 7 MTD partitions on "47040000.spi.0":
[    2.835081] 000000000000-0x000000080000 : "ospi.tiboot3"
[    2.841797] 0x0000080000-0x000000280000 : "ospi.tispl"
    2.854620] 0x000000680000-0x0000006a0000 : "ospi.env"oot"
[   .860847] 0x0000006a0000-0x0000006c0000 : "ospi.env.backup"
[    2.867580] 0x00006c0000-0x0000007c0000 : "ospi.sysfw"
[    2.873889] 0x0000008000-0x000004000000 : "ospi.rootfs"
[    2.889396] m25p80 spi7.0: n25q128a13 (16384 Kbytes)
[    2.896444] am65-cpsw-nuss 46000000.ethernet: rx-flow-id-ba is not set -22
[    2.903553] am65-cpsw-nuss 46000000.ethern: initializing am65 cpsw nuss version 0x6BA07100, cpsw version 0x6BA80100 Ports: 2
[    2.927143] am65-cpsw-nuss 46000000.ethernet: set new flow--base 48
[    2.941896] pps pps0: new PPS source ptp1
[    2.946141] am65-cpsw-nuss6000000.ethernet: CPTS ver 0x4e8a2109, freq:200000000, add_val pps:1
[    2.955092] am65-cpsw-nuss 46000000.ethernet: initialized cpsw ale version 0.4
[    2.962303] am65-cpswuss 46000000.ethernet: ALE Table size 64
[    3.007876] am65-cpsw-nuss 46000000.ethernet: davinci mdio vision 9.7, bus freq 1000000
[    3.016041] libphy: 46000000.hernet: probed
[    3.025668] input: gpio-keys as /devices/platform/gpio-keysnput/input0
[    3.032743] hctosys: unable to open rtc devicertc0)
[    3.155984] ALSA device list:
[    3.158955]   No soundcar found.
[    3.865942] mmcblk1: mmc1:aaaa SA08G 7.40 GiB 0f68049-02...[    3.859016] mmc1: new high speed SDHC card at address aaaa
[    3.8726]  mmcblk1: p1 p2
[    4.549441] EXT4-fs (mmcblk1p2): recovery complete
[    4.561857] EXT4-fs (mmcblk1p2): mounted filesystem withrdered data mode. Opts: (null)
[    4.570007] VFS: Mounted root (ext4 filesystem) on device 1:98.
[    4.585839] devtmpfs: mounted
[    4.589476] Freeing unusedernel memory: 576K
[    4.594060] Run /sbin/init as init procs
[    4.949273] systemd[1]: System time before build time, advancing clock.
[    5.067902] NET: Registered protocol family 10
[    5.0736] Segment Routing with IPv6
[    5.093776] systemd[1]: systemd 239 running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR +SMACK +SYINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCO +BLKID -ELFUTILS +KMOD -IDN2 -)
[    5.115552] systemd[1]: Detected architecture m64.

Welcome to Arago 2019.11!

[    5.141448] systemd[1]: Set hostnamto <am65xx-evm>.
[    5.350907] systemd[1]: File /lib/systemd/system/systemd-journald.service:36 configures an IP rewall (IPAddressDeny=any), but the local system does not suppt BPF/cgroup based firewalling.
[    5.367941] systemd[1]: Proceeding WITHOUT firewalling in effect! (This warning isnly shown for the first loaded unit using IP firewalling.)
[    5.648256] random: systemd: uninitialized urandom read (16ytes read)
[    5.655273] systemd[1]: Listening on initctl Compatibility Named Pipe.
[  OK  Listening on initctl Compatibility Named Pipe.
[    5.680048] random: systemd: uninitialized urandom read (16ytes read)
[    5.686986] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[ K  ] Started Forward Password Requests to Wall Directory Wch.
[    5.708072] random: systemd: uninitialized urandom read (16ytes read)
[    5.715294] systemd[1]: Listening on udev Contr Socket.
[  OK  ] Listening on udev Control Socket.
[    5.732051] sysmd[1]: Reached target Remote File Systems.
[  OK  ] Reached target Remote File Systems.
[    548343] systemd[1]: Listening on udev Kernel Socket.
[  OK  ] Listening on udev Kernel Socket.
[ K  ] Created slice system-serial\x2dgetty.slice.
[    ] Listening on Network Service Netlink Socket.
[  OK  ] Reached target Swap.
[  OK  ] Listening on Process Core Dump Socket.
[  OK  ] Created slice system-getty.slice.
[  OK  ] Listening on Journal Socket (/dev/log).
[  O ] Listening on Journal Socket.
         Starting Create list of required st��…ce nodes for the current kernel...
         Mounting POSIX Message Queue File System...
[  OK  ] Started Hardware RNG Entropy Gatherer Daem.
         Starting udev Coldplug all Devices...
         Mounting Temporary Directory (/tmp)...
         Mounting Huge Pages File System...
         Starting Load Kernel Modules...
         Starting Remount Root and Kernel File Systems...
[    6.079651] cryptodev: loading out-of-tree module taints keel.
[  OK  ] Created slice User and Session Slice.[    093350] cryptodev: driver 1.9 loaded.

[    6.100135] EXT4-f(mmcblk1p2): re-mounted. Opts: (null)
[  OK  ] Reached target Slices.
         Starting Journal Service...
         Mounting Kernel Debug File System...
[  OK  ] Started Dispatch Password Requests to Console Direory Watch.
[  OK  ] Reached target Paths.
[  OK  ] Started Create list of required sta��…viceodes for the current kernel.
[  OK  ] Mounted POSIX Message Queue File System.
[  OK  ] Started Journal Service.
[  OK  ] Mounted Temporary Directory (/tmp).
[  OK  ] Mounted Huge Pages File System.
[  OK  ] Started Load Kernel Modules.
[  OK  ] Started Remount Root and Kernel File Syste.
[  OK  ] Mounted Kernel Debug File System.
         Mounting Kernel Configuration File System...
         Starting Apply Kernel Variables...
         Starting Flush Journal to Persistent Storage...
         Starting Create Static Device Nodes in /dev...
[  OK  ] Started Apply Kernel Variables.le System.
[  OK  ] Started Create Static Device Nodes in /dev
                                                   [  OK  ] Reached target Local File Systems (Pre).
         Mounting /media/ram...
         Mounting /var/volatile...
[  OK  ] Reached target Containers.
         Starting udev Kernel Device Manager...
[  OK  ] Mounted /media/ram.
[  OK  ] Mounted /var/volatile.
[    6.662295] systemd-journald[180]: Received request to flush runtime journal from PID 1
         Stting Load/Save Random Seed...
[  OK  ] Reached target Local File Systems.
[  OK  ] Started Flush Journal to Persistent Storag
[  OK  ] Started Load/Save Random Seed.
[  OK  ] Started udev Kernel Device Manager.
         Starting Create Volatile Files and Directories...
[  OK  ] Started Create Volatile Files and Directories.
         Starting Update UTMP about System Boot/Shutdown...
         Starting Network Time Synchronization...
         Starting Network Service...
[  OK  ] Started Update UTMP about System Boot/Shutwn.
[  OK  ] Started Network Service.
         Starting Wait for Network to be Configured...
         Starting Network Name Resolution...
[  OK  ] Started Network Time Synchronization.
[  OK  ] Found device /dev/ttyS2.
[  OK  ] Reached target System Time Synchronized.
[    8.100834] [drm] Initialized pvr 1.17.4948957 20110701 for 7000000.gpu on minor 0
[    8.167464] dwc3 4030000.usb: Failed to get clk 'ref': -2
[    8.173845] OF: graph:  port node found in /interconnect@100000/phy@4110000
[  OK  ] Found device /dev/ttyS1.
[  OK  ] Started Network Name Resolution.
[  O ] Reached target Host and Network Name Lookups.
[    8.562200] k3_r5_rproc interconnect@100000:interconnect@280000:r5fss@41000000: creating child devices for R5F cores
[    8.620297] platform 41000000.r5f: configured R5F for remotroc mode
[    8.628248] platform 41000000.r5f: assigned reserd memory node r5f-dma-memory@a0000000
[    8.653803] remoteproc remoteproc0: 41000000.r5f is availab
[  OK  ] Started udev Coldplug all Devices.
[ OK  ] Reached target System Initialization.
[  OK  ] Listening on D-Bus System Message Bus Socket.
[  OK  ] Started Daily Cleanup of Temporary Directories.
[    8.830157] TI DP83867 k3-cpsw-mdio:00: attached PHY driverTI DP83867] (mii_bus:phy_addr=k3-cpsw-mdio:00, irq=POLL)
[    8.843687] IPv6: ADDRCONF(NETDEV_UP): eth0: link is n ready
[    8.862132] remoteproc remoteproc0: powering up 41000000.r5
                                                              [    8.868214] remoteproc remoteproc0: Booting fw image am65xcu-r5f0_0-fw, size 4142860
[  OK  ] [    8.877982] atform 41000000.r5f: booting R5F core using boot addr = 0x0
Ltening on dropbear.socket.
[    8.886800] virtio_rpmsg_bus virtio0: rpmsg host is online
[    8.889866] viro_rpmsg_bus virtio0: creating channel rpmsg-proto addr 0x3d
[  8.902297] remoteproc remoteproc0: registered virtio0 (type 7)
[    8.908258] remoteproc remotepr0: remote processor 41000000.r5f is now up
[  OK  Listening on RPCbind Server Activation Socket.
[  OK  ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
[  OK  ] Reached taet Sockets.
[  OK  ] Reached target Basic System.
[  OK  ] Started D-Bus System Message Bus.
         Starting Simple Network Management Protocol (SNMP) Daon....
         Starting Login Service...
         Starting rc.pvr.service...
         Starting RPC Bind Service...
[  OK  ] Started irqbalance daemon.
         Starting Lightning Fast Webserver With Light System Ruirements...
[  OK  ] Started TEE Supplicant.
[    9.349085] PVR_K: UM DDK-(4948957) and KM DDK-(4948957) match. [ OK ]
         Starting Permit User Sessions...
[  OK  ] Started Job spooling tools.
[  OK  ] Started Periodic Command Scheduler.
         Starting Reboot and dump vmcore via kexec...
[  OK  ] Started Daily rotation of log files.
[OK  ] Reached target Timers.
[    9.849108] am65-cpsw-nuss 46000000.ethernet eth0: Link is Down
       Starting Avahi mDNS/DNS-SD Stack...
         Starting Print notice about GPLv3 packages...
         Starting TI IPC Daemon...
[  OK  ] Started rc.pvr.service.
[  OK  ] Started RPC Bind Service.
[  OK  ] Started Lightning Fast Webserver With Light System Requirements.
[  OK  ] Started Permit User Sessions.
[   10.851127] omap_rng 4e10000.trng: Random Number Generator ver. 230b34c
[   10.851255] random: crng init don
                                    [   10.851267] random: 7 urandom warning(s) missed due to ratimiting
  OK  ] Started TI IPC Daemon.mp vmcore via kexec.
[   11.002451] usbcore: registered new interface driver hubfs
[   11.026601] usbcore: registered new device driver usb
[   11.136542] davinci_mdio b232400.mdio: davinci mdio revisio1.7, bus freq 1000000
[   11.146821] libphy: b232400.mdio: probed
[   11.272246] xhci-hcd xhci-hcd.2.auto: xHCI Host Controller
[   11.277908] xi-hcd xhci-hcd.2.auto: new USB bus registered, assigned bus nuer 1
[   11.290541] xhci-hcd xhci-hcd.2.auto: hcc params 0x0298fe6dci version 0x110 quirks 0x0000000000010010
[   11.300449] davci_mdio b232400.mdio: phy[0]: device b232400.mdio:00, driver TI 83867
[   11.300460] davinci_mdio b232400.mdio: phy[3]: devicb232400.mdio:03, driver TI DP83867
[   11.322326] xhci-hcd xhci-hcd.2.auto: irq 301, io mem 0x040000
[   11.329193] usb usb1: New USB device found, idVendor=1b, idProduct=0002, bcdDevice= 4.19
[   11.340782] usb usb1: New USB device stris: Mfr=3, Product=2, SerialNumber=1
[   11.347025] remoteprocemoteproc1: b034000.pru is available
[   11.347146] pru-rproc b034000.pr PRU rproc node pru@b034000 probed successfully
[   11.347671remoteproc remoteproc2: b004000.rtu is available
[   11.347770] pru-rproc b004000.rtu: PRU rproc node r@b004000 probed successfully
[   11.353755] remoteproc remoteoc3: b038000.pru is available
   11.358732] remoteproc remoteproc4: b006000.rtu is available[   11.358847] pru-rproc b006000.rtu: PRU rproc node rtu@b006000 probed succefully
[   11.359394] remoteproc remoteproc5: b134000.pru is ailable
[   11.359491] pru-rproc b134000.pru: PRU rproc node p@b134000 probed successfully
[   11.361012] remoteproc remoteproc6: b104000.rtu is available
[   11.361258] pru-roc b104000.rtu: PRU rproc node rtu@b104000 probed successfully
[   11.391332] roteproc remoteproc7: b138000.pru is available
[   11.391454] pru-rproc b138000.pru: PRUproc node pru@b138000 probed successfully
[   11.394684] remoproc remoteproc8: b106000.rtu is available
[   11.394828] pru-rproc b106000.rtu: PRU rproc nodetu@b106000 probed successfully
[   11.395419] remoteproc remoproc9: b234000.pru is available
[   11.395517] pru-rproc b234000.pru: PRU rproc node pru@b2340 probed successfully
[   11.421236] remoteproc remoteproc10: b204000.rtu is available
[   11.421368] pru-rpr b204000.rtu: PRU rproc node rtu@b204000 probed successfully
  11.421814] remoteproc remoteproc11: b238000.pru is available
[   11.421950] pruproc b238000.pru: PRU rproc node pru@b238000 probed successful
[   11.422301] remoteproc remoteproc12: b206000.rtu is available
[   11.422395] pru-rproc206000.rtu: PRU rproc node rtu@b206000 probed successfully
[ 11.558980] icssg-prueth pruss2_eth: TI PRU ethernet driver initialized:ual EMAC mode
[   11.588778] usb usb1: Product: xHCI Host Conoller
[   11.593770] usb usb1: Manufacturer: Linux 4.19.79-rt28-g5ba82c8f xhci-hcd
[   11.600985] usb usb1: SerialNumber: xhci-hc2.auto
[   11.608535] hub 1-0:1.0: USB hub found
[   11.613673] hub 1-0:1.0: 1 po detected
[   11.618842] xhci-hcd xhci-hcd.2.auto: xHCI Host ntroller
[   11.624462] xhci-hcd xhci-hcd.2.auto: new USB bus registered, assigned bunumber 2
[   11.632276] xhci-hcd xhci-hcd.2.auto: Host suppor USB 3.0 SuperSpeed
   11.649695] usb usb2: New USB device found, idVendor=1d6b, iProduct=0003, bcdDevice= 4.19
[   11.661253] usb usb2: New USdevice strings: Mfr=3, Product=2, SerialNumber=1
[   11.66858 usb usb2: Product: xHCI Host Controller
[   11.673554] usb usb2: Manufacturer: Linux 4.19.79-rt28-g5baf3c8f xhci-hcd
[   11.680550] usb usb2: SerialNumber: xhci-hcd.auto
[   11.686412] hub 2-0:1.0: USB hub found
[   11.691475] hub 2-0:1.0: 1 port detected
[  OK  ] Created slice system-systemd\x2dfsck.slice
                                                   [  OK  ] Started Getty on tty1.
[  OK  ] Started rial Getty on ttyS2.
[  OK  ] Started Serial Getty on ttyS1.
[  OK  ] Rched target Login Prompts.
         Starting Synchronize Syst and HW clocks...
[  OK  ] Started NFS status monitor for NFSv2/3 locking
         Starting weston.service...
[  OK  ] Start Simple Network Management Protocol (SNMP) Daemon..
[FAILED] Failed to start Synchronize System and Hclocks.
See 'systemctl status sync-clocks.service' for detail
[  OK  ] Started Avahi mDNS/DNS-SD Stack.
[OK  ] Started Login Service.
[  OK  ] Started weston.service.
         Starting Matrix GUI...
         Starting telnetd.service...
[  OK  ] Started Matrix GUI.
[  OK  ] Started telnetd.service.
[   13.152865] NET: Registered protocol family 45
[  OK  ] Started Hardware RNG Entropy Gatherer Daem.
         Starting thttpd.service...
[   13.357391] remoteproc remoteproc11: powering up b238000.pr
                                                              [   13.397647] remoteproc remoteproc11: Booting fw image ti-pruss/am65x-pru1-prueth-fw.elf, size 1646
                                                                                                                                                                   [   13.407344] remoteproc remoteproc11: p
[   13.414339] remoteproc remoteproc12: powering up b206000.rtu
[   13.424852] remoteproc remotepr12: Booting fw image ti-pruss/am65x-rtu1-prueth-fw.elf, size 140
[   13.433923] remoteproc remoteproc12: remote processor b2000.rtu is now up
[   13.442712] net eth2: started
[   13.4437] IPv6: ADDRCONF(NETDEV_UP): eth2: link is not ready
[  OK  ] Started thttpd.service.
[   13.499369] remoteproc remoteproc9: powering up b234000.pru[   13.517575] remoteproc remoteproc9: Booting fw image ti-pru/am65x-pru0-prueth-fw.elf, size 16460
[   13.526573] remotepr remoteproc9: remote processor b234000.pru is now up
[   13.533914] remeproc remoteproc10: powering up b204000.rtu
[   13.545934] remoteproc remoteproc10: Booting fw image ti-prs/am65x-rtu0-prueth-fw.elf, size 15540
[   13.555046] remotepc remoteproc10: remote processor b204000.rtu is now up
[   13.565821] net eth1: started
  13.570797] IPv6: ADDRCONF(NETDEV_UP): eth1: link is not read
                                                              [  OK  ] Found device /dev/mmcblk1p1.
         Staing File System Check on /dev/mmcblk1p1...
[  OK  ] Started File System Check on /dev/mmcblk1p
         Mounting /run/media/mmcblk1p1...
[  OK  ] Mounted /run/media/mmcblk1p1.
[  OK  ] Created slice system-systemd\x2dcoredump.slice.
[  OK  ] Started Procs Core Dump (PID 919/UID 0).
***************************************************************
*************************************************************
NOTICE: Thifile system contains the following GPLv3 packages:
        autoconf
        bash-dev
        bash
        bc
        binutils
        cifs-utils
        cpio
        p-symlinks
        cpp
        dosfstools
        elfutils
        g++-symlinks
gawk    g++
        gcc-symlinks
        gcc
        gdb
        gdbserver
        gettext
        glmark2
        gstreamer1.0-libav
        gzip
        hidapi
        libbfd
        libcai-perf-utils
        libdw1
        libelf1
        libgdbm-compat4
        libgdbm-dev     libgdbm6
        libgettextlib
        libgettextsrc
        libgmp10
        libidn2-0
        libmpc3
        libmpfr6
        libreadline-dev
        libreadline7    libunistring2
        m4-dev
        m4
        make
        nettle
        parted
        pdm-analy-detection
        swig-dev
        swig
        which

If you do not wish to distribute GPLv3 components please remove
the above ckages prior to distribution.  This can be done using
the opkremove command.  i.e.:
    opkg remove <package>
Where <package> is the name printed in the list above

NOTE: If t package is a dependency of another package you
      will beotified of the dependent packages.  You should
      use the --force-removal-of-dependent-packages option to
      so remove the dependent packages as well
*************************************************************
***************************************************************
[  OK  ] Started Print notice about GPLv3 packages.
 _____                    _____           _         _   
|  _|___ ___ ___ ___   |  _  |___ ___  |_|___ ___| |_ 
|     |  _| .'| . | . |  |   __|  _| . | | | -_|  _|  _|
|__|__| |__,|_  |___|  |__|  |_| |___|_| |___|___|_|  
             ___|                    |___|            

Arago Project http://arago-project.org am65xx-evm ttyS2

Arago 2019.11 65xx-evm ttyS2

am65xx-evm login: 
 _____                    _____           _         _   
|  _|___ ___ ___ ___   |  _  |___ ___  |_|___ ___| |_ 
|     |  _.'| . | . |  |   __|  _| . | | | -_|  _|  _|
|__|__|_| |__,|_  |___|  |__|  |_| |___|_| |___|___|_|
              |___|                    |___|            

ago Project http://arago-project.org am65xx-evm ttyS2

Arago 2019.11 am65xx-evm ttyS2

am65xx-evm login: root
root@am65xx-evm:~# lsusb
Bus 002 Device 001: ID 1d6b:0003 Linux Foundation 3.0 root hub
Bus 001 Device 001: ID 1d6b:0002 Linux Foundation 2.0 rootub
root@am65xx-evm:~# 
root@am65xx-evm:~# uname -a
Linux am65xx-evm 4.19.79-rt28-g5baf382c8f #1 SMP PREEMPT RT SuJan 5 02:57:52 UTC 2020 aarch64 GNU/Linux