akash@ubuntu:~/ti-processor-sdk-android-am57xx-evm-04.01.00.06$ ./setup.sh Just a simple wrapper over the fastboot.sh to set the appropriate paths. --------------------------------------------------------------------------------" This step will set up minicom (serial communication application) for SDK development For boards that contain a USB-to-Serial converter on the board such as: * BeagleBone * Beaglebone Black * AM335x EVM-SK * AM57xx EVM * K2H, K2L, and K2E EVMs the port used for minicom will be automatically detected. By default Ubuntu will not recognize this device. Setup will add a udev rule to /etc/udev/ so that from now on it will be recognized as soon as the board is plugged in. For other boards, the serial will defualt to /dev/ttyS0. Please update based on your setup. -------------------------------------------------------------------------------- NOTE: If your using any of the above boards simply hit enter and the correct port will be determined automatically at a later step. For all other boards select the serial port that the board is connected to. Which serial port do you want to use with minicom? [ /dev/ttyUSB0 ] Copied existing /home/akash/.minirc.dfl to /home/akash/.minirc.dfl.old Configuration saved to /home/akash/.minirc.dfl. You can change it further from inside minicom, see the Software Development Guide for more information. -------------------------------------------------------------------------------- -------------------------------------------------------------------------------- This step will set up the u-boot variables for booting the EVM. -------------------------------------------------------------------------------- -------------------------------------------------------------------------------- Would you like to create a minicom script to configure the board (y/n)? [ y ] Successfully wrote /home/akash/ti-processor-sdk-android-am57xx-evm-04.01.00.06/bin/setupBoard.minicom Detecting connection to board... /dev/ttyUSB0 -------------------------------------------------------------------------------- Would you like to run the setup script now (y/n)? Please connect the USB and USB/serial cables as described in the Quick Start Guide. Once answering 'y' on the prompt below, you will have 300 seconds to connect the board and power cycle it before the setup times out. After successfully executing this script, your EVM will be set up. After power cycling the board, you will be able to connect to it by executing 'minicom -w' or by using the 'adb' utility. If you prefer a windows host, you can set up Tera Term as explained in the Software Developer's Guide. [ y ] [sudo] password for akash: Welcome to minicom 2.7 OPTIONS: I18n Compiled on Feb 7 2016, 13:37:27. Port /dev/ttyUSB0, 13:06:40 Press CTRL-A Z for help on special keys ����