How to use these files with Code Composer Studio:
-------------------------------------------------

1) First Setup the Code Composer Studio with the appropriate Target Board 
   type/name, I/O port, CPU type and GEL file.
2) Start the Code Composer Studio and create a new project by selecting
   Project-New from the menu and then select the location and name of the 
   project on the computer.
3) From the menu, select Project-Build Options-Target and then on the Compiler
   Tab choose the appropriate device from the Basic-Target Version.
4) From the menu choose Project-Add Files to Project and add the following files
	* vecs.asm
	* uart.c
   Also include the appropriate link command file (*.cmd) and library files (*.lib) 
   from C:\ti according to the target C6000 device used.
5) In the uart.c file change the #define CHIP_6xxx 1 to the appropriate
   number according to the TMS320C6000 DSP used. For instance if the TMS320C6711
   is used, change the above line to #define CHIP_6711 1.
6) Build the project by selecting Project-Build from the menu.
7) Load the program by selecting File-Load Program from the menu.
8) Make appropriate wire connection for McBSP.  See the following picture:

   This diagram shows that DX, DR, FSX, and FSR
   of McBSP1 are all connected together.

       	        ___________________
                |2               1|
                |                 |
                |                 |
                |                 |
                |                 |
                |                 |
                |CLK0         FSX0|
                |DX0              |
                |DR0          FSR0|
                |                 |
           +----|DX1 36    35 FSX1|     
           |    |                 |     
           +----|DR1 42    41 FSR1|----+
           |    |                 |    |
           |    |                 |    | 
           |    |                 |    |
           |    |                 |    |
           |    |                 |    |
           |    |                 |    |
           |    |                 |    |
           |    |_________________|    |
           |                           |
           +---------------------------+

8) Run the program.