dst address 0x81FFF000 dst address 0x83FFE000 dst address 0x85FFD000 dst address 0x87FFC000 dst address 0x89FFB000 dst address 0x8BFFA000 dst address 0x8DFF9000 dst address 0x8FFF8000 dst address 0x91FF7000 dst address 0x93FF6000 dst address 0x95FF5000 dst address 0x97FF4000 dst address 0x99FF3000 dst address 0x9BFF2000 dst address 0x9DFF1000 Error matching value at src and dst address Value at src address 0x40326394 is:0x55 Value at dst address 0x9FC00110 is:0xFFFFFFFF EDMA TEST failed at address 0x9FC00110 **************************************************************** Running DDR test case 2 -- Random memory read/write How many times should the test be repeated(enter a number):2 Enter the start address of the memory to be tested in hex(without 0x):9fc0110 How many times random mem test is to be repeated(enter a number):2 Error matching value at src and dst address Value at src address 0x40326284 is:0xFFFFFFAA Value at dst address 0x9FC0110 is:0x0 DDR TEST failed at address: 0x0 Test count number 0x0 Error matching value at src and dst address Value at src address 0x40326284 is:0xFFFFFFAA Value at dst address 0x9FC0110 is:0x0 DDR TEST failed at address: 0x0 Test count number 0x1 **************************************************************** Running DDR test case 3 -- Sequential memory read/write How many times should the test be repeated(enter a number):1 Enter the start address of the memory to be tested in hex(without 0x):0x9fc00011 Enter the size of the DDR memory to be tested in hex(without 0x): 09fc00011 Enter the pattern used to be tested in hex(without 0x):5 Error matching value at src and dst address Value at src address 0x40326383 is:0x5 Value at dst address 0x9FC00110 is:0xFFFFFFFF EDMA TEST failed at address: 0xFFFFFFFF Test count number 0x0 **************************************************************** Running DDR test case 4 -- Sequential increment pattern How many times should the test be repeated(enter a number):0 Enter the start address of the memory to be tested in hex(without 0x):1 Enter the size of the DDR memory to be tested in hex(without 0x): 1024 Enter the pattern used to be tested in hex(without 0x):56 DDR-- Sequential increment pattern test is complete ============================================================== DDR Stress Test Fail Coming out as time Expired... U-Boot SPL 2017.01-ga08afdf552 (Oct 17 2017 - 17:32:06) DRA762-GP ES1.0 ACD package Trying to boot from MMC2_2 *** Warning - bad CRC, using default environment reading u-boot.img reading u-boot.img reading u-boot.img reading u-boot.img U-Boot 2017.01-ga08afdf552 (Oct 17 2017 - 17:32:06 -0400) CPU : DRA762-GP ES1.0 ACD package Model: TI DRA762 EVM Board: DRA76x EVM REV A.2 DRAM: 4 GiB NAND: 0 MiB MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1 *** Warning - bad CRC, using default environment Warning: fastboot.cpu: unknown CPU rev: 123863299 GUID Partition Table Header signature is wrong: 0x0 != 0x5452415020494645 part_get_info_efi: *** ERROR: Invalid GPT *** GUID Partition Table Header signature is wrong: 0x0 != 0x5452415020494645 part_get_info_efi: *** ERROR: Invalid Backup GPT *** CACHE: Misaligned operation at range [fefb9710, fefb9f10] ** First descriptor is NOT a primary desc on 1:1 ** ERROR: cannot find partition: 'userdata' at /OE/arago-morty-next-build/build-CORTEX_1/arago-tmp-external-linaro-toolchain/work/dra7xx_evm-linux-gnueabi/u-boot-ti-staging/2017.01+gitAUTOINC+a08afdf552-r16/git/arch/arm/mach-omap2/utils.c:96/omap_mmc_get_part_size() Warning: fastboot.userdata_size: unable to calc SCSI: SATA link 0 timeout. AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode flags: 64bit ncq stag pm led clo only pmp pio slum part ccc apst scanning bus for devices... Found 0 device(s). Net: Warning: ethernet@48484000 using MAC address from ROM eth0: ethernet@48484000 Hit any key to stop autoboot: 2 1 0 switch to partitions #0, OK mmc0 is current device SD/MMC found on device 0 reading boot.scr ** Unable to read file boot.scr ** reading uEnv.txt ** Unable to read file uEnv.txt ** switch to partitions #0, OK mmc0 is current device SD/MMC found on device 0 ** Invalid partition 2 ** switch to partitions #0, OK mmc1(part 0) is current device SD/MMC found on device 1 Failed to mount ext2 filesystem... ** Unrecognized filesystem type ** switch to partitions #0, OK mmc1(part 0) is current device mmc - MMC sub system Usage: mmc info - display info of the current MMC device mmc read addr blk# cnt mmc write addr blk# cnt mmc erase blk# cnt mmc rescan mmc part - lists available partition on current mmc device mmc dev [dev] [part] - show or set current mmc device [partition] mmc list - lists available devices mmc hwpartition [args...] - does hardware partitioning arguments (sizes in 512-byte blocks): [user [enh start cnt] [wrrel {on|off}]] - sets user data area attributes [gp1|gp2|gp3|gp4 cnt [enh] [wrrel {on|off}]] - general purpose partition [check|set|complete] - mode, complete set partitioning completed WARNING: Partitioning is a write-once setting once it is set to complete. Power cycling is required to initialize partitions after set to complete. mmc bootbus dev boot_bus_width reset_boot_bus_width boot_mode - Set the BOOT_BUS_WIDTH field of the specified device mmc bootpart-resize - Change sizes of boot and RPMB partitions of specified device mmc partconf dev boot_ack boot_partition partition_access - Change the bits of the PARTITION_CONFIG field of the specified device mmc rst-function dev value - Change the RST_n_FUNCTION field of the specified device WARNING: This is a write-once field and 0 / 1 / 2 are the only valid values. mmc setdsr - set DSR register value mmc - MMC sub system Usage: mmc info - display info of the current MMC device mmc read addr blk# cnt mmc write addr blk# cnt mmc erase blk# cnt mmc rescan mmc part - lists available partition on current mmc device mmc dev [dev] [part] - show or set current mmc device [partition] mmc list - lists available devices mmc hwpartition [args...] - does hardware partitioning arguments (sizes in 512-byte blocks): [user [enh start cnt] [wrrel {on|off}]] - sets user data area attributes [gp1|gp2|gp3|gp4 cnt [enh] [wrrel {on|off}]] - general purpose partition [check|set|complete] - mode, complete set partitioning completed WARNING: Partitioning is a write-once setting once it is set to complete. Power cycling is required to initialize partitions after set to complete. mmc bootbus dev boot_bus_width reset_boot_bus_width boot_mode - Set the BOOT_BUS_WIDTH field of the specified device mmc bootpart-resize - Change sizes of boot and RPMB partitions of specified device mmc partconf dev boot_ack boot_partition partition_access - Change the bits of the PARTITION_CONFIG field of the specified device mmc rst-function dev value - Change the RST_n_FUNCTION field of the specified device WARNING: This is a write-once field and 0 / 1 / 2 are the only valid values. mmc setdsr - set DSR register value Booting from eMMC ... Wrong Image Format for bootm command ERROR: can't get kernel image! => ü U-Boot SPL 2017.01-ga08afdf552 (Oct 17 2017 - 17:32:06) DRA762-GP ES1.0 ACD package Trying to boot from MMC2_2 *** Warning - bad CRC, using default environment reading u-boot.img reading u-boot.img reading u-boot.img reading u-boot.img U-Boot 2017.01-ga08afdf552 (Oct 17 2017 - 17:32:06 -0400) CPU : DRA762-GP ES1.0 ACD package Model: TI DRA762 EVM Board: DRA76x EVM REV A.2 DRAM: 4 GiB NAND: 0 MiB MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1 *** Warning - bad CRC, using default environment Warning: fastboot.cpu: unknown CPU rev: 123863299 GUID Partition Table Header signature is wrong: 0x0 != 0x5452415020494645 part_get_info_efi: *** ERROR: Invalid GPT *** GUID Partition Table Header signature is wrong: 0x0 != 0x5452415020494645 part_get_info_efi: *** ERROR: Invalid Backup GPT *** CACHE: Misaligned operation at range [fefb9710, fefb9f10] ** First descriptor is NOT a primary desc on 1:1 ** ERROR: cannot find partition: 'userdata' at /OE/arago-morty-next-build/build-CORTEX_1/arago-tmp-external-linaro-toolchain/work/dra7xx_evm-linux-gnueabi/u-boot-ti-staging/2017.01+gitAUTOINC+a08afdf552-r16/git/arch/arm/mach-omap2/utils.c:96/omap_mmc_get_part_size() Warning: fastboot.userdata_size: unable to calc SCSI: SATA link 0 timeout. AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode flags: 64bit ncq stag pm led clo only pmp pio slum part ccc apst scanning bus for devices... Found 0 device(s). Net: Warning: ethernet@48484000 using MAC address from ROM eth0: ethernet@48484000 Hit any key to stop autoboot: 2 1 0 switch to partitions #0, OK mmc0 is current device SD/MMC found on device 0 reading boot.scr ** Unable to read file boot.scr ** reading uEnv.txt ** Unable to read file uEnv.txt ** switch to partitions #0, OK mmc0 is current device SD/MMC found on device 0 ** Invalid partition 2 ** switch to partitions #0, OK mmc1(part 0) is current device SD/MMC found on device 1 Failed to mount ext2 filesystem... ** Unrecognized filesystem type ** switch to partitions #0, OK mmc1(part 0) is current device mmc - MMC sub system Usage: mmc info - display info of the current MMC device mmc read addr blk# cnt mmc write addr blk# cnt mmc erase blk# cnt mmc rescan mmc part - lists available partition on current mmc device mmc dev [dev] [part] - show or set current mmc device [partition] mmc list - lists available devices mmc hwpartition [args...] - does hardware partitioning arguments (sizes in 512-byte blocks): [user [enh start cnt] [wrrel {on|off}]] - sets user data area attributes [gp1|gp2|gp3|gp4 cnt [enh] [wrrel {on|off}]] - general purpose partition [check|set|complete] - mode, complete set partitioning completed WARNING: Partitioning is a write-once setting once it is set to complete. Power cycling is required to initialize partitions after set to complete. mmc bootbus dev boot_bus_width reset_boot_bus_width boot_mode - Set the BOOT_BUS_WIDTH field of the specified device mmc bootpart-resize - Change sizes of boot and RPMB partitions of specified device mmc partconf dev boot_ack boot_partition partition_access - Change the bits of the PARTITION_CONFIG field of the specified device mmc rst-function dev value - Change the RST_n_FUNCTION field of the specified device WARNING: This is a write-once field and 0 / 1 / 2 are the only valid values. mmc setdsr - set DSR register value mmc - MMC sub system Usage: mmc info - display info of the current MMC device mmc read addr blk# cnt mmc write addr blk# cnt mmc erase blk# cnt mmc rescan mmc part - lists available partition on current mmc device mmc dev [dev] [part] - show or set current mmc device [partition] mmc list - lists available devices mmc hwpartition [args...] - does hardware partitioning arguments (sizes in 512-byte blocks): [user [enh start cnt] [wrrel {on|off}]] - sets user data area attributes [gp1|gp2|gp3|gp4 cnt [enh] [wrrel {on|off}]] - general purpose partition [check|set|complete] - mode, complete set partitioning completed WARNING: Partitioning is a write-once setting once it is set to complete. Power cycling is required to initialize partitions after set to complete. mmc bootbus dev boot_bus_width reset_boot_bus_width boot_mode - Set the BOOT_BUS_WIDTH field of the specified device mmc bootpart-resize - Change sizes of boot and RPMB partitions of specified device mmc partconf dev boot_ack boot_partition partition_access - Change the bits of the PARTITION_CONFIG field of the specified device mmc rst-function dev value - Change the RST_n_FUNCTION field of the specified device WARNING: This is a write-once field and 0 / 1 / 2 are the only valid values. mmc setdsr - set DSR register value Booting from eMMC ... Wrong Image Format for bootm command ERROR: can't get kernel image! =>