| module ti.uia.events.UIABenchmark |
 |
 |
 |
UIA Benchmark Events
The UIABenchmark module defines events that allow
tooling to analyze the performance of the software
(processing time, latency, etc.)
[
more ... ]
#include <ti/uia/events/UIABenchmark.h>
Functions common to all target modules |
|
|
Constants |
| |
| |
| |
| |
DETAILS
The UIABenchmark module defines events that allow
tooling to analyze the performance of the software
(processing time, latency, etc.)
The generation of UIABenchmark events is controlled by a module's diagnostics
mask, which is described in detail in
xdc.runtime.Diags.
UIABenchmark events are generated only when the Diags.ANALYSIS bit is set
in the module's diagnostics mask.
The following configuration script demonstrates how the application might
control the logging of ANALYSIS events embedded in the Mod module at configuration
time. In this case, the configuration script arranges for the Log
statements within modules to always generate ANALYSIS events.
Without these configuration statements, no ANALYSIS events would be generated
by any modules.
EXAMPLES
Example 1: This is part of the XDC configuration file for the application:
var UIABenchmark = xdc.useModule('ti.uia.events.UIABenchmark');
var Diags = xdc.useModule('xdc.runtime.Diags');
var LoggerSys = xdc.useModule('xdc.runtime.LoggerSys');
var Defaults = xdc.useModule('xdc.runtime.Defaults');
var logger = LoggerSys.create();
Defaults.common$.diags_ANALYSIS = Diags.ALWAYS_ON;
Defaults.common$.logger = logger;
Example 2: The following example configures a module to support logging
of ANALYSIS events, but defers the actual activation and deactivation of the
logging until runtime. See the
Diags_setMask()
function for details on specifying the control string.
This is a part of the XDC configuration file for the application:
var UIABenchmark = xdc.useModule('ti.uia.events.UIABenchmark');
var Diags = xdc.useModule('xdc.runtime.Diags');
var Mod = xdc.useModule('my.pkg.Mod');
Mod.common$.diags_ANALYSIS = Diags.RUNTIME_OFF;
This is a part of the C code for the application:
// turn on logging of ANALYSIS events in the module
Diags_setMask("my.pkg.Mod+Z");
// turn off logging of ANALYSIS events in the module
Diags_setMask("my.pkg.Mod-Z");
| config UIABenchmark_start // module-wide |
 |
Benchmark event used to log the start of an operation
VALUES
fmt
a constant string that provides format specifiers for up to 7 additional parameters
EXAMPLE
The following C code shows how to log a simple
benchmark 'start' event along with a user-specified
format string describing the event.
#include <xdc/runtime/Log.h>
#include <ti/uia/events/UIABenchmark.h>
...
Log_write1(UIABenchmark_start, (IArg)"My benchmark event");
The following text will be displayed for the event:
Start: My benchmark event
| config UIABenchmark_startInstance // module-wide |
 |
Benchmark event used to log the start of an operation instance
extern const Log_Event UIABenchmark_startInstance;
VALUES
fmt
a constant string that provides format specifiers for up to 6 additional parameters
instanceId
a unique instance ID that can be used to match benchmark start and stop events
DETAILS
Event parameter provides instance data to differentiate
between multiple instances that can run in parallel.
EXAMPLE
The following C code shows how to log a benchmark
'startInstance' event along with a user-specified
instance identifier and a format string describing the event.
#include <xdc/runtime/Gate.h>
#include <xdc/runtime/Log.h>
#include <ti/uia/events/UIABenchmark.h>
static volatile int gMyGlobalInstanceId = 0;
...
IArg key;
int localInstanceId;
// protect pre-increment operation from race conditions
key = Gate_enterSystem();
localInstanceId = ++gMyGlobalInstanceId;
Gate_leaveSystem(key);
Log_write2(UIABenchmark_startInstance, (IArg)"My benchmark event: instanceId=%d",localInstanceId);
...
Log_write2(UIABenchmark_stopInstance, (IArg)"My benchmark event: instanceId=%d",localInstanceId);
The following text will be displayed for the event:
StartInstance: My benchmark event: instanceId=1
StopInstance: My benchmark event: instanceId=1
| config UIABenchmark_stop // module-wide |
 |
Benchmark event used to log the end of an operation
VALUES
fmt
a constant string that provides format specifiers for up to 7 additional parameters
EXAMPLE
The following C code shows how to log a simple
benchmark 'stop' event along with a user-specified
format string describing the event.
#include <xdc/runtime/Log.h>
#include <ti/uia/events/UIABenchmark.h>
...
Log_write1(UIABenchmark_stop, (IArg)"My benchmark event");
The following text will be displayed for the event:
| config UIABenchmark_stopInstance // module-wide |
 |
Benchmark event used to log the end of an operation instance
extern const Log_Event UIABenchmark_stopInstance;
VALUES
fmt
a constant string that provides format specifiers for up to 6 additional parameters
instanceId
a unique instance ID that can be used to match benchmark start and stop events
DETAILS
Event parameter provides instance data to differentiate
between multiple instances that can run in parallel.
EXAMPLE
The following C code shows how to log a benchmark
'stopInstance' event along with a user-specified
instance identifier and a format string describing the event.
#include <xdc/runtime/Gate.h>
#include <xdc/runtime/Log.h>
#include <ti/uia/events/UIABenchmark.h>
static volatile int gMyGlobalInstanceId = 0;
...
IArg key;
int localInstanceId;
// protect pre-increment operation from race conditions
key = Gate_enterSystem();
localInstanceId = ++gMyGlobalInstanceId;
Gate_leaveSystem(key);
Log_write2(UIABenchmark_startInstance, (IArg)"My benchmark event: instanceId=%d",localInstanceId);
...
Log_write2(UIABenchmark_stopInstance, (IArg)"My benchmark event: instanceId=%d",localInstanceId);
The following text will be displayed for the event:
StartInstance: My benchmark event: instanceId=1
StopInstance: My benchmark event: instanceId=1
| Module-Wide Built-Ins |
 |
// Get this module's unique id
Bool UIABenchmark_Module_startupDone();
// Test if this module has completed startup
// The heap from which this module allocates memory
Bool UIABenchmark_Module_hasMask();
// Test whether this module has a diagnostics mask
Bits16 UIABenchmark_Module_getMask();
// Returns the diagnostics mask for this module
Void UIABenchmark_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
var UIABenchmark = xdc.useModule('ti.uia.events.UIABenchmark');
module-wide config parameters
msg: "Start: %$S "
};
msg: "StartInstance: %$S "
};
msg: "Stop: %$S "
};
msg: "StopInstance: %$S "
};
| config UIABenchmark.start // module-wide |
 |
Benchmark event used to log the start of an operation
VALUES
fmt
a constant string that provides format specifiers for up to 7 additional parameters
EXAMPLE
The following C code shows how to log a simple
benchmark 'start' event along with a user-specified
format string describing the event.
#include <xdc/runtime/Log.h>
#include <ti/uia/events/UIABenchmark.h>
...
Log_write1(UIABenchmark_start, (IArg)"My benchmark event");
The following text will be displayed for the event:
Start: My benchmark event
C SYNOPSIS
| config UIABenchmark.startInstance // module-wide |
 |
Benchmark event used to log the start of an operation instance
msg: "StartInstance: %$S "
};
VALUES
fmt
a constant string that provides format specifiers for up to 6 additional parameters
instanceId
a unique instance ID that can be used to match benchmark start and stop events
DETAILS
Event parameter provides instance data to differentiate
between multiple instances that can run in parallel.
EXAMPLE
The following C code shows how to log a benchmark
'startInstance' event along with a user-specified
instance identifier and a format string describing the event.
#include <xdc/runtime/Gate.h>
#include <xdc/runtime/Log.h>
#include <ti/uia/events/UIABenchmark.h>
static volatile int gMyGlobalInstanceId = 0;
...
IArg key;
int localInstanceId;
// protect pre-increment operation from race conditions
key = Gate_enterSystem();
localInstanceId = ++gMyGlobalInstanceId;
Gate_leaveSystem(key);
Log_write2(UIABenchmark_startInstance, (IArg)"My benchmark event: instanceId=%d",localInstanceId);
...
Log_write2(UIABenchmark_stopInstance, (IArg)"My benchmark event: instanceId=%d",localInstanceId);
The following text will be displayed for the event:
StartInstance: My benchmark event: instanceId=1
StopInstance: My benchmark event: instanceId=1
C SYNOPSIS
| config UIABenchmark.stop // module-wide |
 |
Benchmark event used to log the end of an operation
VALUES
fmt
a constant string that provides format specifiers for up to 7 additional parameters
EXAMPLE
The following C code shows how to log a simple
benchmark 'stop' event along with a user-specified
format string describing the event.
#include <xdc/runtime/Log.h>
#include <ti/uia/events/UIABenchmark.h>
...
Log_write1(UIABenchmark_stop, (IArg)"My benchmark event");
The following text will be displayed for the event:
C SYNOPSIS
| config UIABenchmark.stopInstance // module-wide |
 |
Benchmark event used to log the end of an operation instance
msg: "StopInstance: %$S "
};
VALUES
fmt
a constant string that provides format specifiers for up to 6 additional parameters
instanceId
a unique instance ID that can be used to match benchmark start and stop events
DETAILS
Event parameter provides instance data to differentiate
between multiple instances that can run in parallel.
EXAMPLE
The following C code shows how to log a benchmark
'stopInstance' event along with a user-specified
instance identifier and a format string describing the event.
#include <xdc/runtime/Gate.h>
#include <xdc/runtime/Log.h>
#include <ti/uia/events/UIABenchmark.h>
static volatile int gMyGlobalInstanceId = 0;
...
IArg key;
int localInstanceId;
// protect pre-increment operation from race conditions
key = Gate_enterSystem();
localInstanceId = ++gMyGlobalInstanceId;
Gate_leaveSystem(key);
Log_write2(UIABenchmark_startInstance, (IArg)"My benchmark event: instanceId=%d",localInstanceId);
...
Log_write2(UIABenchmark_stopInstance, (IArg)"My benchmark event: instanceId=%d",localInstanceId);
The following text will be displayed for the event:
StartInstance: My benchmark event: instanceId=1
StopInstance: My benchmark event: instanceId=1
C SYNOPSIS
| metaonly config UIABenchmark.common$ // module-wide |
 |
Common module configuration parameters
DETAILS
All modules have this configuration parameter. Its name
contains the '$' character to ensure it does not conflict with
configuration parameters declared by the module. This allows
new configuration parameters to be added in the future without
any chance of breaking existing modules.
generated on Tue, 17 Oct 2017 18:21:07 GMT