| module ti.uia.events.UIAEvt |
 |
 |
 |
UIA Standard Events
The UIAEvt module defines events that allow
tooling to display event information
and filter events based on their priority.
[
more ... ]
#include <ti/uia/events/UIAEvt.h>
Functions common to all target modules |
|
|
Constants |
| |
| |
| |
| |
| |
| |
| |
DETAILS
The UIAEvt module defines events that allow
tooling to display event information
and filter events based on their priority.
The events in this module have one of the following event priority levels:
WARNING: used to indicate an unexpected or problematic situation such as when a resource
becomes dangerously low
INFO: used to indicate something of interest or of use in understanding the
current state of the system or behaviour of the software
DETAIL: used to indicate additional information that may be of interest
in troubleshooting problems or improving the software
For each priority level, two predefined event codes
are provided: one for logging a single event code,
and one for logging an event code along with a
reference to a constant formatting string that can
be used to format the text displayed for the event.
The formatting string allows additional arguments
to be displayed along with the event code when the
event is rendered as text (e.g. by DVT).
The following special formatting specifiers may be used in the
msg field of an event's config specification:
%$S - a string parameter that can provide additional formatting specifiers
Note that $S use in strings passed in as a paramter is not supported.
%$F - a specifier for a string parameter containing the file name (__FILE__) and
an integer parameter containing the line number (__LINE__).
The generation of UIAEvt events is controlled by a module's diagnostics
mask, which is described in details in
xdc.runtime.Diags.
UIAEvt warning events are generated only when the Diags.STATUS bit is set
in the module's diagnostics mask. The Diags.STATUS bit is set to ALWAYS_ON
by default. 'UIAEvt' info and detail events are generated only when the
Diags.INFO bit is set in the module's diagnostics mask.
The following configuration script demonstrates how to enable use of
UIAEvt events within an application. Since the Diags.STATUS bits are set
to ALWAYS_ON by default, no explicit code is required to enable the
Diags Masks for these events. The Diags.INFO bitmust be explicitly set
in order to enable info and detail level events.
This is part of the XDC configuration file for the application:
var UIAEvt = xdc.useModule('ti.uia.events.UIAEvt');
var Diags = xdc.useModule('xdc.runtime.Diags');
var LoggerSys = xdc.useModule('xdc.runtime.LoggerSys');
var Defaults = xdc.useModule('xdc.runtime.Defaults');
var logger = LoggerSys.create();
Defaults.common$.logger = logger;
Defaults.common$.diags_INFO = Diags.ALWAYS_ON;
Example 2: The following example configures a module to support logging
of STATUS events and INFO events, but defers the actual activation and deactivation of the
logging until runtime. See the
Diags_setMask()
function for details on specifying the control string.
This is a part of the XDC configuration file for the application:
var UIAEvt = xdc.useModule('ti.uia.events.UIAEvt');
var Diags = xdc.useModule('xdc.runtime.Diags');
var Mod = xdc.useModule('my.pkg.Mod');
Mod.common$.diags_STATUS = Diags.RUNTIME_OFF;
Mod.common$.diags_INFO = Diags.RUNTIME_OFF;
This is a part of the C code for the application:
// turn on logging of STATUS events (S) and INFO events (F)
// in the module
Diags_setMask("my.pkg.Mod+SF");
// turn off logging of STATUS events and INFO events in the module
Diags_setMask("my.pkg.Mod-SF");
| config UIAEvt_detail // module-wide |
 |
Event to use to log a Detail-level Event Code
VALUES
eventCode
integer that identifies the specific detail event being logged
EXAMPLE
The following C code shows how to log a detail-level event code as a UIA event.
#include <xdc/runtime/Log.h>
#include <ti/uia/events/UIAEvt.h>
...
Int myEventCode = 0xE1;
...
Log_write1(UIAEvt_detail, myEventCode);
...
The following text is an example of what will be displayed for the event:
"DETAIL: EventCode:0xE1."
SEE
| config UIAEvt_detailWithStr // module-wide |
 |
Event to use to log a Detail-level Event Code and fmt string
VALUES
eventCode
integer that identifies the specific detail event being logged
fmt
a constant string that provides format specifiers for up to 6 additional parameters
EXAMPLE
The following C code shows how to log a detail-level event code
and format string as a UIA event. It also shows how additional parameters
can be logged along with the event and format string.
#include <xdc/runtime/Log.h>
#include <ti/uia/events/UIAEvt.h>
...
Int myEventCode = 0xE1;
Int anAdditionalParam = 0x6543;
...
Log_write3(UIAEvt_detailWithStr, myEventCode,(IArg)"Descriptive text. anAdditionalParam=0x%x.",anAdditionalParam);
...
The following text is an example of what will be displayed for the event:
"DETAIL: EventCode:0xE1. Some descriptive text. anAdditionalParam=0x6543."
SEE
| config UIAEvt_info // module-wide |
 |
Event to use to log an Informational Event Code
VALUES
eventCode
integer that identifies the type of info event
EXAMPLE
The following C code shows how to log an informational event code as a UIA event.
#include <xdc/runtime/Log.h>
#include <ti/uia/events/UIAEvt.h>
...
Int myInfoCode = 0xC0DE;
...
Log_write1(UIAEvt_info, myInfoCode);
...
The following text is an example of what will be displayed for the event:
"INFO: EventCode:0xC0DE."
SEE
| config UIAEvt_infoWithStr // module-wide |
 |
Event to use to log a Informational Event Code and format string
VALUES
eventCode
integer that identifies the specific info event being logged
fmt
a constant string that provides format specifiers for up to 6 additional parameters
EXAMPLE
The following C code shows how to log an informational event code
and format string as a UIA event. It also shows how additional parameters
can be logged along with the event and format string.
#include <xdc/runtime/Log.h>
#include <ti/uia/events/UIAEvt.h>
...
Int myInfoCode = 0xC0DE;
Int anAdditionalParam = 0x6543;
...
Log_write3(UIAEvt_infoWithStr, myInfoCode,(IArg)"Descriptive text. anAdditionalParam=0x%x.",anAdditionalParam);
...
The following text is an example of what will be displayed for the event:
"INFO: EventCode:0xC0DE. Some descriptive text. anAdditionalParam=0x6543."
SEE
| config UIAEvt_intWithKey // module-wide |
 |
Event to use to log values to be analyzed as Statistics and / or Graphs
VALUES
value
integer value that is to be analyzed
auxData1
auxiliary data that is to be displayed along with the event (use 0 if none)
auxData2
auxiliary data that is to be displayed along with the event (use 0 if none)
key
a constant string that provides format specifiers for up to 4 key entries
EXAMPLE
Example 1:
The following C code shows how to log an intWithKey event code
that logs a value, a format string that defines the key, and
parameters for use within the key format string.
#include <xdc/runtime/Log.h>
#include <ti/uia/events/UIAEvt.h>
...
Int myValue = 1001;
Int myInstanceId = 0x6543;
...
Log_write5(UIAEvt_intWithKey, myValue,0,0,(IArg)"InstanceId=0x%x.",myInstanceId);
...
The following text is an example of what will be displayed for the event:
"VALUE=1001 (AuxData=0,0) Key: InstanceId=0x6543."
Example 2:
The following C code shows how to log an intWithKey event code
that logs a value, a format string that defines the key, and
parameters for use within the key format string, including
the file name and line of code that the event was logged at.
This example uses a special format specifier, %$F, which
is used to format two parameters (__FILE__ and __LINE__)
in a way that tools will be able to display the line of code
that the event was logged from in a source code editor
when the user clicks on the event.
#include <xdc/runtime/Log.h>
#include <ti/uia/events/UIAEvt.h>
...
Int myValue = 1001;
Int myInstanceId = 9876;
...
Log_write7(UIAEvt_intWithKey, myValue,0,0,(IArg)"InstanceId=%d, at %$F.",
myInstanceId,(IArg)__FILE__,(IArg)__LINE__);
...
// If you wish to log only the line number as a key, use the following:
Log_write6(UIAEvt_intWithKey, myValue+1,0,0,(IArg)"InstanceId=%d, at line %d.",
myInstanceId,(IArg)__LINE__);
...
// If you wish to log only the file name as a key and the line number
// as auxiliary data which is logged along with the event, use the following:
Log_write6(UIAEvt_intWithKey, myValue+2,(IArg)__LINE__,0,(IArg)"InstanceId=%d, in file [%s].",
myInstanceId,(IArg)__FILE__);
The following text is an example of what will be displayed for the event,
assuming it was logged from a file named demo.c at line 1234:
"VALUE=1001 (AuxData=0,0) Key: InstanceId=9876, at [../demo.c:1234] ."
"VALUE=1002 (AuxData=0,0) Key: InstanceId=9876, at line 1234."
"VALUE=1003 (AuxData=1234,0) Key: InstanceId=9876, in file [../demo.c]."
| config UIAEvt_warning // module-wide |
 |
Event to use to log a Warning Event Code
VALUES
eventCode
integer that identifies the type of warning
fmt
a constant string that provides format specifiers for up to 6 additional parameters
EXAMPLE
The following C code shows how to log a legacy warning code as a UIA event.
#include <xdc/runtime/Log.h>
#include <ti/uia/events/UIAEvt.h>
...
Int myWarningCode = 0xBAD;
...
Log_write1(UIAEvt_warning, myWarningCode);
...
The following text is an example of what will be displayed for the event:
"WARNING: EventCode:0xBAD."
SEE
| config UIAEvt_warningWithStr // module-wide |
 |
Event to use to log a Warning Event Code and fmt string
extern const Log_Event UIAEvt_warningWithStr;
VALUES
eventCode
integer that identifies the type of warning event
fmt
a constant string that provides format specifiers for up to 6 additional parameters
EXAMPLE
The following C code shows how to log a legacy warning code and string as a UIA event.
#include <xdc/runtime/Log.h>
#include <ti/uia/events/UIAEvt.h>
...
Int myWarningCode = 0xBAD;
String myWarningStr = "Legacy Warning String for warning 0xBAD";
...
Log_write2(UIAEvt_warning,myWarningCode,(IArg)myWarningStr);
...
The following text is an example of what will be displayed for the event:
"WARNING: EventCode:0xBAD. Legacy Warning String for warning 0xBAD"
SEE
| Module-Wide Built-Ins |
 |
// Get this module's unique id
Bool UIAEvt_Module_startupDone();
// Test if this module has completed startup
// The heap from which this module allocates memory
Bool UIAEvt_Module_hasMask();
// Test whether this module has a diagnostics mask
Bits16 UIAEvt_Module_getMask();
// Returns the diagnostics mask for this module
Void UIAEvt_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
var UIAEvt = xdc.useModule('ti.uia.events.UIAEvt');
module-wide config parameters
msg: "DETAIL: EventCode:0x%x"
};
msg: "DETAIL: EventCode:0x%x. %$S"
};
msg: "INFO: EventCode: 0x%x"
};
msg: "INFO: EventCode:0x%x. %$S"
};
msg: "VALUE=%d (AuxData=%d, %d) Key:%$S"
};
msg: "WARNING: EventCode:0x%x"
};
msg: "WARNING: EventCode:0x%x. %$S"
};
| config UIAEvt.detail // module-wide |
 |
Event to use to log a Detail-level Event Code
msg: "DETAIL: EventCode:0x%x"
};
VALUES
eventCode
integer that identifies the specific detail event being logged
EXAMPLE
The following C code shows how to log a detail-level event code as a UIA event.
#include <xdc/runtime/Log.h>
#include <ti/uia/events/UIAEvt.h>
...
Int myEventCode = 0xE1;
...
Log_write1(UIAEvt_detail, myEventCode);
...
The following text is an example of what will be displayed for the event:
"DETAIL: EventCode:0xE1."
SEE
C SYNOPSIS
| config UIAEvt.detailWithStr // module-wide |
 |
Event to use to log a Detail-level Event Code and fmt string
msg: "DETAIL: EventCode:0x%x. %$S"
};
VALUES
eventCode
integer that identifies the specific detail event being logged
fmt
a constant string that provides format specifiers for up to 6 additional parameters
EXAMPLE
The following C code shows how to log a detail-level event code
and format string as a UIA event. It also shows how additional parameters
can be logged along with the event and format string.
#include <xdc/runtime/Log.h>
#include <ti/uia/events/UIAEvt.h>
...
Int myEventCode = 0xE1;
Int anAdditionalParam = 0x6543;
...
Log_write3(UIAEvt_detailWithStr, myEventCode,(IArg)"Descriptive text. anAdditionalParam=0x%x.",anAdditionalParam);
...
The following text is an example of what will be displayed for the event:
"DETAIL: EventCode:0xE1. Some descriptive text. anAdditionalParam=0x6543."
SEE
C SYNOPSIS
| config UIAEvt.info // module-wide |
 |
Event to use to log an Informational Event Code
msg: "INFO: EventCode: 0x%x"
};
VALUES
eventCode
integer that identifies the type of info event
EXAMPLE
The following C code shows how to log an informational event code as a UIA event.
#include <xdc/runtime/Log.h>
#include <ti/uia/events/UIAEvt.h>
...
Int myInfoCode = 0xC0DE;
...
Log_write1(UIAEvt_info, myInfoCode);
...
The following text is an example of what will be displayed for the event:
"INFO: EventCode:0xC0DE."
SEE
C SYNOPSIS
| config UIAEvt.infoWithStr // module-wide |
 |
Event to use to log a Informational Event Code and format string
msg: "INFO: EventCode:0x%x. %$S"
};
VALUES
eventCode
integer that identifies the specific info event being logged
fmt
a constant string that provides format specifiers for up to 6 additional parameters
EXAMPLE
The following C code shows how to log an informational event code
and format string as a UIA event. It also shows how additional parameters
can be logged along with the event and format string.
#include <xdc/runtime/Log.h>
#include <ti/uia/events/UIAEvt.h>
...
Int myInfoCode = 0xC0DE;
Int anAdditionalParam = 0x6543;
...
Log_write3(UIAEvt_infoWithStr, myInfoCode,(IArg)"Descriptive text. anAdditionalParam=0x%x.",anAdditionalParam);
...
The following text is an example of what will be displayed for the event:
"INFO: EventCode:0xC0DE. Some descriptive text. anAdditionalParam=0x6543."
SEE
C SYNOPSIS
| config UIAEvt.intWithKey // module-wide |
 |
Event to use to log values to be analyzed as Statistics and / or Graphs
msg: "VALUE=%d (AuxData=%d, %d) Key:%$S"
};
VALUES
value
integer value that is to be analyzed
auxData1
auxiliary data that is to be displayed along with the event (use 0 if none)
auxData2
auxiliary data that is to be displayed along with the event (use 0 if none)
key
a constant string that provides format specifiers for up to 4 key entries
EXAMPLE
Example 1:
The following C code shows how to log an intWithKey event code
that logs a value, a format string that defines the key, and
parameters for use within the key format string.
#include <xdc/runtime/Log.h>
#include <ti/uia/events/UIAEvt.h>
...
Int myValue = 1001;
Int myInstanceId = 0x6543;
...
Log_write5(UIAEvt_intWithKey, myValue,0,0,(IArg)"InstanceId=0x%x.",myInstanceId);
...
The following text is an example of what will be displayed for the event:
"VALUE=1001 (AuxData=0,0) Key: InstanceId=0x6543."
Example 2:
The following C code shows how to log an intWithKey event code
that logs a value, a format string that defines the key, and
parameters for use within the key format string, including
the file name and line of code that the event was logged at.
This example uses a special format specifier, %$F, which
is used to format two parameters (__FILE__ and __LINE__)
in a way that tools will be able to display the line of code
that the event was logged from in a source code editor
when the user clicks on the event.
#include <xdc/runtime/Log.h>
#include <ti/uia/events/UIAEvt.h>
...
Int myValue = 1001;
Int myInstanceId = 9876;
...
Log_write7(UIAEvt_intWithKey, myValue,0,0,(IArg)"InstanceId=%d, at %$F.",
myInstanceId,(IArg)__FILE__,(IArg)__LINE__);
...
// If you wish to log only the line number as a key, use the following:
Log_write6(UIAEvt_intWithKey, myValue+1,0,0,(IArg)"InstanceId=%d, at line %d.",
myInstanceId,(IArg)__LINE__);
...
// If you wish to log only the file name as a key and the line number
// as auxiliary data which is logged along with the event, use the following:
Log_write6(UIAEvt_intWithKey, myValue+2,(IArg)__LINE__,0,(IArg)"InstanceId=%d, in file [%s].",
myInstanceId,(IArg)__FILE__);
The following text is an example of what will be displayed for the event,
assuming it was logged from a file named demo.c at line 1234:
"VALUE=1001 (AuxData=0,0) Key: InstanceId=9876, at [../demo.c:1234] ."
"VALUE=1002 (AuxData=0,0) Key: InstanceId=9876, at line 1234."
"VALUE=1003 (AuxData=1234,0) Key: InstanceId=9876, in file [../demo.c]."
C SYNOPSIS
| config UIAEvt.warning // module-wide |
 |
Event to use to log a Warning Event Code
msg: "WARNING: EventCode:0x%x"
};
VALUES
eventCode
integer that identifies the type of warning
fmt
a constant string that provides format specifiers for up to 6 additional parameters
EXAMPLE
The following C code shows how to log a legacy warning code as a UIA event.
#include <xdc/runtime/Log.h>
#include <ti/uia/events/UIAEvt.h>
...
Int myWarningCode = 0xBAD;
...
Log_write1(UIAEvt_warning, myWarningCode);
...
The following text is an example of what will be displayed for the event:
"WARNING: EventCode:0xBAD."
SEE
C SYNOPSIS
| config UIAEvt.warningWithStr // module-wide |
 |
Event to use to log a Warning Event Code and fmt string
msg: "WARNING: EventCode:0x%x. %$S"
};
VALUES
eventCode
integer that identifies the type of warning event
fmt
a constant string that provides format specifiers for up to 6 additional parameters
EXAMPLE
The following C code shows how to log a legacy warning code and string as a UIA event.
#include <xdc/runtime/Log.h>
#include <ti/uia/events/UIAEvt.h>
...
Int myWarningCode = 0xBAD;
String myWarningStr = "Legacy Warning String for warning 0xBAD";
...
Log_write2(UIAEvt_warning,myWarningCode,(IArg)myWarningStr);
...
The following text is an example of what will be displayed for the event:
"WARNING: EventCode:0xBAD. Legacy Warning String for warning 0xBAD"
SEE
C SYNOPSIS
| metaonly config UIAEvt.common$ // module-wide |
 |
Common module configuration parameters
DETAILS
All modules have this configuration parameter. Its name
contains the '$' character to ensure it does not conflict with
configuration parameters declared by the module. This allows
new configuration parameters to be added in the future without
any chance of breaking existing modules.
generated on Tue, 17 Oct 2017 18:21:07 GMT