module ti.uia.events.UIAHWICtx

UIA Hardware Interrupt Context Instrumentation

The UIAHWICtx module defines context change events and methods that allow tooling to identify hardware interrupt context switches and to enable HWI-aware filtering, trace and analysis. [ more ... ]
C synopsis target-domain sourced in ti/uia/events/UIAHWICtx.xdc
DETAILS
The UIAHWICtx module defines context change events and methods that allow tooling to identify hardware interrupt context switches and to enable HWI-aware filtering, trace and analysis.
Note: in order to reduce overhead, UIAHWICtx does not support context-aware filtering
The following configuration script demonstrates how the application might control the logging of ANALYSIS events embedded in the Mod module at configuration time. In this case, the configuration script arranges for the Log statements within modules to always generate ANALYSIS events. Without these configuration statements, no ANALYSIS events would be generated by any modules.
EXAMPLES
Example 1: This is part of the XDC configuration file for the application:
  var LogCtxChg = xdc.useModule('ti.uia.runtime.LogCtxChg');
  var Diags = xdc.useModule('xdc.runtime.Diags');
  var LoggerSys = xdc.useModule('xdc.runtime.LoggerSys');
  var Defaults = xdc.useModule('xdc.runtime.Defaults');
  var logger = LoggerSys.create();

  Defaults.common$.diags_ANALYSIS = Diags.ALWAYS_ON;
  Defaults.common$.logger = logger;

  // BIOS specific configuration:
  var Hwi = xdc.useModule('ti.sysbios.hal.Hwi');
  Hwi.addHookSet({
    beginFxn: '&hwiBeginHook',
    endFxn: '&hwiEndHook'
   });

Example 2: The following example configures a module to support logging of ANALYSIS events, but defers the actual activation and deactivation of the logging until runtime. See the Diags_setMask() function for details on specifying the control string.
This is a part of the XDC configuration file for the application:
  var LogCtxChg = xdc.useModule('ti.uia.runtime.LogCtxChg');
  var Diags = xdc.useModule('xdc.runtime.Diags');
  var Mod = xdc.useModule('my.pkg.Mod');

  Mod.common$.diags_ANALYSIS = Diags.RUNTIME_OFF;
This is a part of the C code for the application:
  // turn on logging of ANALYSIS events in the module
  Diags_setMask("my.pkg.Mod+Z");

  // turn off logging of ANALYSIS events in the module
  Diags_setMask("my.pkg.Mod-Z");
 
typedef UIAHWICtx_IsLoggingEnabledFxn
C synopsis target-domain
typedef Bool (*UIAHWICtx_IsLoggingEnabledFxn)(Int);
 
 
config UIAHWICtx_ENABLEMASK  // module-wide

Ctx Filter Enable Mask

C synopsis target-domain
extern const Bits16 UIAHWICtx_ENABLEMASK;
 
DETAILS
configures which bit of the ti_uia_runtime_CtxFilter_gFlags is assigned to control context aware filtering for frame context changes. Must be configured with a value that is 2**SYNCID.
 
config UIAHWICtx_SYNCID  // module-wide

Trace Synchronization ID

C synopsis target-domain
extern const Bits16 UIAHWICtx_SYNCID;
 
DETAILS
configures the value to be written into the 4 bit context change type field used by the UIASync trace synchronization
 
config UIAHWICtx_isLoggingEnabledFxn  // module-wide
C synopsis target-domain
extern const IUIACtx_IsLoggingEnabledFxn UIAHWICtx_isLoggingEnabledFxn;
 
 
config UIAHWICtx_start  // module-wide

Hardware Interrupt start event

C synopsis target-domain
extern const Log_Event UIAHWICtx_start;
 
VALUES
fmt — a constant string that describes the HWI and provides a format specifier for the HWI handle
handle — an integer which uniquely identifies the HWI
DETAILS
Used to log the start of a hardware interrupt service routine
EXAMPLE
The following C code shows how to log a Context Change event that identifies the start of a HWI. It implements a BIOS hook function. Alternatively, the LogCtxChg_hwiStart API can be called directly from the HWI service routine.
  #include <ti/uia/runtime/LogCtxChg.h>
   ...
  Void hwiBeginHook(Hwi_Handle handle) {
    LogCtxChg_hwiStart("Hwi_Handle:0x%x",handle);
  }
This event has an associated format string (%$S) which is recursively formatted with any addition arguments. The following text is an example of what will be displayed for the event:
  "HWI start: Hwi_Handle:0x80001200"

 
config UIAHWICtx_stop  // module-wide

Hardware Interrupt exit event

C synopsis target-domain
extern const Log_Event UIAHWICtx_stop;
 
VALUES
fmt — a constant string that describes the HWI and provides a format specifier for the HWI handle
handle — an integer which uniquely identifies the HWI
DETAILS
Used to log the end of a hardware interrupt service routine
EXAMPLE
The following C code shows how to log a Context Change event that identifies the end of a HWI. It implements a BIOS hook function. Alternatively, the LogCtxChg_hwiStop API can be called directly from the HWI service routine.
  #include <ti/uia/runtime/LogCtxChg.h>
   ...
  Void hwiEndHook(Hwi_Handle handle) {
    LogCtxChg_hwiStop("Hwi_Handle:0x%x",handle);
  }
This event has an associated format string (%$S) which is recursively formatted with any addition arguments. The following text is an example of what will be displayed for the event:
  "HWI stop: Hwi_Handle:0x80001200"

Module-Wide Built-Ins

C synopsis target-domain
Types_ModuleId UIAHWICtx_Module_id();
// Get this module's unique id
 
Bool UIAHWICtx_Module_startupDone();
// Test if this module has completed startup
 
IHeap_Handle UIAHWICtx_Module_heap();
// The heap from which this module allocates memory
 
Bool UIAHWICtx_Module_hasMask();
// Test whether this module has a diagnostics mask
 
Bits16 UIAHWICtx_Module_getMask();
// Returns the diagnostics mask for this module
 
Void UIAHWICtx_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
 
Configuration settings sourced in ti/uia/events/UIAHWICtx.xdc
var UIAHWICtx = xdc.useModule('ti.uia.events.UIAHWICtx');
module-wide config parameters
    UIAHWICtx.SYNCID// Trace Synchronization ID = Bits16 undefined;
    UIAHWICtx.isLoggingEnabledFxn//  = Bool(*)(Int) null;
        mask: Diags.ANALYSIS,
        msg: "HWI start: %$S"
    };
        mask: Diags.ANALYSIS,
        msg: "HWI stop: %$S"
    };
 
 
 
config UIAHWICtx.ENABLEMASK  // module-wide

Ctx Filter Enable Mask

Configuration settings
UIAHWICtx.ENABLEMASK = Bits16 undefined;
 
DETAILS
configures which bit of the ti_uia_runtime_CtxFilter_gFlags is assigned to control context aware filtering for frame context changes. Must be configured with a value that is 2**SYNCID.
C SYNOPSIS
 
config UIAHWICtx.SYNCID  // module-wide

Trace Synchronization ID

Configuration settings
UIAHWICtx.SYNCID = Bits16 undefined;
 
DETAILS
configures the value to be written into the 4 bit context change type field used by the UIASync trace synchronization
C SYNOPSIS
 
config UIAHWICtx.isLoggingEnabledFxn  // module-wide
Configuration settings
UIAHWICtx.isLoggingEnabledFxn = Bool(*)(Int) null;
 
C SYNOPSIS
 
config UIAHWICtx.start  // module-wide

Hardware Interrupt start event

Configuration settings
UIAHWICtx.start = Log.EventDesc {
    mask: Diags.ANALYSIS,
    msg: "HWI start: %$S"
};
 
VALUES
fmt — a constant string that describes the HWI and provides a format specifier for the HWI handle
handle — an integer which uniquely identifies the HWI
DETAILS
Used to log the start of a hardware interrupt service routine
EXAMPLE
The following C code shows how to log a Context Change event that identifies the start of a HWI. It implements a BIOS hook function. Alternatively, the LogCtxChg_hwiStart API can be called directly from the HWI service routine.
  #include <ti/uia/runtime/LogCtxChg.h>
   ...
  Void hwiBeginHook(Hwi_Handle handle) {
    LogCtxChg_hwiStart("Hwi_Handle:0x%x",handle);
  }
This event has an associated format string (%$S) which is recursively formatted with any addition arguments. The following text is an example of what will be displayed for the event:
  "HWI start: Hwi_Handle:0x80001200"

C SYNOPSIS
 
config UIAHWICtx.stop  // module-wide

Hardware Interrupt exit event

Configuration settings
UIAHWICtx.stop = Log.EventDesc {
    mask: Diags.ANALYSIS,
    msg: "HWI stop: %$S"
};
 
VALUES
fmt — a constant string that describes the HWI and provides a format specifier for the HWI handle
handle — an integer which uniquely identifies the HWI
DETAILS
Used to log the end of a hardware interrupt service routine
EXAMPLE
The following C code shows how to log a Context Change event that identifies the end of a HWI. It implements a BIOS hook function. Alternatively, the LogCtxChg_hwiStop API can be called directly from the HWI service routine.
  #include <ti/uia/runtime/LogCtxChg.h>
   ...
  Void hwiEndHook(Hwi_Handle handle) {
    LogCtxChg_hwiStop("Hwi_Handle:0x%x",handle);
  }
This event has an associated format string (%$S) which is recursively formatted with any addition arguments. The following text is an example of what will be displayed for the event:
  "HWI stop: Hwi_Handle:0x80001200"

C SYNOPSIS
 
metaonly config UIAHWICtx.common$  // module-wide

Common module configuration parameters

Configuration settings
UIAHWICtx.common$ = Types.Common$ undefined;
 
DETAILS
All modules have this configuration parameter. Its name contains the '$' character to ensure it does not conflict with configuration parameters declared by the module. This allows new configuration parameters to be added in the future without any chance of breaking existing modules.
generated on Tue, 17 Oct 2017 18:21:08 GMT