module ti.uia.events.UIAMessage

UIA Message Events

The UIAMessage module defines events that allow tooling to monitor messages between tasks and CPUs. [ more ... ]
C synopsis target-domain sourced in ti/uia/events/UIAMessage.xdc
DETAILS
The UIAMessage module defines events that allow tooling to monitor messages between tasks and CPUs.
The generation of UIAMessage events is controlled by a module's diagnostics mask, which is described in details in xdc.runtime.Diags. UIAMessage info events are generated only when the Diags.INFO bit is set in the module's diagnostics mask.
The following configuration script demonstrates how to enable use of UIAMessage events within an application. The Diags.INFO bitmust be explicitly set in order to enable these events.
This is part of the XDC configuration file for the application:
  var UIAMessage = xdc.useModule('ti.uia.events.UIAMessage');
  var Diags = xdc.useModule('xdc.runtime.Diags');
  var LoggerSys = xdc.useModule('xdc.runtime.LoggerSys');
  var Defaults = xdc.useModule('xdc.runtime.Defaults');
  var logger = LoggerSys.create();

  Defaults.common$.logger = logger;
  Defaults.common$.diags_INFO = Diags.ALWAYS_ON;

Example 2: The following example configures a module to support logging of STATUS events and INFO events, but defers the actual activation and deactivation of the logging until runtime. See the Diags_setMask() function for details on specifying the control string.
This is a part of the XDC configuration file for the application:
  var UIAMessage = xdc.useModule('ti.uia.events.UIAMessage');
  var Diags = xdc.useModule('xdc.runtime.Diags');
  var Mod = xdc.useModule('my.pkg.Mod');

  Mod.common$.diags_STATUS = Diags.RUNTIME_OFF;
  Mod.common$.diags_INFO = Diags.RUNTIME_OFF;
This is a part of the C code for the application:
  // turn on logging of STATUS events (S) and INFO events (F)
  // in the module
  Diags_setMask("my.pkg.Mod+SF");

  // turn off logging of STATUS events and INFO events in the module
  Diags_setMask("my.pkg.Mod-SF");
 
config UIAMessage_msgReceived  // module-wide

Message Received event

C synopsis target-domain
extern const Log_Event UIAMessage_msgReceived;
 
VALUES
NumBytes — length of the message in bytes
Flags — any flags associated with the message
MsgId — the message ID for the message
Destination ProcID — the procID for the message destination
Reply ProcID — the procID that the reply will be sent to
Source ProcID — the procID of the message sender
HeapId — the HeapID associated with the message
DETAILS
  #include <xdc/runtime/Log.h>
  #include <ti/uia/events/UIAMessage.h>
  ...
  Log_write7(UIAMessage_msgReceived, numBytes,flags,msgId,destProcId,replyProcId,srcProcId,heapId);
  ...
  "Msg Received [NumBytes]0x32 [Flags]0xF [MsgId]0x8357 [Dest(ProcID)]0x2 [Reply(ProcID)]0x3 [Src(ProcID)]0x1 [HeapId]0x56"

EXAMPLE
The following C code shows how to log a msgReceived event
 
config UIAMessage_msgSent  // module-wide

Message Sent event

C synopsis target-domain
extern const Log_Event UIAMessage_msgSent;
 
VALUES
NumBytes — length of the message in bytes
Flags — any flags associated with the message
MsgId — the message ID for the message
Destination ProcID — the procID for the message destination
Reply ProcID — the procID that the reply will be sent to
Source ProcID — the procID of the message sender
HeapId — the HeapID associated with the message
DETAILS
  #include <xdc/runtime/Log.h>
  #include <ti/uia/events/UIAMessage.h>
  ...
  Log_write7(UIAMessage_msgSent, numBytes,flags,msgId,destProcId,replyProcId,srcProcId,heapId);
  ...
  "Msg Sent [NumBytes]0x32 [Flags]0xF [MsgId]0x8357 [Dest(ProcID)]0x2 [Reply(ProcID)]0x3 [Src(ProcID)]0x1 [HeapId]0x56"

EXAMPLE
The following C code shows how to log a msgSent event
 
config UIAMessage_replyReceived  // module-wide

Reply Received event

C synopsis target-domain
extern const Log_Event UIAMessage_replyReceived;
 
VALUES
MsgId — the message ID for the message
ReplyId — the reply's message ID
NumBytes — length of the message in bytes
Sender ProcID — the procID that the reply will be sent to
Destination ProcID — the procID for the message destination
DETAILS
  #include <xdc/runtime/Log.h>
  #include <ti/uia/events/UIAMessage.h>
  ...
  Log_write5(UIAMessage_replyReceived,msgId,replyId,numBytes,senderProcId,destProcId);
  ...
  "Msg Sent [MsgId]0x8357 [NumBytes]0x32 [Flags]0xF [Dest(ProcID)]0x2 [Reply(ProcID)]0x3 [Src(ProcID)]0x1 [HeapId]0x56"

EXAMPLE
The following C code shows how to log a msgSent event
 
config UIAMessage_replySent  // module-wide

Reply Sent event

C synopsis target-domain
extern const Log_Event UIAMessage_replySent;
 
VALUES
NumBytes — length of the message in bytes
Flags — any flags associated with the message
MsgId — the message ID for the message
Destination ProcID — the procID for the message destination
Reply ProcID — the procID that the reply will be sent to
Source ProcID — the procID of the message sender
HeapId — the HeapID associated with the message
DETAILS
  #include <xdc/runtime/Log.h>
  #include <ti/uia/events/UIAMessage.h>
  ...
  Log_write7(UIAMessage_replySent, numBytes,flags,msgId,destProcId,replyProcId,srcProcId,heapId);
  ...
  "Reply Sent [NumBytes]0x32 [Flags]0xF [MsgId]0x8357 [Dest(ProcID)]0x2 [Reply(ProcID)]0x3 [Src(ProcID)]0x1 [HeapId]0x56"


EXAMPLE
The following C code shows how to log a msgSent event
Module-Wide Built-Ins

C synopsis target-domain
Types_ModuleId UIAMessage_Module_id();
// Get this module's unique id
 
Bool UIAMessage_Module_startupDone();
// Test if this module has completed startup
 
IHeap_Handle UIAMessage_Module_heap();
// The heap from which this module allocates memory
 
Bool UIAMessage_Module_hasMask();
// Test whether this module has a diagnostics mask
 
Bits16 UIAMessage_Module_getMask();
// Returns the diagnostics mask for this module
 
Void UIAMessage_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
 
Configuration settings sourced in ti/uia/events/UIAMessage.xdc
var UIAMessage = xdc.useModule('ti.uia.events.UIAMessage');
module-wide config parameters
        mask: Diags.INFO,
        msg: "Msg Received [NumBytes]0x%x [Flags]0x%x [MsgId]0x%x [Dest(ProcID)]0x%x [Reply(ProcID)]0x%x [Src(ProcID)]0x%x [HeapId]0x%x"
    };
        mask: Diags.INFO,
        msg: "Msg Sent [NumBytes]0x%x [Flags]0x%x [MsgId]0x%x [Dest(ProcID)]0x%x [Reply(ProcID)]0x%x [Src(ProcID)]0x%x [HeapId]0x%x"
    };
        mask: Diags.INFO,
        msg: "Reply Recieved [MsgId]0x%x [ReplyId]0x%x [NumBytes]0x%x [Sender]0x%x [Dest]0x%x "
    };
        mask: Diags.INFO,
        msg: "Reply Sent [NumBytes]0x%x [Flags]0x%x [MsgId]0x%x [Dest(ProcID)]0x%x [Reply(ProcID)]0x%x [Src(ProcID)]0x%x [HeapId]0x%x"
    };
 
 
 
config UIAMessage.msgReceived  // module-wide

Message Received event

Configuration settings
UIAMessage.msgReceived = Log.EventDesc {
    mask: Diags.INFO,
    msg: "Msg Received [NumBytes]0x%x [Flags]0x%x [MsgId]0x%x [Dest(ProcID)]0x%x [Reply(ProcID)]0x%x [Src(ProcID)]0x%x [HeapId]0x%x"
};
 
VALUES
NumBytes — length of the message in bytes
Flags — any flags associated with the message
MsgId — the message ID for the message
Destination ProcID — the procID for the message destination
Reply ProcID — the procID that the reply will be sent to
Source ProcID — the procID of the message sender
HeapId — the HeapID associated with the message
DETAILS
  #include <xdc/runtime/Log.h>
  #include <ti/uia/events/UIAMessage.h>
  ...
  Log_write7(UIAMessage_msgReceived, numBytes,flags,msgId,destProcId,replyProcId,srcProcId,heapId);
  ...
  "Msg Received [NumBytes]0x32 [Flags]0xF [MsgId]0x8357 [Dest(ProcID)]0x2 [Reply(ProcID)]0x3 [Src(ProcID)]0x1 [HeapId]0x56"

EXAMPLE
The following C code shows how to log a msgReceived event
C SYNOPSIS
 
config UIAMessage.msgSent  // module-wide

Message Sent event

Configuration settings
UIAMessage.msgSent = Log.EventDesc {
    mask: Diags.INFO,
    msg: "Msg Sent [NumBytes]0x%x [Flags]0x%x [MsgId]0x%x [Dest(ProcID)]0x%x [Reply(ProcID)]0x%x [Src(ProcID)]0x%x [HeapId]0x%x"
};
 
VALUES
NumBytes — length of the message in bytes
Flags — any flags associated with the message
MsgId — the message ID for the message
Destination ProcID — the procID for the message destination
Reply ProcID — the procID that the reply will be sent to
Source ProcID — the procID of the message sender
HeapId — the HeapID associated with the message
DETAILS
  #include <xdc/runtime/Log.h>
  #include <ti/uia/events/UIAMessage.h>
  ...
  Log_write7(UIAMessage_msgSent, numBytes,flags,msgId,destProcId,replyProcId,srcProcId,heapId);
  ...
  "Msg Sent [NumBytes]0x32 [Flags]0xF [MsgId]0x8357 [Dest(ProcID)]0x2 [Reply(ProcID)]0x3 [Src(ProcID)]0x1 [HeapId]0x56"

EXAMPLE
The following C code shows how to log a msgSent event
C SYNOPSIS
 
config UIAMessage.replyReceived  // module-wide

Reply Received event

Configuration settings
UIAMessage.replyReceived = Log.EventDesc {
    mask: Diags.INFO,
    msg: "Reply Recieved [MsgId]0x%x [ReplyId]0x%x [NumBytes]0x%x [Sender]0x%x [Dest]0x%x "
};
 
VALUES
MsgId — the message ID for the message
ReplyId — the reply's message ID
NumBytes — length of the message in bytes
Sender ProcID — the procID that the reply will be sent to
Destination ProcID — the procID for the message destination
DETAILS
  #include <xdc/runtime/Log.h>
  #include <ti/uia/events/UIAMessage.h>
  ...
  Log_write5(UIAMessage_replyReceived,msgId,replyId,numBytes,senderProcId,destProcId);
  ...
  "Msg Sent [MsgId]0x8357 [NumBytes]0x32 [Flags]0xF [Dest(ProcID)]0x2 [Reply(ProcID)]0x3 [Src(ProcID)]0x1 [HeapId]0x56"

EXAMPLE
The following C code shows how to log a msgSent event
C SYNOPSIS
 
config UIAMessage.replySent  // module-wide

Reply Sent event

Configuration settings
UIAMessage.replySent = Log.EventDesc {
    mask: Diags.INFO,
    msg: "Reply Sent [NumBytes]0x%x [Flags]0x%x [MsgId]0x%x [Dest(ProcID)]0x%x [Reply(ProcID)]0x%x [Src(ProcID)]0x%x [HeapId]0x%x"
};
 
VALUES
NumBytes — length of the message in bytes
Flags — any flags associated with the message
MsgId — the message ID for the message
Destination ProcID — the procID for the message destination
Reply ProcID — the procID that the reply will be sent to
Source ProcID — the procID of the message sender
HeapId — the HeapID associated with the message
DETAILS
  #include <xdc/runtime/Log.h>
  #include <ti/uia/events/UIAMessage.h>
  ...
  Log_write7(UIAMessage_replySent, numBytes,flags,msgId,destProcId,replyProcId,srcProcId,heapId);
  ...
  "Reply Sent [NumBytes]0x32 [Flags]0xF [MsgId]0x8357 [Dest(ProcID)]0x2 [Reply(ProcID)]0x3 [Src(ProcID)]0x1 [HeapId]0x56"


EXAMPLE
The following C code shows how to log a msgSent event
C SYNOPSIS
 
metaonly config UIAMessage.common$  // module-wide

Common module configuration parameters

Configuration settings
UIAMessage.common$ = Types.Common$ undefined;
 
DETAILS
All modules have this configuration parameter. Its name contains the '$' character to ensure it does not conflict with configuration parameters declared by the module. This allows new configuration parameters to be added in the future without any chance of breaking existing modules.
generated on Tue, 17 Oct 2017 18:21:08 GMT