module ti.uia.events.UIAThreadCtx

UIA Thread Context Instrumentation

The UIAThreadCtx module defines context change events and methods that allow tooling to identify thread context switches and to enable thread-aware filtering, trace and analysis. [ more ... ]
C synopsis target-domain sourced in ti/uia/events/UIAThreadCtx.xdc
#include <ti/uia/events/UIAThreadCtx.h>
Functions
UInt 
UInt 
Bool 
Void 
UInt 
Functions common to all target modules
Typedefs
typedef Bool 
Constants
extern const Log_Event 
extern const Log_Event 
extern const Bits16 
extern const Bits16 
 
DETAILS
The UIAThreadCtx module defines context change events and methods that allow tooling to identify thread context switches and to enable thread-aware filtering, trace and analysis.
It inherits IUIACtx, which defines a function pointer to an isLoggingEnabled function which, if configured to point to a function, will evaluate the function prior to logging the context change event and will determine whether to log the event based on the return value of the function. If the function is not configured, logging will be conditional upon ti_uia_runtime_CtxFilter_module->mIsLoggingEnabled.
The generation of UIAThreadCtx events is also controlled by a module's diagnostics mask, which is described in details in xdc.runtime.Diags. 'UIAThreadCtx` events are generated only when the Diags.ANALYSIS bit is set in the module's diagnostics mask.
The following configuration script demonstrates how the application might control the logging of ANALYSIS events embedded in the Mod module at configuration time. In this case, the configuration script arranges for the Log statements within modules to always generate ANALYSIS events. Without these configuration statements, no ANALYSIS events would be generated by any modules.
EXAMPLES
Example 1: This is part of the XDC configuration file for the application:
  var LogCtxChg = xdc.useModule('ti.uia.runtime.LogCtxChg');
  var Diags = xdc.useModule('xdc.runtime.Diags');
  var LoggerSys = xdc.useModule('xdc.runtime.LoggerSys');
  var Defaults = xdc.useModule('xdc.runtime.Defaults');
  var logger = LoggerSys.create();

  Defaults.common$.diags_ANALYSIS = Diags.ALWAYS_ON;
  Defaults.common$.logger = logger;

Example 2: The following example configures a module to support logging of ANALYSIS events, but defers the actual activation and deactivation of the logging until runtime. See the Diags_setMask() function for details on specifying the control string.
This is a part of the XDC configuration file for the application:
  var LogCtxChg = xdc.useModule('ti.uia.runtime.LogCtxChg');
  var Diags = xdc.useModule('xdc.runtime.Diags');
  var Mod = xdc.useModule('my.pkg.Mod');

  Mod.common$.diags_ANALYSIS = Diags.RUNTIME_OFF;
This is a part of the C code for the application:
  // turn on logging of ANALYSIS events in the module
  Diags_setMask("my.pkg.Mod+Z");

  // turn off logging of ANALYSIS events in the module
  Diags_setMask("my.pkg.Mod-Z");
 
typedef UIAThreadCtx_IsLoggingEnabledFxn
C synopsis target-domain
typedef Bool (*UIAThreadCtx_IsLoggingEnabledFxn)(Int);
 
 
config UIAThreadCtx_ENABLEMASK  // module-wide

Ctx Filter Enable Mask

C synopsis target-domain
extern const Bits16 UIAThreadCtx_ENABLEMASK;
 
DETAILS
configures which bit of the ti_uia_runtime_CtxFilter_gFlags is assigned to control context aware filtering for frame context changes. Must be configured with a value that is 2**SYNCID.
 
config UIAThreadCtx_SYNCID  // module-wide

Trace Synchronization ID

C synopsis target-domain
extern const Bits16 UIAThreadCtx_SYNCID;
 
DETAILS
configures the value to be written into the 4 bit context change type field used by the UIASync trace synchronization
 
config UIAThreadCtx_ctxChg  // module-wide

threadSwitch Context Change event

C synopsis target-domain
extern const Log_Event UIAThreadCtx_ctxChg;
 
VALUES
fmt — a constant string that describes the context change and provides a format specifier for newThreadId
newThreadId — an integer which uniquely identifies the new context
DETAILS
Used to log a thread switch Note that the previous thread Id is logged automatically by the ti_uia_runtime_LogCtxChg_thread API. If ti_uia_events_UIAThreadCtx_isLoggingEnabledFxn is not NULL it is called and its return value determines whether logging is enabled or not.
EXAMPLE
The following C code shows how to log a Thread Context Change event that identifies a new thread using a BIOS task switch hook function
  #include <ti/uia/runtime/LogCtxChg.h>
  ...
  Void  tskSwitchHook(Task_Handle hOldTask,Task_Handle hNewTask){
          LogCtxChg_thread("thread: new = 0x%x",(Int)hNewTask);
  }
This event prints the Log call site (%$F) and a format string (%$S) which is recursively formatted with any addition arguments. The following text is an example of what will be displayed for the event:
  "Thread Ctx Change at Line 123 in demo.c [Prev. thread ID=0x1234] New thread ID=0x1235"

 
config UIAThreadCtx_ctxChgWithFunc  // module-wide

threadSwitch Context Change event with prempted function and resumed function addresses

C synopsis target-domain
extern const Log_Event UIAThreadCtx_ctxChgWithFunc;
 
VALUES
fmt — a constant string that describes the context change and provides a format specifier for newThreadId
newThreadId — an integer which uniquely identifies the new context
oldFunc — the address of the function that was preempted
newFunc — the address of the function that is being resumed
DETAILS
Used to log a thread switch along with function info (preempted function and new function) Note that the previous thread Id is logged automatically by the ti_uia_runtime_LogCtxChg_threadAndFunc API. If ti_uia_events_UIAThreadCtx_isLoggingEnabledFxn is not NULL it is called and its return value determines whether logging is enabled or not.
EXAMPLE
The following C code shows how to log a Thread Context Change event that identifies a new thread, the preempted function and the preempting function.
  #include <ti/uia/runtime/LogCtxChg.h>
  ...
  LogCtxChg_threadAndFunc("New thread ID=0x%x, oldFunc=0x%x, newFunc=0x%x",(Int)hNewTask, (Int)&oldFunc,(Int)&newFunc);

This event prints the Log call site (%$F) and a format string (%$S) which is recursively formatted with any addition arguments. The following text is an example of what will be displayed for the event:
  "Thread CtxChgWithFunc at Line 123 in demo.c [Prev. thread ID=0x1234] New thread ID=0x1235, oldFunc=0x80001200, newFunc=0x80001080"

 
config UIAThreadCtx_isLoggingEnabledFxn  // module-wide
C synopsis target-domain
extern const IUIACtx_IsLoggingEnabledFxn UIAThreadCtx_isLoggingEnabledFxn;
 
 
UIAThreadCtx_getCtxId()  // module-wide

Get the ID for the current thread

C synopsis target-domain
UInt UIAThreadCtx_getCtxId();
 
RETURNS
returns the thread ID logged by the last call to UIAThreadCtx_logCtxChg.
 
UIAThreadCtx_getEnableOnValue()  // module-wide

Get the EnableOn value

C synopsis target-domain
UInt UIAThreadCtx_getEnableOnValue();
 
RETURNS
returns the thread ID value that logging will be enabled for.
 
UIAThreadCtx_isLoggingEnabled()  // module-wide

returns true if the new context matches the value to enable logging with

C synopsis target-domain
Bool UIAThreadCtx_isLoggingEnabled(UInt newThreadId);
 
ARGUMENTS
newThreadId — the new thread ID
DETAILS
Default implementation of the IUIACtx_IsLoggingEnabledFxn for user context. To enable context-aware filtering, in the .cfg script assign UIAThreadCtx_isLoggingEnabledFxn = '&UIAThreadCtx_isLoggingEnabled' or assign your own implementation of this function.
RETURNS
true if logging is enabled
 
UIAThreadCtx_setEnableOnValue()  // module-wide

Set the EnableOn value

C synopsis target-domain
Void UIAThreadCtx_setEnableOnValue(UInt value);
 
ARGUMENTS
value — the CtxId value that logging will be enabled for.
 
UIAThreadCtx_setOldValue()  // module-wide

sets ti_uia_events_UIAThreadCtx_gLastValue to the new value and returns the old value before it was updated

C synopsis target-domain
UInt UIAThreadCtx_setOldValue(UInt newValue);
 
ARGUMENTS
newValue — the new value to save in the global variable
(return0 the original value of the global variable before it was updated.
Module-Wide Built-Ins

C synopsis target-domain
Types_ModuleId UIAThreadCtx_Module_id();
// Get this module's unique id
 
Bool UIAThreadCtx_Module_startupDone();
// Test if this module has completed startup
 
IHeap_Handle UIAThreadCtx_Module_heap();
// The heap from which this module allocates memory
 
Bool UIAThreadCtx_Module_hasMask();
// Test whether this module has a diagnostics mask
 
Bits16 UIAThreadCtx_Module_getMask();
// Returns the diagnostics mask for this module
 
Void UIAThreadCtx_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
 
Configuration settings sourced in ti/uia/events/UIAThreadCtx.xdc
var UIAThreadCtx = xdc.useModule('ti.uia.events.UIAThreadCtx');
module-wide config parameters
        mask: Diags.ANALYSIS,
        msg: "Thread Ctx Change at %$F [Prev. thread ID = 0x%x] %$S"
    };
        mask: Diags.ANALYSIS,
        msg: "Thread CtxChgWithFunc at %$F [Prev. threadId = 0x%x] %$S"
    };
    UIAThreadCtx.isLoggingEnabledFxn//  = Bool(*)(Int) null;
 
 
 
config UIAThreadCtx.ENABLEMASK  // module-wide

Ctx Filter Enable Mask

Configuration settings
UIAThreadCtx.ENABLEMASK = Bits16 undefined;
 
DETAILS
configures which bit of the ti_uia_runtime_CtxFilter_gFlags is assigned to control context aware filtering for frame context changes. Must be configured with a value that is 2**SYNCID.
C SYNOPSIS
 
config UIAThreadCtx.SYNCID  // module-wide

Trace Synchronization ID

Configuration settings
UIAThreadCtx.SYNCID = Bits16 undefined;
 
DETAILS
configures the value to be written into the 4 bit context change type field used by the UIASync trace synchronization
C SYNOPSIS
 
config UIAThreadCtx.ctxChg  // module-wide

threadSwitch Context Change event

Configuration settings
UIAThreadCtx.ctxChg = Log.EventDesc {
    mask: Diags.ANALYSIS,
    msg: "Thread Ctx Change at %$F [Prev. thread ID = 0x%x] %$S"
};
 
VALUES
fmt — a constant string that describes the context change and provides a format specifier for newThreadId
newThreadId — an integer which uniquely identifies the new context
DETAILS
Used to log a thread switch Note that the previous thread Id is logged automatically by the ti_uia_runtime_LogCtxChg_thread API. If ti_uia_events_UIAThreadCtx_isLoggingEnabledFxn is not NULL it is called and its return value determines whether logging is enabled or not.
EXAMPLE
The following C code shows how to log a Thread Context Change event that identifies a new thread using a BIOS task switch hook function
  #include <ti/uia/runtime/LogCtxChg.h>
  ...
  Void  tskSwitchHook(Task_Handle hOldTask,Task_Handle hNewTask){
          LogCtxChg_thread("thread: new = 0x%x",(Int)hNewTask);
  }
This event prints the Log call site (%$F) and a format string (%$S) which is recursively formatted with any addition arguments. The following text is an example of what will be displayed for the event:
  "Thread Ctx Change at Line 123 in demo.c [Prev. thread ID=0x1234] New thread ID=0x1235"

C SYNOPSIS
 
config UIAThreadCtx.ctxChgWithFunc  // module-wide

threadSwitch Context Change event with prempted function and resumed function addresses

Configuration settings
UIAThreadCtx.ctxChgWithFunc = Log.EventDesc {
    mask: Diags.ANALYSIS,
    msg: "Thread CtxChgWithFunc at %$F [Prev. threadId = 0x%x] %$S"
};
 
VALUES
fmt — a constant string that describes the context change and provides a format specifier for newThreadId
newThreadId — an integer which uniquely identifies the new context
oldFunc — the address of the function that was preempted
newFunc — the address of the function that is being resumed
DETAILS
Used to log a thread switch along with function info (preempted function and new function) Note that the previous thread Id is logged automatically by the ti_uia_runtime_LogCtxChg_threadAndFunc API. If ti_uia_events_UIAThreadCtx_isLoggingEnabledFxn is not NULL it is called and its return value determines whether logging is enabled or not.
EXAMPLE
The following C code shows how to log a Thread Context Change event that identifies a new thread, the preempted function and the preempting function.
  #include <ti/uia/runtime/LogCtxChg.h>
  ...
  LogCtxChg_threadAndFunc("New thread ID=0x%x, oldFunc=0x%x, newFunc=0x%x",(Int)hNewTask, (Int)&oldFunc,(Int)&newFunc);

This event prints the Log call site (%$F) and a format string (%$S) which is recursively formatted with any addition arguments. The following text is an example of what will be displayed for the event:
  "Thread CtxChgWithFunc at Line 123 in demo.c [Prev. thread ID=0x1234] New thread ID=0x1235, oldFunc=0x80001200, newFunc=0x80001080"

C SYNOPSIS
 
config UIAThreadCtx.isLoggingEnabledFxn  // module-wide
Configuration settings
UIAThreadCtx.isLoggingEnabledFxn = Bool(*)(Int) null;
 
C SYNOPSIS
 
metaonly config UIAThreadCtx.common$  // module-wide

Common module configuration parameters

Configuration settings
UIAThreadCtx.common$ = Types.Common$ undefined;
 
DETAILS
All modules have this configuration parameter. Its name contains the '$' character to ensure it does not conflict with configuration parameters declared by the module. This allows new configuration parameters to be added in the future without any chance of breaking existing modules.
generated on Tue, 17 Oct 2017 18:21:08 GMT