module ti.uia.family.dm.TimestampDM816XTimer

Implementation of ITimestampProvider using DM General purpose 32b timer. NOTE: for ARM devices, address values should be virtual addresses as seen by the CPU

C synopsis target-domain sourced in ti/uia/family/dm/TimestampDM816XTimer.xdc
#include <ti/uia/family/dm/TimestampDM816XTimer.h>
Functions
Void 
Functions common to all ITimestampClient modules
Bits32 
Void 
Void 
Functions common to all target modules
Typedefs
typedef enum
typedef enum
typedef struct
typedef struct
typedef enum
typedef struct
typedef struct
typedef struct
Constants
extern const Bool 
extern const Types_FreqHz 
extern const Types_FreqHz 
extern const Ptr 
extern const Int 
extern const Ptr 
 
 
enum TimestampDM816XTimer_BaseAdrs

Enumeration that defines the base addresses for each timer instance of the DM8168 device

C synopsis target-domain
typedef enum TimestampDM816XTimer_BaseAdrs {
    TimestampDM816XTimer_BaseAdrs_ARM_Timer4,
    TimestampDM816XTimer_BaseAdrs_ARM_Timer5,
    TimestampDM816XTimer_BaseAdrs_ARM_Timer6,
    TimestampDM816XTimer_BaseAdrs_ARM_Timer7,
    TimestampDM816XTimer_BaseAdrs_C6000_Timer4,
    TimestampDM816XTimer_BaseAdrs_C6000_Timer5,
    TimestampDM816XTimer_BaseAdrs_C6000_Timer6,
    TimestampDM816XTimer_BaseAdrs_C6000_Timer7
} TimestampDM816XTimer_BaseAdrs;
 
 
enum TimestampDM816XTimer_PrcmClkMuxBaseAdrs

PRCM CM_TIMERX_CLKSEL Timer clock mux select line

C synopsis target-domain
typedef enum TimestampDM816XTimer_PrcmClkMuxBaseAdrs {
    TimestampDM816XTimer_PrcmClkMuxBaseAdrs_Timer4,
    TimestampDM816XTimer_PrcmClkMuxBaseAdrs_Timer5,
    TimestampDM816XTimer_PrcmClkMuxBaseAdrs_Timer6,
    TimestampDM816XTimer_PrcmClkMuxBaseAdrs_Timer7
} TimestampDM816XTimer_PrcmClkMuxBaseAdrs;
 
DETAILS
The following enum provides the physical addresses of the PRCM Clock Mux register used for Timers 4,5,6 and 7. If the virtual address of the register is not the same as the physical address, AND the autostart config option is true, the prcmClkMuxBaseAdrs must be configured with the virtual address of the register.
 
enum TimestampDM816XTimer_TimerInstance
C synopsis target-domain
typedef enum TimestampDM816XTimer_TimerInstance {
    TimestampDM816XTimer_TimerInstance_UserConfigured,
    TimestampDM816XTimer_TimerInstance_Timer4,
    TimestampDM816XTimer_TimerInstance_Timer5,
    TimestampDM816XTimer_TimerInstance_Timer6,
    TimestampDM816XTimer_TimerInstance_Timer7
} TimestampDM816XTimer_TimerInstance;
 
 
struct TimestampDM816XTimer_Tclr

Timer Control Register (TCLR)

C synopsis target-domain
typedef struct TimestampDM816XTimer_Tclr {
    Bits32 ptv;
    // Trigger output mode
    Bits8 pre;
    // Prescalar enable
    Bits8 ce;
    // Compare enable
    Bits8 scpwm;
    // Pulse-width modulation
    Bits16 tcm;
    // Transition capture mode
    Bits16 trg;
    // Trigger output mode
    Bits8 pt;
    // Pulse or toggle select bit
    Bits8 captmode;
    // Capture mode select bit
    Bits8 gpocfg;
    // PWM output/event detection input pin
} TimestampDM816XTimer_Tclr;
 
 
struct TimestampDM816XTimer_Tier

Timer IRQENABLE CLR (IRQENABLE_CLR)

C synopsis target-domain
typedef struct TimestampDM816XTimer_Tier {
    Bits8 mat_it_ena;
    // Enable match interrupt
    Bits8 ovf_it_ena;
    // Enable overflow interrupt
    Bits8 tcar_it_ena;
    // Enable capture interrupt
} TimestampDM816XTimer_Tier;
 
 
struct TimestampDM816XTimer_TiocpCfg

Timer OCP Configuration Register (TIOCP_CFG) - L4 interface Configuration

C synopsis target-domain
typedef struct TimestampDM816XTimer_TiocpCfg {
    Bits8 idlemode;
    // 0=force-idle;1=no-idle;2=Smart-idle;3=Smart-idle
    Bits8 emufree;
    // 0=counter frozen; 1=counter free-running
    Bits8 softreset;
    // 0=normal mode; 1=soft reset
} TimestampDM816XTimer_TiocpCfg;
 
 
struct TimestampDM816XTimer_Tsicr

L4 Interface Synchronization Control Register (TSICR)

C synopsis target-domain
typedef struct TimestampDM816XTimer_Tsicr {
    Bits8 sft;
    // Reset software functional registers
    Bits8 posted;
    // Posted mode selection
} TimestampDM816XTimer_Tsicr;
 
 
struct TimestampDM816XTimer_Twer

Timer IRQ WAKEUP ENABLE (IRQWAKEEN)

C synopsis target-domain
typedef struct TimestampDM816XTimer_Twer {
    Bits8 mat_wup_ena;
    // Enable match wake-up
    Bits8 ovf_wup_ena;
    // Enable overflow wake-up
    Bits8 tcar_wup_ena;
    // Enable capture wake-up
} TimestampDM816XTimer_Twer;
 
 
config TimestampDM816XTimer_autoStart  // module-wide

Controls whether the module initializes the timer or not

C synopsis target-domain
extern const Bool TimestampDM816XTimer_autoStart;
 
DETAILS
Must be set to true for one and only one CPU in the device
 
config TimestampDM816XTimer_maxBusClockFreq  // module-wide

The highest bus clock frequency used to drive the timer

C synopsis target-domain
extern const Types_FreqHz TimestampDM816XTimer_maxBusClockFreq;
 
DETAILS
The default ticks per second rate of the timer is calculated by dividing the timer's bus clock frequency by the cyclesPerTick config parameter.
The default ticks per second rate of the timer is calculated by dividing the timer's bus clock frequency by the cyclesPerTick config parameter.
RETURNS
the 32 MSBs of the highest bus clock frequency used to drive the timer.
 
config TimestampDM816XTimer_maxTimerClockFreq  // module-wide

The highest timer clock frequency

C synopsis target-domain
extern const Types_FreqHz TimestampDM816XTimer_maxTimerClockFreq;
 
DETAILS
The default ticks per second rate of the timer is calculated by dividing the timer's bus clock frequency by the cyclesPerTick config parameter.
The default ticks per second rate of the timer is calculated by dividing the timer's bus clock frequency by the cyclesPerTick config parameter.
RETURNS
the 32 LSBs of the highest timer clock frequency (i.e. ticksPerSecond).
 
config TimestampDM816XTimer_prcmClkMuxBaseAdrs  // module-wide

Base address of the PRCM register used to select the timer clock source

C synopsis target-domain
extern const Ptr TimestampDM816XTimer_prcmClkMuxBaseAdrs;
 
DETAILS
If the virtual address of the register is not the same as the physical address, AND the autostart config option is true, the prcmClkMuxBaseAdrs must be configured with the virtual address of the register. Otherwise set to null to allow module to automatically use the physical address for the specified timer.
 
config TimestampDM816XTimer_prcmClkMuxInitValue  // module-wide

Value to write into the prcmClkMux register in order to configure timer clock

C synopsis target-domain
extern const Int TimestampDM816XTimer_prcmClkMuxInitValue;
 
DETAILS
If autoStart is TRUE and prcmClkMuxBaseAdrs is not null OR timerNumber is set to a value other than UserConfigured the module will writh the prcmClkMuxInitValue into the PRCM clock mux register upon startup.
By default, the value written, sets CLKSEL to SYS_CLK (b24 = 0) and sets MODULEMODE to 2 (Module is enabled).
 
config TimestampDM816XTimer_tclr  // module-wide
C synopsis target-domain
extern const TimestampDM816XTimer_Tclr TimestampDM816XTimer_tclr;
 
 
config TimestampDM816XTimer_tier  // module-wide
C synopsis target-domain
extern const TimestampDM816XTimer_Tier TimestampDM816XTimer_tier;
 
 
config TimestampDM816XTimer_timerBaseAdrs  // module-wide

Base address of the timer to be used as the global timer

C synopsis target-domain
extern const Ptr TimestampDM816XTimer_timerBaseAdrs;
 
DETAILS
If the virtual address of the timer is not the same as the physical address, AND the autostart config option is true, the timerBaseAdrs must be configured with the virtual address of the timer. Otherwise set to null to allow module to automatically use the physical address for the specified timer.
 
config TimestampDM816XTimer_timerNumber  // module-wide

Number of the timer to use as the global timer

C synopsis target-domain
extern const TimestampDM816XTimer_TimerInstance TimestampDM816XTimer_timerNumber;
 
DETAILS
The global timer provides a common time reference for all CPUs. This configuration parameter specifies which timer to use as the global timer. All CPUs on the device must be configured to use the same timer as the global timer. Must be a value of TimerInstance_Timer4,5,6,7 or TimerInstance_UserConfigured. If configured as TimerInstance_UserConfigured, then the module's timerBaseAdrs must be configured with the timer's virtual address and the module's prcmClkMuxBaseAdrs must be configured with the PRCM clock mux register's virtual address. Note: Timers 0-2 are reserved for Linux. Timer 3 is reserved for the DSP.
 
config TimestampDM816XTimer_tiocpCfg  // module-wide
C synopsis target-domain
extern const TimestampDM816XTimer_TiocpCfg TimestampDM816XTimer_tiocpCfg;
 
 
config TimestampDM816XTimer_tsicr  // module-wide

Default value of tsicr to use when configuring the timer

C synopsis target-domain
extern const TimestampDM816XTimer_Tsicr TimestampDM816XTimer_tsicr;
 
DETAILS
Only used if autoStart is true
 
config TimestampDM816XTimer_twer  // module-wide
C synopsis target-domain
extern const TimestampDM816XTimer_Twer TimestampDM816XTimer_twer;
 
 
TimestampDM816XTimer_get32()  // module-wide

Return a 32-bit timestamp

C synopsis target-domain
Bits32 TimestampDM816XTimer_get32();
 
RETURNS
Returns a 32-bit timestamp value. Use getFreq to convert this value into units of real time.
Returns a 32-bit timestamp value. Use getFreq to convert this value into units of real time.
SEE
 
TimestampDM816XTimer_get64()  // module-wide

Return a 64-bit timestamp

C synopsis target-domain
Void TimestampDM816XTimer_get64(Types_Timestamp64 *result);
 
ARGUMENTS
result — pointer to 64-bit result
This parameter is a pointer to a structure representing a 64-bit wide timestamp value where the current timestamp is written.
If the underlying hardware does not support 64-bit resolution, the hi field of result is always set to 0; see xdc.runtime.Types.Timestamp64. So, it is possible for the lo field to wrap around without any change to the hi field. Use getFreq to convert this value into units of real time.
pointer to 64-bit result
This parameter is a pointer to a structure representing a 64-bit wide timestamp value where the current timestamp is written.
If the underlying hardware does not support 64-bit resolution, the hi field of result is always set to 0; see xdc.runtime.Types.Timestamp64. So, it is possible for the lo field to wrap around without any change to the hi field. Use getFreq to convert this value into units of real time.
SEE
 
TimestampDM816XTimer_getFreq()  // module-wide

Get the timestamp timer's frequency (in Hz)

C synopsis target-domain
Void TimestampDM816XTimer_getFreq(Types_FreqHz *freq);
 
ARGUMENTS
freq — pointer to a 64-bit result
This parameter is a pointer to a structure representing a 64-bit wide frequency value where the timer's frequency (in Hz) is written; see xdc.runtime.Types.FreqHz. This function provides a way of converting timestamp values into units of real time.
pointer to a 64-bit result
This parameter is a pointer to a structure representing a 64-bit wide frequency value where the timer's frequency (in Hz) is written; see xdc.runtime.Types.FreqHz. This function provides a way of converting timestamp values into units of real time.
SEE
 
TimestampDM816XTimer_setMSW()  // module-wide
C synopsis target-domain
Void TimestampDM816XTimer_setMSW(Int value);
 
Module-Wide Built-Ins

C synopsis target-domain
Types_ModuleId TimestampDM816XTimer_Module_id();
// Get this module's unique id
 
Bool TimestampDM816XTimer_Module_startupDone();
// Test if this module has completed startup
 
IHeap_Handle TimestampDM816XTimer_Module_heap();
// The heap from which this module allocates memory
 
Bool TimestampDM816XTimer_Module_hasMask();
// Test whether this module has a diagnostics mask
 
Bits16 TimestampDM816XTimer_Module_getMask();
// Returns the diagnostics mask for this module
 
Void TimestampDM816XTimer_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
 
Configuration settings sourced in ti/uia/family/dm/TimestampDM816XTimer.xdc
var TimestampDM816XTimer = xdc.useModule('ti.uia.family.dm.TimestampDM816XTimer');
module-wide constants & types
 
 
 
        obj.ptv// Trigger output mode = Bits32  ...
        obj.pre// Prescalar enable = Bits8  ...
        obj.ce// Compare enable = Bits8  ...
        obj.scpwm// Pulse-width modulation = Bits8  ...
        obj.tcm// Transition capture mode = Bits16  ...
        obj.trg// Trigger output mode = Bits16  ...
        obj.pt// Pulse or toggle select bit = Bits8  ...
        obj.captmode// Capture mode select bit = Bits8  ...
        obj.gpocfg// PWM output/event detection input pin = Bits8  ...
 
        obj.mat_it_ena// Enable match interrupt = Bits8  ...
        obj.ovf_it_ena// Enable overflow interrupt = Bits8  ...
        obj.tcar_it_ena// Enable capture interrupt = Bits8  ...
 
        obj.emufree// 0=counter frozen; 1=counter free-running = Bits8  ...
        obj.softreset// 0=normal mode; 1=soft reset = Bits8  ...
 
        obj.sft// Reset software functional registers = Bits8  ...
        obj.posted// Posted mode selection = Bits8  ...
 
        obj.mat_wup_ena// Enable match wake-up = Bits8  ...
        obj.ovf_wup_ena// Enable overflow wake-up = Bits8  ...
        obj.tcar_wup_ena// Enable capture wake-up = Bits8  ...
module-wide config parameters
        lo: 27000000,
        hi: 0
    };
        lo: 27000000,
        hi: 0
    };
        ptv: 0,
        pre: 0,
        ce: 0,
        scpwm: 0,
        tcm: 0,
        trg: 0,
        pt: 0,
        captmode: 0,
        gpocfg: 0
    };
        mat_it_ena: 0,
        ovf_it_ena: 1,
        tcar_it_ena: 0
    };
        idlemode: 0,
        emufree: 0,
        softreset: 1
    };
        sft: 0,
        posted: 1
    };
        mat_wup_ena: 0,
        ovf_wup_ena: 0,
        tcar_wup_ena: 0
    };
 
 
 
enum TimestampDM816XTimer.BaseAdrs

Enumeration that defines the base addresses for each timer instance of the DM8168 device

Configuration settings
values of type TimestampDM816XTimer.BaseAdrs
    const TimestampDM816XTimer.BaseAdrs_ARM_Timer4;
    const TimestampDM816XTimer.BaseAdrs_ARM_Timer5;
    const TimestampDM816XTimer.BaseAdrs_ARM_Timer6;
    const TimestampDM816XTimer.BaseAdrs_ARM_Timer7;
    const TimestampDM816XTimer.BaseAdrs_C6000_Timer4;
    const TimestampDM816XTimer.BaseAdrs_C6000_Timer5;
    const TimestampDM816XTimer.BaseAdrs_C6000_Timer6;
    const TimestampDM816XTimer.BaseAdrs_C6000_Timer7;
 
C SYNOPSIS
 
enum TimestampDM816XTimer.PrcmClkMuxBaseAdrs

PRCM CM_TIMERX_CLKSEL Timer clock mux select line

Configuration settings
values of type TimestampDM816XTimer.PrcmClkMuxBaseAdrs
    const TimestampDM816XTimer.PrcmClkMuxBaseAdrs_Timer4;
    const TimestampDM816XTimer.PrcmClkMuxBaseAdrs_Timer5;
    const TimestampDM816XTimer.PrcmClkMuxBaseAdrs_Timer6;
    const TimestampDM816XTimer.PrcmClkMuxBaseAdrs_Timer7;
 
DETAILS
The following enum provides the physical addresses of the PRCM Clock Mux register used for Timers 4,5,6 and 7. If the virtual address of the register is not the same as the physical address, AND the autostart config option is true, the prcmClkMuxBaseAdrs must be configured with the virtual address of the register.
C SYNOPSIS
 
enum TimestampDM816XTimer.TimerInstance
Configuration settings
values of type TimestampDM816XTimer.TimerInstance
    const TimestampDM816XTimer.TimerInstance_UserConfigured;
    const TimestampDM816XTimer.TimerInstance_Timer4;
    const TimestampDM816XTimer.TimerInstance_Timer5;
    const TimestampDM816XTimer.TimerInstance_Timer6;
    const TimestampDM816XTimer.TimerInstance_Timer7;
 
C SYNOPSIS
 
struct TimestampDM816XTimer.Tclr

Timer Control Register (TCLR)

Configuration settings
var obj = new TimestampDM816XTimer.Tclr;
 
    obj.ptv = Bits32  ...
    // Trigger output mode
    obj.pre = Bits8  ...
    // Prescalar enable
    obj.ce = Bits8  ...
    // Compare enable
    obj.scpwm = Bits8  ...
    // Pulse-width modulation
    obj.tcm = Bits16  ...
    // Transition capture mode
    obj.trg = Bits16  ...
    // Trigger output mode
    obj.pt = Bits8  ...
    // Pulse or toggle select bit
    obj.captmode = Bits8  ...
    // Capture mode select bit
    obj.gpocfg = Bits8  ...
    // PWM output/event detection input pin
 
C SYNOPSIS
 
struct TimestampDM816XTimer.Tier

Timer IRQENABLE CLR (IRQENABLE_CLR)

Configuration settings
var obj = new TimestampDM816XTimer.Tier;
 
    obj.mat_it_ena = Bits8  ...
    // Enable match interrupt
    obj.ovf_it_ena = Bits8  ...
    // Enable overflow interrupt
    obj.tcar_it_ena = Bits8  ...
    // Enable capture interrupt
 
C SYNOPSIS
 
struct TimestampDM816XTimer.TiocpCfg

Timer OCP Configuration Register (TIOCP_CFG) - L4 interface Configuration

Configuration settings
var obj = new TimestampDM816XTimer.TiocpCfg;
 
    obj.idlemode = Bits8  ...
    // 0=force-idle;1=no-idle;2=Smart-idle;3=Smart-idle
    obj.emufree = Bits8  ...
    // 0=counter frozen; 1=counter free-running
    obj.softreset = Bits8  ...
    // 0=normal mode; 1=soft reset
 
C SYNOPSIS
 
struct TimestampDM816XTimer.Tsicr

L4 Interface Synchronization Control Register (TSICR)

Configuration settings
var obj = new TimestampDM816XTimer.Tsicr;
 
    obj.sft = Bits8  ...
    // Reset software functional registers
    obj.posted = Bits8  ...
    // Posted mode selection
 
C SYNOPSIS
 
struct TimestampDM816XTimer.Twer

Timer IRQ WAKEUP ENABLE (IRQWAKEEN)

Configuration settings
var obj = new TimestampDM816XTimer.Twer;
 
    obj.mat_wup_ena = Bits8  ...
    // Enable match wake-up
    obj.ovf_wup_ena = Bits8  ...
    // Enable overflow wake-up
    obj.tcar_wup_ena = Bits8  ...
    // Enable capture wake-up
 
C SYNOPSIS
 
config TimestampDM816XTimer.autoStart  // module-wide

Controls whether the module initializes the timer or not

Configuration settings
TimestampDM816XTimer.autoStart = Bool false;
 
DETAILS
Must be set to true for one and only one CPU in the device
C SYNOPSIS
 
config TimestampDM816XTimer.maxBusClockFreq  // module-wide

The highest bus clock frequency used to drive the timer

Configuration settings
TimestampDM816XTimer.maxBusClockFreq = Types.FreqHz {
    lo: 27000000,
    hi: 0
};
 
DETAILS
The default ticks per second rate of the timer is calculated by dividing the timer's bus clock frequency by the cyclesPerTick config parameter.
The default ticks per second rate of the timer is calculated by dividing the timer's bus clock frequency by the cyclesPerTick config parameter.
RETURNS
the 32 MSBs of the highest bus clock frequency used to drive the timer.
C SYNOPSIS
 
config TimestampDM816XTimer.maxTimerClockFreq  // module-wide

The highest timer clock frequency

Configuration settings
TimestampDM816XTimer.maxTimerClockFreq = Types.FreqHz {
    lo: 27000000,
    hi: 0
};
 
DETAILS
The default ticks per second rate of the timer is calculated by dividing the timer's bus clock frequency by the cyclesPerTick config parameter.
The default ticks per second rate of the timer is calculated by dividing the timer's bus clock frequency by the cyclesPerTick config parameter.
RETURNS
the 32 LSBs of the highest timer clock frequency (i.e. ticksPerSecond).
C SYNOPSIS
 
config TimestampDM816XTimer.prcmClkMuxBaseAdrs  // module-wide

Base address of the PRCM register used to select the timer clock source

Configuration settings
TimestampDM816XTimer.prcmClkMuxBaseAdrs = Ptr null;
 
DETAILS
If the virtual address of the register is not the same as the physical address, AND the autostart config option is true, the prcmClkMuxBaseAdrs must be configured with the virtual address of the register. Otherwise set to null to allow module to automatically use the physical address for the specified timer.
C SYNOPSIS
 
config TimestampDM816XTimer.prcmClkMuxInitValue  // module-wide

Value to write into the prcmClkMux register in order to configure timer clock

Configuration settings
TimestampDM816XTimer.prcmClkMuxInitValue = Int 0x0000002;
 
DETAILS
If autoStart is TRUE and prcmClkMuxBaseAdrs is not null OR timerNumber is set to a value other than UserConfigured the module will writh the prcmClkMuxInitValue into the PRCM clock mux register upon startup.
By default, the value written, sets CLKSEL to SYS_CLK (b24 = 0) and sets MODULEMODE to 2 (Module is enabled).
C SYNOPSIS
 
config TimestampDM816XTimer.tclr  // module-wide
Configuration settings
TimestampDM816XTimer.tclr = TimestampDM816XTimer.Tclr {
    ptv: 0,
    pre: 0,
    ce: 0,
    scpwm: 0,
    tcm: 0,
    trg: 0,
    pt: 0,
    captmode: 0,
    gpocfg: 0
};
 
C SYNOPSIS
 
config TimestampDM816XTimer.tier  // module-wide
Configuration settings
TimestampDM816XTimer.tier = TimestampDM816XTimer.Tier {
    mat_it_ena: 0,
    ovf_it_ena: 1,
    tcar_it_ena: 0
};
 
C SYNOPSIS
 
config TimestampDM816XTimer.timerBaseAdrs  // module-wide

Base address of the timer to be used as the global timer

Configuration settings
TimestampDM816XTimer.timerBaseAdrs = Ptr null;
 
DETAILS
If the virtual address of the timer is not the same as the physical address, AND the autostart config option is true, the timerBaseAdrs must be configured with the virtual address of the timer. Otherwise set to null to allow module to automatically use the physical address for the specified timer.
C SYNOPSIS
 
config TimestampDM816XTimer.timerNumber  // module-wide

Number of the timer to use as the global timer

Configuration settings
 
DETAILS
The global timer provides a common time reference for all CPUs. This configuration parameter specifies which timer to use as the global timer. All CPUs on the device must be configured to use the same timer as the global timer. Must be a value of TimerInstance_Timer4,5,6,7 or TimerInstance_UserConfigured. If configured as TimerInstance_UserConfigured, then the module's timerBaseAdrs must be configured with the timer's virtual address and the module's prcmClkMuxBaseAdrs must be configured with the PRCM clock mux register's virtual address. Note: Timers 0-2 are reserved for Linux. Timer 3 is reserved for the DSP.
C SYNOPSIS
 
config TimestampDM816XTimer.tiocpCfg  // module-wide
Configuration settings
TimestampDM816XTimer.tiocpCfg = TimestampDM816XTimer.TiocpCfg {
    idlemode: 0,
    emufree: 0,
    softreset: 1
};
 
C SYNOPSIS
 
config TimestampDM816XTimer.tsicr  // module-wide

Default value of tsicr to use when configuring the timer

Configuration settings
TimestampDM816XTimer.tsicr = TimestampDM816XTimer.Tsicr {
    sft: 0,
    posted: 1
};
 
DETAILS
Only used if autoStart is true
C SYNOPSIS
 
config TimestampDM816XTimer.twer  // module-wide
Configuration settings
TimestampDM816XTimer.twer = TimestampDM816XTimer.Twer {
    mat_wup_ena: 0,
    ovf_wup_ena: 0,
    tcar_wup_ena: 0
};
 
C SYNOPSIS
 
metaonly config TimestampDM816XTimer.canCpuCyclesPerTickBeChanged  // module-wide

Indicates whether the timer's cycles per tick divide down ratio can be changed or not

Configuration settings
TimestampDM816XTimer.canCpuCyclesPerTickBeChanged = Bool false;
 
RETURNS
true if the timer's CPU cycles per tick can be changed
true if the timer's CPU cycles per tick can be changed
 
metaonly config TimestampDM816XTimer.canFrequencyBeChanged  // module-wide

Indicates whether the timer frequency can be changed or not

Configuration settings
TimestampDM816XTimer.canFrequencyBeChanged = Bool false;
 
RETURNS
true if the timer's clock frequency can be changed
true if the timer's clock frequency can be changed
 
metaonly config TimestampDM816XTimer.common$  // module-wide

Common module configuration parameters

Configuration settings
TimestampDM816XTimer.common$ = Types.Common$ undefined;
 
DETAILS
All modules have this configuration parameter. Its name contains the '$' character to ensure it does not conflict with configuration parameters declared by the module. This allows new configuration parameters to be added in the future without any chance of breaking existing modules.
 
metaonly config TimestampDM816XTimer.cpuCyclesPerTick  // module-wide

The number of CPU cycles each tick of the timestamp corresponds to

Configuration settings
TimestampDM816XTimer.cpuCyclesPerTick = UInt32 0;
 
DETAILS
A value of 0 indicates that no conversion between the timer's tick count and CPU cycles is possible.
A value of 0 indicates that no conversion between the timer's tick count and CPU cycles is possible.
generated on Tue, 17 Oct 2017 18:21:12 GMT