This general purpose logger is useful in situations where a very small
memory overhead is required
The logger stores all events in a single buffer with a compact
UIAPacket event packet structure that allows them to be sent directly
to System Analyzer via JTAG.
LoggerMin was designed to have as minimal impact as possible on an
application when calling a Log function. There are several configuration
parameters that allow an application to get the optimal performance in
exchange for certain restrictions.
Interrupts are disabled during the duration of the log call.
The following XDC configuration statements
create a logger module, and assign it as the default logger for all
modules.
The following XDC configuration statements show how to use LoggingSetup
with LoggerMin.
| enum LoggerMin_TimestampSize |
 |
Enum of size of timestamps to log with events
typedef enum LoggerMin_TimestampSize {
LoggerMin_TimestampSize_NONE,
// No timestamps will be logged with events
LoggerMin_TimestampSize_32b,
// 32-bit timestamp
LoggerMin_TimestampSize_64b
// 64-bit timestamp
} LoggerMin_TimestampSize;
| config LoggerMin_bufSize // module-wide |
 |
LoggerMin buffer size in MAUs (Minimum Addressable Units e.g.
Bytes)
extern const SizeT LoggerMin_bufSize;
DETAILS
The buffer size must be less than 65536 bytes.
NOTE: the buffer size must contain an integer number of 32-bit words
(e.g. if a MAU = 1 byte, then the buffer size must be a multiple of 4).
The buffer size must also be at least maxEventSize + 64.
| config LoggerMin_supportLoggerDisable // module-wide |
 |
Allow Logger instances to be enabled/disabled during runtime
extern const Bool LoggerMin_supportLoggerDisable;
DETAILS
LoggerMin footprint is smaller when supportLoggerDisable is
false.
| config LoggerMin_timestampSize // module-wide |
 |
Configure the size of the timestamp to use.
For minimum event footprint, configure as TimestampSize_32b (default)
DETAILS
Having a timestamp allows an instrumentation host (e.g.
System Analyzer) to display events with the correct system time.
| Module-Wide Built-Ins |
 |
// Get this module's unique id
Bool LoggerMin_Module_startupDone();
// Test if this module has completed startup
// The heap from which this module allocates memory
Bool LoggerMin_Module_hasMask();
// Test whether this module has a diagnostics mask
Bits16 LoggerMin_Module_getMask();
// Returns the diagnostics mask for this module
Void LoggerMin_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
| Instance Object Types |
 |
typedef struct LoggerMin_Object LoggerMin_Object;
// Opaque internal representation of an instance object
// Client reference to an instance object
typedef struct LoggerMin_Struct LoggerMin_Struct;
// Opaque client structure large enough to hold an instance object
// Convert this instance structure pointer into an instance handle
// Convert this instance handle into an instance structure pointer
| Instance Config Parameters |
 |
typedef struct LoggerMin_Params {
// Instance config-params structure
// Common per-instance configs
} LoggerMin_Params;
// Initialize this config-params structure with supplier-specified defaults before instance creation
| Runtime Instance Creation |
 |
// Allocate and initialize a new instance object and return its handle
// Initialize a new instance object inside the provided structure
ARGUMENTS
params
per-instance config params, or NULL to select default values (target-domain only)
eb
active error-handling block, or NULL to select default policy (target-domain only)
| Instance Deletion |
 |
// Finalize and free this previously allocated instance object, setting the referenced handle to NULL
// Finalize the instance object inside the provided structure
| LoggerMin_disable() // instance |
 |
Disable a log
ARGUMENTS
handle
handle of a previously-created LoggerMin instance object
DETAILS
Events written to a disabled log are silently discarded.
RETURNS
The function returns the state of the log (TRUE if enabled,
FALSE if disabled) before the call. This return value allows
clients to restore the previous state.
Note: not thread safe.
| LoggerMin_enable() // instance |
 |
Enable a log
ARGUMENTS
handle
handle of a previously-created LoggerMin instance object
RETURNS
The function returns the state of the log (TRUE if enabled,
FALSE if disabled) before the call. This return value allows
clients to restore the previous state.
Note: not thread safe.
| LoggerMin_write0() // instance |
 |
Process a log event with 0 arguments
ARGUMENTS
handle
handle of a previously-created LoggerMin instance object
DETAILS
Same as write4 except with 0 arguments rather than 4.
SEE
| LoggerMin_write1() // instance |
 |
Process a log event with 1 argument
ARGUMENTS
handle
handle of a previously-created LoggerMin instance object
DETAILS
Same as write4 except with 1 arguments rather than 4.
SEE
| LoggerMin_write2() // instance |
 |
Process a log event with 2 arguments
ARGUMENTS
handle
handle of a previously-created LoggerMin instance object
DETAILS
Same as write4 except with 2 arguments rather than 4.
SEE
| LoggerMin_write4() // instance |
 |
Process a log event with 4 arguments
ARGUMENTS
handle
handle of a previously-created LoggerMin instance object
evt
event to be logged
mid
module ID of the module which logged the event
a1
arbitrary argument passed by caller
DETAILS
The
evt argument is of type Log.Event, which encodes the
Log.EventId, the
Diags.Mask, and the
Diags.EventLevel of the event. The event ID can be obtained
via
Types.getEventId(evt), the Diags mask can be obtained via
Diags.getMask(evt), and the event level can be obtained via
Diags.getLevel(evt).
The modId argument is the module ID of the module that logged the
event.
The event information can be used by the logger to handle different
events specially. For example, the event ID can be used to compare
against other known Log.Events.
if (Log_getEventId(MY_EVENT) == Log_getEventId(evt)) {
:
}
The Diags mask and event level can be used for filtering of events
based on event level (see
IFilterLogger), or even routing
events to separate loggers based on diags category (see, for example,
LoggerBuf.statusLogger).
The Diags mask and event level are useful for handling the event, but
are generally not recorded by the logger because they are not needed in
decoding and displaying the event. A more suitable value to record is a
Types.Event, which encodes the event ID and module ID. For
example, the
Log.EventRec type stores a
Types.Event
in its record definition. A
Types.Event can be created using
the
Types.makeEvent API given the event ID and module ID.
The event ID value of
0 is used to indicate an event triggered by a
call to one of the
Log_print[0-6] methods. These
methods take a format string rather than a
Log_Event argument and,
as a result, the event ID encoded in
evt is
0 and the parameter
a1 is the format string.
Non-zero event IDs can also be used to access the
msg string
associated with the
Log.EventDesc that originally
defined the
Log event.
Log_EventId id = Log_getEventId(evt));
if (id != 0) {
String msg = Text_ropeText(id);
System_aprintf(msg, a1, a2, a3, a4);
}
This works because an event's ID is simply an offset into a table
of characters (maintained by the
Text module)
containing the event's msg string.
The arguments a1, a2, etc. are parameters that are to be interpreted
according to the message format string associated with evt.
SEE
| LoggerMin_write8() // instance |
 |
Process a log event with 8 arguments
Void LoggerMin_write8(
LoggerMin_Handle handle,
Log_Event evt,
Types_ModuleId mid,
IArg a1,
IArg a2,
IArg a3,
IArg a4,
IArg a5,
IArg a6,
IArg a7,
IArg a8);
ARGUMENTS
handle
handle of a previously-created LoggerMin instance object
DETAILS
Same as write4 except with 8 arguments rather than 4.
SEE
| Instance Convertors |
 |
// unconditionally move one level up the inheritance hierarchy
// conditionally move one level down the inheritance hierarchy; NULL upon failure
| Instance Built-Ins |
 |
Int LoggerMin_Object_count();
// The number of statically-created instance objects
// The handle of the i-th statically-created instance object (array == NULL)
// The handle of the first dynamically-created instance object, or NULL
// The handle of the next dynamically-created instance object, or NULL
// The heap used to allocate dynamically-created instance objects
// The label associated with this instance object
// The name of this instance object
| enum LoggerMin.TimestampSize |
 |
Enum of size of timestamps to log with events
values of type LoggerMin.TimestampSize
const LoggerMin.TimestampSize_NONE;
// No timestamps will be logged with events
const LoggerMin.TimestampSize_32b;
// 32-bit timestamp
const LoggerMin.TimestampSize_64b;
// 64-bit timestamp
C SYNOPSIS
| metaonly struct LoggerMin.RecordView |
 |
var obj = new LoggerMin.RecordView;
obj.sequence = Int ...
obj.timestampRaw = Long ...
obj.modName = String ...
obj.text = String ...
obj.eventId = Int ...
obj.eventName = String ...
obj.arg0 = IArg ...
obj.arg1 = IArg ...
obj.arg2 = IArg ...
obj.arg3 = IArg ...
obj.arg4 = IArg ...
obj.arg5 = IArg ...
obj.arg6 = IArg ...
obj.arg7 = IArg ...
| metaonly struct LoggerMin.RtaData |
 |
Data added to the RTA MetaData file to support System Analyzer
var obj = new LoggerMin.RtaData;
obj.instanceId = Int ...
| config LoggerMin.bufSize // module-wide |
 |
LoggerMin buffer size in MAUs (Minimum Addressable Units e.g.
Bytes)
LoggerMin.bufSize = SizeT 512;
DETAILS
The buffer size must be less than 65536 bytes.
NOTE: the buffer size must contain an integer number of 32-bit words
(e.g. if a MAU = 1 byte, then the buffer size must be a multiple of 4).
The buffer size must also be at least maxEventSize + 64.
C SYNOPSIS
| config LoggerMin.supportLoggerDisable // module-wide |
 |
Allow Logger instances to be enabled/disabled during runtime
LoggerMin.supportLoggerDisable = Bool false;
DETAILS
LoggerMin footprint is smaller when supportLoggerDisable is
false.
C SYNOPSIS
| config LoggerMin.timestampSize // module-wide |
 |
Configure the size of the timestamp to use.
For minimum event footprint, configure as TimestampSize_32b (default)
DETAILS
Having a timestamp allows an instrumentation host (e.g.
System Analyzer) to display events with the correct system time.
C SYNOPSIS
| metaonly config LoggerMin.bufSection // module-wide |
 |
Section name for the buffer managed by the static instance
LoggerMin.bufSection = String null;
DETAILS
The default section is the 'dataMemory' in the platform.
| metaonly config LoggerMin.common$ // module-wide |
 |
Common module configuration parameters
DETAILS
All modules have this configuration parameter. Its name
contains the '$' character to ensure it does not conflict with
configuration parameters declared by the module. This allows
new configuration parameters to be added in the future without
any chance of breaking existing modules.
| metaonly config LoggerMin.memoryAlignmentInMAUs // module-wide |
 |
Memory Alignment in MAUs (Minimum Addressable Units)
LoggerMin.memoryAlignmentInMAUs = Int 1;
DETAILS
Specifies alignment to use when allocating the internal packet buffer
Set to 1 if no alignment is required.
| metaonly LoggerMin.getMetaArgs() // module-wide |
 |
Returns any meta data needed to support RTA
LoggerMin.getMetaArgs(Any inst, Any instNum) returns Any
DETAILS
This meta data should be returned in the form of a structure which
can be converted into XML. This data is added to the RTA XML file
during the application's configuration, and can be accessed later
through the xdc.rta.MetaData module.
The MetaData is returned per instance of the ILogger module. The
instance object is passed to the function as the first argument.
The second argument is the index of the instance in the list of
the ILogger's static instances.
| Instance Config Parameters |
 |
var params = new LoggerMin.Params;
// Instance config-params object
| Static Instance Creation |
 |
var params =
new LoggerMin.
Params;
// Allocate instance config-params
params.config = ...
// Assign individual configs
var inst = LoggerMin.create(params);
// Create an instance-object
ARGUMENTS
params
per-instance config params, or NULL to select default values (target-domain only)
eb
active error-handling block, or NULL to select default policy (target-domain only)